Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
mPPE-Slide14

Design engineers need not be faced with the ultimatum of having to choose between space savings and reliability when using mPPE insulation in their equipment components. Its innovative design allows for the smaller diameters without sacrificing performance of the product. As seen with Alpha Wire’s introduction of EcoWire® Plus, mPPE insulation can be formulated to offer additional benefits such as superior fluid resistance. Such benefits prove beneficial when components are used in cleanroom environments. Another AlphaWire benefit is one that has not been touched upon yet, but provides significant advantages for use within semiconductor manufacturing equipment. mPPE insulation offers strong outgassing benefits; up to 91% lower outgassing than PVC, which is crucial for these applications. From wafer fabrication and processing equipment to semiconductor packaging equipment, mPPE insulated wire and cable can easily find its place.

PTM Published on: 2013-05-08