mPPE insulation also provides significant benefits in the semiconductor manufacturing industry. Because this is such a booming industry in regards to advancing technology, there is no room for downtime. There are several ways that mPPE can keep the user’s equipment running smoothly. As quickly as smartphones and tablets are being introduced, the need for smaller semiconductor chips and technologies grows even faster. Manufacturing equipment needs to increase in complexity in order to keep up with the technological advances. As the complexity increases it is necessary for the components within to shrink and allow room for advancement. It is also imperative that such components are reliable in order to minimize downtime, and it is clear that engineers are hesitant to swap components that could sacrifice performance when reliability is on the line. Similarly, tough cleanroom environment regulations make it difficult to find suitable replacements that adhere to the manufacturing guidelines. What semiconductor manufacturing equipment needs today is a regulatory approved product that can offer fluid and abrasion resistance. The good news is, this is an application where mPPE insulation excels once again.