Ti450 Infrared Camera with MultiSharp™ Focus

Fluke offers its Ti450 thermal imager with MultiSharp™ focus that delivers focus near and far in one image

Image of Fluke's Ti450 Infrared Camera with MultiSharp™ FocusFluke's Ti450 brings 640 x 480 SuperResolution to the awarding winning Ti400 form factor. Now even more detail can be seen with 4x the pixel data. SuperResolution captures multiple images and combines them to create a 640 x 480 image.

Focus is one of the most important aspects of thermography and an out of focus image can give data that can lead to misdiagnosis, costing thousands. With the Fluke Ti450, worrying about focus is now obsolete. With MultiSharp™ focus, images are automatically focused throughout the field of view, even if the user started with a completely blurry target. That is because the camera takes multiple images and combines them to give a clear, accurate focus on targets near and far. Simply point and shoot.

With the push of a button, a built-in laser distance meter instantly calculates and displays the distance to the designated target. The focus engine immediately adjusts the focus.

Images can be wirelessly synced directly from a camera to the Fluke Connect® system, and attach to an asset record or work order. Having access to maintenance records simultaneously at the inspection site and from the office or an off-site location enables faster decision making and real time collaboration between team members. The camera display can be streamed live to a smartphone or PC and remotely control the camera. Infrared lenses can make it possible to inspect targets that would be challenging to see with a standard IR lens due to their size and distance. The Ti450 is compatible with 2x and 4x telephoto and wide angle lenses.

View Associated Lenses and Accessories

Features
  • Capture a clear, accurate image focused throughout the field of view with MultiSharp™ focus. Simply point and shoot and the camera, automatically processes a stack of images focused near and far
  • Get an instant in-focus image of a designated target. LaserSharp® auto focus, exclusive to Fluke uses a built-in laser distance meter that calculates and displays the distance from the designated target with pinpoint accuracy
  • Get 4x the pixels with SuperResolution, which captures multiple images and combines them to create a 640 x 480 image
  • Save time by wirelessly syncing images directly from the camera to the Fluke Connect® system and attached to an asset record or work order
  • Get the context of the visual and infrared details all in one precisely blended or picture-in-picture image with IR-Fusion® technology
  • Monitor processes with video recording, video streaming, and remote control
  • See the details needed with interchangeable smart lenses, 2x and 4x telephoto and wide angle. No calibration required

Ti450 Infrared Camera with MultiSharp Focus

ImageManufacturer Part NumberDescriptionAvailable QuantityPriceView Details
THERMAL IMAGER; 320X240; 60 HZ MFLK-TI450 60HZTHERMAL IMAGER; 320X240; 60 HZ M0 - ImmediateSee Page for PricingView Details
Published: 2016-05-23