RICHTEK
RICHTEK
RT8239A/B/C
18
DS8239A/B/C-06 October 2012www.richtek.com
©
Copyright 2012 Richtek Technology Corporation. All rights reserved. is a registered trademark of Richtek Technology Corporation.
IL
t
IPEAK
ILOAD
ILIMIT
Figure 4. “Valley” Current Limit
The RT8239A/B/C uses the on resistance of the
synchronous rectifier as the current sense element and
supports temperature compensated MOSFET RDS(ON)
sensing. The RILIM resistor between the ENTRIPx pin and
ultrasonic controller pulls LGATEx high and turns on the
low side MOSFET to induce a negative inductor current.
After the output voltage falls below the reference voltage,
the controller turns off the low side MOSFET (LGATEx
pulled low) and triggers a constant on-time (UGATEx driven
high). When the on-time has expired, the controller re-
enables the low side MOSFET until the controller detects
that the inductor current dropped below the zero crossing
threshold.
Linear Regulators (LDOx)
The RT8239A/B/C includes 5V (LDO5) and 3.3V (LDO3)
linear regulators. The regulators can supply up to 100mA
for external loads. Bypass LDOx with a minimum 4.7μF
ceramic capacitor. When VOUT1 is higher than the switch
over threshold (4.66V), an internal 1.5Ω P-MOSFET switch
connects BYP1 to the LDO5 pin while simultaneously
disconnects the internal linear regulator.
Current Limit Setting (ENTRIPx)
The RT8239A/B/C has cycle-by-cycle current limit control.
The current limit circuit employs a unique “valley” current
sensing algorithm. If the magnitude of the current sense
signal at PHASEx is above the current limit threshold,
the PWM is not allowed to initiate a new cycle (Figure 4).
The actual peak current is greater than the current limit
threshold by an amount equal to the inductor ripple current.
Therefore, the exact current limit characteristic and
maximum load capability are a function of the sense
resistance, inductor value, and battery and output voltage.
GND sets the current limit threshold. The resistor, RILIM,
is connected to a current source from ENTRIPx which is
10μA (typ.) at room temperature. The current source has
a 4700ppm/°C temperature slope to compensate the
temperature dependency of the RDS(ON). When the voltage
drop across the sense resistor or low side MOSFET
equals 1/10 the voltage across the RILIM resistor, positive
current limit will be activated. The high side MOSFET will
not be turned on until the voltage drop across the MOSFET
falls below 1/10 the voltage across the RILIM resistor.
Choose a current limit resistor according to the following
equation :
VILIM = (RILIM x 10μA) / 10 = IILIM x RDS(ON)
RILIM = (IILIM x RDS(ON)) x 10 / 10μA
Carefully observe the PC board layout guidelines to ensure
that noise and DC errors do not corrupt the current sense
signal at PHASEx and GND. Mount or place the IC close
to the low side MOSFET.
Charge Pump (SECFB)
The external 14V charge pump is driven by LGATEx. When
LGATEx is low, C1 will be charged by VOUT1 through D1.
C1 voltage is equal to VOUT1 minus the diode drop. When
LGATEx becomes high, C1 transfers the charge to C2
through D2 and charges C2 voltage to VLGATEX plus C1
voltage. As LGATEx transitions low on the next cycle, C3
is charged to C2 voltage minus a diode drop through D3.
Finally, C3 charges C4 through D4 when LGATEx switches
high. Thus, the total charge pump voltage, VCP, is :
VCP = VOUT1 + 2 x VLGATEx − 4 x VD
where VLGATEx is the peak voltage of the LGATEx driver
which is equal to LDO5 and VD is the forward voltage
dropped across the Schottky diode.
The SECFB pin in the RT8239B/C is used to monitor the
charge pump via a resistive voltage divider to generate
approximately 14V DC voltage and the clock driver uses
VOUT1 as its power supply. In the event where SECFB
drops below its feedback threshold, an ultrasonic pulse
will occur to refresh the charge pump driven by LGATEx.
If there's an overload on the charge pump in which SECFB
can not reach more than its feedback threshold, the