In summary, SSD endurance is not something that users should fear. With a little bit of research and workload analysis, users should feel confident that the SSD they select will perform well over the lifetime of their system. The SSD choices available allow a user to not overspend on endurance they do not need or underspend on an SSD that may wear out prematurely. It is best practice to purchase SSDs from reputable manufacturers and understanding the workload going into an SSD purchase. This will allow the customer to make the best SSD selection for the environment while knowing there is excellent product support from the manufacturer if needed.