Scheme-it Frequently Asked Questions


Where can I find complete tutorials on this?

Click on help in the upper right corner then click help page, and there will be videos and other documentation.

How to download the circuit I have designed?

On the main task bar, at the top of the screen click "export", you can then format it and save it to your desired location.

How do I assign pin numbers to an IC?

If you select the IC, you would need to create a text box to assign pin numbers. If you make custom IC’s using custom symbols then you can name the pins you create on them by clicking on them and editing them.

When I share a link to the schematic I’ve made, it has to be public. Does this mean that anyone can see my schematic, is there a possibility for me to share my schematic?

Only people with the link can view the schematic you created. You can use the share option on the top menu bar. Once you select it you can email another person the link directly so they can access it at a later time.

If it is a private schematic, can it still be viewed by others?

Yes, if you send them the link.

How do I share my schematic?

On the top task bar, select [Share]. Then save your project. Once you have saved the project, click on [Share] again on the task bar. From here you can select this project to be public or private, also note the options available to send a link directly to someone or send it via email, then click [Close].

1. Click [Share] on the task bar
2. Save your project
3. Select whether you want public or private and click close

How to create a title block?

Use the basic Rectangle shape in Diagram Symbols > Basic Shapes, and use the Label item in the same category.

How do I add a text box to my schematic design?

Click “insert” on the top menu bar, and then select “text box” and it will appear on your screen.

How do I change size of text / font?

After you click on the text box or symbol, then in the upper right of the screen, the Font Properties will appear. Under [Basic style] are the options for font size, which are the box's labeled "Tt and tT". "Tt" will make the font smaller each time you click "Tt". To make the font larger, click "tT", this will make the font size larger each time you click "tT".

1. Click on the textbox and go to Font Properties on the right
2. Click on the tT on the right and your text will get Bigger

I'm unable to create text that is vertical rather than horizontal, is there a way to do it?

No option for vertical text in Scheme-it. Possible option would be to create a text box by clicking [Insert] on the top task bar and selecting [Textbox]. Press and hold [Shift], and while holding [Shift], press [Enter] to make it drop down to the next line.

1. Click [Insert] on the task bar
2. Click [Textbox]
3. Press and hold Shift then press Enter

I cannot copy a part on my schematic

Right click on the part select copy, then paste. You may also hold ctrl + C.

How can I download Scheme-it?

Scheme-it is free to use in any customer’s browser and can be accessed easily from Digi-Key’s website. Unfortunately the program cannot be downloaded for use offline; it runs in an Internet-enabled browser off of our servers.

I am using your schematics drawing app. Save as is not working, do you know why?

Check to make sure that you are signed into our site, and depending on the size, there is a limit to how much can be saved.

How can I export (pdf) with the gridlines?

You cannot export them to a pdf, the gridlines will always disappear.

I am using Scheme-it and trying to export a schematic to a PDF.

On the top menu bar select export, then click on Document (PDF). From there you can select if you want the current page or all of the pages, the orientation, and the paper size.

How do I export a schematic?

On the top task bar select [Export]. Then select the appropriate file type to export the schematic.

1. Click [Export] on the task bar
2. Select the type of file you want to export it as
3. Save the file of the schematic

How do I delete a schematic?

You cannot delete an open project. On the top task bar, select [Open]. You will see the list of saved projects. To the right of the project name is a column [Delete] with a trash can next to each project. Click on the trash can next to the project to be deleted and then type DELETE in the provided prompt and click [Ok].

1. Click [Open] on the task bar
2. Click on the trashcan next to the project you want to delete
3. Type DELETE in the box and click ok

How to save a project?

On the top menu bar select save or save as. You must be signed into your Digi-Key account.

I'm wondering how to add notes to a schematic?

On the top menu bar select insert, then text box. This will allow you to add notes.

I'm trying to label individual circuit lines.

There is not an option to label a line, you will need to insert a text box and drop the text box next to the line you wish to label. You can also go to Diagram Symbols, to Basic Shapes, and select label. This makes a text box directly.

How can I get my files back?

There is no way to get the file back once it is deleted.

How do I insert an image into my schematic?

Click [Insert] on the top task bar. Select [Image] from the dropdown and enter the valid form of URL such as .png, .jpg, or a .jpeg. The symbol will appear on your schematic.

1. Click [Insert] on the task bar
2. Select Image
3. Enter a valid file or link in the box and select link

How do I write a name next to a symbol?

Click insert on the top menu bar and select text box then put the text box next to it.

Can you tell me how to rename a schematic?

Once you are logged into your account you can select "save as" and rename the file.

The only option I have is "Import BOM" on the left hand side. There is no list of the symbols or any other categories, how do I get them back?

If a part number was searched and the searched part was not cleared, by selecting the double X’s in the search box to clear the inquiry, the full list of symbols will not appear again until the search is cleared. Make sure that you click on both of the X’s, otherwise the categories will not reappear. If you use backspace to delete the part searched, you can click the search icon and they will reappear.

1. Click on the X on the left first.
2. Once you have clicked on both X’s Click Search icon

Is there a way to export the file from the Scheme-it to a MS Visio format?

Scheme-it does not have an option for MS Visio format.

Is there a way I can import a symbol?

On the top menu bar select import, then select image and add your link.

How do you save a project, and why is Scheme-it is not allowing me to save projects?

On the top menu bar select [save] or [save as] to save your project. Make sure that you are logged into your account before trying to save! If the problem persists please send an email to webmaster@digikey.com. There is also a size limitation to how much can be saved at once.

How can I open a .vsd file sent by a colleague?

Scheme-it is unable to find your colleague's project in whatever location it's in, and you'll need to move it to the same folder as your older projects.

I am using Scheme-it and trying to export a schematic to a PDF, is there an option for CAD?

On the top menu bar select [export], and then click on Document (PDF). From there you can select if you want the current page or all of the pages, the orientation, and the paper size. Scheme-it is unable to export to CAD, can only export to .png, .svg, pdf, or an SCHBOM file.

How can I import my BOM?

You must log into your Digi-Key account before you import a BOM; it will not work if you are not logged in. Once logged in, go through the steps to import by clicking Import BOM on the left hand side. Also make sure that you do not have multiple files of the BOM open. If you encounter problems try to refresh the page.

I am trying to print, but the image is too small, how can I make it larger? If they are too small is there a way that I can only print part of my schematic?

Click on the Export function in the top bar, you should be able to export the schematic as a PDF.  Doing this, you can select "Active Area" in the "Export Area" drop-down menu, which constricts the PDF to just the area of the tool you've used; printing from that PDF, rather than from Scheme-it directly. You can also select from the preferences tab to “fit to one page”. If not all the parts print, it is because there is a size limitation to how much you can print. If there is an issue with that try printing the schematic in multiple pages.

I can’t get it to fill the page, it is very tiny.

You will need to use the zoom in and out features to get your schematic to the proper size, next to the minus symbol there is a magnifying glass with a square in it, click on it and it will zoom in to a normal size.

Can I import an image or a symbol into Scheme-it?

On the top menu bar select “insert”, then “image”, from there you will have to enter a valid URL ( .png, .jpg, .jpeg ): in order to link it to your schematic.


Symbol


I am looking for a schematic symbol not found in the Scheme-it library, where would I find this? Do you have parts that have more pins than the original or do you just have one symbol for them?

Not all the parts have schematics in the Scheme-it library. What you can do instead is build your own IC with the custom symbol option. Go to Custom Symbols > Symbol Primitives and you’ll see different shapes of Part Body, as well as Top/Bottom/Left/Right pin’s. The body can be dragged onto the schematic, and the pins can be dragged onto the appropriate spots on the custom part body. Using this system, you can build most any IC schematic symbol you should need. If you find a schematic symbol that you need, but you need it to have more I/O’s you would still need to create a custom symbol as you cannot add pins to the schematic symbol that was loaded from the Scheme-it library.

I’m trying to use Scheme-it to make a simple wiring diagram for an on/off switch, but can’t seem to get the hang of it?

Under schematic symbols on the left you can go to switches. Select the switch that you would like to use, if you do not see the one you want, you would need to make a custom symbol (a square) then add the pins to the switch as you like. Then grab the other parts and drag and drop wires.

I am looking for an IGBT that has a specific symbol like an inductor or a capacitor.

Go to Schematic symbols, click on transistors and select one from the drop down.

I can't seem to find a simple bulb icon; do you know where I can find one?

Go to System Icons>System Level Components, then half way down the page is a light bulb, which you will need to add pins.

How do I access internal block diagrams of certain integrated circuits?

Internal block diagrams may be found on datasheet, search part number on Digi-Key website to view datasheet.

I am looking for a single wire bridge.

In the Schematic Symbols>Connectors>Screw Terminal; or go to Ports and create a node as a junction of a single wire or multiple wires.

Is there a way to draw lines and arrows that are not part of the circuit?

There are a few options for different arrows under Diagram Symbols.

How can I create 3 input nand gate?

The only premade version for a three input nand gate is part number 74HC10PW-Q100 a Triple 3-input nand gate under Manufacturers >NXP>Automotive>logic, but for the signal 3-input device, you would need to create this symbol using Custom Symbols> Symbol Primitives and then three pins and blank box. Another option would be to use a valid URL of a symbol and click insert on the top menu bar and enter the link. The symbol will show up on the schematic.

How do I connect the 3 pins of the regulator to the input, ground and output?

Click on the part, drag your "wire" to the next part, and click again.

I have a custom symbol which I have inserted a pin on the right; however, it will not allow me to add a pin on the left. How to add the pin on the left?

Make sure to place the pin directly over the custom symbol, it will automatically get matched to the part when done correctly.

How do I insert a generic voltage source with +15 volts?

Go to schematic symbols, click on the sources tab, or you can use a vrail symbol under the port sub header. Another option is to use a valid URL of a symbol and click “insert” on the top menu bar and enter the link. The symbol will appear on your schematic.

How do I get a symbol for a voltage source?

The voltage source for AC and DC is located under Schematic Symbols, then under Ports, scroll down and select the appropriate option.

1. On the left, click on schematic symbols
2. Scroll down to Ports
3. Click on the desired voltage source

I want to create a circuit with a lamp in it, but I can't seem to find the symbol for a lamp, which is just a circle with a cross in it.

We do not carry a lamp symbol with a cross in it, nor can it be made with a primitive symbol. You may find a valid URL of a symbol and click “insert” on the top menu bar and enter the link. The symbol will appear on your schematic.

How do I copy-paste a custom symbol from one design to another?

Copy the part while it is in design, then open another design and paste it.

Where can I find a 555 timer component?

Scheme-it does not have a 555 timer loaded into the library. You may need to build a custom symbol, or you may use a valid URL of a symbol and click “insert” on the top menu bar and enter the link. The symbol will appear on your schematic.

I want to use the 1x4 header on the left hand side of the schematic. When I rotate it the pin numbers are backwards.

Unfortunately the numbers will stay backwards when using the header. Whether you rotate or flip horizontally or vertically also.

Is there a way to add pins and part numbers and id’s to the symbol, or do I have to start from a custom symbol?

If you have a custom symbol you can add pins to it, then click insert on the top task bar and add a text box next to it and label the pin, the part number, and any other information that you would like about the part.

I was unable to find a shape of an op amp with 9 pins.

In Scheme-it, this shape has not a part of the library. You may build it with a custom symbol, or you may use a valid URL of a symbol and click “insert” on the top menu bar and enter the link. The symbol will appear on your schematic.

How do I change the endpoints of a wire?

Use a node to make the connection wherever you would like. Go to schematic symbols on the dropdown on the left. Go to port, and then select port node. Drag it anywhere on the schematic, then connect the wire to the port node, as the new endpoint.

1. You need an endpoint to place your wire or lead
2. GO to schematic symbols, and scroll down to ports
3. Click on Port, Node
4. Click and drag it onto the schematic and connect the wire/lead to it.

How do I draw a wire?

You will need to have parts with pins on them, hover over the pin and it should light up with a green box, then click and drag the wire to the next connection point.You will need to have parts with pins on them, hover over the pin and it should light up with a green box, then click and drag the wire to the next connection point.

How do I change the color of a wire?

Click on the wire, then on the right sidebar click on Line Properties tab and select a color by clicking on the black colored box under Line Style. Once the color is selected, press [ok] and the wire color will change on the schematic. /p>

1. Click on the wire
2. Go to Line Properties and click on the color bar
3. Select the color you want and click [Ok]
4. The color of the wire changed on the schematic

For the logic gates, do you have any with four inputs?

No we do not have any that go up to four, you may use a Custom Symbols>Symbol Primitives and create your own.

Say I wanted to run a wire in parallel; would I just do that off the wire?

Yes, click and hold on the original wire and drag it to where you want to connect it.

Looking for an incandescent lamp.

Look under Schematic Symbols > Optoelectronics > Lamp, Incandescent, Var 1.

Do you have shielded single and multi-conductor available?

No, we only have just plain wire, which can be dashed or slotted. You may be able to insert a textbox and label the wire shielded or give it a certain number of conductors.

I was wondering if this Scheme-it also works with the DIP8 configuration like for op amps.

No, you would need to create a custom primitive symbol in order to achieve that.

Do you have automotive symbols for your design tool, such as headlights and turn signals?

Unfortunately there are no symbols designed for parts of a motor vehicle such as headlight's or turn signals.

Can custom symbols be saved and reused in Scheme-it?

No, you may save a schematic and then copy and paste the symbol from one schematic to another schematic.

How can I get current source symbol?

Go to schematic symbols, then to Sources.

I need a potentiometer schematic symbol.

Potentiometers are under resistors. It is the last listing, referred to as variable.

Do you have watt-meters available in the schematics symbols?

No we do not have those symbols in Scheme-it. Another option would be to use a valid URL of a symbol and click “insert” on the top menu bar and enter the link. The symbol will appear on your schematic.

How to draw a diagonal resistor in a circuit.

There is not a way to make them diagonal, only vertical or horizontal. Another option would be to use a valid URL of a symbol and click “insert” on the top menu bar and enter the link. The symbol will appear on your schematic.

I have found the components used, but am unable to find where I can establish pin-outs.

Find the part on our site and look for the pin outs on the datasheet.

I want to show direction of current on the connecting wire with arrow.

Schematic Symbols > Ports > Port: Input Pin or Port: Output Pin.

Is there any way that I can copy & paste pins to a custom object?

Scheme-it does not provide this functionality. You will need to physically add the pins from the Custom Symbols>Symbols Primitives drop down.

How do I insert a 0V endpoint into my schematic?

You will need to select a node and label it as a 0v endpoint.

Looking for a simple transformer.

Go to schematic symbols then select transformers & chokes.

I need an ohmmeter schematic symbol.

An ohmmeter schematic is not available in Scheme-it; you may be able to use a DMM symbol. Another option would be to use a valid URL of a symbol and click “insert” on the top menu bar and enter the link. The symbol will appear on your schematic.

I could not find the symbol for a simple RGB LED.

We do not have a symbol for an RGB, you may be able to use three single LED symbols. Another option would be to use a valid URL of a symbol and click “insert” on the top menu bar and enter the link. The symbol will appear on your schematic.

Is there a schematic on stepper motors, with Nema 17 connected with driver bl-bt 6560?

Stepper Motor symbols can be found under Schematic Symbols>Motors, however, no stepper motor symbols in the Scheme-it library for this exact configuration, select a custom symbol to create that symbol.

How can I make a connector, 2 rows wide 3 pins per row?

Using Custom Symbols > Symbol Primitives > Part Body: Rectangle; and Schematic Symbols > Ports > Port: Port, Node for pins.

I am looking for a 4x4 keypad, do you have any?I am looking for a 4x4 keypad, do you have any?

There are no 4x4 keypad symbols loaded into Scheme-it. You will need to create a custom symbol to use, or use a valid URL of a symbol and click “insert” on the top menu bar and enter the link. The symbol will appear on your schematic.

Is there a way to use "pins" for connections of wire to components without the custom feature?

Go to schematic symbols then to port, and select port node.

Is there a symbol for a solenoid?

Search solenoid, or go to system icons, then to system level components. Or use a valid URL of a symbol and click “insert” on the top menu bar and enter the link. The symbol will appear on your schematic.

Where are the capacitor symbols?

Schematic Symbols > Passives (just under the Optoelectronics bar) > Capacitors.

Is there any option to use bubbled PMOS transistors?

No, you would need to create a custom symbol, or use a valid URL of a symbol and click “insert” on the top menu bar and enter the link. The symbol will appear on your schematic.

Will the Digi-Key Part Numbers (which look like they have good models) go directly to PCB footprints?

No, they will not go directly to PCB footprints.

Trying to find normally open and normally closed relays, do you have other options with more poles and throws?

Click on Schematic Symbols> Electromechanical>Relay. In there you will find the relays. For more poles and throws you would need to create a custom symbol to use as a relay. Another option would be to use a valid URL of a symbol and click “insert” on the top menu bar and enter the link. The symbol will appear on your schematic.

Looking for NO/NC contacts for a relay, do you have them?

We do not have that option for a relay. You could use a textbox to label a contact NO or NC but there is no specific symbol for it. You may create it in paint, and then import the picture of the new relay

I am wondering if you have a Zener diode in the list of component symbols.

Go to schematic symbols, then to diodes.

Where can I find the wire which is being connected to an op-amp?

Select your part then hover over the pin, a green box should light up then you can select the box and drag your wire to the next connection.

Can custom symbols be saved and reused in Scheme-it, and is there a way to retrieve my work if I did not save it and closed out of the program

No, you may save a schematic and then copy and paste the symbol from schematic to schematic only. There is no “auto save” feature for the program so, if you do not save your project there is no way for us to retrieve it.

I am trying to draw a panel with R, Y, and B connections.

You will need to create a custom symbol, and then add pins to it to make your connections.

Trying to add a pin to my part.

You can only add pins to parts that are custom symbols. Select Schematic Symbols, then to Ports and match it up level to the component to make it appear attached.

Instead of using component symbol I need to draw a box for a transistor.

You can use a custom symbol, and then add pins to the part, or use a valid URL of a symbol and click “insert” on the top menu bar and enter the link. The symbol will appear on your schematic.

I am looking for the ohm or Omega symbol.

Scheme-it does not have the ohm symbol listed. You can insert a URL to get one on your project. On the top menu bar select insert, then image, then copy and paste the link and the picture will be on your project.

I need to create a custom box.

Go to Custom Symbols>Symbol Primitives and select the part body and the pins needed for the part.

How do you connect two resistors?

Place the resistors butted up to each other and they will connect. If you keep them apart you can hover over the end of one and a green box will pop up. Click on the green box and drag it to the connection of the next resistor.

I am looking for a symbol not found in the Scheme-it library. Where would I find this?

Most specific ICs don’t have their own individual icon you can drop onto schematics in Scheme-it. What you can do instead is build your own IC with the custom symbol system. Go to Custom Symbols > Symbol Primitives and you’ll see different shapes of Part Body, as well as Top/Bottom/Left/Right legs. The body can be dragged onto the schematic, and the legs can be dragged onto the appropriate spots on the custom part body. Using this system, you can build most any IC schematic symbol you should need.


Properties


I would like to label wiring and the outputs of a part in a schematic

To label the wire, you will need to insert a text box from the top task bar. You can make multiple text boxes to make multiple labels for your wire or component. On the right hand side under Diagram Symbols you can go under basic shapes and select a label as well. The label has the same properties as the text box.

How do I change size of text / font?

After you click on the text box or symbol, then in the upper right of the screen, the Font Properties will appear. Under "Basic style" are the options for font size, which are the boxes labeled "Tt and tT". "Tt" will make the font smaller each time you click "Tt", and "tT" will make the font size larger each time you click.

May I know how to rotate a symbol?

Right click on the part and select rotate, or click on the part and click the “R” button on your keypad and the part will rotate. This may be done multiple times if you need additional rotation on the part. Note: Custom symbols do not have this feature available.

1. Right click on the part and scroll down to rotate
2. After you click rotate you will see that the part has rotated

I need to add in the actual resistor values and voltages, can you help?

Click insert then text box, then you can add the values above the part. Or go to the Properties tab on the right and enter the values. Be sure to click on the part first.

I want to know how to give values to my parts?

Click on the symbol you want to define. Then click on "Part Properties" on the right sidebar. From there enter the part name and value. Make sure to select the box next to the value or name, otherwise it will not show on the schematic.

1. Click on the part and go to Part Properties
2. Click on the check box to show the values/name you create.

Is it possible to free draw a schematic, or is there a way to just insert lines?

You can create custom symbols and drag and drop wires for connection points, or you could be creative and custom make line diagrams with nodes and ports as connection points. You cannot have floating lines, they need to be connected to a part

Is there a way to extend the length of a line without it connecting to anything else?

No, the line must be connected to two points, a beginning and an end, you may be able to use a port or node, to try and gain some length.

Will you build a schematic for me?

We do not offer any design services within Scheme-it.

Is Scheme-it free to use

Scheme-it is a freely available tool customers can use as much as they like without charge. There is no Scheme-it ‘license’, and you can use it to design schematics, flow charts, diagrams, and anything else they need for your business or any projects you might have without any legal entanglements. So long as you don’t try and sell access to Scheme-it yourself, you should be good to go.

Is there an update I can download to this Scheme-it?

No, all updating is done internally.

The Scheme-it software is very slow today

It may be due to maintenance on the software. Try to save your project and restart the program.

Can I change colors of the wire connections on this program?

You can change the color of the wire, but not the color of the connections.

How to change name of component selected?

There will be a part properties tab on the right when the part is selected In the part properties you can add the value and the name of the part.

I cannot connect a line without going from symbol to symbol, is there any way around it?

You can do this by going under the schematic symbols, then ports, and then port nodes. This will give you the ability to just connect the nodes rather than the parts.

Can I use two colors on one line, or change the color of a part, port or the connections on the part?

No, you can only change it to one color. However, you could put in a node or a junction and color the line individually to and from that point. You cannot color the wire connections, the color of the part, or the color of the port. You can change the color of the wire by clicking on the wire, which opens the "Line Properties" on the right margin, click on the black box to the right of the "Line style". This will open the color options. Click on the color you want to change the wire color to and then click "OK".

I was wondering if there is a way to insert lines into my schematic. Is there a possibility to erase only part of a line?

No, the only way to have lines on the schematic is by connecting wires to the parts, you cannot free draw. You would have to erase the whole wire and not just a segment of it, or you could use ports to be the end point and the start of a wire.

How do I draw a construction line?

You cannot just draw lines, you can only draw wires that connect the pins, however, you can change the line properties to be dashed, solid, or dotted.

How do I copy something on page 1 and paste it on page 2?

Copy what you want, then click the plus sign on the bottom of page one, then paste on page 2.

Can I select a different cursor?

Scheme-it does not have that feature.

How do I move multiple components?

Click and drag over the parts to highlight them. From there you can click and drag the components you highlighted.

1. Click and drag over all the components and unclick
2. Click and drag on the components
3. You can place them wherever you would like on the schematic.

How to vary the thickness of the wire to show the mode of operation?

Once you create the line there will be a line properties tab on the right. You can change the line style to dotted, dashed, or solid.

How to group components?

You need to highlight the entire group, and on the right hand side click on "group".

How do I edit a part's name?

Click right on the part and go into edit properties, from there you can name and add values to the part.

How do I erase a segment of a line?

You would have to erase the whole wire and not just a segment of it, or you could use ports to be the end point and the start of a wire.

How to name the ports?

Click on the port, on the right hand side the part properties tab will show and you can name it and add values there.

I have just built a circuit and while doing a rotate I have lost my circuit off the screen.

Try the undo button, control+Z, or zoom out of the page.

Is it possible to select a component and tell it to replace it with a different one in-place?

No, you would need to delete components and redraw the schematic.

Is there a way to create a name for premade symbols?

Click on the part and on the right there will be part properties; you can change the name from there.

I am having trouble with pdf in Scheme-it, the margins are off, and I am trying to export a drawing into a PDF file but only about a 1/3 of the drawing actually gets exported. Is there a way to only export a portion of my schematic?

After exporting, you will get an option to save as a pdf. When saving try a different paper size and see if that works. There is also a size limitation which may cause you to have to break it down to multiple pages. Make sure to also select active area to make sure you get the whole schematic. When exporting, also make sure to go through the properties tab to ensure margins are correct. If you want to only export part of it you can break the pdf down by adding pages on your schematic.

I want to change the color of the figures I drew.

You can change the color of the line, but not the color of the part.

I would like to move the text items around a component.

You can click on the part number that comes up, once you click on it, a green box should appear around the label, and now drag the part and move it to your desired location.

Can you tell me how to draw resistance values?

You would use the symbol for a resistor and a text box to label it your resistance value, or you can select the resistor, and on the right hand side there will be a Properties tab. From that tab, enter the value and the name of the part.

How do I draw block diagram using Scheme-it?

You would need to use a custom symbol and label the parts as you want them to appear on the schematic. You can do that with a text box from the top task bar by selecting “insert”.

How do you copy a circuit diagram and paste it to a word document?

You cannot copy and paste directly from your schematic, however, you can export the schematic to a pdf then, copy and paste from the pdf to Microsoft Word.

I would like to copy part of another schematic and paste it into Scheme-it.

You cannot directly copy and paste from Scheme-it. However, if you have a link of it in a valid URL such as a .png, .jpg, or a .jpeg you can use the “insert” feature and copy the link.

The problem is that when I'm connecting pins with wires, the wires overlap. So I want to move them so they don't overlap.

Click and make your connection, then go around the object and click again. Then go around the other side and click again. As long as you have not connected the wire between two points you can click and drag wherever you want to make the wires go around objects.

Can I link two parts into one?

You will need to create a custom symbol in order achieve a part that is two in one. Another option is to create it in paint then insert it into your schematic.

Program has stopped working.

The site may be under maintenance, restart the design tool, or send an email to webmaster@digikey.com.