GWS500 Installation Manual TDK-Lambda General Safeq lnstrucfions: A
Page 1 of 12 PA590-04-01G (a)
G
WS
5
0
0
Installation Manual
ENGLISH
General Safety Instructions:
READ SAFETY INSTRUCTIONS
Servicing:
These products are not customer serviceable TDK-Lambda UK LTD and their authorised agents only are permitted
to carry out repairs.
Critical Components:
These products are not authorised for use as critical components in nuclear control systems, life support systems or
equipment for use in hazardous environments without the express written approval of the Managing Director of TDK-
Lambda EMEA.
Product Usage:
These products are designed for use within a host equipment which restricts access to authorised competent
personnel.
This product is a component power supply and is only to be installed by qualified persons within other equipment and
must be not operated as a stand alone product.
This product is for sale to business to business customers and can be obtained via distribution channels.
It is not intended for sale to end users.
This product is a component power supply and does not fall within the scope of the EMC directive. Compliance with
the EMC directive must be considered in the final installation. Please contact your local TDK-Lambda office.
Environmental:
These products are IPX0, and therefore chemicals/solvents, cleaning agents and other liquids must not be used.
Environment:
This power supply is a switch mode power supply for use in applications within a Pollution Degree 2, overvoltage
category II environment. Material Group IIIb PCB’s are used within it.
Output Loading:
The output power taken from the power supply must not exceed the rating stated on the power supply label, except
as stated in the product limitations in this handbook.
Input Parameters:
This product must be operated within the input parameters stated in the product limitations in this handbook.
End of Life Disposal:
The unit contains components that require special disposal. Make sure that the unit is properly disposed of at the
end of its service life and in accordance with local regulations.
RISK OF ELECTRIC SHOCK
High Voltage Warning:
Dangerous voltages are present within the power supply.The professional installer must protect service personnel
from inadvertent contact with these dangerous voltages in the end equipment.
WARNING: When installed in a Class 1 end equipment, this product must be reliably earthed and professionally
installed.
The (+) or (-) output(s) can be earthed or left floating.
The unit cover(s)/chassis (where applicable) must not be made user accessible.
The mains input connector is not acceptable for use as field wiring terminals.
GWSSOO Installation Manual TDK-Lambda
Page 2 of 12 PA590-04-01G (a)
G
WS
5
0
0
Installation Manual
For encased products, do not use mounting screws, which penetrate the unit more than; See drawings.
Internal fuses protect the unit and must not be replaced by the user. In case of internal defect, the unit must be
returned to TDK-Lambda UK LTD or one of their authorised agents.
A suitable mechanical, electrical and fire enclosure must be provided by the end use equipment for mechanical,
electric shock and fire hazard protection.
Energy Hazards:
The main output of this product is capable of providing hazardous energy (240VA). Final equipment manufacturers
must provide protection to service personnel against inadvertent contact with the output terminals.
The unit cover/chassis, where applicable, is designed to protect skilled personnel from hazards. They must not be
used as part of the external covers of any equipment where they may be accessible to operators, since under full
load conditions, part or parts of the unit chassis may reach temperatures in excess of those considered safe for
operator access.
GWS500 Installation Manual TDK-Lambda All emeine Sicherheifisvorschriften: A
Page 3 of 12 PA590-04-01G (a)
G
WS
5
0
0
Installation Manual
DEUTSCH
Allgemeine Sicherheitsvorschriften:
LESEN SIE DIE SICHERHEITSVORSCHRIFTEN
Wartung:
Diese Produkte können nicht durch den Kunden gewartet werden. Nur TDK-Lambda UK LTD. und deren
zugelassene Vertriebshändler sind zur Durchführung von Reparaturen berechtigt.
Kritische Komponenten:
Diese Produkte sind nicht für die Verwendung als kritische Komponenten in nuklearen Kontrollsystemen,
Lebenserhaltungssystemen oder Geräten in gefährlichen Umgebungen geeignet, sofern dies nicht ausdrücklich und
in Schriftform durch den Geschäftsführer von TDK-Lambda EMEA genehmigt wurde.
Produktverwendung:
Diese Produkte sind zur Verwendung innerhalb von Host-Anlagen gedacht, die einen auf das Fachpersonal
beschränkten Zugang haben.
Dieses Produkt ist eine Stromversorgungs-Komponente und sie darf nur von qualifiziertem Personal in andere
Geräte eingebaut werden und sie darf NICHT als eigenständiges ("Stand-Alone") Gerät betrieben werden.
Dieses Produkt ist für den Verkauf an Geschäftskunden entwickelt worden und es kann über Distributionskanäle
bezogen werden.
Es ist NICHT für den Verkauf an Endkunden gedacht und konzipiert.
Dieses Produkt ist eine Stromversorgungsbaugruppe und sie fällt NICHT in den Bereich der EMV Direktive.
Die Konformität mit der EMV Richtlinie muss in der finalen Gesamtinstallation betrachtet werden.
Bitte kontaktieren Sie Ihr regionales TDK-Lambda Vertriebsbüro im Falle von Rückfragen.
Umwelt:
Diese Produkte sind IPX0, aus diesem Grund dürfen keine Chemikalien/Lösungsmittel, Reinigungsmittel und andere
Flüssigkeiten verwendet werden.
Umgebung:
Dieses Netzteil ist ein Schaltnetzteil zur Verwendung in einer Umgebung mit einem Verschmutzungsgrad 2,
Überspannungskategorie II. Materialgruppe IIIb mit darin verwendeten PCBs.
Ausgangsstrom:
Der Ausgangsstrom des Netzteiles darf die Leistung, die auf dem Label des Netzteiles vermerkt ist, nur dann
überschreiten, wenn dies in den Produktgrenzen dieses Handbuches ausgezeichnet ist.
Eingangsparameter:
Dieses Produkt muss innerhalb der Eingangsparameter, die in den Produktgrenzen dieses Handbuches angegeben
sind, betrieben werden.
Entsorgung am Ende der Betriebszeit:
Das Gerät enthält Komponenten die unter Sondermüll fallen. Das Gerät muss am Ende der Betriebszeit
ordnungsgemäß und in Übereinstimmung mit den regionalen Bestimmungen entsorgt werden.
GEFAHR DURCH ELEKTRISCHEN SCHLAG
Hochspannungswarnung:
Innerhalb des Netzteiles gibt es gefährliche Spannungen.Der Elektroinstallateur muss das Wartungspersonal vor
versehentlichem Kontakt mit den gefährlichen Spannungen im Endgerät schützen.
WARNUNG! Falls Sie unser Netzgerät in eine Anwendung mit Schutzklasse 1 eingebaut haben, stellen Sie sicher,
dass es fachgerecht installiert und zuverlässig geerdet ist.
GWSSOO Installation Manual TDK-Lambda
Page 4 of 12 PA590-04-01G (a)
G
WS
5
0
0
Installation Manual
Die (+) oder (-) Ausgänge können geerdet werden oder unangeschlossen bleiben.
Die Abdeckung des Gerätes/das Gehäuse darf für den Benutzer nicht zugänglich sein.
Der Haupteingangsanschluss ist nicht für die Verwendung als Feldverdrahtungsanschluss geeignet.
Für ummantelt Produkte, verwenden Sie keine Schrauben, die das Gerät mehr als durchdringen; siehe Zeichnung
Eine interne Sicherung schützt das Gerät und darf durch den Benutzer nicht ausgetauscht werden. Im Fall von
internen Defekten muss das Gerät an TDK-Lambda UK LTD oder einen der autorisierten Vertriebshändler
zurückgeschickt werden.
Ein geeignetes mechanisches, elektrisches und brandgeschütztes Gehäuse muss als Schutz vor der Gefahr von
mechanischen Risiken, Stromschlägen und Brandschutz in dem Endgerät vorgesehen werden.
Gefahren durch elektrische Energie:
Von bestimmten Modulen kann je nach Einstellung der Ausgangsspannung gefährliche elektrische Energie
ausgehen (240 VA). Die Endgerätehersteller müssen einen Schutz für Servicepersonal vor unbeabsichtigtem
Kontakt mit den Ausgangsanschlüssen dieser Module vorsehen. Kann aufgrund der Einstellung gefährliche
elektrische Energie auftreten, dürfen die Modulanschlüsse für den Benutzer nicht zugänglich sein.
Die Geräteabdeckung/das Gehäuse ist so entworfen, dass das Fachpersonal vor Gefahren geschützt wird. Sie
dürfen nicht als Teil der externen Abdeckung für Geräte verwendet werden, die für den Betreiber zugänglich sein
müssen, da Teile oder das gesamte Gerätegehäuse unter voller Auslastung übermäßige Temperaturen erreichen
kann, die für den Zugang des Betreibers nicht mehr als sicher betrachtet werden.
Gwssoo Installation Manual TDK-Lambda Consi nes énérales de sécurifié: A
Page 5 of 12 PA590-04-01G (a)
G
WS
5
0
0
Installation Manual
FRANÇAIS
Consignes générales de sécurité:
LIRE LES CONSIGNES DE SECURITE
Entretien:
Ces produits ne peuvent pas être réparés par l’utilisateur. Seuls, TDK-Lambda UK LTD et ses agents agréés sont
autorisés à effectuer des réparations.
Composants critiques:
Ces produits ne doivent pas être utilisés en tant que composants critiques dans des systèmes de commande
nucléaire, dans des systèmes de sauvetage ou dans des équipements utilisés dans des environnements dangereux,
sans l'autorisation écrite expresse du directeur général de TDK-Lambda EMEA.
Utilisation du produit:
Ces produits sont conçus pour être utilisés dans un équipement hôte dont l'accès n'est autorisé qu'aux personnes
compétentes.
Ce produit est une alimentation considérée comme un composant devant être installé par des personnes qualifiées,
dans un autre équipement. Il ne doit pas être utilisé en tant que produit fini.
Ce produit est destiné à la vente entre entreprises et peut être obtenu via des canaux de distribution.
Il n’est pas prévu à la vente pour les particuliers.
Ce produit est une alimentation considérée comme un composant, il ne relève pas du champ d’application de la
directive CEM. Le respect de la directive CEM doit être pris en compte dans l’installation finale. Veuillez contacter
votre bureau TDK-Lambda le plus proche.
Environnement:
Ces produits sont IPX0, et donc on ne doit pas utiliser des produits chimiques/solvants, des produits de nettoyage et
d'autres liquides.
Environnement fonctionnel :
Cette alimentation fonctionne en mode commutation pour utilisation dans des applications fonctionnant dans un
environnement avec Degré de Pollution 2 et catégorie de surtension II. Elle utilise des cartes des circuits imprimés
(PCB) de Groupe IIIb.
Intensité soutirée:
L'intensité soutirée de l'alimentation ne doit pas dépasser l'intensité nominale marquée sur la plaque signalétique,
sauf indications contraires dans les limitations du produit décrit dans ce manuel.
Paramètres d'entrée:
Ce produit doit être utilisé à l'intérieur des paramètres d'entrée indiqués dans les limitations du produit dans ce
manuel.
Elimination en fin de vie:
L'alimentation contient des composants nécessitant des dispositions spéciales pour leur élimination. Vérifiez que
cette alimentation est mise au rebut correctement en fin de vie utile et conformément aux réglementations locales en
vigueur.
RISQUE DE CHOC ELECTRIQUE
Attention-Danger haute tension:
Des tensions dangereuses sont présentes dans l'alimentation. L'installateur doit protéger le personnel d'entretien
contre un contact involontaire avec ces tensions dangereuses dans l'équipement final.
AVERTISSEMENT: Si ce produit est installé dans un équipement final de classe I, il doit être mis à la terre de
manière fiable et installé par un professionnel averti.
GWSSOO Installation Manual TDK-Lambda
Page 6 of 12 PA590-04-01G (a)
G
WS
5
0
0
Installation Manual
Les sorties (+) ou (-) peuvent être raccordées à la terre ou laissées flotttantes.
Le couvercle/châssis de l'alimentation ne doit pas être accessible à l'utilisateur.Le connecteur d'entrée d'alimentation
principale ne doit pas être utilisé comme borne de raccordement.
N'utilisez pas de vis pénétrant dans le module sur une profondeur supérieure à :Voir dessins.
Un fusible interne protège le module et ne doit pas être remplacé par l'utilisateur. En cas de défaut interne, le module
doit être renvoyé à TDK-Lambda UK LTD ou l'un de ses agents agréés.
Une enceinte appropriée doit être prévue par l'utilisateur final pour assurer la protection contre les chocs
mécaniques, les chocs électriques et l'incendie.
Energies dangereuses :
Certains modules peuvent générer une énergie dangereuse (240 VA) selon le réglage de tension de sortie. Le
fabricant de l'équipement final doit assurer la protection des techniciens d'entretien contre un contact involontaire
avec les bornes de sortie de ces modules. Si une telle tension dangereuse risque de se produire, les bornes ou les
connexions du module ne doivent pas être accessibles par l'utilisateur.
Le couvercle et le châssis du module sont conçus pour protéger des personnels expérimentés. Ils ne doivent pas
être utilisés comme couvercles extérieurs d'un équipement, accessible aux opérateurs car en condition de puissance
maximum, des parties du châssis peuvent atteindre des températures considérées comme dangereuses pour
l'opérateur.
Gwssoo Installation Manual TDK-Lambda Norme generali di sicurezza: A
Page 7 of 12 PA590-04-01G (a)
G
WS
5
0
0
Installation Manual
ITALIANO
Norme generali di sicurezza:
SI PREGA DI LEGGERE LE NORME DI SICUREZZA
Manutenzione:
Il cliente non può eseguire alcuna manutenzione su questi prodotti. L'esecuzione delle eventuali riparazioni è
consentita solo a TDK-Lambda UK LTD e ai suoi agenti autorizzati.
Componenti critici:
Non si autorizza l'uso di questi prodotti come componenti critici all'interno di sistemi di controllo nucleari, sistemi
necessari alla sopravvivenza o apparecchiature destinate all'impiego in ambienti pericolosi, senza l'esplicita
approvazione scritta dell'Amministratore Delegato di TDK-Lambda EMEA.
Uso dei prodotti:
Questi prodotti sono progettati per l'uso all'interno di un'apparecchiatura ospite che limiti l'accesso al solo personale
competente e autorizzato.
Questo prodotto è da considerarsi come un alimentatore professionale componente e come tale deve essere
installato da personale qualificato all'interno di altre apparecchiature e non può essere utilizzato come prodotto
indipendente.
Questo prodotto non è inteso per la vendita al dettaglio o agli utilizzatori finali.
Questo alimentatore è da considerarsi come un componente e come tale non è assogettato dagli scopi della direttiva
EMC. Conformità alla direttiva EMC deve essere considerata nell'installazione finale di utilizzo. Gli uffici di TDK-
Lambda Sas Succursale Italiana sono a vostra disposizione per ulteriori ragguagli.
Condizioni ambientali:
Questi prodotti sono classificati come IPX0, dunque non devono essere utilizzati sostanze chimiche/solventi, prodotti
per la pulizia o liquidi di altra natura.
Ambiente:
Questo prodotto è un alimentatore a commutazione, destinato all'uso in applicazioni rientranti in ambienti con le
seguenti caratteristiche: Livello inquinamento 2, Categoria sovratensione II. Questo prodotto contiene schede di
circuiti stampati in materiali di Gruppo IIIb.
Carico in uscita:
La potenza in uscita ottenuta dall'alimentatore non deve superare la potenza nominale indicata sulla targhetta
dell'alimentatore, fatto salvo dove indicato nei limiti per i prodotto specificati in questo manuale.
Parametri di alimentazione:
Questo prodotto deve essere utilizzato entro i parametri di alimentazione indicati nei limiti per il prodotto, specificati
in questo manuale.
Smaltimento:
L'unità contiene componenti che richiedono procedure speciali di smaltimento. Accertarsi che l'unità venga smaltita
in modo corretto al termine della vita utile e nel rispetto delle normative locali.
RISCHIO DI SCOSSA ELETTRICA
Avvertimento di alta tensione:
All'interno dell'alimentatore sono presenti tensioni pericolose. Gli installatori professionali devono proteggere il
personale di manutenzione dal rischio di contatto accidentale con queste tensioni pericolose all'interno
dell'apparecchiatura finale.
ATTENZIONE: Se installato in un’attrezzatura di classe I, questo prodotto deve essere collegato a terra in modo
affidabile ed installato in modo professionale.
GWSSOO Installation Manual TDK-Lambda
Page 8 of 12 PA590-04-01G (a)
G
WS
5
0
0
Installation Manual
Le uscite (+) o (-) possono essere messa a terra o lasciate isolate.
I coperchi/il telaio dell'unità non devono essere accessibili da parte dell'utente.
Il connettore dell'alimentazione principale non può essere utilizzato come terminale di collegamento di campo.
Non utilizzare viti che penetrano nell'unità per più di : Vedi disegni
Un fusibile interno protegge l'unità e non deve essere sostituito dall'utente. Nell'eventualità di un difetto interno,
restituire l'unità a TDK-Lambda UK LTD o a uno dei suoi agenti autorizzati.
L'apparecchiatura finale deve includere una recinzione meccanica, elettrica e antincendio per proteggere dai pericoli
di natura meccanica, dalle scosse elettriche e dai pericoli di incendio.
Pericoli energetici:
Alcuni moduli sono in grado di erogare energia pericolosa (240 VA) a seconda della tensione in uscita impostata. I
produttori delle apparecchiature finali sono tenuti a proteggere il personale di manutenzione dal rischio di contatto
accidentale con questi terminali dei moduli di uscita. Se impostati su livelli che non escludono l'erogazione di energia
pericolosa, questi terminali o collegamenti non devono risultare accessibili da parte dell'utente.
Il coperchio/telaio dell'unità è realizzato per proteggere il personale esperto dai pericoli. Non deve essere usato
come parte degli involucri esterni di qualsiasi apparecchiatura, se risulta accessibile da parte degli addetti, poiché è
possibile che in condizioni di pieno carico una o più parti del telaio dell'unità giunga/giungano a temperature superiori
ai limiti considerati sicuri per l'accesso da parte degli addetti.
GWS500 Installation Manual TDK-Lambda lnstrucciones enerales de se uridad: A
Page 9 of 12 PA590-04-01G (a)
G
WS
5
0
0
Installation Manual
ESPAÑOL
Instrucciones generales de seguridad:
LEA LAS INSTRUCCIONES DE SEGURIDAD
Servicio:
Estos productos no pueden ser reparados por los clientes. TDK-Lambda UK LTD. y sus agentes autorizados son
los únicos que pueden llevar a cabo las reparaciones.
Componentes fundamentales:
Estos productos no pueden ser utilizados como componentes fundamentales en sistemas de control nuclear,
sistemas de soporte vital o equipos a utilizar en entornos peligrosos sin el consentimiento expreso por escrito del
Director General de TDK-Lambda EMEA.
Uso de los productos:
Estos productos han sido diseñados para ser utilizados en un equipo central que restrinja el acceso al personal
cualificado autorizado.
Este producto es una fuente de alimentación y sólo puede ser instalado por personal cualificado dentro de otros
equipos y no debe ser tratado como un producto independiente. Este producto debe ser vendido entre empresas
profesionales y solo puede obtenerse a través de los canales de distribución .No está destinado para la venta a
usuarios finales
Este producto es una fuente de alimentación y no se ve afectada por la directiva EMC . El cumplimiento de la
directiva EMC se debe considerar en la instalación final. Por favor, póngase en contacto con su oficina local de TDK
– Lambda.
Medioambiental:
Estos productos son IPX0 y, por tanto, no pueden utilizarse sustancias químicas/disolventes, agentes de limpieza ni
otros líquidos.
Medio ambiente:
Esta fuente de alimentación es una fuente de alimentación de modo conmutado a utilizar en aplicaciones dentro de
un entorno con un Grado de contaminación 2 y una Categoría de sobretensión II. En él se utilizan policloruros de
bifenilo del Grupo de materiales IIIb.
Carga de salida:
La potencia de salida tomada de la fuente de alimentación no puede sobrepasar el valor nominal indicado en la
etiqueta de la fuente de alimentación, excepto en los casos indicados en las limitaciones del producto en este
manual.
Parámetros de entrada:
Este producto debe ser utilizado dentro de los parámetros de entrada indicados en las limitaciones del producto en
este manual.
Desecho de la unidad:
La unidad contiene componentes que deben ser desechados de una manera especial. Asegúrese de desechar
correctamente la unidad al final de su vida útil y conforme a las normas locales vigentes.
PELIGRO DE DESCARGAS ELÉCTRICAS
Advertencia de alta tensión:
En esta fuente de alimentación hay tensiones peligrosas. El instalador profesional debe proteger al personal de
servicio contra cualquier contacto accidental con estas tensiones peligrosas en el equipo final.
ADVERTENCIA: La instalación de este producto en un equipo de clase I la deben llevar a cabo profesionales y el
producto debe estar conectado a tierra.
GWSSOO Installation Manual TDK-Lambda
Page 10 of 12 PA590-04-01G (a)
G
WS
5
0
0
Installation Manual
La salida o salidas (+) o (-) pueden conectarse a tierra o se las puede dejar flotando.
Debe impedirse el acceso de los usuarios a la cubierta o cubiertas y al chasis de la unidad.
El conector de entrada de la red no es apto para ser utilizado a modo de bornes de cableado de campo.
No utilice tornillos de montaje susceptibles de penetrar en la unidad más de: Ver dibujos.
Un fusible interno protege la unidad y este no debe ser nunca reemplazado por el usuario. En caso de existir algún
defecto interno, la unidad debe ser enviada a TDK-Lambda UK LTD o a uno de sus agentes autorizados.
El equipo de uso final debe constituir un recinto de protección mecánica, eléctrica y contra incendios de protección
mecánica, contra descargas eléctricas y contra el peligro de incendios.
Peligros de energía:
Algunos módulos pueden generar energía peligrosa (240VA) dependiendo de la configuración de la tensión de
salida. Los fabricantes de equipos finales deben proteger al personal de servicio contra un contacto accidental con
estos bornes de salida de los módulos. Si se configura de modo que pueda generarse energía peligrosa, hay que
evitar que el usuario pueda acceder a los bornes o conexiones del módulo.
La cubierta/chasis de la unidad ha sido diseñada para que proteja a las personas cualificadas de los peligros. No
deben ser utilizadas como parte de las cubiertas externas de cualquier equipo al que pueden acceder los operarios,
ya que bajo unas condiciones de carga completa, la pieza o piezas del chasis de la unidad pueden alcanzar
temperaturas superiores a las consideradas seguras para el acceso de los operarios.
Gwssoo Installation Manual TDK-Lambda lnstru fies erais de se uran a: A
Page 11 of 12 PA590-04-01G (a)
G
WS
5
0
0
Installation Manual
PORTUGUÊS
Instruções gerais de segurança:
LEIA AS INSTRUÇÕES DE SEGURANÇA
Manutenção:
Estes produtos não são podem ser submetidos a manutenção por parte do cliente. Apenas a TDK-Lambda UK LTD
e os seus agentes autorizados têm permissão para realizar reparações.
Componentes essenciais:
Não é autorizada a utilização destes produtos como componentes essenciais de sistemas de controlo nuclear,
sistemas de suporte de vida ou equipamento para utilização em ambientes perigosos sem a expressa autorização
por escrito do Director-Geral da TDK-Lambda EMEA.
Utilização do produto:
Estes produtos foram concebidos para utilização dentro de um equipamento de alojamento que apenas permita o
acesso a pessoal qualificado autorizado.
Este produto é uma alimentaçao considerado com um componente para ser instalado por pessoas qualificadas, em
outros equipamentos. Não deve ser usado como um produto acabado.
Este produto é destinado para venda entre as empresas e pode ser obtido através de canais de distribuição.
Não se destina à venda aos particulares.
Este produto é uma alimentaçao considerado com um componente, não é dentro do appliquation âmbito da directiva
CEM.
Conformidade com a directiva CEM devem ser considerados na instalação final.
Entre em contacto com seu escritório TDK-Lambda mais próximo.
Ambiental:
Estes produtos são IPX0 e, como tal, não se devem utilizar químicos/solventes, agentes de limpeza e outros
líquidos.
Ambiente:
Esta fonte de alimentação é uma fonte de alimentação do modo de comutação para utilização em aplicações com
um Nível de Poluição 2 e ambientes da categoria de sobretensão II. São utilizadas placas de circuitos impressos do
grupo de materiais IIIb.
Carga de saída:
A potência de saída extraída da fonte de alimentação não deve exceder a classificação assinalada na etiqueta da
fonte de alimentação, excepto quando indicado nas limitações do produto neste guia.
Parâmetros de entrada:
Este produto deve ser utilizado dentro dos parâmetros de entrada indicados nas limitações do produto neste guia.
Eliminação no fim de vida:
A unidade contém componentes que necessitam de procedimentos especiais de eliminação. Certifique-se de que a
unidade é devidamente eliminada no fim da sua vida útil e que tal é feito em conformidade com os regulamentos
locais.
RISCO DE CHOQUE ELÉCTRICO
Aviso de alta tensão:
Estão presentes tensões perigosas dentro da fonte de alimentação. O profissional que realizar a instalação deve
proteger o pessoal de assistência contra contactos inadvertidos com estas tensões perigosas do equipamento final.
AVISO: Quando instalado num equipamento de Classe I, este produto deve ser ligado à terra de forma fiável e
instalado por um profissional.
.
Gwssoo Installation Manual TDK-Lambda TDK-Lambda
Page 12 of 12 PA590-04-01G (a)
G
WS
5
0
0
Installation Manual
As saídas (+) e (-) podem ser ligadas à terra ou deixadas soltas.
O chassis/cobertura(s) da unidade não deve estar acessível ao utilizador.
O conector de entrada de alimentação não deve ser utilizado como terminal de cablagens no local.
Não utilize parafusos de montagem, uma vez que estes penetrarão na unidade em mais do que: Veja os desenhos
Existe um fusível interno que protege a unidade e que não deve ser substituído pelo utilizador. Em caso de defeito
interno, a unidade deve ser devolvida à TDK-Lambda UK LTD ou a um dos seus agentes autorizados.
O equipamento de utilização final deve fornecer um bastidor com protecção mecânica, eléctrica e contra incêndios
adequada.
Perigos de energia:
Alguns módulos tem a capacidade de fornecer energia perigosa (240 VA), de acordo com a configuração da tensão
de saída. O equipamento final do fabricante deve garantir que o pessoal de assistência está protegido contra
contactos inadvertidos com estes terminais de saída do módulo. Se essa energia perigosa for produzida, as
ligações e os terminais do módulo não devem ser acessíveis pelos utilizadores.
O chassis/cobertura da unidade está concebido de forma a proteger o pessoal especializado de perigos. Não devem
ser utilizados como parte das coberturas externas de qualquer equipamento em que possam estar acessíveis aos
operadores, uma vez que em condições de carga máxima, algumas peças do chassis da unidade podem atingir
temperaturas superiores às consideradas seguras para o acesso do operador.
TDK-Lambda UK Ltd
Kingsley Avenue, Ilfracombe
Devon, EX34 8ES
Telephone - Sales and Service +44 (0)1271 856666
Head Office and Works +44 (0)1271 856600
Facsimile +44 (0)1271 864894
WEBSITE: www.uk.tdk-lambda.com
G WS5 00 Series Instruction Manual
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
BEFORE USING THE POWER SUPPLY UNIT
Pay attention to all warnings and cautions before using the unit. Incorrect usage could lead to an electrical
shock, damage to the unit or a fire hazard.
WARNING and CAUTION
Do not modify.
Do not touch the internal components, they may have high voltage or high temperature. You may get
electrical shock or burned.
When the unit is operating, keep your hands and face away from it as you may be injured by flying debris in
the event of a fault.
This power supply is designed for use within an end product. Stick the WARNING label for users on the
system equipment and notify in the system instruction manual.
Never operate the unit under over current or short-circuit conditions for more than 30 seconds or outside its
specified Input Voltage Range, which could result in damage but there is no possibility of fire or burning.
Confirm connections to input/output terminals are correct as indicated in the instruction manual.
This power supply has a possibility for hazardous voltage to appear at output terminal depending on the type
of failure. The outputs of these products must be earthed in the end equipment to maintain SELV.
If the outputs are not earthed, they must be considered hazardous and must not be made user accessible.
Note: CE MARKING
CE marking, when applied to the GWS series products, indicates compliance with the Low Voltage Directive
(2014/35/EU) in that it complies with EN60950-1 2nd Edition.
DWG NO. : PA590-04-01G
APPD CHK DWG
GWS 500 12 1 El
1
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
1. Model Name Identification Method
GWS 50012 /
2. Terminal Explanation
2-1. Front Panel Explanation
(1) L : Input terminal Live line (Fuse in line)
(2) N : Input terminal Neutral line
(3) : Protective Earth (Frame Ground, FG)
(4) - V : - Output terminal
(5) +V : + Output terminal
(6) Output monitoring indicator (Green LED : ON)
(7) V.ADJ : Output voltage adjustment trimmer (The output voltage rises when the trimmer is turned clockwise.)
(8) CN201: Remote Sensing, DCOK, 5VSB, Remote On/Off and PV signals (Refer to 2.2)
(*1)
blank: Standard type
/BAT: Battery charging for 24V (21~29V/17.6A)
& 48V (42~58V/8.8A) only
/T: OTP auto recovery after unit cools down
/RL: Remote ON/OFF reverse logic (Active High)
/F: Full cover without internal fan but require
external forced air cooling.
/L: Without cover but require external forced air
cooling.
Option (*1)
Rated Output Voltage
Output Power type
Series name
umum: CN201 4 a sauna: m um as)» PCB
2
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
2-2. CN201 Connector Pin Configuration and Function
Pin No. Configuration Function
1 +Vm +Output Voltage Monitor
2 +S +Sensing
3 -Vm -Output Voltage Monitor
4 -S -Sensing
5 DCOK DCOK signal is an open collector output signal, referenced to
pin6 (COM). As the output voltage drops, DCOK signal will
output “High”.
6 COM Return loop for DCOK signal.
7 5VSB Auxiliary voltage output, 4.75~5.25V, referenced to pin8 (5V
COM). The maximum load current is 0.3A. This output is not
controlled by the remote ON/OFF control.
8 5V COM Return loop for 5VSB output.
9 CNT+ Remote ON/OFF control terminal (When CNT+ is pulled to
TTL low, power supply unit turns ON. Otherwise, it turns
OFF)
10 CNT- Return loop for CNT+ signal
11 PV Output voltage external control terminal
12 COM Return loop for PV signal.
CN201 Connector, Housing and Terminal Pins
PART DESCRIPTION PART NAME MANUFACTURER
PIN HEADER S12B-PHDSS(LF)(SN) JST
SOCKET HOUSING PHDR-12VS JST
TERMINAL PINS SPHD-002T-P0.5(AWG28~24)
SPHD-001T-P0.5(AWG26~22) JST
HAND CRIMPING TOOL YRS-620(SPHD-002T-P0.5)
YC-610R(SPHD-001T-P0.5) JST
RED 2 TWBT< black="" be="" red="" 10="" 9="" 12="" el="" el="">
3
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
2-3. Basic Connection (Local sensing)
(1) Connect “+S” terminal to “+Vm” terminal with sensing wire
(2) Connect “-S” terminal to “-Vm” terminal with sensing wire
(3) Connect “CNT+” terminal to “CNT-” terminal with wire
Please use attached connector for each connection.
2-4. Remote Sensing (+S, -S terminal)
(1) Connect “+S” terminal to “+” terminal of load with sensing wire
(2) Connect “-S” terminal to “-” terminal of load with sensing wire
(3) Connect “CNT+” terminal to “CNT-” terminal with wire
This function compensates voltage drop of wiring from output terminals to load terminals. Connect “+S” terminal to “+”
terminal of load and “-S” terminal to “-” terminal of load with sensing wires. The total line voltage drop (+ side line and
- side line) shall be less than 0.3V. In case that sensing lines are too long, it is necessary to put an electrolytic capacitor in
following places:
(1) across the load terminal,
(2) between “+S” terminal and “+V” terminal,
(3) between “S” terminal and “V” terminal.
When the function of remote sensing is not in use, connect +S terminal to +Vm terminal, and –S terminal to –Vm
terminal by the attachment connector. If remote sensing terminals are opened, the stability and the accuracy of the
output deteriorated. Therefore, terminal +S, -S must be connected.
Load
CN20 1 -S
+Vm
+V
-Vm
+S
-V
+
_
+
+
Ba Connecuon Local Sen ng CNYOV {W (x , . E ”9.,“ Ac INPUY Es—zsowc ON/OFF control reg uired Csz cwzm N «v -v -v Q N L z n . . n. a sst a n . 5 + D . v . 4 1n , p-Lo/oj _ 9 u . . 1: WWW 25725;“: CNZM DCOK oulgu 'gnal regu‘ ed Csz +v ~v-v -V\7[N L I' .5“ 5.4.! m '12 AC wpur 2572mm PV control reg uired *cmm CN2D‘ A; AC \NPUT 5572mm
4
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
3. Terminal Connection Method
Please pay extra attention to the wiring. Incorrect connection may cause damage the power supply.
When connecting input, output wiring, and CN201, input AC-Line should be OFF.
The output load line and input line shall be separated to improve noise immunity.
The protective earth (PE) must be connected to the terminal.
Remote sensing lines shall be twisted or use shielded wires.
Remote ON/OFF control lines shall be twisted or use shielded wire.
Current for each terminal screw shall be 40A or less.
Basic Connection (Local Sensing)
Connect with the attached connector to CN201
ON/OFF control required
“CNT-“ terminal is ground for “CNT+” terminal.
DCOK output signal required
Open collector method shown below shall be used
“COM“ terminal is ground for “DCOK” terminal.
PV control required
Inject external voltage between 3~6V
“COM“ terminal is ground for “PV” terminal.
5
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
4. Explanation Of Functions And Precautions
4-1. Input Voltage Range
Input voltage range is single phase 85 ~ 264VAC (47 ~ 63Hz) or 120 ~ 373VDC.
Input voltage which is out of specification, may damage the unit. For cases where conformance to various
safety specifications (UL,CSA,EN) are required, input voltage range will be 100~240VAC (50/60Hz).
Note: GWS500 series is able to withstand Input Surge of 300VAC for 5 seconds.
4-2. Output Voltage Range
V.ADJ trimmer is for output voltage adjustment within the range of specifications. Turning the trimmer clockwise will
increase the output voltage. Kindly note that over voltage protection ( OVP ) function may trigger if the output voltage is
increased excessively. Please ensure that the output power is below the rated output power, and output current is below
the maximum output current (12V & 48V) or below the peak output current (24V & 36V) when output voltage is raised.
4-3. Over Voltage Protection (OVP)
The OVP function will shutdown the output. To reset OVP, remove the input of power supply for a few minutes, and
then re-input. Alternatively, use CNT reset (Remote ON/OFF: OFF to ON). OVP setting is fixed and cannot be adjusted
externally.
4-4. Over Current Protection (OCP)
OCP function operates when the output current exceeds OCP specifications. OCP characteristic is constant current
limiting within their voltage range for 24V ~ 48V while hiccup mode for 12V. The output will automatically recover
when the overload condition is removed. Do not operate overload or shorted conditions for more than 30 seconds, which
could result in damage. There is no possibility of fire or burning. OCP setting is fixed and not to be adjusted externally.
4-5. Over Temperature Protection (OTP)
Over Temperature Protection function (manual reset type) is provided. When ambient or internal temperature rises
abnormally, OTP function will shut down the output. To recover the unit, first shut down the AC input and let the unit
cool down before turning ON the AC input. Alternatively, use CNT reset (Remote ON/OFF: OFF to ON) after letting the
unit cool down.
As for the /T option model, the unit automatically recovers after it cools down without the need for AC recycle or CNT
reset.
Power Supply DCOK - ov 55mg“: 2 A COM Power Supply 35m Source Current H CNT+ Relay. Transistor. m. Switch : Cm_
6
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
4-6. Low Output Detection Circuit (DCOK)
Low output voltage detection circuit is provided. DCOK signal is only valid after AC input is turn-on for more than one
sec. DCOK signal will turn “High” level to indicate abnormal status when the output voltage becomes less than
approximately 80% of rated. It uses the open collector method as shown below
4-7. Remote ON/OFF Control
Remote ON/OFF control is provided.
Using this function, output on/off is allowed to be controlled without input voltage on/off. The output is turned ON when
CNT+ and CNT- terminals are shorted, while the output is turned OFF when these terminals are opened. When this
function is not used, connect CNT+ and CNT- terminals together. The specifications for this function are as follows
(1) TTL compatible.
(2) The maximum input voltage to CNT+ terminal is 12V, and the maximum allowable reverse voltage is -1V.
(3) The source current for CNT+ terminal is 3.5mA.
(4) A switch or a relay or a transistor or a FET can be used as ON/OFF switch.
The /RL option model reverses the logic of the remote ON/OFF function.
Voltage Range between CNT+ and CNT- Output Status
Standard type /RL option
2.4 ≤ H ≤ 12.0V or Open OFF ON
0.0 ≤ L ≤ 0.8V or Short ON OFF
*ij 8 4: VI“: *ij 2 4: VI“: 2‘ II Lo + meem wave—m: , +\m:‘ 6X @-
7
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
4-8. Output Ripple & Noise
Ripple & noise are measured at 20MHz by using a 300mm twisted pair of load wires terminated with a 0.1uF film
capacitor & 47uF electrolytic capacitor. When load lines are longer, ripple becomes larger. The output ripple cannot be
measured accurately if the probe ground lead of oscilloscope is too long. At low temperature, large ripple & noise may
also be observed due to large ESR of the internal Electrolytic Capacitors especially at -25°C.
4-9. Series Operation
For series operation, either method ( A ) or ( B ) is possible.
Method ( A ) Method ( B )
4-10. Parallel Operation
(A) Operation to increase the Output Current is not possible.
(B) Operation as a Backup Power Supply is possible as follows:
1. Set the power supply output voltage higher by the amount of forward voltage drop ( VF) of the diode.
2. Please adjust the output voltage of each power supply to be the same.
3. Please use within the specifications for output voltage, output current and output power.
(A) (B)
Load
+V m
-V m
Power Supply
-S
+S
+V m
-V m
-S
+S
+Vm
-Vm
Load
Power Supply
-S
+S
+Vm
-Vm
-S
+S
Load
+V m
-V m
Load
Power Supply
-S
+S
+V m
-V m
-S
+S
+V m
-V m
Load
Power Supply
-S
+S
+V m
-V m
-S
+S
@9 ~ij 24 & 48V Mudcl I2 & 3h Mudcl ‘4 8: 4x\' Modal W 90% x094, 60%
8
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
4-11. Output Voltage External Control (PV)
Output voltage external control function is available. Output voltage can be varied by applying an external voltage
(3–6V) to “PV” terminal and “COM” terminal. Please consider the following characteristics.
Note:
For 12V & 36V output model, limit output voltage variation range at 60% ~ 110%. At PV voltage variation 3V ~ 5.5V.
For 24V output model, limit output voltage variation range at 60% ~ 120%. At PV voltage variation 3V ~ 6V.
For 48V output model, limit output voltage variation range at 80% ~ 120%. At PV voltage variation 4V ~ 6V.
Connection method
PV voltage (Nominal Input Voltage)
Output Voltage Linearity (12V, 24V, 36V & 48V)
5.5V
6V5V
Nominal
Vout
0
6
0%
3V
110%
120%
Output Voltage
8
0%
4V
48V Model
12~36V Model
12 &
36V Model
+Vm
-Vm
Load
Power Supply
-S
+S
PV
COM
External voltage
Output Voltage Derating
Output Voltage
100%
83%
Nominal Vout
0
110%
120%
90%
Load Current
8
0%
6
0%
48V Model
12~36V Model
9
0%
+ 1 j + G) G 9 -Vm j g} Output vunage Output Voltage Adjust Output Voltage Adjust 14v Medal 4svuede1 29v ‘sv 313nm] Manual ‘5 um; b \‘adj \ m, m t . ZIV' iiiiiiiiiiii I; ******* g ‘3 ********************* my ; 38 4V 14 4v (3 0 o 1 ‘ 6-“ Load c \ment 5 SA Load I: uzent
9
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
4-12. Battery Charging (/BAT) option
An option model for battery charging operation is available. It comes in two output voltages namely, 24V & 48V with
ex-factory setting of 29V & 58V respectively.
However, in conjunction with the Vadj and PV functions, the output voltage can be set to the range shown on the charts
below.
24/BAT should be used to charge 24V battery while 48/BAT should be used to charge 48V battery.
Battery charging (Constant Current) is applicable for valid output voltage range. The unit may hiccup below this voltage
range.
Connection method
+Vm
-Vm
Load
Power Supply
-S
+S
PV
COM
External voltage
10
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
4-13. Output Peak Current
For 24V, 36V output model, please meet the following conditions. Reduce peak current value according to output
derating as section 6-2.
Input voltage range : AC85V~265V
Continuous Peak output time (τ): Within 10 seconds
Peak output current (Ip) : Within the rated peak output current
Average DC output current (Im) : Within the rated output current, Iav
4-14. Auxiliary Supply
Auxiliary supply (5V, 0.3A max) is provided to ease customer application. Aux voltage is always available as long as
input power in the specified voltage range is present.
4-15. Output Dynamic Load Response
During output dynamic load test from no load condition, the output voltage level might experience a higher voltage dip
of 15% (typ).
For example, VIN = 230VAC Dynamic Load = 0% - 100% Ta = 25degC, the output voltage level dip will be -15% (typ).
Ip : Peak output current (A)
Iav : Rated output current (A)
Im : Average output current (A)
τ: Peak current pulse width
(sec)
T : Period (sec)
0A
Im
Ip
τ
T
(Ip-a) xτ
T
Im = + a Iav
Duty = x100(%) 35(%)
τ
T
aA
Isolation mm Ill' Ill' Hr? Ill' II}- wkhs‘und voltage T551"
11
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
5. Isolation / Withstand Voltage
5-1. Isolation Test
Isolation resistance between output and (chassis) shall be more than 100Mat 500VDC. For safety, voltage setting
of DC isolation tester must be done before the test. Ensure that the unit is fully discharged after the test.
(a) Output ~ (chassis) : 500VDC, 100Mor more
5-2. Withstand Voltage
This series is designed to withstand 4.25kVDC between input and output, 2.25kVDC between input and (chassis)
and 500VDC between output and (chassis) each for 1 minute. When testing withstand voltage, set current limit of
withstand voltage test equipment at 20mA ( Output - (chassis) : 100mA ). The applied voltage must be gradually
increased from zero to testing value and then gradually decreased for shut down. When timer is used, the power supply
may be damaged by high impulse voltage at timer switch on and off. Connect input and output as follows:
(a) Input ~ (chassis) : solid line (c) Output ~ (chassis) : 500VDC, 1min (100mA)
2.25kVDC, 1min (20mA)
(b) Input ~ Output : dotted line
4.25kVDC, 1min ( 20mA )
I I I _r__ I w-----r---"r-----r-----r----- _ _ _ _ r _ _ _ _ _ F _ _ _ _ _ _ G: 934
12
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
6. Mounting Directions
6-1. Output Derating according to the Mounting Directions
Recommended standard mounting is Method ( A ). Method ( B ) is also possible.
Refer to the Derating below.
(A) Standard Mounting (B)
6-2. Output Derating
For /L and /F option, the system is forced air cooling with external airflow of at least 15cfm and air blowing out from the
opposite side of the input/output connectors.
70
50
Airflow
(≥ 15 cfm)
OUTPUT DERATING CURVE
0
20
40
60
80
100
120
-25 0 25 50 75 100
Ta (oC)
MOUNTING
A,B
70
50
*DIB/Qm mfimfifia mmmmmmm D1 #
13
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
The Output Derating with external fan depends on the airflow conditions and the temperature rise for the components.
The method stipulated below provides a way to decide for the safe operation of this power supply. As shown, this table
provides a list of the maximum temperature allowed for specified components. The component temperature is measured
according to IEC60950-1 2nd edition Clause 4.5.
Maximum rated temperature for these components are taken from the component specification provided by the original
manufacturers. These are the worse case allowable temperature.
Temperature is measured using thermal couple K-type, and using CYANOACRYLATE adhesive or equivalent to secure
to the hottest point of these components.
In order to decide the worse case temperature rise, the selected measurement point should not face direct airflow and the
equipment powered should operate under worse case operating conditions.
*1. Absolute temperature (Maximum temperature) during normal operating conditions. Higher temperature will probably
cause shorter life span for the power supply.
Please refer to the component side layout drawing below for temperature measurement. Airflow should cool down all the
components evenly.
Location No Parts Name Maximum Temperature (oC) *1
D1 Bridge Diode 112 (130)
D16/Q10 Schottky Diode/Mosfet 109 (130)
Q1 Mosfet 123 (130)
Q4 Mosfet 102 (130)
T1 Transformer 125 (130)
More than 50mm More than 50mm § I:> ‘ z \ AIR mow TOP F 7 BACK sum ~n I:> 2”" AIR FLOW FRONT SIDE EEEEEEE ELLV’HEIWVN
14
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
6-3 Mounting Method
1) This is forced air cooling type power supply. In consideration of the heat radiation and safety, please keep a distance
of more than 50mm between the power supply front & back.
2) Maximum allowable penetration of mounting screws into the power-supply is 5mm.
3) Recommended torque for mounting screws (M4): 1.27 Nm (13.0 kgfcm).
4) For /L option, please provide clearance 4mm or more on top of power supply to peripheral parts.
7. Wiring Method
The input and output load wires shall be separated to improve noise immunity.
Both wires must be as thick and short as possible to have lower impedance.
Noise can be reduced by connecting a film capacitor with 0.1uF capacitance across the load terminals.
For safety and EMI considerations, connect the terminal of GWS500 series to mounting set ground terminal
The recommended wire type :
MODEL Recommended Wire Recommended torque
Recommended crimp-type terminal
D (Max) T (Max) Mounting Pieces (Max)
GWS500 AWG18-10 M4 Screws
1.27 Nm (13 kgfcm) 6.8mm 0.8mm 4
Note 1 : When using separate loads, it is recommended to use 4 pieces of 0.8mm thick crimp-type terminal.
Note 2 : For recommended wire diameter, refer to wire maker recommended allowable current and voltage drop.
8. External Fuse Rating
Refer to the following fuse rating when selecting the external input fuse. Surge current flows when input turns on. Do
not select the fuse according to input current (rms) values under the actual load condition.
GWS500 : F10AH , 250V
s 5 A fitioxrui m w Flu exh-um mun-n ("O t [S at fault, Ple
15
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
9. Fan Life Expectancy.
The fan life has limitation. Therefore, periodic maintenance by exchanging the life-expired fan is required for the power
supply. The following figure shows the life of fan.
Measurement point of fan exhausts temperature
10. Before concluding that the unit is at fault, Please make the following checks.
(1) Check if the rated input voltage is connected and within specification.
(2) Check if the wiring of input and output is correct.
(3) Check if the I/O terminal connection is properly tightened by required torque.
(4) Check if the wire thickness is enough.
(5) Check if the output voltage trimmer (V.ADJ) is properly adjusted. OVP might be triggered and output is
shutdown.
(6) Is the chassis of power supply abnormally hot? The output is shutdown by OTP operation. Please disconnect or
turn off the AC input and let the unit cool down sufficiently before turning ON the AC input again.
(7) Check if the output current and output wattage does not exceed the specification.
(8) Audible noise may be heard when input voltage waveform is not sinusoidal.
(9) Audible noise may be heard during dynamic load operation.
(10) Ensure that a large capacitor is not connected across the output terminals. Please use within maximum
capacitance shown below.
Maximum external capacitance
MODEL 12V 24V 36V 48V
GWS500 10,000uF 5,000uF 1,000uF
Air Flow
P.S.
50mm
Temperature
measurement point
FRONT SIDE
16
TDK-Lambda
GWS 500 Series
INSTRUCTION MANUAL
11. Warranty Condition
This product is under warranty for 5 years from the date of shipment. During the warranty period, TDK-Lambda will, at
its option, either repair or replace products prove to be defective. However, the built-in FAN motor replacement is
charged. Please contact to our sales office for FAN replacement.
Warranty applies but not limited to the following.
(1) Average operating temperature (ambient temperature of the power supply unit) is under 40oC.
(2) Average load factor is 80% or less.
(3) Installation method: Standard installation.
Following cases will not be covered by warranty.
(1) Improper usage and mis-handling like dropping or applying shock to the unit and defects from operation exceeding
specification of the product.
(2) Defects resulting from natural disaster (fire, flood).
(3) Unauthorized modification or repair.