Extractor Tool for 1 .50mm (.059") GP Cnmp Termmals KN® molex \_/ Prod ucts DRIVER
Extractor Tool for 1.50mm (.059") CP Crimp Terminals
Doc No: ATS-638132300 Release Date: 04-11-07 UNCONTROLLED COPY Page 1 of 2
Revision: B Revision Date: 01-27-09
Extractor Tool
Instruction Sheet
Order No. 63813-2300
FEATURES
This Extractor Tool is for the removal of 98915 & 64323 Series female terminals from CMC connector.
SCOPE
Products: 1.50mm (.059") CP Crimp Terminal for CMC connector.
Terminal Series No.
Terminal Order No.
98915-1029
98915-1039
98915-1219
98915
98915-1319
64323-1029
64323-1039
64323-1219
64323
64323-1319
OPERATION:
When removing a damaged crimped wire from the CMC connector follow the steps below:
1. The secondary lock on the CMC connector will need to be opened first. See Figure 1.
2. Using a screwdriver insert the flat edge under the tab of the secondary lock and pull up. Use your fingers
to open the lock completely.
SECONDARY LOCK
Figure 1
SCREWDRIVE
R
CMC
CONNECTOR
WIRE
Extractor Tool for 1 .50mm (.059") GP Cnmp Termmals
Extractor Tool for 1.50mm (.059") CP Crimp Terminals
Doc No: ATS-638132300 Release Date: 04-11-07 UNCONTROLLED COPY Page 2 of 2
Revision: B Revision Date: 01-27-09
ORIENT BLADES INTO
HOUSING CAVITIES
PUSH
EXTRACTOR
TOOL INTO
FRONT FACE
Figure 2
CRIMPED WIRE
MARKINGS ON
BACK
AND FRONT OF HOUSING
SECONDARY
LOCK OPEN
3. Position the blades of the extraction tool into the two small cavities of the slot in the front face of the housing as
shown in Figure 2. Use the identifying markings on both the front and back of the connector to locate the opening
used to extract the crimped wire.
4. Push extractor tool into the desired slot until it clicks or comes to a stop. Do not force the extractor tool any
further or there can be damage to the housing.
5. Gently push the wire forward towards the housing and then pull out of the CMC housing.
6. Molex does not offer repair parts for Extractor Tools due to the inexpensive nature of these tools.
Americas Headquarters
Lisle, Illinois 60532 U.S.A.
1-800-78MOLEX
amerinfo@molex.com
Far East North Headquarters
Yamato, Kanagawa, Japan
81-462-65-2324
feninfo@molex.com
Far East South Headquarters
Jurong, Singapore
65-6-268-6868
fesinfo@molex.com
European Headquarters
Munich, Germany
49-89-413092-0
eurinfo@molex.com
Corporate Headquarters
2222 Wellington Ct.
Lisle, IL 60532 U.S.A.
630-969-4550
Fax: 630-969-1352
Visit our Web site at http://www.molex.com