0011020001 Instr Sheet Datasheet by Molex

View All Related Products | Download PDF Datasheet
Insertinn Tonl /'\® molex \_/ TERMINAL INSERTION:
Insertion Tool
Doc No. 11-02-0001 Release Date: 07-25-02 UNCONTROLLED COPY Page 1 of 1
Revision: B Revision Date: 02-17-04
Insertion Tool
Instruction Sheet
Order No. 11-02-0001
(HT-1807)
This Insertion tool is used for insertion of .062”diameter series pin and socket male and female terminals in plug
and receptacle housings. This tool is designed to assure proper seating of terminals and reduce operator fatigue.
TERMINAL INSERTION:
Individual terminals may be inserted in the housing using
this Insertion tool.
1) To properly use this tool, with the flat side facing up,
place the ring over the ring finger past the first joint
(See Figure 1). Place the wire in the groove of the
tool so that the terminal is touching the end of tool
(See Figure 2).
2) With your thumb securely holding the wire in the
groove, push the terminal into the housing as far as
the shoulder on the tool will permit. The terminal
then should be locked in place.
Optional: The terminal can be partially inserted in
the terminal housing first, and then the Insertion tool
can be used to firmly seat the terminal.
Molex Tooling Group
1150 E. Diehl Road
Naperville, IL 60563
(630) 969-4550; FAX (630) 505-0049
Figure 1
WIR
E
RING OF
TOOL OVER
FINGER
Figure
2
INSERTIO
N
TOO
L
TERMINA
L
TERMINA
L
AGAINST
TOO
L

Products related to this Datasheet

INSERTION TOOL HT1807