HT-71800 Extractor Tool
Doc No. 11-03-0036 Release Date: 05-29-85 UNCONTROLLED COPY Page 1 of 2
Revision: C Revision Date: 02-18-02
Insertion / Extractor Tool
Instruction Sheet
Order No. 11-03-0036
(HT-71800)
For the removal of SL Modular Interconnection Product Wire-to-Wire and Wire-to-Board Terminal series in interim clips or panel mount
modules, and both male and female crimp terminals.
TERMINAL EXTRACTION:
Individual terminals may be removed from the housing using this
SL tool.
1. Push the terminal forward in the housing so that the locking
tang is clearly visible. Using the tab labeled “M” on the SL
tool, insert into the slot on the back of the housing and firmly
depress the locking tang until the shoulder rests upon the
housing.
2. Carefully pull the terminated wire out of the connector in the
direction of the arrow in Figure 1.
LOCKING-TANG RESET:
Once the terminated wire is extracted, the locking tang will need to be repositioned in order to obtain retention in the housing.
1. Insert the probe of the SL tool under the depressed locking tang as shown in Figure 2.
2. Gently pivot the SL tool towards the I.D. slots until the tang is bent up into original position and the scribe line is parallel to the
body of the terminal see Figure 3. Pull out the SL tool and the terminal now can be re-inserted into the housing.
TERMINAL
Figure 2
WIRE
SL TOOL
TERMINAL
Figure 3
WIRE
SL TOOL
PARALLEL
HOUSING OR
MODULE
Figure 1
SL TOOL
WIRES
19.05
.75
86.75
3.40

HT-71800 Extractor Tool
Doc No. 11-03-0036 Release Date: 05-29-85 UNCONTROLLED COPY Page 2 of 2
Revision: C Revision Date: 02-18-02
Figure 5
CLIP INTERIM
HOUSING
WIRE
CLIP
SL TOOL
SL TOOL
PANEL
MOUNT WIRE
HOUSING
Figure 6
PANEL MOUNT
TERMINAL EXTRACTION FROM INTERIM OR PANEL MOUNT CLIP:
Most of the interim clips have small slots either on the top or the bottom of the part depending on
the size of the clip. Smaller clips less then 12 circuits have the slots on the bottom. (Figure 4 is
oriented from the bottom.) If there are no slots for extraction, then housings must be removed
from clip.
To extract terminals:
1. Push the terminal forward in the interim clip or module and the housing or so that the locking
tang is clearly visible. Using the tab labeled “C” on the SL tool insert into the slot on the back
of the clip. Firmly depress the locking tang.
2. Pull the terminated wire out in the direction of the arrow. See Figure 4.
HOUSING EXTRACTION:
This operation is used to remove a housing from an interim clip or panel mount clip.
1. Slide the SL tool under the plastic tab on the clip or panel mount and lift up. Carefully open only far enough to extract the
housing.
2. Pull the housing out in the direction of the arrow. See Figure 2.
Molex Application Tooling Group
1150 E. Diehl Road
Naperville, IL 60563
Tel: (630) 969-4550
Fax: (630) 505-0049
WIRE
Figure 4
SL TOOL
INTERIM
C
LIP
Products related to this Datasheet
TOOL HAND EXTRACTION