Pi RTC (DS1307) Datasheet by Seeed Technology Co., Ltd

View All Related Products | Download PDF Datasheet
«bseeed
Pi RTC (DS1307)
The Pi RTC is based on the clock chip DS1307, it can provide a real-time clock(RTC) for raspberry pi via the I2C interface. Real-time clock of
this module counts seconds,minutes, hours, date of the month,month, day of the week, and year with leap-year compensation valid up to
2100. The clock operates in either the 24-hour or 12-hour format with AM/PM indicator. If you want to keep this module timing when the
Raspberry Pi is powered off, you need to put a 3-Volt CR1225 lithium cell in the battery-holder.
Note
The battery is not included.
Features
Support Raspberry Pi 2/ 3 B/B+ Zero
Suport seconds,minuutes,hours,day of week,month, year
Support 24-hour or 12-hour format with AM/PM indicator
56-byte, battery-backed, nonvolatile (NV) RAM for data storage
Two-wire serial interface
Programmable squarewave output signal
Automatic power-fail detect and switch circuitry
GND GP|O7 SCL_3V3 SDA_3V3 3V3 RX TX GND SV SV
Specification
Item Value
Operating Voltage 5V
Interface I2C
I2C Address 0x68
Typical applications
Any applications need Real Time on Raspberry.
Pin Out
Note
RX/TX is not used in this module, but the 5x2 header takes up the RX/TX pin of the Raspberry Pi, so we bring the RX/TX out and come with
a 2pin header.
2N7002A, ANIMM
Schemaitc
Bi-directional level shifter circuit
This is a typical Bi-directional level shifter circuit to connect two different voltage section of an I2C bus. The I2C bus of Raspberry Pi uses
3.3V, however the chip DS1307 works at 5V, so this circuit will be needed. In the schematic above, Q1 and Q2 are N-Channel MOSFET
2N7002A, which act as a bidirectional switch. In order to better understand this part, you can refer to the AN10441
Platforms Supported
Arduino Raspberry Pi BeagleBone Wio LinkIt ONE
Getting Started
Materials required
Raspberry Pi Pi RTC(DS1307)
Note
Please plug the USB cable gently, otherwise you may damage the port. Please use the USB cable with 4 wires inside, the 2 wires cable can't
transfer data. If you are not sure about the wire you have, you can click here to buy
Install
The driver we provide only applied for Raspbian Jessie/Stretch.
Tip
If you do not know how to use a raspberry pi, please check here before start.
Step 1. Driver Installation
Tap the following command in your terminal
1 git clone https://github.com/Seeed-Studio/pi-hats.git
When the download finish, tap the following command in your terminal
1
2 cd pi-hats
sudo ./install.sh -u rtc_ds1307
Step 2. Power off Raspberry Pi
1 sudo shutdown -h now
Step 3. Insert the HAT to Raspberry Pi
Please make sure plug the pin 1 of this hat into the pin 1 of raspberry GPIO, just like the picture above.
Step 4. Power up Raspberry Pi
Usage
Now you can use the command to check whether the driver is installed successfully.
1 ./install.sh -l
If you want uninstall the driver you can use the command below:
1 sudo ./install.sh -u
Now let's see what the RTC module can do:
Read hardware clock and print result
1 sudo hwclock -r
Set the system time from the hardware clock
1 sudo hwclock -s
Set the hardware clock from the current system time
1 sudo hwclock -w
More usage
1 hwclock --help
Tech Support
Please do not hesitate to submit the issue into our forum
http://wiki.seeedstudio.com/Pi_RTCDS1307/12418

Products related to this Datasheet

PI RTC (DS1307)