114,115,117 Users Manual Datasheet by Fluke Electronics
View All Related Products | Download PDF Datasheet
®
PN 2572573
July 2006, Rev. 1, 2/07
© 2006, 2007 Fluke Corporation, All rights reserved. Printed in China
All product names are trademarks of their respective companies.
114, 115, and 117
True-rms Multimeters
Users Manual
LIMITED WARRANTY AND LIMITATION OF LIABILITY
This Fluke product will be free from defects in material and workmanship for three
years from the date of purchase. This warranty does not cover fuses, disposable bat-
teries, or damage from accident, neglect, misuse, alteration, contamination, or abnor-
mal conditions of operation or handling. Resellers are not authorized to extend any
other warranty on Fluke’s behalf. To obtain service during the warranty period, contact
your nearest Fluke authorized service center to obtain return authorization information,
then send the product to that Service Center with a description of the problem.
THIS WARRANTY IS YOUR ONLY REMEDY. NO OTHER WARRANTIES, SUCH AS
FITNESS FOR A PARTICULAR PURPOSE, ARE EXPRESSED OR IMPLIED. FLUKE
IS NOT LIABLE FOR ANY SPECIAL, INDIRECT, INCIDENTAL OR CONSEQUEN-
TIAL DAMAGES OR LOSSES, ARISING FROM ANY CAUSE OR THEORY. Since
some states or countries do not allow the exclusion or limitation of an implied warranty
or of incidental or consequential damages, this limitation of liability may not apply to
you.
Fluke Corporation
P.O. Box 9090
Everett, WA 98206-9090
U.S.A.
Fluke Europe B.V.
P.O. Box 1186
5602 BD Eindhoven
The Netherlands
11/99

1
True-rms Multimeters
Introduction
The Fluke Model 114, Model 115, and Model 117 are
battery-powered, true-rms multimeters (hereafter "the
Meter") with a 6000-count display and a bar graph. This
manual applies to all three models. All figures show the
Model 117.
These meters meet CAT III IEC 61010-1 2nd Edition
standards. The IEC 61010-1 2nd Edition safety standard
defines four measurement categories (CAT I to IV)
based on the magnitude of danger from transient
impulses. CAT III meters are designed to protect
against transients in fixed-equipment installations at the
distribution level.
Contacting Fluke
To contact Fluke, call:
USA: 1-888-99-FLUKE (1-888-993-5853)
Canada: 1-800-36-FLUKE (1-800-363-5853)
Europe: +31 402-675-200
Japan: +81-3-3434-0181
Singapore +65-738-5655
Anywhere in the world: +1-425-446-5500
Visit Fluke's web site at www.fluke.com.
Register your Meter at register.fluke.com.
Unsafe Voltage
To alert you to the presence of a potentially
hazardous voltage, the Y symbol is displayed when
the Meter measures a voltage ≥30 V or a voltage
overload (OL) condition. When making frequency
measurements >1 kHz, the Y symbol is unspecified.
Test Lead Alert
XWWarning
Personal injury or damage to the
Meter can occur if you attempt to
make a measurement with a lead in an
incorrect terminal.
To remind you to check that the test leads are in the
correct terminals, LEAd is briefly displayed and an
audible beep sounds when you move the rotary
switch to or from any A (Amps) position.

114, 115, and 117
Users Manual
2
Safety Information
A "XWWarning" statement identifies hazardous conditions and actions that could cause bodily harm or death.
A "WCaution" statement identifies conditions and actions that could damage the Meter or the equipment under test.
To avoid possible electric shock or personal injury, follow these guidelines:
• Use the Meter only as specified in this manual or the protection provided by the Meter might
be impaired.
• Do not use the Meter or test leads if they appear damaged, or if the Meter is not operating
properly.
• Always use proper terminals, switch position, and range for measurements.
• Verify the Meter's operation by measuring a known voltage. If in doubt, have the Meter
serviced.
• Do not apply more than the rated voltage, as marked on Meter, between terminals or
between any terminal and earth ground.
• Use caution with voltages above 30 V ac rms, 42 V ac peak, or 60 V dc. These voltages pose
a shock hazard.
• Disconnect circuit power and discharge all high-voltage capacitors before testing
resistance, continuity, diodes, or capacitance.
• Do not use the Meter around explosive gas or vapor.
• When using test leads or probes, keep your fingers behind the finger guards.
• Only use test leads that have the same voltage, category, and amperage ratings as the meter
and that have been approved by a safety agency.
• Remove test leads from Meter before opening the battery door or Meter case.

True-rms Multimeters
Safety Information
3
• Comply with local and national safety requirements when working in hazardous locations.
• Use proper protective equipment, as required by local or national authorities when working
in hazardous areas.
• Avoid working alone.
• Use only the replacement fuse specified or the protection may be impaired.
• Check the test leads for continuity before use. Do not use if the readings are high or noisy.
• Do not use the Auto Volts function to measure voltages in circuits that could be damaged by
this function’s low input impedance (≈3 kΩ)(114 and 117 only).
Symbols
B AC (Alternating Current) I Fuse
F DC (Direct Current) T Double Insulated
X Hazardous voltage W Important Information; Refer to manual
N Battery (Low battery when shown on the
display.) J Earth ground
~ Do not dispose of this product as unsorted
municipal waste. Contact Fluke or a
qualified recycler for disposal.
D AC and DC

114, 115, and 117
Users Manual
4
Display
VoltAlert
11
7
17 18
12
13
14
9
6
5
4
3
2
1
16 15
8
10
edy02f.eps
No. Symbol Meaning Model
A w The Meter is in the VoltAlert™ non-contact voltage detect mode. 117
B s The Meter function is set to Continuity. 114, 115, & 117
C R The Meter function is set to Diode Test 115 & 117
D O Input is a negative value. 114, 115, & 117
E Y X Unsafe voltage. Measured input voltage ≥30 V, or voltage
overload condition (OL). 114, 115, & 117

True-rms Multimeters
Display
5
F K Display hold enabled. Display freezes present reading. 114, 115, & 117
G M
VWX
MIN MAX AVG mode enabled.
Maximum, minimum, average or present reading displayed 114, 115, & 117
H (Red LED) Voltage presence through the non-contact VoltAlert sensor 117
I LoZ The Meter is measuring voltage or capacitance with a low input
impedance. 114, 115 & 117
J nµF mVµA
MkΩ kHz Measurement units. 114, 115, & 117
K DC AC Direct current or alternating current 114, 115 & 117
L N Battery low warning. 114, 115, & 117
M 610000 mV Indicates the Meter’s range selection. 114, 115, & 117
N (Bar graph) Analog display. 114, 115, & 117
O Auto Volts
Auto
Manual
The Meter is in the Auto Volts function.
Autoranging. The Meter selects the range for best resolution.
Manual ranging. User sets the Meter’s range.
114 & 117
114, 115, & 117
114, 115, & 117
P + Bar graph polarity 114, 115, & 117
Q 0L W The input is too large for the selected range. 114, 115, & 117
R LEAd W Test lead alert. Briefly displayed whenever the Meter’s
function switch is rotated to or from any A position. 115 & 117

114, 115, and 117
Users Manual
6
Terminals
10 A
FUSED
COM V
A
1
2
3
edy01f.eps
No. Description Model
A Input terminal for measuring ac and dc current to 10 A. 115 & 117
B Common (return) terminal for all measurements. 114, 115, & 117
C Input terminal for measuring voltage, continuity, resistance, capacitance,
frequency and testing diodes. 114, 115, & 117
Error Messages
bAtt Battery must be replaced before the Meter will operate.
CAL Err Calibration required. Meter calibration is required before the Meter will operate.
EEPr Err Internal error. The Meter must be repaired before it will operate.
F11 Err Internal error. The Meter must be repaired before it will operate.

True-rms Multimeters
Rotary Switch Positions
7
Rotary Switch Positions
Switch
Position Measurement Function Model
x Automatically selects ac or dc volts based on the sensed input with a low
impedance input. 114 & 117
e
Hz (button)
AC voltage from 0.06 to 600 V.
Frequency from 5 Hz to 50 kHz.
114, 115 & 117
115 & 117
D DC voltage from .001 V to 600 V. 114, 115 & 117
l AC voltage from 6.0 to 600 mV, dc-coupled. DC voltage from 0.1 to 600 mV. 114, 115 & 117
Ω Ohms from 0.1 Ω to 40 MΩ. 114, 115 & 117
s Continuity beeper turns on at < 20 Ω and turns off at >250 Ω. 114, 115 & 117
R Diode Test. Displays OL above 2.0 V. 115 & 117
S Farads from 1 nF to 9999 μF. 115 & 117
j
Hz (button)
AC current from 0.1 A to 10 A (>10 to 20 A, 30 seconds on, 10 minutes off).
>10.00 A display flashes. >20 A, OL is displayed. DC-coupled.
Frequency from 45 Hz to 5 kHz.
115 & 117
I DC current from 0.001 A to 10 A (>10 to 20 A, 30 seconds on, 10 minutes off).
>10.00 A display flashes. >20 A, OL is displayed. 115 & 117
w Non-contact sensing of ac voltage. 117
Note: All ac functions and Auto-V LoZ are true-rms. AC voltage is ac-coupled. Auto-V LoZ, AC mV and AC
amps are dc-coupled.

114, 115, and 117
Users Manual
8
Battery Saver ("Sleep Mode")
The Meter automatically enters "Sleep mode" and blanks
the display if there is no function change, range change, or
button press for 20 minutes. Pressing any button or
turning the rotary switch awakens the Meter. To disable the
Sleep mode, hold down the g button while turning the
Meter on. The Sleep mode is always disabled in the MIN
MAX AVG mode.
MIN MAX AVG Recording Mode
The MIN MAX AVG recording mode captures the minimum
and maximum input values (ignoring overloads), and
calculates a running average of all readings. When a new
high or low is detected, the Meter beeps.
• Put the Meter in the desired measurement function and
range.
• Press p to enter MIN MAX AVG mode.
• Mand MAX are displayed and the highest
reading detected since entering MIN MAX AVG is
displayed.
• Press p to step through the low (MIN), average
(AVG), and present readings.
• To pause MIN MAX AVG recording without erasing
stored values, press f. K is displayed.
• To resume MIN MAX AVG recording, press fagain.
• To exit and erase stored readings, press p for at
least one second or turn the rotary switch.
Display HOLD
XWWarning
To avoid electric shock, when Display
HOLD is activated, be aware that the
display will not change when you
apply a different voltage.
In the Display HOLD mode, the Meter freezes the display.
1. Press fto activate Display HOLD. (K is
displayed.)
2. To exit and return to normal operation, press f or
turn the rotary switch.
Backlight
Press Q to toggle the backlight on and off. The backlight
automatically turns off after 40 seconds. To disable
backlight auto-off, hold down Q while turning the Meter
on.
Manual and Autoranging
The Meter has both Manual and Autorange modes.
• In the Autorange mode, the Meter selects the range with
the best resolution.
• In the Manual Range mode, you override Autorange and
select the range yourself.

True-rms Multimeters
Power-Up Options
9
When you turn the Meter on, it defaults to Autorange and
Auto is displayed.
1. To enter the Manual Range mode, press q.
Manual is displayed.
2. In the Manual Range mode, press qto increment
the range. After the highest range, the Meter wraps to
the lowest range.
Note
You cannot manually change the range in the
MIN MAX AVG or Display HOLD modes.
If you press qwhile in MIN MAX AVG or
Display Hold, the Meter beeps twice, indicating
an invalid operation and the range does not
change.
3. To exit Manual Range, press q for at least 1 second
or turn the rotary switch. The Meter returns to
Autorange and Auto is displayed.
Power-Up Options
To select a Power-Up Option, hold down the button
indicated in the following table while turning the Meter on.
Power-Up Options are canceled when you turn the Meter
off and when sleep mode is activated.
Button Power-Up Options
f Turns on all display segments.
p Disables beeper. bEEP is displayed when
enabled.
q Enables low impedance capacitance
measurements. LCAP is displayed when
enabled. See page 14.
g Disables automatic power-down ("Sleep
mode"). PoFF is displayed when enabled.
Q Disables auto backlight off. LoFF is
displayed when enabled.
Making Basic Measurements
The figures on the following pages show how to make
basic measurements.
When connecting the test leads to the circuit or device,
connect the common (COM) test lead before connecting
the live lead; when removing the test leads, remove the live
lead before removing the common test lead.

114, 115, and 117
Users Manual
10
Measuring Resistance
edy04f.eps
XWWarning
To avoid electric shock, injury, or
damage to the Meter, disconnect
circuit power and discharge all high-
voltage capacitors before testing
resistance, continuity, diodes, or
capacitance.
Testing for Continuity
edy06f.eps
Note
The continuity function works best as a fast,
convenient method to check for opens and
shorts. For maximum accuracy in making
resistance measurements, use the Meter’s
resistance (e) function.

True-rms Multimeters
Making Basic Measurements
11
Measuring AC and DC Voltage
Volts DC Volts AC
V
edy03f.eps
Using Auto Volts Selection (114 & 117 only)
With the function switch in the x position, the Meter
automatically selects a dc or ac voltage measurement
based on the input applied between the V or + and COM
jacks.
This function also sets the Meter’s input impedance to
approximately 3 kΩ to reduce the possibility of false
readings due to ghost voltages.
Measuring AC and DC Millivolts
Millivolts DC Millivolts AC
DC
edy18f.eps
With the function switch in the l position, the Meter
measures ac plus dc millivolts. Press g to switch the
Meter to dc millivolts.

114, 115, and 117
Users Manual
12
Measuring AC or DC Current (115 & 117)
XWWarning
To avoid personal injury or damage to the
Meter:
• Never attempt to make an in-circuit
current measurement when the open-
circuit potential to earth is
>600 V.
• Check the Meter's fuse before testing.
(See “Testing the Fuse”)
• Use the proper terminals, switch
position, and range for your measure-
ment.
• Never place the probes in parallel with a
circuit or component when the leads are
plugged into the A (Amps) terminals.
A
1
2 3
edy08f.eps
Turn circuit power off, break the circuit, insert the Meter in
series with the circuit, and then turn circuit power on.

True-rms Multimeters
Making Basic Measurements
13
Measuring Current above 10 Amps
The millivolt and voltage function of the Meter can be used
with an optional mV/A output Current Probe to measure
currents that exceed the rating of the Meter. Make sure the
Meter has the correct function selected, AC or DC, for your
current probe. Refer to a Fluke catalog or contact your
local Fluke representative for compatible current clamps.
edy14f.eps
Measuring Capacitance (115 & 117 only)
edy05f.eps

114, 115, and 117
Users Manual
14
Measuring Frequency (115 & 117 only)
XWWarning
To avoid electrical shock, disregard the bar
graph for frequencies >1 kHz. If the
frequency of the measured signal is >1 kHz,
the bar graph and Z are unspecified.
VoltAlert
AC Voltage Frequency AC Current Frequency
Hz
edy09f.eps
The Meter measures the frequency of a signal by counting
the number of times the signal crosses a trigger level each
second. The trigger level is 0 V, 0 A for all ranges.
Press g to turn the frequency measurement function
on and off. Frequency works with ac functions only.
In frequency, the bar graph and range annunciator indicate
the ac voltage or current present.
Select progressively lower ranges using manual ranging
for a stable reading.
Detecting AC Voltage Presence (117 only)
VoltAlert
VoltAlert
Lo
Neutral
Hot
RANGE
VoltAlert
edy13f.eps

True-rms Multimeters
Making Basic Measurements
15
To detect the presence of ac voltage, place the top of the
Meter close to a conductor. The Meter gives an audible as
well as visual indication when voltage is detected. There
are two sensitivity settings. The “Lo” setting can be used
on flush mounted wall sockets, power strips, flush
mounted industrial outlets and various power cords. The
“Hi” setting allows for ac voltage detection on other styles
of recessed power connectors or sockets where the actual
ac voltage is recessed within the connector itself. The
VoltAlert detector works in bare wire applications with
voltages as low as 24 V in the “Hi” setting.
XW Warning
If there is no indication, voltage could
still be present. Do not rely on the
VoltAlert detector with shielded wire.
Operation may be effected by
differences in socket design,
insulation thickness and type.
Making Low Impedance Capacitance
Measurements (115 & 117 only)
For making capacitance measurements on cables with
ghost voltage, hold qwhile turning on the Meter to
switch the Meter into LoZ, (low input impedance)
Capacitance mode. In this mode, capacitance
measurements will have a lower accuracy and lower
dynamic range. This setting is not saved when the Meter is
turned off or goes into sleep mode.
Testing Diodes (115 & 117)
Forward Bias
Single
Beep
Reverse Bias
Shorted
and
Open
Bad Diode Bad Diode
Good Diode Good Diode
edy07f.eps

114, 115, and 117
Users Manual
16
Using the Bargraph
The bar graph is like the needle on an analog meter. It has
an overload indicator (>) to the right and a polarity
indicator (+)to the left.
Because the bar graph is much faster than the digital
display, the bar graph is useful for making peak and null
adjustments.
The bar graph is disabled when measuring capacitance. In
frequency, the bar graph and range annunciator indicates
the underlying voltage or current up to 1 kHz.
The number of segments indicates the measured value and
is relative to the full-scale value of the selected range.
In the 60 V range, for example (see below), the major
divisions on the scale represent 0, 15, 30, 45, and 60 V. An
input of −30 V turns on the negative sign and the segments
up to the middle of the scale.
aej11f.eps
Testing the Fuse (115 & 117 only)
Test fuse as shown below.
<.5 OK
OK
edy10f.eps

True-rms Multimeters
Maintenance
17
Maintenance
Maintenance of the Meter consists of battery and fuse
replacement, as well as case cleaning.
Replacing the Battery and Fuse
XWWarning
To avoid shock, injury, or damage to
the Meter:
• Remove test leads from the Meter
before opening the case or battery door.
• Use ONLY a fuse with the amperage,
interrupt voltage, and speed ratings
specified.
To remove the battery door for battery replacement:
1. Remove the test leads from the Meter
2. Remove the battery door screw.
3. Use the finger recess to lift the door slightly.
4. Lift the door straight up to separate it from the case.
The battery fits inside the battery door, which is then
inserted into the case, bottom edge first, until it is fully
seated. Do not attempt to install the battery directly into the
case.
5. Install and tighten battery door screw.
Fuse
edy11f.eps

114, 115, and 117
Users Manual
18
To open the case for fuse replacement:
1. Remove the test leads from the Meter
2. Remove the Meter from its holster.
3. Remove two screws from the case bottom.
4. Separate the case bottom from the case top.
5. Remove the fuse from its holder and replace it with an
11 A, 1000 V, FAST fuse having a minimum interrupt
rating of 17,000 A. Use only Fluke PN 803293.
6. To re-assemble the Meter, first attach the case bottom
to the case top, then install the two screws. Finally,
insert the Meter into its holster.
Cleaning
Wipe the case with a damp cloth and mild detergent. Do
not use abrasives, isopropyl alcohol, or solvents to clean
the case or lens/window. Dirt or moisture in the terminals
can affect readings.

True-rms Multimeters
General Specifications
19
General Specifications
Accuracy is specified for 1 year after calibration, at operating temperatures of 18 °C to 28 °C, with
relative humidity at 0 % to 90 %.
Extended specifications are available at www.Fluke.com.
Maximum voltage between any
terminal and earth ground...................................... 600 V
Surge Protection ..................................................... 6 kV peak per IEC 61010-1 600V CAT III,
Pollution Degree 2
W Fuse for A input (115 & 117 only): .................... 11 A, 1000 V FAST 17 kA Fuse (Fluke PN 803293)
Display ..................................................................... Digital: 6,000 counts, updates 4/sec
Bar Graph: 33 segments, updates 32/sec
Temperature............................................................. Operating: -10 °C to + 50 °C
Storage: -40 °C to + 60 °C
Temperature Coefficient......................................... 0.1 x (specified accuracy)/°C (<18 °C or >28 °C)
Operating Altitude ................................................... 2,000 meters
Battery....................................................................... 9 Volt Alkaline, NEDA 1604A / IEC 6LR61
Battery Life............................................................... Alkaline: 400 hours typical, without backlight
Safety Compliances ................................................ Complies with ANSI/ISA 82.02.01 (61010-1) 2004,
CAN/CSA-C22.2 No 61010-1-04, UL 6101B (2003)
and IEC/EN 61010-1 2nd Edition for measurement
Category III, 600 V, Pollution Degree 2, EMC
EN61326-1

114, 115, and 117
Users Manual
20
Certifications ............................................................UL, P, CSA, TÜV, ; (N10140), VDE
IP Rating (dust and water protection) ......................... IP42
Table 1. Accuracy Specifications
Function Range Resolution Accuracy
± ([% of Reading] + [Counts]) Model
DC millivolts 600.0 mV 0.1 mV 0.5 % + 2 114,
115, 117
DC Volts 6.000 V
60.00 V
600.0 V
0.001 V
0.01 V
0.1 V 0.5 % + 2 114,
115, 117
DC, 45 to 500 Hz 500 Hz to 1 kHz
Auto-V LoZ[1] True-rms 600.0 V 0.1 V 2.0 % + 3 4.0 % + 3 114, 117
45 to 500 Hz 500 Hz to 1 kHz
AC millivolts[1] True-
rms 600.0 mV 0.1 mV 1.0 % + 3 2.0 % + 3 114,
115, 117
AC Volts[1] True-rms 6.000 V
60.00 V
600.0 V
0.001 V
0.01 V
0.1 V 1.0 % + 3 2.0 % + 3 114,
115, 117

True-rms Multimeters
General Specifications
21
Table 1 Accuracy Specifications (cont.)
Function Range Resolution Accuracy
± ([% of Reading] + [Counts]) Model
Continuity 600 Ω 1 Ω Beeper on < 20 Ω, off > 250 Ω;
detects opens or shorts of
500 μs or longer.
114, 115,
117
Ohms
600.0 Ω
6.000 kΩ
60.00 kΩ
600.0 kΩ
6.000 MΩ
40.00 MΩ
0.1 Ω
0.001 kΩ
0.01 kΩ
0.1 kΩ
0.001 MΩ
0.01 MΩ
0.9 % + 2
0.9 % + 1
0.9 % + 1
0.9 % + 1
0.9 % + 1
5 % + 2
114, 115,
117
Diode test 2.000 V 0.001 V 0.9 % + 2 115, 117
Capacitance 1000 nF
10.00 μF
100.0 μF
9999 μF
1 nF
0.01 μF
0.1 μF
1 μF
1.9 % + 2
1.9 % + 2
1.9 % + 2
100 μF - 1000 μF: 1.9 % + 2
> 1000 μF: 5 % + 20
115, 117
Lo-Z Capacitance
(Power-up option) 1 nF to 500 μF 10% + 2 typical 115, 117

114, 115, and 117
Users Manual
22
Table 1 Accuracy Specifications (cont.)
Function Range Resolution
Accuracy
± ([% of Reading] + [Counts]) Model
AC Amps True-
rms[1]
(45 Hz to 500 Hz)
6.000 A
10.00 A[3]
20 A for 30 seconds max.,
10 minutes rest min.
0.001 A
0.01 A 1.5 % + 3 115, 117
DC Amps
6.000 A
10.00 A[3]
20 A for 30 seconds max.,
10 minutes rest min.
0.001 A
0.01 A 1.0 % + 3 115, 117
Hz (V or A input)[2]
99.99 Hz
999.9 Hz
9.999 kHz
50.00 kHz
0.01 Hz
0.1 Hz
0.001 kHz
0.01 kHz
0.1 % + 2 115, 117
Notes:
[1] All ac ranges except Auto-V LoZ are specified from 1 % to 100 % of range. Auto-V LoZ is specified from 0.0 V.
Because inputs below 1 % of range are not specified, it is normal for this and other true-rms meters to display non-
zero readings when the test leads are disconnected from a circuit or are shorted together. For volts, crest factor of
≤3 at 4000 counts, decreasing linearly to 1.5 at full scale. For amps, crest factor of ≤3. AC volts is ac-coupled. Auto-
V LoZ, AC mV, and AC amps are dc-coupled.
[2] AC Volts Hz is ac-coupled and specified from 5 Hz to 50 kHz. AC Amps Hz is dc-coupled and specified from 45 Hz
to 5 kHz.
[3] >10 A unspecified.

True-rms Multimeters
General Specifications
23
Table 2. Input Characteristics
Function Input Impedance
(Nominal)
Common Mode Rejection Ratio
(1 kΩ Unbalanced)
Normal Mode
Rejection
Volts AC >5 MΩ <100 pF >60 dB at dc, 50 or 60 Hz
Volts DC >10 MΩ <100 pF >100 dB at dc, 50 or 60 Hz >60 dB at 50 or 60
Hz
Auto-V LoZ ~3 kΩ <500 pF >60 dB at dc, 50 or 60 Hz
Open Circuit Test Voltage Full Scale Voltage Short Circuit
Current
To 6.0 MΩ 40 MΩ Ohms <2.7 V dc
<0.7 V dc <0.9 V dc
<350 μA
Diode Test <2.7 V dc 2.000 V dc <1.2 mA

114, 115, and 117
Users Manual
24