KM4o Installation Manual TDK-Lambda General Safeg lnstruclions: A
Page 1 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
ENGLISH
General Safety Instructions:
READ SAFETY INSTRUCTIONS
Servicing:
These products are not customer serviceable TDK-Lambda UK LTD and their authorised agents only are permitted
to carry out repairs.
Critical Components:
These products are not authorised for use as critical components in nuclear control systems, life support systems or
equipment for use in hazardous environments without the express written approval of the Managing Director of TDK-
Lambda EMEA.
Product Usage:
These products are designed for use within a host equipment which restricts access to authorised competent
personnel.
This product is a component power supply and is only to be installed by qualified persons within other equipment and
must be not operated as a stand alone product.
This product is for sale to business to business customers and can be obtained via distribution channels.
It is not intended for sale to end users.
This product is a component power supply and does not fall within the scope of the EMC directive. Compliance with
the EMC directive must be considered in the final installation. Please contact your local TDK-Lambda office.
Environmental:
These products are IPX0, and therefore chemicals/solvents, cleaning agents and other liquids must not be used.
Environment:
This power supply is a switch mode power supply for use in applications within a Pollution Degree 2, overvoltage
category II environment. Material Group IIIb PCB’s are used within it.
Output Loading:
The output power taken from the power supply must not exceed the rating stated on the power supply label, except
as stated in the product limitations in this handbook.
Input Parameters:
This product must be operated within the input parameters stated in the product limitations in this handbook.
End of Life Disposal:
The unit contains components that require special disposal. Make sure that the unit is properly disposed of at the
end of its service life and in accordance with local regulations.
RISK OF ELECTRIC SHOCK
High Voltage Warning:
Dangerous voltages are present within the power supply. The professional installer must protect service personnel
from inadvertent contact with these dangerous voltages in the end equipment.
WARNING: When installed in a Class 1 end equipment, this product must be reliably earthed and professionally
installed.
The (+) or (-) output(s) can be earthed or left floating.
The unit cover(s)/chassis (where applicable) must not be made user accessible.
The mains input connector is not acceptable for use as field wiring terminals.
KM40 lnstallalion Manual TDK-Lambda
Page 2 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
For encased products, do not use mounting screws, which penetrate the unit more than; See drawings.
Internal fuses protect the unit and must not be replaced by the user. In case of internal defect, the unit must be
returned to TDK-Lambda UK LTD or one of their authorised agents.
A suitable mechanical, electrical and fire enclosure must be provided by the end use equipment for mechanical,
electric shock and fire hazard protection.
The unit cover/chassis, where applicable, is designed to protect skilled personnel from hazards. They must not be
used as part of the external covers of any equipment where they may be accessible to operators, since under full
load conditions, part or parts of the unit chassis may reach temperatures in excess of those considered safe for
operator access.
KM4o Installation Manual TDK-Lambda All emeine Sicherheitsvorschrillen: A
Page 3 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
DEUTSCH
Allgemeine Sicherheitsvorschriften:
LESEN SIE DIE SICHERHEITSVORSCHRIFTEN
Wartung:
Diese Produkte können nicht durch den Kunden gewartet werden. Nur TDK-Lambda UK LTD. und deren
zugelassene Vertriebshändler sind zur Durchführung von Reparaturen berechtigt.
Kritische Komponenten:
Diese Produkte sind nicht für die Verwendung als kritische Komponenten in nuklearen Kontrollsystemen,
Lebenserhaltungssystemen oder Geräten in gefährlichen Umgebungen geeignet, sofern dies nicht ausdrücklich und
in Schriftform durch den Geschäftsführer von TDK-Lambda EMEA genehmigt wurde.
Produktverwendung:
Diese Produkte sind zur Verwendung innerhalb von Host-Anlagen gedacht, die einen auf das Fachpersonal
beschränkten Zugang haben.
Dieses Produkt ist eine Stromversorgungs-Komponente und sie darf nur von qualifiziertem Personal in andere
Geräte eingebaut werden und sie darf NICHT als eigenständiges ("Stand-Alone") Gerät betrieben werden.
Dieses Produkt ist für den Verkauf an Geschäftskunden entwickelt worden und es kann über Distributionskanäle
bezogen werden.
Es ist NICHT für den Verkauf an Endkunden gedacht und konzipiert.
Dieses Produkt ist eine Stromversorgungsbaugruppe und sie fällt NICHT in den Bereich der EMV Direktive.
Die Konformität mit der EMV Richtlinie muss in der finalen Gesamtinstallation betrachtet werden.
Bitte kontaktieren Sie Ihr regionales TDK-Lambda Vertriebsbüro im Falle von Rückfragen.
Umwelt:
Diese Produkte sind IPX0, aus diesem Grund dürfen keine Chemikalien/Lösungsmittel, Reinigungsmittel und andere
Flüssigkeiten verwendet werden.
Umgebung:
Dieses Netzteil ist ein Schaltnetzteil zur Verwendung in einer Umgebung mit einem Verschmutzungsgrad 2,
Überspannungskategorie II. Materialgruppe IIIb mit darin verwendeten PCBs.
Ausgangsstrom:
Der Ausgangsstrom des Netzteiles darf die Leistung, die auf dem Label des Netzteiles vermerkt ist, nur dann
überschreiten, wenn dies in den Produktgrenzen dieses Handbuches ausgezeichnet ist.
Eingangsparameter:
Dieses Produkt muss innerhalb der Eingangsparameter, die in den Produktgrenzen dieses Handbuches angegeben
sind, betrieben werden.
Entsorgung am Ende der Betriebszeit:
Das Gerät enthält Komponenten die unter Sondermüll fallen. Das Gerät muss am Ende der Betriebszeit
ordnungsgemäß und in Übereinstimmung mit den regionalen Bestimmungen entsorgt werden.
GEFAHR DURCH ELEKTRISCHEN SCHLAG
Hochspannungswarnung:
Innerhalb des Netzteiles gibt es gefährliche Spannungen. Der Elektroinstallateur muss das Wartungspersonal vor
versehentlichem Kontakt mit den gefährlichen Spannungen im Endgerät schützen.
WARNUNG! Falls Sie unser Netzgerät in eine Anwendung mit Schutzklasse 1 eingebaut haben, stellen Sie sicher,
dass es fachgerecht installiert und zuverlässig geerdet ist.
KM40 lnstallalion Manual TDK-Lambda
Page 4 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
Die (+) oder (-) Ausgänge können geerdet werden oder unangeschlossen bleiben.
Die Abdeckung des Gerätes/das Gehäuse darf für den Benutzer nicht zugänglich sein.
Der Haupteingangsanschluss ist nicht für die Verwendung als Feldverdrahtungsanschluss geeignet.
Für ummantelt Produkte, verwenden Sie keine Schrauben, die das Gerät mehr als durchdringen; siehe Zeichnung
Eine interne Sicherung schützt das Gerät und darf durch den Benutzer nicht ausgetauscht werden. Im Fall von
internen Defekten muss das Gerät an TDK-Lambda UK LTD oder einen der autorisierten Vertriebshändler
zurückgeschickt werden.
Ein geeignetes mechanisches, elektrisches und brandgeschütztes Gehäuse muss als Schutz vor der Gefahr von
mechanischen Risiken, Stromschlägen und Brandschutz in dem Endgerät vorgesehen werden.
Die Geräteabdeckung/das Gehäuse ist so entworfen, dass das Fachpersonal vor Gefahren geschützt wird. Sie
dürfen nicht als Teil der externen Abdeckung für Geräte verwendet werden, die für den Betreiber zugänglich sein
müssen, da Teile oder das gesamte Gerätegehäuse unter voller Auslastung übermäßige Temperaturen erreichen
kann, die für den Zugang des Betreibers nicht mehr als sicher betrachtet werden.
KM4o Installation Manual TDK-Lambda Consi nes éne’ralesde sécur ' A
Page 5 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
FRANÇAIS
Consignes générales de sécurité:
LIRE LES CONSIGNES DE SECURITE
Entretien:
Ces produits ne peuvent pas être réparés par l’utilisateur. Seuls, TDK-Lambda UK LTD et ses agents agréés sont
autorisés à effectuer des réparations.
Composants critiques:
Ces produits ne doivent pas être utilisés en tant que composants critiques dans des systèmes de commande
nucléaire, dans des systèmes de sauvetage ou dans des équipements utilisés dans des environnements dangereux,
sans l'autorisation écrite expresse du directeur général de TDK-Lambda EMEA.
Utilisation du produit:
Ces produits sont conçus pour être utilisés dans un équipement hôte dont l'accès n'est autorisé qu'aux personnes
compétentes.
Ce produit est une alimentation considérée comme un composant devant être installé par des personnes qualifiées,
dans un autre équipement. Il ne doit pas être utilisé en tant que produit fini.
Ce produit est destiné à la vente entre entreprises et peut être obtenu via des canaux de distribution.
Il n’est pas prévu à la vente pour les particuliers.
Ce produit est une alimentation considérée comme un composant, il ne relève pas du champ d’application de la
directive CEM. Le respect de la directive CEM doit être pris en compte dans l’installation finale. Veuillez contacter
votre bureau TDK-Lambda le plus proche.
Environnement:
Ces produits sont IPX0, et donc on ne doit pas utiliser des produits chimiques/solvants, des produits de nettoyage et
d'autres liquides.
Environnement fonctionnel :
Cette alimentation fonctionne en mode commutation pour utilisation dans des applications fonctionnant dans un
environnement avec Degré de Pollution 2 et catégorie de surtension II. Elle utilise des cartes des circuits imprimés
(PCB) de Groupe IIIb.
Intensité soutirée:
L'intensité soutirée de l'alimentation ne doit pas dépasser l'intensité nominale marquée sur la plaque signalétique,
sauf indications contraires dans les limitations du produit décrit dans ce manuel.
Paramètres d'entrée:
Ce produit doit être utilisé à l'intérieur des paramètres d'entrée indiqués dans les limitations du produit dans ce
manuel.
Elimination en fin de vie:
L'alimentation contient des composants nécessitant des dispositions spéciales pour leur élimination. Vérifiez que
cette alimentation est mise au rebut correctement en fin de vie utile et conformément aux réglementations locales en
vigueur.
RISQUE DE CHOC ELECTRIQUE
Attention-Danger haute tension:
Des tensions dangereuses sont présentes dans l'alimentation. L'installateur doit protéger le personnel d'entretien
contre un contact involontaire avec ces tensions dangereuses dans l'équipement final.
AVERTISSEMENT: Si ce produit est installé dans un équipement final de classe I, il doit être mis à la terre de
manière fiable et installé par un professionnel averti.
KM40 lnstallalion Manual TDK-Lambda
Page 6 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
Les sorties (+) ou (-) peuvent être raccordées à la terre ou laissées flotttantes.
Le couvercle/châssis de l'alimentation ne doit pas être accessible à l'utilisateur.Le connecteur d'entrée d'alimentation
principale ne doit pas être utilisé comme borne de raccordement.
N'utilisez pas de vis pénétrant dans le module sur une profondeur supérieure à :Voir dessins.
Un fusible interne protège le module et ne doit pas être remplacé par l'utilisateur. En cas de défaut interne, le module
doit être renvoyé à TDK-Lambda UK LTD ou l'un de ses agents agréés.
Une enceinte appropriée doit être prévue par l'utilisateur final pour assurer la protection contre les chocs
mécaniques, les chocs électriques et l'incendie.
Le couvercle et le châssis du module sont conçus pour protéger des personnels expérimentés. Ils ne doivent pas
être utilisés comme couvercles extérieurs d'un équipement, accessible aux opérateurs car en condition de puissance
maximum, des parties du châssis peuvent atteindre des températures considérées comme dangereuses pour
l'opérateur.
KM4o Installation Manual TDK-Lambda Norme genera curezza: A
Page 7 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
ITALIANO
Norme generali di sicurezza:
SI PREGA DI LEGGERE LE NORME DI SICUREZZA
Manutenzione:
Il cliente non può eseguire alcuna manutenzione su questi prodotti. L'esecuzione delle eventuali riparazioni è
consentita solo a TDK-Lambda UK LTD e ai suoi agenti autorizzati.
Componenti critici:
Non si autorizza l'uso di questi prodotti come componenti critici all'interno di sistemi di controllo nucleari, sistemi
necessari alla sopravvivenza o apparecchiature destinate all'impiego in ambienti pericolosi, senza l'esplicita
approvazione scritta dell'Amministratore Delegato di TDK-Lambda EMEA.
Uso dei prodotti:
Questi prodotti sono progettati per l'uso all'interno di un'apparecchiatura ospite che limiti l'accesso al solo personale
competente e autorizzato.
Questo prodotto è da considerarsi come un alimentatore professionale componente e come tale deve essere
installato da personale qualificato all'interno di altre apparecchiature e non può essere utilizzato come prodotto
indipendente.
Questo prodotto non è inteso per la vendita al dettaglio o agli utilizzatori finali.
Questo alimentatore è da considerarsi come un componente e come tale non è assogettato dagli scopi della direttiva
EMC. Conformità alla direttiva EMC deve essere considerata nell'installazione finale di utilizzo. Gli uffici di TDK-
Lambda Sas Succursale Italiana sono a vostra disposizione per ulteriori ragguagli.
Condizioni ambientali:
Questi prodotti sono classificati come IPX0, dunque non devono essere utilizzati sostanze chimiche/solventi, prodotti
per la pulizia o liquidi di altra natura.
Ambiente:
Questo prodotto è un alimentatore a commutazione, destinato all'uso in applicazioni rientranti in ambienti con le
seguenti caratteristiche: Livello inquinamento 2, Categoria sovratensione II. Questo prodotto contiene schede di
circuiti stampati in materiali di Gruppo IIIb.
Carico in uscita:
La potenza in uscita ottenuta dall'alimentatore non deve superare la potenza nominale indicata sulla targhetta
dell'alimentatore, fatto salvo dove indicato nei limiti per i prodotto specificati in questo manuale.
Parametri di alimentazione:
Questo prodotto deve essere utilizzato entro i parametri di alimentazione indicati nei limiti per il prodotto, specificati
in questo manuale.
Smaltimento:
L'unità contiene componenti che richiedono procedure speciali di smaltimento. Accertarsi che l'unità venga smaltita
in modo corretto al termine della vita utile e nel rispetto delle normative locali.
RISCHIO DI SCOSSA ELETTRICA
Avvertimento di alta tensione:
All'interno dell'alimentatore sono presenti tensioni pericolose. Gli installatori professionali devono proteggere il
personale di manutenzione dal rischio di contatto accidentale con queste tensioni pericolose all'interno
dell'apparecchiatura finale.
ATTENZIONE: Se installato in un’attrezzatura di classe I, questo prodotto deve essere collegato a terra in modo
affidabile ed installato in modo professionale.
KM40 lnstallalion Manual TDK-Lambda
Page 8 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
Le uscite (+) o (-) possono essere messa a terra o lasciate isolate.
I coperchi/il telaio dell'unità non devono essere accessibili da parte dell'utente.
Il connettore dell'alimentazione principale non può essere utilizzato come terminale di collegamento di campo.
Non utilizzare viti che penetrano nell'unità per più di : Vedi disegni
Un fusibile interno protegge l'unità e non deve essere sostituito dall'utente. Nell'eventualità di un difetto interno,
restituire l'unità a TDK-Lambda UK LTD o a uno dei suoi agenti autorizzati.
L'apparecchiatura finale deve includere una recinzione meccanica, elettrica e antincendio per proteggere dai pericoli
di natura meccanica, dalle scosse elettriche e dai pericoli di incendio.
Il coperchio/telaio dell'unità è realizzato per proteggere il personale esperto dai pericoli. Non deve essere usato
come parte degli involucri esterni di qualsiasi apparecchiatura, se risulta accessibile da parte degli addetti, poiché è
possibile che in condizioni di pieno carico una o più parti del telaio dell'unità giunga/giungano a temperature superiori
ai limiti considerati sicuri per l'accesso da parte degli addetti.
KM4o Installation Manual TDK-Lambda lnslrucciones enerales de se uridad: A
Page 9 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
ESPAÑOL
Instrucciones generales de seguridad:
LEA LAS INSTRUCCIONES DE SEGURIDAD
Servicio:
Estos productos no pueden ser reparados por los clientes. TDK-Lambda UK LTD. y sus agentes autorizados son
los únicos que pueden llevar a cabo las reparaciones.
Componentes fundamentales:
Estos productos no pueden ser utilizados como componentes fundamentales en sistemas de control nuclear,
sistemas de soporte vital o equipos a utilizar en entornos peligrosos sin el consentimiento expreso por escrito del
Director General de TDK-Lambda EMEA.
Uso de los productos:
Estos productos han sido diseñados para ser utilizados en un equipo central que restrinja el acceso al personal
cualificado autorizado.
Este producto es una fuente de alimentación y sólo puede ser instalado por personal cualificado dentro de otros
equipos y no debe ser tratado como un producto independiente. Este producto debe ser vendido entre empresas
profesionales y solo puede obtenerse a través de los canales de distribución .No está destinado para la venta a
usuarios finales
Este producto es una fuente de alimentación y no se ve afectada por la directiva EMC . El cumplimiento de la
directiva EMC se debe considerar en la instalación final. Por favor, póngase en contacto con su oficina local de TDK
– Lambda.
Medioambiental:
Estos productos son IPX0 y, por tanto, no pueden utilizarse sustancias químicas/disolventes, agentes de limpieza ni
otros líquidos.
Medio ambiente:
Esta fuente de alimentación es una fuente de alimentación de modo conmutado a utilizar en aplicaciones dentro de
un entorno con un Grado de contaminación 2 y una Categoría de sobretensión II. En él se utilizan policloruros de
bifenilo del Grupo de materiales IIIb.
Carga de salida:
La potencia de salida tomada de la fuente de alimentación no puede sobrepasar el valor nominal indicado en la
etiqueta de la fuente de alimentación, excepto en los casos indicados en las limitaciones del producto en este
manual.
Parámetros de entrada:
Este producto debe ser utilizado dentro de los parámetros de entrada indicados en las limitaciones del producto en
este manual.
Desecho de la unidad:
La unidad contiene componentes que deben ser desechados de una manera especial. Asegúrese de desechar
correctamente la unidad al final de su vida útil y conforme a las normas locales vigentes.
PELIGRO DE DESCARGAS ELÉCTRICAS
Advertencia de alta tensión:
En esta fuente de alimentación hay tensiones peligrosas. El instalador profesional debe proteger al personal de
servicio contra cualquier contacto accidental con estas tensiones peligrosas en el equipo final.
ADVERTENCIA: La instalación de este producto en un equipo de clase I la deben llevar a cabo profesionales y el
producto debe estar conectado a tierra.
KM40 lnstallalion Manual TDK-Lambda
Page 10 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
La salida o salidas (+) o (-) pueden conectarse a tierra o se las puede dejar flotando.
Debe impedirse el acceso de los usuarios a la cubierta o cubiertas y al chasis de la unidad.
El conector de entrada de la red no es apto para ser utilizado a modo de bornes de cableado de campo.
No utilice tornillos de montaje susceptibles de penetrar en la unidad más de: Ver dibujos.
Un fusible interno protege la unidad y este no debe ser nunca reemplazado por el usuario. En caso de existir algún
defecto interno, la unidad debe ser enviada a TDK-Lambda UK LTD o a uno de sus agentes autorizados.
El equipo de uso final debe constituir un recinto de protección mecánica, eléctrica y contra incendios de protección
mecánica, contra descargas eléctricas y contra el peligro de incendios.
La cubierta/chasis de la unidad ha sido diseñada para que proteja a las personas cualificadas de los peligros. No
deben ser utilizadas como parte de las cubiertas externas de cualquier equipo al que pueden acceder los operarios,
ya que bajo unas condiciones de carga completa, la pieza o piezas del chasis de la unidad pueden alcanzar
temperaturas superiores a las consideradas seguras para el acceso de los operarios.
KM4o Installation Manual TDK-Lambda lnslru fies erais de se uran a: A
Page 11 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
PORTUGUÊS
Instruções gerais de segurança:
LEIA AS INSTRUÇÕES DE SEGURANÇA
Manutenção:
Estes produtos não são podem ser submetidos a manutenção por parte do cliente. Apenas a TDK-Lambda UK LTD
e os seus agentes autorizados têm permissão para realizar reparações.
Componentes essenciais:
Não é autorizada a utilização destes produtos como componentes essenciais de sistemas de controlo nuclear,
sistemas de suporte de vida ou equipamento para utilização em ambientes perigosos sem a expressa autorização
por escrito do Director-Geral da TDK-Lambda EMEA.
Utilização do produto:
Estes produtos foram concebidos para utilização dentro de um equipamento de alojamento que apenas permita o
acesso a pessoal qualificado autorizado.
Este produto é uma alimentaçao considerado com um componente para ser instalado por pessoas qualificadas, em
outros equipamentos. Não deve ser usado como um produto acabado.
Este produto é destinado para venda entre as empresas e pode ser obtido através de canais de distribuição.
Não se destina à venda aos particulares.
Este produto é uma alimentaçao considerado com um componente, não é dentro do appliquation âmbito da directiva
CEM.
Conformidade com a directiva CEM devem ser considerados na instalação final.
Entre em contacto com seu escritório TDK-Lambda mais próximo.
Ambiental:
Estes produtos são IPX0 e, como tal, não se devem utilizar químicos/solventes, agentes de limpeza e outros
líquidos.
Ambiente:
Esta fonte de alimentação é uma fonte de alimentação do modo de comutação para utilização em aplicações com
um Nível de Poluição 2 e ambientes da categoria de sobretensão II. São utilizadas placas de circuitos impressos do
grupo de materiais IIIb.
Carga de saída:
A potência de saída extraída da fonte de alimentação não deve exceder a classificação assinalada na etiqueta da
fonte de alimentação, excepto quando indicado nas limitações do produto neste guia.
Parâmetros de entrada:
Este produto deve ser utilizado dentro dos parâmetros de entrada indicados nas limitações do produto neste guia.
Eliminação no fim de vida:
A unidade contém componentes que necessitam de procedimentos especiais de eliminação. Certifique-se de que a
unidade é devidamente eliminada no fim da sua vida útil e que tal é feito em conformidade com os regulamentos
locais.
RISCO DE CHOQUE ELÉCTRICO
Aviso de alta tensão:
Estão presentes tensões perigosas dentro da fonte de alimentação. O profissional que realizar a instalação deve
proteger o pessoal de assistência contra contactos inadvertidos com estas tensões perigosas do equipamento final.
AVISO: Quando instalado num equipamento de Classe I, este produto deve ser ligado à terra de forma fiável e
instalado por um profissional.
.
KM4o Installation Manual TDK-Lambda TDK-Lambda www.uk.tdk-Iambda.com
Page 12 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
As saídas (+) e (-) podem ser ligadas à terra ou deixadas soltas.
O chassis/cobertura(s) da unidade não deve estar acessível ao utilizador.
O conector de entrada de alimentação não deve ser utilizado como terminal de cablagens no local.
Não utilize parafusos de montagem, uma vez que estes penetrarão na unidade em mais do que: Veja os desenhos
Existe um fusível interno que protege a unidade e que não deve ser substituído pelo utilizador. Em caso de defeito
interno, a unidade deve ser devolvida à TDK-Lambda UK LTD ou a um dos seus agentes autorizados.
O equipamento de utilização final deve fornecer um bastidor com protecção mecânica, eléctrica e contra incêndios
adequada.
O chassis/cobertura da unidade está concebido de forma a proteger o pessoal especializado de perigos. Não devem
ser utilizados como parte das coberturas externas de qualquer equipamento em que possam estar acessíveis aos
operadores, uma vez que em condições de carga máxima, algumas peças do chassis da unidade podem atingir
temperaturas superiores às consideradas seguras para o acesso do operador.
TDK-Lambda UK Ltd
Kingsley Avenue, Ilfracombe
Devon, EX34 8ES
Telephone - Sales and Service +44 (0)1271 856666
Head Office and Works +44 (0)1271 856600
Facsimile +44 (0)1271 864894
WEBSITE: www.uk.tdk-lambda.com
KM40 Installation Manual TDKLambda Top View
Page 13 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
Special Instructions for medical applications (IEC/EN/UL/CSA 60601-1)
These products are designed for continuous operation within an overall enclosure, and must be mounted such that
access to the mains terminals is restricted. See clause 16, IEC60601-1, EN60601-1 and UL/CSA 60601-1.
Input Connection – KMx40 –xx
Pin Single O/P Dual O/P Triple O/P
1 AC (L) AC (L) AC (L)
2 AC (N) AC (N) AC (N)
3 +DC out +DC out +DC out
4 No pin No pin +5V
5 -DC out GND GND
6 No pin No pin GND for +5V
7 No
Connection -DC out -DC out
These products are NOT suitable for use in the presence of flammable anaesthetic mixtures with air or with oxygen,
or with nitrous oxide.
These products are classed as ordinary equipment, type B and have a reinforced barrier between input and output to
IEC60601-1, EN60601-1 and UL/CSA 60601-1. They are NOT protected against the ingress of water.
Reference should be made to local regulations concerning the disposal of these products at the end of their useful
life.
Environmental Specifications:
Description Operation Storage
Use Indoor indoor
Temperature -25°C - +50°C -40°C - +100°C
Humidity 20 - 95% RH, non-condensing 20 - 95% RH, non-
condensing
Altitude -200m - 5000m -200m - 5000m
Pressure 70kPa - 106kPa 54kPa - 106kPa
Orientation ALL
Shock <196.1m/s
2
(20G)
Vibration 23.52m/s
2
(10-55Hz): constant sweep 1min X, Y, Z for 1 hour
Material Group IIIb
Pollution Degree 2
Overvoltage Category II
Construction Class II
KM40 Installation Manual TDKLambda
Page 14 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
Level of Insulation:
Primary mains circuits to secondary: 4.25 - 4.35kVDC
Safety Approvals:
IEC/UL/EN60601-1, (2nd Edition)
UL/cUL60950-1 (2nd Edition)
IEC / EN60950-1(2nd Edition)
CE marking when applied to any KMx15any product indicates compliance with the Low Voltage Directive
(2006/95/EC) in that it complies with EN60950-1 (2nd Edition).
Fusing: Internal fuses (F1): Single fuse in the L line, T3.15AL, 250V, not Serviceable
External fusing: Recommended 3.15A/250V slow blow
Input Parameters:
Standard 60950-1
Rated input voltage 100-240 VAC
Input voltage range 90 – 264VAC
Input frequency range 47 – 63Hz
Maximum input current
115/240VAC 130mA/
0.70mA 270mA/
0.130mA 400mA/
0.200mA
Inrush current 20A max at 230VAC (25°C cold start)
Output Parameters:
Model Vout (V) Output
current (A) Max
capacitive
load (µF)
40W
Single O/P
3.3 4.4 70000
5 4.4 33000
9 2.4 10000
12 1.8 4000
15 1.4 3000
24 0.9 1200
40W
Dual O/P
+5/-5 1.5/1.5 6000
+12/-12 0.625/0.625 1000
+15/-15 0.5/0.5 2000
40W
Triple O/P (Note 1) +5/+12/-12 2/0.2/0.2 18000/150
+5/+15/-15 2/0.15/0.15 18000/400
Note 1: For Triple output modules the main 5V output is isolated from the other ±12V or ±15V outputs (dependant on model). A minimum load of
25% is required on the ±12V and ±15V outputs.
All outputs are SELV except under the following circumstance: Outputs connected in series are non-SELV if the total
output voltage exceeds 60Vdc
If the total voltage of outputs connected in series exceed the 60Vdc SELV limit then all outputs must be considered
non-SELV.
Non-SELV outputs are hazardous and must not be made user accessible. Consideration must be given to service
engineers making inadvertent contact with the output terminals in the end equipment.
KM40 lnstallalion Manual TDK-Lambda ngfi? ® 53.5 55.3; a; ‘- Jms WW "M" TDK-Lambda www. k.ldk—lambda.com
Page 15 of 15 17167 issue 7 August 2016
KM
4
0
Installation Manual
Cooling for unit
The KMx40 series are convection cooled, derating for recommended installation shown.
Max case temperature 95°C.
Mounting position
Equipment top
The KMx40 family of component power supplies is designed for use within other equipment or enclosures which
restrict access to authorised competent personnel only.
Mechanical Outline Drawings:
KMx40-xx
TDK-Lambda UK Ltd
Kingsley Avenue, Ilfracombe
Devon, EX34 8ES
Telephone - Sales and Service +44 (0)1271 856666
Head Office and Works +44 (0)1271 856600
Facsimile +44 (0)1271 864894
WEBSITE: www.uk.tdk-lambda.com