TPI317C Datasheet by TPI (Test Products Int)

View All Related Products | Download PDF Datasheet
1?? .
Test the TPI advantage
Copyright © 2010 Test Products International, Inc.
Field calibration for thermometers
TPI 317c FIELD CALIBRATION
www.tpi-
thevalueleader.com
Field calibration
for thermometers
317c 09.10
Acessories
Adapters
Cables/Connectors
Oscilloscope Probes
Test Leads
Clamp-on meters
(Current)
Combustion Efficiency
Analyzers
Gas Detection
Carbon Monoxide (CO)
Combustibles
Refrigeration
Indoor Air Quality
(IAQ)
Manometers
(Pressure)
Multimeters
(DMMs)
Oscilloscopes
(Hand held)
Specialty Testers
Insulation
Multifunction
Photo-tachometer
Temperature
Contact
Non-Contact (IR)
Pocket Digital
Temperature Probes
J-Type
K-Type
T-Type
Thermistor
Test Leads &
Accessories
Fused
Modular
Push-on
Screw-on
TPI
Headquarters:
9615 SW Allen Blvd.
Beaverton, OR 97005
USA
503-520-9197
Fax: 503-520-1225
Step-by-Step Procedures
1. Fill a plastic or metal container with crushed ice and add clean water to a depth of at least 4
inches. Stir the ice and water for 2 to 3 minutes prior to performing calibration to ensure
the water is completely chilled. Make certain there is plenty of ice in the mixture and always
use clean water. Distilled water works well. The temperature of an ice bath is approximately
32°F (0°C).
2. Insert the stainless steel shaft of the 317c into the ice bath making sure at least one inch of
the tip is immersed. Allow the reading on the thermometer to stabilize.
Note: The temperature reading must be within 23°F to 41°F (-5°C to 5°C) for calibration
to have effect.
3. Press and hold the D-H/CAL button for approximately 8 seconds until "CAL" is displayed.
"CAL" will display for approximately 2 seconds and then the 317c will return to normal
operation. Calibration is complete.
Note: If the temperature reading was not within 23°F to 41°F (-5°C to 5°C) when step 3 was
performed no change in calibration occurred. The 31
7c
was designed with this feature to
prevent improper calibration.

Products related to this Datasheet

THERM POCKET STYLE W/AIR TIP