Radio FeatherWIng Guide Datasheet by Adafruit Industries LLC
View All Related Products | Download PDF Datasheet
Radio FeatherWing
Created by lady ada
Last updated on 2019-06-22 06:39:37 PM UTC

Overview
Add short-hop wireless to your Feather with these Radio Featherwings. These add-ons for any Feather board will let
you integrate packetized radio (with the RFM69 radio) or LoRa radio (with the RFM9x's). These radios are good options
for kilometer-range radio, and paired with one of our WiFi, cellular or Bluetooth Feathers, will let you bridge from
433/900 MHz to the Internet or your mobile device.
These radio modules come in four variants (two modulation types and two frequencies) The RFM69's are easiest to
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 4 of 69

work with, and are well known and understood. The LoRa radios are exciting, longer-range and more powerful but also
more expensive.
RFM69 @ 433 MHz - basic packetized FSK/GFSK/MSK/GMSK/OOK radio at 433 MHz for use in Europe ITU 1
license-free ISM, or for amateur use with restrictions (check your local amateur regulations!)
RFM69 @ 900 MHz - basic packetized FSK/GFSK/MSK/GMSK/OOK radio at 868 or 915 MHz for use in Americas
ITU 2 license-free ISM, or for amateur use with restrictions (check your amateur regulations!)
RFM98 @ 433 MHz - LoRa capable radio at 433 MHz for use in Europe ITU 1 license-free ISM, or for amateur use
with restrictions (check your local amateur regulations!)
RFM95 @ 900 MHz - LoRa capable radio at 868 or 915 MHz for use in Americas ITU 2 license-free ISM, or for
amateur use with restrictions (check your local amateur regulations!)
The radio modules themselves have the same pinout so the PCB is the same, but the library usage and wiring may
vary. All use SPI for interfacing, and there are great Arduino libraries available for both.
RFM69 Specs
SX1231 based module with SPI interface
Packet radio with ready-to-go Arduino libraries
Uses the license-free ISM bands
+13 to +20 dBm up to 100 mW Power Output Capability (power output selectable in software)
50mA (+13 dBm) to 150mA (+20dBm) current draw for transmissions
Range of approx. 350 meters, depending on obstructions, frequency, antenna and power output
Create multipoint networks with individual node addresses
Encrypted packet engine with AES-128
RFM9x Specs
SX127x LoRa® based module with SPI interface
Packet radio with ready-to-go Arduino libraries
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 5 of 69

Uses the license-free ISM bands
+5 to +20 dBm up to 100 mW Power Output Capability (power output selectable in software)
~300uA during full sleep, ~120mA peak during +20dBm transmit, ~40mA during active radio listening.
Our initial tests with default library settings: over 1.2mi/2Km line-of-sight with wire quarter-wave antennas. (With
setting tweaking and directional antennas, 20Km is possible (https://adafru.it/mGa)).
Currently tested to work with the Feather ESP8266, Feather 32u4, Feather M0, WICED Feather (RFM69 library only)
and Teensy 3 Feather series, some wiring is required to configure the FeatherWing for the chipset you plan to use.
All radios are sold individually and can only talk to radios of the same part number. E.g. RFM69 900 MHz can only talk
to RFM69 900 MHz, LoRa 433 MHz can only talk to LoRa 433, etc.
Each radio 'Wing comes with some header. Some soldering is required to attach the header. You will need to cut and
solder on a small piece of wire (any solid or stranded core is fine) in order to create your antenna. Optionally you can
pick up a uFL or SMA edge-mount connector and attach an external duck.
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 6 of 69

Pinouts
SPI Data Pins (Fixed)
The three SPI data pins (MOSI/MISO/SCK) are hardwired to these three pads, which are use for the default SPI
interface on all Feathers:
SPI Control Pins (Flexible)
You also need three more pins to control the radio: CS, RST and IRQ
Since there is no guaranteed Feather pin that is interrupt-capable, we set it up so you can fly-wire these three to any
three pins available. For the non-Serial/IC pins on the right, we name them A thru F. We also indicate the
RX/TX/SDA/SCL pins if you need to use those:
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 7 of 69

Wire them with three short jumpers like so:
RFM GPIO
There's some other GPIO pins that you may want to use - they can be configured to give you notice of things like
packet completion or incoming data. They're all on the left. DIO0 is also known as IRQ so we don't have that
duplicated on the left breakouts
Antenna
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 8 of 69

For an antenna, you have three options:
Plain wire antenna (cut a quarter-wavelength piece and solder it into the pad/hole
uFL connector (not included) (http://adafru.it/1661), which can be soldered and then used to attach a uFL antenna
or adapter
SMA edge-launch (not included) (http://adafru.it/1865), for use with any SMA connector
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 9 of 69

Wiring
Because each Feather uses a different processor, there is some light wiring that needs to be done to configure the
radio pins. In particular, an interrupt-capable pin is required for IRQ but there is no one irq pin that is the same on all
the Feathers!
So, while MOSI/MISO/SCK are fixed, you will want to solder three short wires for CS, RST and IRQ
Here is our tested/suggested wiring configurations and code snippets for defining the pins
ESP8266 Wiring
The ESP does not have a lot of spare pins, and the SPI pins are taken, so here's what we've tested that works:
This leaves the I2C default pins (4 and 5) available
Feather 32u4
The 32u4 doesn't have a lot of IRQs and the only ones available are on pins 0, 1, 2, 3 which are also the Serial RX/TX
and I2C pins. So it's not great because you have to give up one of those pins.
#define RFM95_CS 2 // "E"
#define RFM95_RST 16 // "D"
#define RFM95_INT 15 // "B"
#define RFM69_CS 2
#define RFM69_RST 16
#define RFM69_IRQ 15
#define RFM69_IRQN digitalPinToInterrupt(RFM69_IRQ )
#define RFM95_CS 10 // "B"
#define RFM95_RST 11 // "A"
#define RFM95_INT 2 // "SDA" (only SDA/SCL/RX/TX have IRQ!)
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 10 of 69

Feather M0
The Feather M0 is really easy to use, a ton of interrupts so wiring is easy
Other Boards
For other boards like the ESP32 or nRF52, any pin can be an interrupt, so feel free to use any wiring setup you like!
#define RFM69_CS 10 // "B"
#define RFM69_RST 11 // "A"
#define RFM69_IRQ 2 // "SDA" (only SDA/SCL/RX/TX have IRQ!)
#define RFM69_IRQN digitalPinToInterrupt(RFM69_IRQ )
#define RFM95_CS 10 // "B"
#define RFM95_RST 11 // "A"
#define RFM95_INT 6 // "D"
#define RFM69_CS 10 // "B"
#define RFM69_RST 11 // "A"
#define RFM69_IRQ 6 // "D"
#define RFM69_IRQN digitalPinToInterrupt(RFM69_IRQ )
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 11 of 69

Assembly
Antenna Options
These radio Wings do not have a built-in antenna. Instead, you have three options for attaching an antenna. For most
low cost radio nodes, a wire works great. If you need to put the radio into an enclosure, soldering in uFL and using a
uFL to SMA adapter will let you attach an external antenna. You can also solder an SMA edge-mount connector directly
Wire Antenna
A wire antenna, aka "quarter wave whip antenna" is low cost and works very well! You just have to cut the wire down
to the right length.
Cut a stranded or solid core wire the the proper length
for the module/frequency
433 MHz - 6.5 inches, or 16.5 cm
868 MHz - 3.25 inches or 8.2 cm
915 MHz - 3 inches or 7.8 cm
Strip a mm or two off the end of the wire, tin and solder
into the ANT pad.
uFL Connector
If you want an external antenna that is a few inches away from the radio, you need to do a tiny bit more work but its not
too difficult.
You'll need to get an SMT uFL connector, these are fairly standard (http://adafru.it/1661)
You'll also need a uFL to SMA adapter (http://adafru.it/851) (or whatever adapter you need for the antenna you'll be
using, SMA is the most common
Of course, you will also need an antenna of some sort, that matches your radio frequency
uFL connectors are rated for 30 connection cycles, but be careful when connecting/disconnecting to not rip
the pads off the PCB. Once a uFL/SMA adapter is connected, use strain relief!
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 12 of 69

Once done, check your work visually
SMA Edge-Mount Connector
These strong edge connectors are used for many 'duck' antennas, and can also be panel mounted
You'll need an SMA (or, if you need RP-SMA for some
reason) Edge-Mount connector with 1.6mm spacing
The SMA connector 'slides on' the top of the PCB
Solder all 5 connections (4 ground/mechanical and 1
signal)
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 16 of 69

Using the RFM69 Radio
This page is shared between the RFM69 breakout and
the all-in-one Feather RFM69's. The example code and
overall functionality is the same, only the pinouts used
may differ! Just make sure the example code is using
the pins you have wired up.
Before beginning make sure you have your Arduino or Feather working smoothly, it will make this part a lot easier.
Once you have the basic functionality going - you can upload code, blink an LED, use the serial output, etc. you can
then upgrade to using the radio itself.
Note that the sub-GHz radio is not designed for streaming audio or video! It's best used for small packets of data. The
data rate is adjustable but its common to stick to around 19.2 Kbps (thats bits per second). Lower data rates will be
more successful in their transmissions
You will, of course, need at least two paired radios to do any testing! The radios must be matched in frequency (e.g.
900 MHz & 900 MHz are ok, 900 MHz & 433 MHz are not). They also must use the same encoding schemes, you
cannot have a 900 MHz RFM69 packet radio talk to a 900 MHz RFM9x LoRa radio.
"Raw" vs Packetized
The SX1231 can be used in a 'raw rx/tx' mode where it just modulates incoming bits from pin #2 and sends them on the
radio, however there's no error correction or addressing so we wont be covering that technique.
Instead, 99% of cases are best off using packetized mode. This means you can set up a recipient for your data, error
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 19 of 69

correction so you can be sure the whole data set was transmitted correctly, automatic re-transmit retries and return-
receipt when the packet was delivered. Basically, you get the transparency of a data pipe without the annoyances of
radio transmission unreliability
Arduino Libraries
These radios have really great libraries already written, so rather than coming up with a new standard we suggest
using existing libraries such as LowPowerLab's RFM69 Library (https://adafru.it/mCz) and AirSpayce's Radiohead
library (https://adafru.it/mCA) which also suppors a vast number of other radios
These are really great Arduino Libraries, so please support both companies in thanks for their efforts!
We recommend using the Radiohead library - it is very cross-platform friendly and used a lot in the community!
RadioHead Library example
To begin talking to the radio, you will need to download our small fork of the Radiohead from our github
repository (https://adafru.it/vgE). You can do that by visiting the github repo and manually downloading or, easier, just
click this button to download the zip
https://adafru.it/vgF
https://adafru.it/vgF
Rename the uncompressed folder RadioHead and check that the RadioHead folder contains files like RH_RFM69.cpp
and RH_RFM69.h (and many others!)
Place the RadioHead library folder in your
arduinosketchfolder
/libraries/ folder.
You may need to create the libraries subfolder if it's your first library. Restart the IDE.
We also have a great tutorial on Arduino library installation at:
http://learn.adafruit.com/adafruit-all-about-arduino-libraries-install-use (https://adafru.it/aYM)
Basic RX & TX example
Lets get a basic demo going, where one radio transmits and the other receives. We'll start by setting up the transmitter
Basic Transmitter example code
This code will send a small packet of data once a second to another RFM69 radio, without any addressing.
Open up the example RadioHead -> feather -> RadioHead69_RawDemo_TX
Load this code into your Transmitter Arduino or Feather!
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 20 of 69

Once uploaded you should see the following on the serial console
Now open up another instance of the Arduino IDE - this is so you can see the serial console output from the TX device
while you set up the RX device.
Basic receiver example code
Before uploading, check for the #define FREQUENCY RF69_915MHZ line and comment that out (and
uncomment the line above) to match the frequency of the hardware you're using
These examples are optimized for the Feather 32u4/M0. If you're using differnet wiring,
uncomment/comment/edit the sections defining the pins depending on which chipset and wiring you are
using! The pins used will vary depending on your setup!
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 21 of 69

This code will receive and reply with a small packet of data.
Open up the example RadioHead -> feather -> RadioHead69_RawDemo_RX
Load this code into your Receiver Arduino/Feather!
Now open up the Serial console on the receiver, while also checking in on the transmitter's serial console. You should
see the receiver is...well, receiving packets
Before uploading, check for the #define FREQUENCY RF69_915MHZ line and comment that out (and
uncomment the line above) to match the frequency of the hardware you're using
These examples are optimized for the Feather 32u4/M0. If you're using differnet wiring,
uncomment/comment/edit the sections defining the pins depending on which chipset and wiring you are
using! The pins used will vary depending on your setup!
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 22 of 69

And, on the transmitter side, it is now printing Got Reply after each transmisssion because it got a reply from the
receiver
That's pretty much the basics of it! Lets take a look at the examples so you know how to adapt to your own radio
network
Radio Freq. Config
Each radio has a frequency that is configurable in software. You can actually tune outside the recommended
frequency, but the range won't be good. 900 MHz can be tuned from about 850-950MHz with good performance. 433
MHz radios can be tuned from 400-460 MHz or so.
For all radios they will need to be on the same frequency. If you have a 433MHz radio you will want to stick to 433. If
you have a 900 Mhz radio, go with 868 or 915MHz, just make sure all radios are on the same frequency
Configuring Radio Pinout
At the top of the sketch you can also set the pinout. The radios will use hardware SPI, but you can select any pins for
RFM69_CS (an output), RFM_IRQ (an input) and RFM_RST (an output). RFM_RST is manually used to reset the radio at
the beginning of the sketch. RFM_IRQ must be an interrupt-capable pin. Check your board to determine which pins
you can use!
Also, an LED is defined.
For example, here is the Feather 32u4 pinout
// Change to 434.0 or other frequency, must match RX's freq!
#define RF69_FREQ 915.0
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 23 of 69

If you're using a Feather M0, the pinout is slightly different:
If you're using an Arduino UNO or compatible, we recommend:
If you're using a FeatherWing or different setup, you'll have to set up the #define statements to match your wiring
You can then instantiate the radio object with our custom pin numbers. Note that the IRQ is defined by the IRQ pin not
number (sometimes they differ).
Setup
We begin by setting up the serial console and hard-resetting the RFM69
#if defined (__AVR_ATmega32U4__) // Feather 32u4 w/Radio
#define RFM69_CS 8
#define RFM69_INT 7
#define RFM69_RST 4
#define LED 13
#endif
#if defined(ARDUINO_SAMD_FEATHER_M0) // Feather M0 w/Radio
#define RFM69_CS 8
#define RFM69_INT 3
#define RFM69_RST 4
#define LED 13
#endif
#if defined (__AVR_ATmega328P__) // UNO or Feather 328P w/wing
#define RFM69_INT 3 //
#define RFM69_CS 4 //
#define RFM69_RST 2 // "A"
#define LED 13
#endif
// Singleton instance of the radio driver
RH_RF69 rf69(RFM69_CS, RFM69_INT);
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 24 of 69

If you are using a board with 'native USB' make sure the while (!Serial) line is commented out if you are not tethering to
a computer, as it will cause the microcontroller to halt until a USB connection is made!
Initializing Radio
Once initialized, you can set up the frequency, transmission power, radio type and encryption key.
For the frequency, we set it already at the top of the sketch
For transmission power you can select from 14 to 20 dBi. Lower numbers use less power, but have less range. The
second argument to the function is whether it is an HCW type radio, with extra amplifier. This should
always
be set to
true!
Finally, if you are encrypting data transmission, set up the encryption key
void setup()
{
Serial.begin(115200);
//while (!Serial) { delay(1); } // wait until serial console is open, remove if not tethered to computer
pinMode(LED, OUTPUT);
pinMode(RFM69_RST, OUTPUT);
digitalWrite(RFM69_RST, LOW);
Serial.println("Feather RFM69 RX Test!");
Serial.println();
// manual reset
digitalWrite(RFM69_RST, HIGH);
delay(10);
digitalWrite(RFM69_RST, LOW);
delay(10);
if (!rf69.init()) {
Serial.println("RFM69 radio init failed");
while (1);
}
Serial.println("RFM69 radio init OK!");
// Defaults after init are 434.0MHz, modulation GFSK_Rb250Fd250, +13dbM (for low power module)
// No encryption
if (!rf69.setFrequency(RF69_FREQ)) {
Serial.println("setFrequency failed");
}
// If you are using a high power RF69 eg RFM69HW, you *must* set a Tx power with the
// ishighpowermodule flag set like this:
rf69.setTxPower(20, true); // range from 14-20 for power, 2nd arg must be true for 69HCW
// The encryption key has to be the same as the one in the server
uint8_t key[] = { 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08,
0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08};
rf69.setEncryptionKey(key);
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 25 of 69

Basic Transmission Code
If you are using the transmitter, this code will wait 1 second, then transmit a packet with "Hello World #" and an
incrementing packet number, then check for a reply
Its pretty simple, the delay does the waiting, you can replace that with low power sleep code. Then it generates the
packet and appends a number that increases every tx. Then it simply calls send() waitPacketSent() to wait until is is
done transmitting.
It will then wait up to 500 milliseconds for a reply from the receiver with waitAvailableTimeout(500) . If there is a reply,
it will print it out. If not, it will complain nothing was received. Either way the transmitter will continue the loop and sleep
for a second until the next TX.
Basic Receiver Code
The Receiver has the same exact setup code, but the loop is different
void loop() {
delay(1000); // Wait 1 second between transmits, could also 'sleep' here!
char radiopacket[20] = "Hello World #";
itoa(packetnum++, radiopacket+13, 10);
Serial.print("Sending "); Serial.println(radiopacket);
// Send a message!
rf69.send((uint8_t *)radiopacket, strlen(radiopacket));
rf69.waitPacketSent();
// Now wait for a reply
uint8_t buf[RH_RF69_MAX_MESSAGE_LEN];
uint8_t len = sizeof(buf);
if (rf69.waitAvailableTimeout(500)) {
// Should be a reply message for us now
if (rf69.recv(buf, &len)) {
Serial.print("Got a reply: ");
Serial.println((char*)buf);
Blink(LED, 50, 3); //blink LED 3 times, 50ms between blinks
} else {
Serial.println("Receive failed");
}
} else {
Serial.println("No reply, is another RFM69 listening?");
}
}
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 26 of 69

Instead of transmitting, it is constantly checking if there's any data packets that have been received. available() will
return true if a packet with the proper encryption has been received. If so, the receiver prints it out.
It also prints out the RSSI which is the receiver signal strength indicator. This number will range from about -15 to -80.
The larger the number (-15 being the highest you'll likely see) the stronger the signal.
If the data contains the text "Hello World" it will also reply to the packet.
Once done it will continue waiting for a new packet
Basic Receiver/Transmitter Demo w/OLED
OK once you have that going you can try this example, RadioHead69_RawDemoTXRX_OLED. We're using the
Feather with an OLED wing but in theory you can run the code without the OLED and connect three buttons to GPIO
#9, 6, and 5 on the Feathers. Upload the same code to each Feather. When you press buttons on one Feather they will
be printed out on the other one, and vice versa. Very handy for testing bi-directional communication!
void loop() {
if (rf69.available()) {
// Should be a message for us now
uint8_t buf[RH_RF69_MAX_MESSAGE_LEN];
uint8_t len = sizeof(buf);
if (rf69.recv(buf, &len)) {
if (!len) return;
buf[len] = 0;
Serial.print("Received [");
Serial.print(len);
Serial.print("]: ");
Serial.println((char*)buf);
Serial.print("RSSI: ");
Serial.println(rf69.lastRssi(), DEC);
if (strstr((char *)buf, "Hello World")) {
// Send a reply!
uint8_t data[] = "And hello back to you";
rf69.send(data, sizeof(data));
rf69.waitPacketSent();
Serial.println("Sent a reply");
Blink(LED, 40, 3); //blink LED 3 times, 40ms between blinks
}
} else {
Serial.println("Receive failed");
}
}
}
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 27 of 69

This demo code shows how you can listen for packets and also check for button presses (or sensor data or whatever
you like) and send them back and forth between the two radios!
Addressed RX and TX Demo
OK so the basic demo is well and good but you have to do a lot of
management
of the connection to make sure
packets were received. Instead of manually sending acknowledgements, you can have the RFM69 and library do it for
you! Thus the Reliable Datagram part of the RadioHead library.
Load up the RadioHead69_AddrDemo_RX and RadioHead69_AddrDemo_TX sketches to each of your boards
This example lets you have many 'client' RFM69's all sending data to one 'server'
Each client can have its own address set, as well as the server address. See this code at the beginning:
For each client, have a unique MY_ADDRESS. Then pick one server that will be address #1
Once you upload the code to a client, you'll see the following in the serial console:
Don't forget to check the frequency set in the example, and that the pinouts match your wiring!!!
// Where to send packets to!
#define DEST_ADDRESS 1
// change addresses for each client board, any number :)
#define MY_ADDRESS 2
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 28 of 69

Because the data is being sent to address #1, but #1 is not acknowledging that data.
If you have the server running, with no clients, it will sit quietly:
Turn on the client and you'll see acknowledged packets!
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 29 of 69

And the server is also pretty happy
The secret sauce is the addition of this new object:
Which as you can see, is the manager for the RFM69. In setup() you'll need to init it, although you still configure the
underlying rfm69 like before:
And when transmitting, use sendToWait which will wait for an ack from the recepient (at DEST_ADDRESS)
// Class to manage message delivery and receipt, using the driver declared above
RHReliableDatagram rf69_manager(rf69, MY_ADDRESS);
if (!rf69_manager.init()) {
Serial.println("RFM69 radio init failed");
while (1);
}
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 30 of 69

on the 'other side' use the recvFromAck which will receive and acknowledge a packet
That function will wait forever. If you'd like to timeout while waiting for a packet, use recvfromAckTimeout which will
wait an indicated # of milliseconds
if (rf69_manager.sendtoWait((uint8_t *)radiopacket, strlen(radiopacket), DEST_ADDRESS)) {
// Wait for a message addressed to us from the client
uint8_t len = sizeof(buf);
uint8_t from;
if (rf69_manager.recvfromAck(buf, &len, &from)) {
if (rf69_manager.recvfromAckTimeout(buf, &len, 2000, &from))
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 31 of 69

CircuitPython for
RFM69
It's easy to use the RFM69HCW radio with CircuitPython and the Adafruit CircuitPython
RFM69 (https://adafru.it/BjE) module. This module allows you to easily write Python code that sends and receives
packets of data with the radio. Be careful to note this library is for the RFM69 radio only and will not work with the
RFM9X LoRa radios!
Design Considerations
One thing to be aware of before you use the RFM69 series of radios with CircuitPython are some of the limitations and
design considerations for its module. Keep these in mind as you think about projects using the RFM69 and
CircuitPython:
You can only send and receive packets up to 60 bytes in length at a time. The size of the radio's internal buffer
dictates this limit so if you want to send longer messages you'll need to break them into a series of smaller send
calls in your application code.
Receiving packets is a 'best effort' in pure Python code. Unlike the Arduino versions of the RFM69 library there is
no interrupt support which means when a packet is received it must be immediately processed by the Python
code or it could be lost. For your application it will work best to only receive small, single packet messages at a
time. Don't try to receive kilobytes of data or else you'll lose packets. This module is really intended for simple
single packet messages like 'ON', 'OFF', etc.
Sending and receiving packets will 'block' your Python code until the packet is fully processed. This means you
can't do a lot of other things while sending and waiting for packets to be received. Design your application so
the radio usage is the primary scenario and very little other tasks need to happen in the background.
The module is written to be compatible with the RadioHead RFM69 Arduino library. This means by default the
module will setup the radio with the same GFSK, 250kbit/s, 250khz deviation, and bit whitening radio
configuration so it can send and receive data with itself and other RadioHead-driven modules. In addition the
CircuitPython module uses the same sync word and packet preamble (4 bytes) as RadioHead. If you want to use
different modulations or settings you'll need to configure the radio yourself (see the initialization
code (https://adafru.it/BjF) for the registers and bits to access, however you will need to consult the datasheet for
the necessary values).
The CircuitPython module does not support advanced RadioHead features like guaranteed delivery or its internal
node addressing scheme. Only the simple 'raw' RadioHead examples are supported (i.e. broadcasting a packet
to all listening radios). You can however enable encryption and set an AES encryption key just like with the
RadioHead library. If you need guaranteed delivery or other advanced features you'll need to implement them in
your application code, or design your application be resilient to failures or missed messages.
Wiring With Breakout
First wire up a RFM69 breakout to your board as shown on the previous pages for Arduino. Note that the G0/interrupt
line is not used by the CircuitPython module and can remain unconnected. Here's an example of wiring a Feather M0
to the radio with a SPI connection:
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 32 of 69

Board 3V to radio VIN
Board GND to radio GND
Board SCK to radio SCK
Board MOSI to radio MOSI
Board MISO to radio MISO
Board D5 to radio CS (or any other digital I/O pin)
Board D6 to radio RST (or any other digital I/O pin)
Usage with All-In-One Feather M0
Alternatively you can use the Feather M0 RFM69 board but be sure you've loaded the adafruit-circuitpython-
feather_m0_rfm69-*.bin (https://adafru.it/tBa) version of CircuitPython on your board! This is very important as the
RFM69 build has special pins added to the board module which are used to access the radio's control lines!
For details on how to load a binary circuitpython build, check out our Non-UF2-Install guide (https://adafru.it/Bed)
Adafruit Feather M0 RFM69HCW Packet Radio - 868 or 915
MHz
$24.95
IN STOCK
ADD TO CART
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 33 of 69

Module Install
Next you'll need to install the Adafruit CircuitPython RFM69 (https://adafru.it/BjE) module on your CircuitPython board.
Before you do that make sure you are running the latest version of Adafruit CircuitPython (https://adafru.it/Amd) for
your board too (again be sure to the load the Feather M0 RFM69 version if you're using that board and want to use its
built-in radio module).
Next you'll need to install the necessary libraries to use the hardware--carefully follow the steps to find and install these
libraries from Adafruit's CircuitPython library bundle (https://adafru.it/zdx). Our introduction guide has a great page on
how to install the library bundle (https://adafru.it/ABU) for both express and non-express boards.
Remember for non-express boards like the, you'll need to manually install the necessary libraries from the bundle:
adafruit_rfm69.mpy
adafruit_bus_device
You can also download the adafruit_rfm69.mpy from its releases page on Github (https://adafru.it/Bl2).
Before continuing make sure your board's lib folder or root filesystem has
the adafruit_rfm69.mpy, and adafruit_bus_device files and folders copied over.
Next connect to the board's serial REPL (https://adafru.it/Awz)so you are at the CircuitPython >>> prompt.
Usage
To demonstrate the usage of the radio we'll initialize it and send and receive data from the board's Python REPL.
Run the following code to import the necessary modules and initialize the SPI connection with the sensor:
Now define a few of the pins connected to the RFM69, specifically the CS and RST pins:
Adafruit Feather M0 RFM69HCW Packet Radio - 433MHz
$24.95
IN STOCK
ADD TO CART
import board
import busio
import digitalio
spi = busio.SPI(board.SCK, MOSI=board.MOSI, MISO=board.MISO)
cs = digitalio.DigitalInOut(board.D5)
reset = digitalio.DigitalInOut(board.D6)
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 34 of 69

However if you're using the Feather M0 RFM69 board with a built-in RFM69 radio (and you've loaded the special
version of CircuitPython just for this board as mentioned above), you instead want to use these pins for the CS and RST
lines:
You're ready to import the RFM69 module and create an instance of the RFM69 class inside it. Before you create the
radio module instance you'll need to check if you're using a 433mhz or 915mhz radio module as the initializer requires
the frequency to be specified--confirm which frequency your module uses and run one of the following lines.
For a 915mhz radio use:
Or for a 433mhz radio use:
Notice the initializer takes the following required parameters:
spi - The SPI bus connected to the board.
cs - The DigitalInOut instance connected to the CS line of the radio.
reset - The DigitalInOut instance connected to the RST or reset line of the radio.
frequency - The frequency in megahertz of the radio module. Remember this frequency depends on which type
of radio you're using and the frequency you desire to use!
In addition there are some optional parameters you might specify:
baudrate - The baud rate to use for the SPI connection to the radio. By default this is 10mhz which is as fast as
the radio can handle, but in some cases it might be too fast if you're wiring up a breakout to a breadboard
(breadboards can be notorious for not working well with high speed signals). If you run into odd errors like being
unable to find the RFM69 radio try lowering the baudrate by specifying a baudrate=1000000 keyword (which
sets the speed to a lower 1mhz value).
Once the RFM69 class is created and initialized you're ready to start sending and receiving data.
Remember by default the module will be configured to interface with the "RadioHead" RFM69 setup so you can also
send and receive packets with an Arduino running the 'raw' TX/RX examples!
To send a message simply call the send function and provide a string or byte string of data:
Remember you can only send a message up to 60 bytes in length at a time! Attempting to send a message longer
than 60 bytes will fail with an exception error. If you need to send a longer message it will have to be broken up into
multiple send calls and reconstructed on the receiving side.
cs = digitalio.DigitalInOut(board.RFM69_CS)
reset = digitalio.DigitalInOut(board.RFM69_RST)
import adafruit_rfm69
rfm69 = adafruit_rfm69.RFM69(spi, cs, reset, 915.0)
import adafruit_rfm69
rfm69 = adafruit_rfm69.RFM69(spi, cs, reset, 433.0)
rfm69.send('Hello world!')
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 35 of 69

If you have another RFM69 on the same frequency and modulation waiting to receive messages (like another
CircuitPython module running receive code below) you should see it receive the message.
You can even have an Arduino running the RadioHead library's raw RX example see the message that was sent (be
sure this receiving side has an encryption key setup exactly the same way as the sending side, see the
encryption_key property discussion further below):
To receive a message simply call the receive function. This function will wait for half a second for any packet to be
received. If a packet is found it will be returned as a byte string (remember packets are at most 60 bytes long), or if no
packet was found a result of None is returned.
You can increase the amount of time the module waits for a packet to be received by specifying the time in seconds as
a parameter to the receive call:
Notice this waits longer at the REPL for a packet to be received before returning. If you have another RFM69 setup try
having it send a message while the other is waiting to receive it. You should see a byte string returned. You can also
have an Arduino running the RadioHead library's raw TX example send messages that are received by your code
(again it must be setup with the same encryption key):
rfm69.receive()
rfm69.receive(timeout_s=5.0) # Wait 5 seconds instead of 0.5 seconds.
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 36 of 69

One thing to note in Python byte strings aren't exactly like text strings and you might not be able to do all the text
processing (like find, replace, etc.) as you expect. However you can convert a byte string into text by assuming a
specific text encoding like ASCII. For example to receive a packet and convert the contents to an ASCII text string you
can run code like:
Notice this code first receives a packet, then checks if one was actually found (the packet is not None check--if no
packet is received a value of None is returned), and then converts the packet data to a string assuming an ASCII text
encoding.
Beyond RX & TX
Beyond basic sending and receiving there are a few properties of the RFM69 class you might want to interact with:
encryption_key - This is an optional 16 byte string that defines the AES encryption key used by the radio for
sending and receiving packets. Both the sending and receiving code must have the exact same encryption key
set or they'll be unable to see each other's packets! See the simpletest.py example (https://adafru.it/Bl3) below
for an example of setting the encryption_key to match the default key from RadioHead library raw examples. By
default the RFM69 class assumes no encryption key is set, and you can set this property to the value None to
disable encryption.
rssi - The received signal strength indicator is a property you can read to see the strength of the radio signal
being received. This is updated when packets are received and returns a value in decibels (typically negative, so
the
smaller
the number and closer to 0, the higher the strength / better the signal).
That's all there is to the basic RFM69 radio usage!
Remember the CircuitPython module is designed for sending and
packet = rfm69.receive() # Wait for a packet to be received (up to 0.5 seconds)
if packet is not None:
packet_text = str(packet, 'ascii')
print('Received: {0}'.format(packet_text))
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 37 of 69

receiving small up to 60 byte control messages and not large or high bandwidth amounts of data.
Here's a complete example of sending a message and waiting to receive and print any received messages. Save this
as main.py on your board and open the serial REPL to see it print data and any received messages. If you have two
boards and radios setup to run this code at the same time they'll send each other a message on start up!
# Simple example to send a message and then wait indefinitely for messages
# to be received. This uses the default RadioHead compatible GFSK_Rb250_Fd250
# modulation and packet format for the radio.
# Author: Tony DiCola
import board
import busio
import digitalio
import adafruit_rfm69
# Define radio parameters.
RADIO_FREQ_MHZ = 915.0 # Frequency of the radio in Mhz. Must match your
# module! Can be a value like 915.0, 433.0, etc.
# Define pins connected to the chip, use these if wiring up the breakout according to the guide:
CS = digitalio.DigitalInOut(board.D5)
RESET = digitalio.DigitalInOut(board.D6)
# Or uncomment and instead use these if using a Feather M0 RFM69 board
# and the appropriate CircuitPython build:
#CS = digitalio.DigitalInOut(board.RFM69_CS)
#RESET = digitalio.DigitalInOut(board.RFM69_RST)
# Define the onboard LED
LED = digitalio.DigitalInOut(board.D13)
LED.direction = digitalio.Direction.OUTPUT
# Initialize SPI bus.
spi = busio.SPI(board.SCK, MOSI=board.MOSI, MISO=board.MISO)
# Initialze RFM radio
rfm69 = adafruit_rfm69.RFM69(spi, CS, RESET, RADIO_FREQ_MHZ)
# Optionally set an encryption key (16 byte AES key). MUST match both
# on the transmitter and receiver (or be set to None to disable/the default).
rfm69.encryption_key = b'\x01\x02\x03\x04\x05\x06\x07\x08\x01\x02\x03\x04\x05\x06\x07\x08'
# Print out some chip state:
print('Temperature: {0}C'.format(rfm69.temperature))
print('Frequency: {0}mhz'.format(rfm69.frequency_mhz))
print('Bit rate: {0}kbit/s'.format(rfm69.bitrate/1000))
print('Frequency deviation: {0}hz'.format(rfm69.frequency_deviation))
# Send a packet. Note you can only send a packet up to 60 bytes in length.
# This is a limitation of the radio packet size, so if you need to send larger
# amounts of data you will need to break it into smaller send calls. Each send
# call will wait for the previous one to finish before continuing.
rfm69.send(bytes('Hello world!\r\n',"utf-8"))
print('Sent hello world message!')
# Wait to receive packets. Note that this library can't receive data at a fast
# rate, in fact it can only receive and process one 60 byte packet at a time.
# This means you should only use this for low bandwidth scenarios, like sending
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 38 of 69

# This means you should only use this for low bandwidth scenarios, like sending
# and receiving a single message at a time.
print('Waiting for packets...')
while True:
packet = rfm69.receive()
# Optionally change the receive timeout from its default of 0.5 seconds:
#packet = rfm69.receive(timeout=5.0)
# If no packet was received during the timeout then None is returned.
if packet is None:
# Packet has not been received
LED.value = False
print('Received nothing! Listening again...')
else:
# Received a packet!
LED.value = True
# Print out the raw bytes of the packet:
print('Received (raw bytes): {0}'.format(packet))
# And decode to ASCII text and print it too. Note that you always
# receive raw bytes and need to convert to a text format like ASCII
# if you intend to do string processing on your data. Make sure the
# sending side is sending ASCII data before you try to decode!
packet_text = str(packet, 'ascii')
print('Received (ASCII): {0}'.format(packet_text))
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 39 of 69

Using the RFM9X Radio
Before beginning make sure you have your Feather working smoothly, it will make this part a lot easier. Once you have
the basic Feather functionality going - you can upload code, blink an LED, use the serial output, etc. you can then
upgrade to using the radio itself.
Note that the sub-GHz radio is not designed for streaming audio or video! It's best used for small packets of data. The
data rate is adjustbale but its common to stick to around 19.2 Kbps (thats bits per second). Lower data rates will be
more successful in their transmissions
You will, of course, need at least two paired radios to do any testing! The radios must be matched in frequency (e.g.
900 MHz & 900 MHz are ok, 900 MHz & 433 MHz are not). They also must use the same encoding schemes, you
cannot have a 900 MHz RFM69 packet radio talk to a 900 MHz RFM96 LoRa radio.
Arduino Library
These radios have really excellent code already written, so rather than coming up with a new standard we suggest
using existing libraries such as AirSpayce's Radiohead library (https://adafru.it/mCA) which also supports a vast number
of other radios
This is a really great Arduino Library, so please support them in thanks for their efforts!
RadioHead RFM9x Library example
To begin talking to the radio, you will need to download the RadioHead library (https://adafru.it/mCA). You can do that
by visiting the github repo and manually downloading or, easier, just click this button to download the zip
corresponding to version 1.62
Note that while all the code in the examples below are based on this version you can visit the RadioHead
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 40 of 69

documentation page to get the most recent version which may have bug-fixes or more
functionality (https://adafru.it/mCA)
https://adafru.it/q6f
https://adafru.it/q6f
Uncompress the zip and find the folder named RadioHead and check that the RadioHead folder contains
RH_RF95.cpp and RH_RF95.h (as well as a few dozen other files for radios that are supported)
Place the RadioHead library folder your arduinosketchfolder/libraries/ folder.
You may need to create the libraries subfolder if its your first library. Restart the IDE.
We also have a great tutorial on Arduino library installation at:
http://learn.adafruit.com/adafruit-all-about-arduino-libraries-install-use (https://adafru.it/aYM)
Basic RX & TX example
Lets get a basic demo going, where one Feather transmits and the other receives. We'll start by setting up the
transmitter
Transmitter example code
This code will send a small packet of data once a second to node address #1
Load this code into your Transmitter Arduino/Feather!
Before uploading, check for the #define RF95_FREQ 915.0 line and change that to 433.0 if you are using the
433MHz version of the LoRa radio!
Uncomment/comment the sections defining the pins for Feather 32u4, Feather M0, etc depending on which
chipset and wiring you are using! The pins used will vary depending on your setup!
// Feather9x_TX
// -*- mode: C++ -*-
// Example sketch showing how to create a simple messaging client (transmitter)
// with the RH_RF95 class. RH_RF95 class does not provide for addressing or
// reliability, so you should only use RH_RF95 if you do not need the higher
// level messaging abilities.
// It is designed to work with the other example Feather9x_RX
#include <SPI.h>
#include <RH_RF95.h>
/* for feather32u4
#define RFM95_CS 8
#define RFM95_RST 4
#define RFM95_INT 7
*/
/* for feather m0
#define RFM95_CS 8
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 41 of 69

#define RFM95_CS 8
#define RFM95_RST 4
#define RFM95_INT 3
*/
/* for shield
#define RFM95_CS 10
#define RFM95_RST 9
#define RFM95_INT 7
*/
/* Feather 32u4 w/wing
#define RFM95_RST 11 // "A"
#define RFM95_CS 10 // "B"
#define RFM95_INT 2 // "SDA" (only SDA/SCL/RX/TX have IRQ!)
*/
/* Feather m0 w/wing
#define RFM95_RST 11 // "A"
#define RFM95_CS 10 // "B"
#define RFM95_INT 6 // "D"
*/
#if defined(ESP8266)
/* for ESP w/featherwing */
#define RFM95_CS 2 // "E"
#define RFM95_RST 16 // "D"
#define RFM95_INT 15 // "B"
#elif defined(ESP32)
/* ESP32 feather w/wing */
#define RFM95_RST 27 // "A"
#define RFM95_CS 33 // "B"
#define RFM95_INT 12 // next to A
#elif defined(NRF52)
/* nRF52832 feather w/wing */
#define RFM95_RST 7 // "A"
#define RFM95_CS 11 // "B"
#define RFM95_INT 31 // "C"
#elif defined(TEENSYDUINO)
/* Teensy 3.x w/wing */
#define RFM95_RST 9 // "A"
#define RFM95_CS 10 // "B"
#define RFM95_INT 4 // "C"
#endif
// Change to 434.0 or other frequency, must match RX's freq!
#define RF95_FREQ 915.0
// Singleton instance of the radio driver
RH_RF95 rf95(RFM95_CS, RFM95_INT);
void setup()
{
pinMode(RFM95_RST, OUTPUT);
digitalWrite(RFM95_RST, HIGH);
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 42 of 69

Serial.begin(115200);
while (!Serial) {
delay(1);
}
delay(100);
Serial.println("Feather LoRa TX Test!");
// manual reset
digitalWrite(RFM95_RST, LOW);
delay(10);
digitalWrite(RFM95_RST, HIGH);
delay(10);
while (!rf95.init()) {
Serial.println("LoRa radio init failed");
while (1);
}
Serial.println("LoRa radio init OK!");
// Defaults after init are 434.0MHz, modulation GFSK_Rb250Fd250, +13dbM
if (!rf95.setFrequency(RF95_FREQ)) {
Serial.println("setFrequency failed");
while (1);
}
Serial.print("Set Freq to: "); Serial.println(RF95_FREQ);
// Defaults after init are 434.0MHz, 13dBm, Bw = 125 kHz, Cr = 4/5, Sf = 128chips/symbol, CRC on
// The default transmitter power is 13dBm, using PA_BOOST.
// If you are using RFM95/96/97/98 modules which uses the PA_BOOST transmitter pin, then
// you can set transmitter powers from 5 to 23 dBm:
rf95.setTxPower(23, false);
}
int16_t packetnum = 0; // packet counter, we increment per xmission
void loop()
{
delay(1000); // Wait 1 second between transmits, could also 'sleep' here!
Serial.println("Transmitting..."); // Send a message to rf95_server
char radiopacket[20] = "Hello World # ";
itoa(packetnum++, radiopacket+13, 10);
Serial.print("Sending "); Serial.println(radiopacket);
radiopacket[19] = 0;
Serial.println("Sending...");
delay(10);
rf95.send((uint8_t *)radiopacket, 20);
Serial.println("Waiting for packet to complete...");
delay(10);
rf95.waitPacketSent();
// Now wait for a reply
uint8_t buf[RH_RF95_MAX_MESSAGE_LEN];
uint8_t len = sizeof(buf);
Serial.println("Waiting for reply...");
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 43 of 69

Once uploaded you should see the following on the serial console
Now open up another instance of the Arduino IDE - this is so you can see the serial console output from the TX Feather
while you set up the RX Feather.
Receiver example code
This code will receive and acknowledge a small packet of data.
Load this code into your Receiver Arduino/Feather!
Serial.println("Waiting for reply...");
if (rf95.waitAvailableTimeout(1000))
{
// Should be a reply message for us now
if (rf95.recv(buf, &len))
{
Serial.print("Got reply: ");
Serial.println((char*)buf);
Serial.print("RSSI: ");
Serial.println(rf95.lastRssi(), DEC);
}
else
{
Serial.println("Receive failed");
}
}
else
{
Serial.println("No reply, is there a listener around?");
}
}
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 44 of 69

Make sure the #define RF95_FREQ 915.0 matches your transmitter Feather!
Uncomment/comment the sections defining the pins for Feather 32u4, Feather M0, etc depending on which
chipset and wiring you are using! The pins used will vary depending on your setup!
// Feather9x_RX
// -*- mode: C++ -*-
// Example sketch showing how to create a simple messaging client (receiver)
// with the RH_RF95 class. RH_RF95 class does not provide for addressing or
// reliability, so you should only use RH_RF95 if you do not need the higher
// level messaging abilities.
// It is designed to work with the other example Feather9x_TX
#include <SPI.h>
#include <RH_RF95.h>
/* for Feather32u4 RFM9x
#define RFM95_CS 8
#define RFM95_RST 4
#define RFM95_INT 7
*/
/* for feather m0 RFM9x
#define RFM95_CS 8
#define RFM95_RST 4
#define RFM95_INT 3
*/
/* for shield
#define RFM95_CS 10
#define RFM95_RST 9
#define RFM95_INT 7
*/
/* Feather 32u4 w/wing
#define RFM95_RST 11 // "A"
#define RFM95_CS 10 // "B"
#define RFM95_INT 2 // "SDA" (only SDA/SCL/RX/TX have IRQ!)
*/
/* Feather m0 w/wing
#define RFM95_RST 11 // "A"
#define RFM95_CS 10 // "B"
#define RFM95_INT 6 // "D"
*/
#if defined(ESP8266)
/* for ESP w/featherwing */
#define RFM95_CS 2 // "E"
#define RFM95_RST 16 // "D"
#define RFM95_INT 15 // "B"
#elif defined(ESP32)
/* ESP32 feather w/wing */
#define RFM95_RST 27 // "A"
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 45 of 69

#define RFM95_CS 33 // "B"
#define RFM95_INT 12 // next to A
#elif defined(NRF52)
/* nRF52832 feather w/wing */
#define RFM95_RST 7 // "A"
#define RFM95_CS 11 // "B"
#define RFM95_INT 31 // "C"
#elif defined(TEENSYDUINO)
/* Teensy 3.x w/wing */
#define RFM95_RST 9 // "A"
#define RFM95_CS 10 // "B"
#define RFM95_INT 4 // "C"
#endif
// Change to 434.0 or other frequency, must match RX's freq!
#define RF95_FREQ 915.0
// Singleton instance of the radio driver
RH_RF95 rf95(RFM95_CS, RFM95_INT);
// Blinky on receipt
#define LED 13
void setup()
{
pinMode(LED, OUTPUT);
pinMode(RFM95_RST, OUTPUT);
digitalWrite(RFM95_RST, HIGH);
Serial.begin(115200);
while (!Serial) {
delay(1);
}
delay(100);
Serial.println("Feather LoRa RX Test!");
// manual reset
digitalWrite(RFM95_RST, LOW);
delay(10);
digitalWrite(RFM95_RST, HIGH);
delay(10);
while (!rf95.init()) {
Serial.println("LoRa radio init failed");
while (1);
}
Serial.println("LoRa radio init OK!");
// Defaults after init are 434.0MHz, modulation GFSK_Rb250Fd250, +13dbM
if (!rf95.setFrequency(RF95_FREQ)) {
Serial.println("setFrequency failed");
while (1);
}
Serial.print("Set Freq to: "); Serial.println(RF95_FREQ);
// Defaults after init are 434.0MHz, 13dBm, Bw = 125 kHz, Cr = 4/5, Sf = 128chips/symbol, CRC on
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 46 of 69

Now open up the Serial console on the receiver, while also checking in on the transmitter's serial console. You should
see the receiver is...well, receiving packets
// Defaults after init are 434.0MHz, 13dBm, Bw = 125 kHz, Cr = 4/5, Sf = 128chips/symbol, CRC on
// The default transmitter power is 13dBm, using PA_BOOST.
// If you are using RFM95/96/97/98 modules which uses the PA_BOOST transmitter pin, then
// you can set transmitter powers from 5 to 23 dBm:
rf95.setTxPower(23, false);
}
void loop()
{
if (rf95.available())
{
// Should be a message for us now
uint8_t buf[RH_RF95_MAX_MESSAGE_LEN];
uint8_t len = sizeof(buf);
if (rf95.recv(buf, &len))
{
digitalWrite(LED, HIGH);
RH_RF95::printBuffer("Received: ", buf, len);
Serial.print("Got: ");
Serial.println((char*)buf);
Serial.print("RSSI: ");
Serial.println(rf95.lastRssi(), DEC);
// Send a reply
uint8_t data[] = "And hello back to you";
rf95.send(data, sizeof(data));
rf95.waitPacketSent();
Serial.println("Sent a reply");
digitalWrite(LED, LOW);
}
else
{
Serial.println("Receive failed");
}
}
}
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 47 of 69

You can see that the library example prints out the hex-bytes received 48 65 6C 6C 6F 20 57 6F 72 6C 64 20 23 30 0
20 20 20 20 0 , as well as the ASCII 'string' Hello World . Then it will send a reply.
And, on the transmitter side, it is now printing that it got a reply after each transmisssion And hello back to you
because it got a reply from the receiver
That's pretty much the basics of it! Lets take a look at the examples so you know how to adapt to your own radio setup
Feather Radio Pinout
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 48 of 69

This is the pinout setup for all Feather 32u4 RFM9X's:
This is the pinout for all Feather M0 RFM9X's:
Frequency
You can dial in the frequency you want the radio to communicate on, such as 915.0, 434.0 or 868.0 or any number
really. Different countries/ITU Zones have different ISM bands so make sure you're using those or if you are licensed,
those frequencies you may use
You can then instantiate the radio object with our custom pin numbers.
Setup
We begin by setting up the serial console and hard-resetting the Radio
Remove the while (!Serial); line if you are not tethering to a computer, as it will cause the Feather to halt until a USB
/* for feather32u4 */
#define RFM95_CS 8
#define RFM95_RST 4
#define RFM95_INT 7
/* for feather m0 */
#define RFM95_CS 8
#define RFM95_RST 4
#define RFM95_INT 3
// Change to 434.0 or other frequency, must match RX's freq!
#define RF95_FREQ 915.0
// Singleton instance of the radio driver
RH_RF95 rf95(RFM95_CS, RFM95_INT);
void setup()
{
pinMode(LED, OUTPUT);
pinMode(RFM95_RST, OUTPUT);
digitalWrite(RFM95_RST, HIGH);
while (!Serial); // wait until serial console is open, remove if not tethered to computer
Serial.begin(9600);
delay(100);
Serial.println("Feather LoRa RX Test!");
// manual reset
digitalWrite(RFM95_RST, LOW);
delay(10);
digitalWrite(RFM95_RST, HIGH);
delay(10);
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 49 of 69

connection is made!
Initializing Radio
The library gets initialized with a call to init(). Once initialized, you can set the frequency. You can also configure the
output power level, the number ranges from 5 to 23. Start with the highest power level (23) and then scale down as
necessary
Transmission Code
If you are using the transmitter, this code will wait 1 second, then transmit a packet with "Hello World #" and an
incrementing packet number
Its pretty simple, the delay does the waiting, you can replace that with low power sleep code. Then it generates the
packet and appends a number that increases every tx. Then it simply calls send to transmit the data, and passes in the
array of data and the length of the data.
Note that this does not any addressing or subnetworking - if you want to make sure the packet goes to a particular
while (!rf95.init()) {
Serial.println("LoRa radio init failed");
while (1);
}
Serial.println("LoRa radio init OK!");
// Defaults after init are 434.0MHz, modulation GFSK_Rb250Fd250, +13dbM
if (!rf95.setFrequency(RF95_FREQ)) {
Serial.println("setFrequency failed");
while (1);
}
Serial.print("Set Freq to: "); Serial.println(RF95_FREQ);
// Defaults after init are 434.0MHz, 13dBm, Bw = 125 kHz, Cr = 4/5, Sf = 128chips/symbol, CRC on
// The default transmitter power is 13dBm, using PA_BOOST.
// If you are using RFM95/96/97/98 modules which uses the PA_BOOST transmitter pin, then
// you can set transmitter powers from 5 to 23 dBm:
rf95.setTxPower(23, false);
void loop()
{
delay(1000); // Wait 1 second between transmits, could also 'sleep' here!
Serial.println("Transmitting..."); // Send a message to rf95_server
char radiopacket[20] = "Hello World # ";
itoa(packetnum++, radiopacket+13, 10);
Serial.print("Sending "); Serial.println(radiopacket);
radiopacket[19] = 0;
Serial.println("Sending..."); delay(10);
rf95.send((uint8_t *)radiopacket, 20);
Serial.println("Waiting for packet to complete..."); delay(10);
rf95.waitPacketSent();
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 50 of 69

radio, you may have to add an identifier/address byte on your own!
Then you call waitPacketSent() to wait until the radio is done transmitting. You will not get an automatic
acknowledgement, from the other radio unless it knows to send back a packet. Think of it like the 'UDP' of radio - the
data is sent, but its not certain it was received! Also, there will not be any automatic retries.
Receiver Code
The Receiver has the same exact setup code, but the loop is different
Instead of transmitting, it is constantly checking if there's any data packets that have been received. available() will
return true if a packet with proper error-correction was received. If so, the receiver prints it out in hex and also as a
'character string'
It also prints out the RSSI which is the receiver signal strength indicator. This number will range from about -15 to about
-100. The larger the number (-15 being the highest you'll likely see) the stronger the signal.
Once done it will automatically reply, which is a way for the radios to know that there was an acknowledgement
It simply sends back a string and waits till the reply is completely sent
void loop()
{
if (rf95.available())
{
// Should be a message for us now
uint8_t buf[RH_RF95_MAX_MESSAGE_LEN];
uint8_t len = sizeof(buf);
if (rf95.recv(buf, &len))
{
digitalWrite(LED, HIGH);
RH_RF95::printBuffer("Received: ", buf, len);
Serial.print("Got: ");
Serial.println((char*)buf);
Serial.print("RSSI: ");
Serial.println(rf95.lastRssi(), DEC);
// Send a reply
uint8_t data[] = "And hello back to you";
delay(200);
rf95.send(data, sizeof(data));
rf95.waitPacketSent();
Serial.println("Sent a reply");
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 51 of 69

CircuitPython for RFM9x
LoRa
It's easy to use the RFM9x LoRa radio with CircuitPython and the Adafruit CircuitPython
RFM9x (https://adafru.it/BjD) module. This module allows you to easily write Python code that sends and receives
packets of data with the radio. Be careful to note this library is for the RFM95/96/97/98 LoRa radio only and will
not work with the simper RFM69 packet radio.
Design Considerations
One thing to be aware of before you use the RFM9x series of radios with CircuitPython are some of the limitations and
design considerations for its module. Keep these in mind as you think about projects using the RFM9x and
CircuitPython:
You can only send and receive packets up to 252 bytes in length at a time. The size of the radio's internal buffer
dictates this limit so if you want to send longer messages you'll need to break them into a series of smaller send
calls in your application code.
Receiving packets is a 'best effort' in pure Python code. Unlike the Arduino versions of the RFM9x library there is
no interrupt support which means when a packet is received it must be immediately processed by the Python
code or it could be lost. For your application it will work best to only receive small, single packet messages at a
time. Don't try to receive kilobytes of data or else you'll lose packets. This module is really intended for simple
single packet messages like 'ON', 'OFF', etc.
Sending and receiving packets will 'block' your Python code until the packet is fully processed. This means you
can't do a lot of other things while sending and waiting for packets to be received. Design your application so
the radio usage is the primary scenario and very little other tasks need to happen in the background.
The module is written to be compatible with the RadioHead RFM95 Arduino library. This means by default the
module will setup the radio with the same modulation and configuration for transmitting and receiving at the
maximum distance with LoRa support. In addition the CircuitPython module uses the same packet preamble (8
bytes) and header (4 bytes) as RadioHead. If you want to use different modulations or settings you'll need to
configure the radio yourself after carefully consulting the datasheet.
The CircuitPython module does not support advanced RadioHead features like guaranteed delivery or its internal
node addressing scheme. Only the simple 'raw' RadioHead examples are supported (i.e. broadcasting a packet
to all listening radios).
Encryption and sync words are also not supported by the LoRa radio module. You must perform these
operations yourself in your application code if they're desired.
Wiring With Breakout
First wire up a RFM9x breakout to your board as shown on the previous pages for Arduino. Note that the G0/interrupt
line is not used by the CircuitPython module and can remain unconnected. Here's an example of wiring a Feather M0
to the radio with a SPI connection:
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 52 of 69

Board 3V to radio VIN
Board GND to radio GND
Board SCK to radio SCK
Board MOSI to radio MOSI
Board MISO to radio MISO
Board D5 to radio CS (or any other digital I/O pin)
Board D6 to radio RST (or any other digital I/O pin)
Usage with All-In-One Feather M0
Alternatively you can use the Feather M0 RFM9x board but be sure you've loaded the adafruit-circuitpython-
feather_m0_rfm9x-*.bin (https://adafru.it/tBa) version of CircuitPython on your board! This is very important as the
RFM9x build has special pins added to the board module which are used to access the radio's control lines!
For details on how to load a binary circuitpython build, check out our Non-UF2-Install guide (https://adafru.it/Bed)
The Feather M0 LoRa does NOT come with UF2 bootloader or CircuitPython pre-installed, you must do 2
things before you can use it with CircuitPython - update the bootloader manually, and install CircuitPython
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 53 of 69

Module Install
Next you'll need to install the Adafruit CircuitPython RFM9x (https://adafru.it/BjD) module on your CircuitPython board.
Before you do that make sure you are running the latest version of Adafruit CircuitPython (https://adafru.it/Amd) for
your board too (again be sure to the load the Feather M0 RFM9x version if you're using that board and want to use its
built-in radio module).
Next you'll need to install the necessary libraries to use the hardware--carefully follow the steps to find and install these
libraries from Adafruit's CircuitPython library bundle (https://adafru.it/zdx). Our introduction guide has a great page on
how to install the library bundle (https://adafru.it/ABU) for both express and non-express boards.
Remember for non-express boards like the, you'll need to manually install the necessary libraries from the bundle:
adafruit_rfm9x.mpy
adafruit_bus_device
You can also download the adafruit_rfm9x.mpy from its releases page on Github (https://adafru.it/Bl1).
Before continuing make sure your board's lib folder or root filesystem has
the adafruit_rfm9x.mpy, and adafruit_bus_device files and folders copied over.
Next connect to the board's serial REPL (https://adafru.it/Awz)so you are at the CircuitPython >>> prompt.
Usage
To demonstrate the usage of the radio we'll initialize it and send and receive data from the board's Python REPL.
Adafruit Feather M0 with RFM95 LoRa Radio - 900MHz
OUT OF STOCK
OUT OF STOCK
Adafruit Feather M0 RFM96 LoRa Radio - 433MHz
$34.95
IN STOCK
ADD TO CART
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 54 of 69

Run the following code to import the necessary modules and initialize the SPI connection with the radio:
Now define a few of the pins connected to the RFM9x, specifically the CS and RST pins:
However if you're using the Feather M0 RFM69 board with a built-in RFM9x radio (and you've loaded the special
version of CircuitPython just for this board as mentioned above), you instead want to use these pins for the CS and RST
lines:
You're ready to import the RFM9x module and create an instance of the RFM9x class inside it. Before you create the
radio module instance you'll need to check if you're using a 433mhz or 915mhz radio module as the initializer requires
the frequency to be specified--confirm which frequency your module uses and run one of the following lines.
For a 915mhz radio use:
Or for a 433mhz radio use:
Notice the initializer takes the following required parameters:
spi - The SPI bus connected to the board.
cs - The DigitalInOut instance connected to the CS line of the radio.
reset - The DigitalInOut instance connected to the RST or reset line of the radio.
frequency - The frequency in megahertz of the radio module. Remember this frequency depends on which type
of radio you're using and the frequency you desire to use!
In addition there are some optional parameters you might specify:
baudrate - The baud rate to use for the SPI connection to the radio. By default this is 10mhz which is as fast as
the radio can handle, but in some cases it might be too fast if you're wiring up a breakout to a breadboard
(breadboards can be notorious for not working well with high speed signals). If you run into odd errors like being
unable to find the RFM9x radio try lowering the baudrate by specifying a baudrate=1000000 keyword (which
sets the speed to a lower 1mhz value).
import board
import busio
import digitalio
spi = busio.SPI(board.SCK, MOSI=board.MOSI, MISO=board.MISO)
cs = digitalio.DigitalInOut(board.D5)
reset = digitalio.DigitalInOut(board.D6)
cs = digitalio.DigitalInOut(board.RFM9X_CS)
reset = digitalio.DigitalInOut(board.RFM9X_RST)
import adafruit_rfm9x
rfm9x = adafruit_rfm9x.RFM9x(spi, cs, reset, 915.0)
import adafruit_rfm9x
rfm9x = adafruit_rfm9x.RFM9x(spi, cs, reset, 433.0)
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 55 of 69

Once the RFM9x class is created and initialized you're ready to start sending and receiving data.
Remember by default the module will be configured to interface with the "RadioHead" RFM9x setup so you can also
send and receive packets with an Arduino running the RFM95 TX/RX examples!
To send a message simply call the send function and provide a string or byte string of data:
Remember you can only send a message up to 252 bytes in length at a time! Attempting to send a message longer
than 252 bytes will fail with an exception error. If you need to send a longer message it will have to be broken up into
multiple send calls and reconstructed on the receiving side.
If you have another RFM9x on the same frequency waiting to receive messages (like another CircuitPython module
running receive code below) you should see it receive the message.
You can even have an Arduino running the RadioHead library's RFM95 client example see the message that was sent:
To receive a message simply call the receive function. This function will wait for half a second for any packet to be
received. If a packet is found it will be returned as a byte string (remember packets are at most 252 bytes long), or if
no packet was found a result of None is returned.
You can increase the amount of time the module waits for a packet to be received by specifying the time in seconds as
a parameter to the receive call:
rfm9x.send('Hello world!')
rfm9x.receive()
rfm9x.receive(timeout_s=5.0) # Wait 5 seconds instead of 0.5 seconds.
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 56 of 69

Notice this waits longer at the REPL for a packet to be received before returning. If you have another RFM9x setup try
having it send a message while the other is waiting to receive it. You should see a byte string returned. You can also
have an Arduino running the RadioHead library's RFM95 client example send messages that are received by your
code:
One thing to note in Python byte strings aren't exactly like text strings and you might not be able to do all the text
processing (like find, replace, etc.) as you expect. However you can convert a byte string into text by assuming a
specific text encoding like ASCII. For example to receive a packet and convert the contents to an ASCII text string you
can run code like:
Notice this code first receives a packet, then checks if one was actually found (the packet is not None check--if no
packet is received a value of None is returned), and then converts the packet data to a string assuming an ASCII text
encoding.
Beyond RX & TX
Beyond basic sending and receiving there are a few properties of the RFM69 class you might want to interact with:
tx_power - This is a power level (in dB) to use when transmitting with the radio. By default this is set to a
moderate 13 dB value, however you can increase this depending on the type of radio you're using. For high
power radios (the modules sold by Adafruit) they support a range of TX power from 5 to 23 dB. Try increasing
this to the maximum 23 dB level (however check your local laws for permission to transmit with such power!) to
get the most distance and range.
rssi - The received signal strength indicator is a property you can read to see the strength of the radio signal
being received. This is updated when packets are received and returns a value in decibels (typically negative, so
the
smaller
the number and closer to 0, the higher the strength / better the signal).
packet = rfm9x.receive() # Wait for a packet to be received (up to 0.5 seconds)
if packet is not None:
packet_text = str(packet, 'ascii')
print('Received: {0}'.format(packet_text))
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 57 of 69

That's all there is to the basic RFM9x radio usage!
Remember the CircuitPython module is designed for sending and
receiving small up to 252 byte control messages and not large or high bandwidth amounts of data.
Here's a complete example of sending a message and waiting to receive and print any received messages. Save this
as main.py on your board and open the serial REPL to see it print data and any received messages. If you have two
boards and radios setup to run this code at the same time they'll send each other a message on start up!
Temporarily unable to load content:
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 58 of 69

Radio Range F.A.Q.
Which gives better range, LoRa or RFM69?
All other things being equal (antenna, power output, location) you will get better range with LoRa than with RFM69
modules. We've found 50% to 100% range improvement is common.
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 59 of 69

What ranges can I expect for RFM69 radios?
The RFM69 radios have a range of approx. 500 meters line of sight with tuned uni-directional antennas. Depending
on obstructions, frequency, antenna and power output, you will get lower ranges -
especially
if you are not line of
sight.
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 60 of 69

What ranges can I expect for RFM9X LoRa radios?
The RFM9x radios have a range of up to 2 km line of sight with tuned uni-directional antennas. Depending on
obstructions, frequency, antenna and power output, you will get lower ranges -
especially
if you are not line of sight.
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 61 of 69

I don't seem to be getting the range advetised! Is my module broken?
Your module is probably
not
broken. Radio range is dependant on
a lot of things
and all must be attended to to
make sure you get the best performance!
1. Tuned antenna for your frequency - getting a well tuned antenna is incredibly important. Your antenna must be
tuned for the exact frequency you are using
2. Matching frequency - make sure all modules are on the same exact frequency
3. Matching settings - all radios must have the same settings so they can communicate
4. Directional vs non-directional antennas - for the best range,
directional
antennas like Yagi will direct your energy
in one path instead of all around
5. Good power supply - a nice steady power supply will keep your transmissions clean and strong
6. Max power settings on the radios - they can be set for higher/lower power! Don't forget to set them to max.
7. Line of sight - No obstructions, walls, trees, towers, buildings, mountains, etc can be in the way of your radio path.
Likewise, outdoors is way better than indoors because its very hard to bounce radio paths around a building
8. Radio transmission speed - trying to transmit more data faster will be hard. Go for small packets, with lots of
retransmissions. Lowering the baud rate on the radio (see the libraries for how to do this) will give you better
reliability
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 62 of 69

How do I pick/design the right antenna?
Various antennas will cost diferent amounts and give you different directional gain. In general, spending a lot on a
large fixed antenna can give you better power transfer if the antenna is well tuned. For most simple uses, a wire
works pretty well
The ARRL antena book is recommended if you want to learn how to do the modeling and analysis
But nothing beats actual tests in your environment!
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 63 of 69

What frequency is my module?
Look for a little colored paint dot on top of the module.
GREEN or BLUE = 900 MHz
RED = 433 MHz
Every now and then the paint dot shows up without a color or with the ink dot burnt. This is just a manufacturing
variance and there is nothing wrong with the board. You should get the frequency you ordered though. So if you
plan on mixing these up, you may want to add a new mark of your own.
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 64 of 69

My radio has a burnt blob on it, is it damaged?
Nope! The radios have an ink dot on them, which sometimes gets toasty when we put the board through the oven,
or rework it, so it may have a burnt appearance. The chip is fine!
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 65 of 69

© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 66 of 69

Downloads
Datasheets & Files
RFM9x
SX127x Datasheet (https://adafru.it/oBm)- The RFM9X LoRa radio chip itself
RFM9X (https://adafru.it/mFX) - The radio module, which contains the SX1272 chipset
FCC Test Report (https://adafru.it/q6A)
ETSI Test Report (https://adafru.it/r6a)
RoHS Report (https://adafru.it/r6b)
RFM69
SX1231 Datasheet (https://adafru.it/mCv) - The RFM69 radio chip itself
RFM69HCW datasheet (https://adafru.it/mCu)- contains the SX1231 datasheet plus details about the
module (https://adafru.it/mFX)
RoHS Test Report (https://adafru.it/oC1)
RoHS Test Report (https://adafru.it/oC2)
REACH Test Report (https://adafru.it/oC3)
ETSI Test Report (https://adafru.it/r6c)
FCC Test Report (https://adafru.it/r6d)
EagleCAD PCB files on GitHub (https://adafru.it/r6e)
Fritzing object in Adafruit Fritzing library (https://adafru.it/aP3)
Schematic
(Pinouts are the same for all four radio versions)
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 67 of 69

Fabrication Print
Dimensions in inches
© Adafruit Industries https://learn.adafruit.com/radio-featherwing Page 68 of 69

© Adafruit Industries Last Updated: 2019-06-22 06:39:37 PM UTC Page 69 of 69