CY4500 Quick Start Guide Datasheet by Cypress Semiconductor Corp

View All Related Products | Download PDF Datasheet
a. m... w. wa fi-HFHEHFMHWIGfl .4 Mummm roamglmob Ma Wm 4 i umwwswm 4@w . “mum. ,. Mummmmwmwnm , . Mwmm.kmwua , a manna-mm _ a woman“. _ a "3mm _ 3 WW“,
CY4500 QUICK START GUIDE
CY4500 EZ-PDTM PROTOCOL ANALYZER
1
Review the Analyzer Contents
Download and install the latest Analyzer Setup CY4500
Setup.exe from www.cypress.com/CY4500
• Connect the CY4500
EZ-PD
Protocol Analyzer to your PC
via the USB2.0 Type-A to Micro-B Cable provided with the
Analyzer. Observe LED1 (white color) blink continuously
LED1
2
The driver for this Analyzer is installed automatically.
The board enumerates as Cypress EZ-PD Analyzer
under Universal Serial Bus Controllers in
Windows Device Manager
If the driver is not automatically installed, follow the
note given on the next page to perform a manual
installation
• Launch the
EZ-PD
Analyzer Utility from Start >
All Programs > Cypress > EZ-PD Analyzer Utility
• Click the Start Capturing icon. Alternatively, you
can start capturing data by clicking on Actions >
Start Capturing from the menu bar
4
Upgrade the EZ-PD Protocol Analyzer firmware to the latest version before using the analyzer hardware. For more details,
click Help > User Manual in the EZ-PD Analyzer Utility and refer to Upgrade Firmware section
Note 1:
Turn over for steps 5 and 6
3
EZ-PDTM Protocol
Analyzer Hardware
USB 2.0 Type-A to Micro-B Cable
Jumper Wires (6 nos.)
CY4500 QUICK START GUIDE
CY4500 EZ-PDTM PROTOCOL ANALYZER
• Connect the CY4500
EZ-PD
Protocol Analyzer’s Type-C
plug to the receptacle of a Type-C host device (Notebook
shown as an example)
• Connect a USB Type-C power adapter or other device (not
provided with the Analyzer) to the Type-C receptacle of the
CY4500
EZ-PD
Protocol Analyzer
• The GUI captures the Power Delivery Packets sent on the CC
lines and displays them on the screen. Your display will look
similar to the one shown here
• Click on each message in the main panel for its detailed
description on the side panel of the GUI
• Refer to the
EZ-PD
Analyzer Utility User Guide for additional
details by clicking Help > User Manual
5 6
J7: USB Micro B Connector
J2: USB Type-C Receptacle
PSoC
®
5LP Device
J3: USB Type-C Plug
J1 & J8: USB Type-C Signal and
Message Trigger Header
a. To manually install the driver, in Windows Device Manger, locate the EZ-PD Protocol Analyzer under Other
devices or Unknown devices. Right-click the device and select Update Driver Software. Choose Browse
my computer for driver software
b. Browse to the location <Install Directory>\CY4500 EZ-PD Protocol Analyzer\1.0\EZ-PD Analyzer
Utility\drivers\bin. Select a driver based on the OS and click on Next. E.g. the driver for Win7 64-bit OS
is available at <Install Directory>\CY4500 EZ-PD Protocol Analyzer\1.0\EZ-PD Analyzer Utility
\drivers\bin\Win7\x64. The default <Install Directory> is C:\Program Files\Cypress for a 32-bit
operating system (OS) and C:\Program Files (x86)\Cypress for a 64-bit OS
© 2016-2018 Cypress Semiconductor Corporation. All rights reserved.
All trademarks or registered trademarks referenced herein are the properties of their respective owners.
Doc.#:002-12171 Rev.*D
For the latest information about the Analyzer, visit www.cypress.com/CY4500
Note 3:
J1 & J8: Signal Names
Note 2: Ensure that the Type-C host and power adapter/device
connected to the CY4500 do not exceed 5V on
the CC lines to avoid potential damage to the
CY4500 hardware
CY4500 EZ-PD
TM
Protocol Analyzer Hardware Details

Products related to this Datasheet

EZ-PD PROTOCOL ANALYZER KIT