NUCLEO-zzzzKx Data Brief Datasheet by STMicroelectronics

View All Related Products | Download PDF Datasheet
me ,uugmen'ed l7 arm MBED
NUCLEO-G431KB example. Boards with
different references show different
layouts. Picture is not contractual.
Features
Common features
STM32 microcontroller in 32-pin package
1 user LED
1 reset push-button
Board connectors:
◦ Arduino Nano V3 expansion connector
Micro-AB USB connector for the ST-LINK
Flexible power-supply options: ST-LINK, USB VBUS or external sources
On-board ST-LINK debugger/programmer with USB re-enumeration
capability: mass storage, Virtual COM port and debug port
Comprehensive free software libraries and examples available with the
STM32Cube MCU Package
Support of a wide choice of Integrated Development Environments (IDEs)
including IAR, Keil® and GCC-based IDEs
Board-specific features
24 MHz crystal oscillator
Arm® Mbed Enabled compliant
Description
The STM32 Nucleo-32 board provides an affordable and flexible way for users to try
out new concepts and build prototypes by choosing from the various combinations of
performance and power consumption features, provided by the STM32
microcontroller.
The Arduino Nano V3 connectivity support allows the easy expansion of the
functionality of the STM32 Nucleo open development platform with a wide choice of
specialized shields.
The STM32 Nucleo-32 board does not require any separate probe as it integrates the
ST-LINK debugger/programmer.
The STM32 Nucleo-32 board comes with the STM32 comprehensive free software
libraries and examples available with the STM32Cube MCU Package.
Product status link
NUCLEOXXXXKX
NUCLEO-F031K6, NUCLEO-F042K6,
NUCLEO-F301K8, NUCLEO-F303K8,
NUCLEO-G031K8, NUCLEO-G431KB,
NUCLEO-L011K4, NUCLEO-L031K6,
NUCLEO-L412KB, NUCLEO-L432KC.
STM32 Nucleo-32 boards
NUCLEOXXXXKX
Data brief
DB2638 - Rev 8 - June 2019
For further information contact your local STMicroelectronics sales office.
www.st.com
1Ordering information
To order an STM32 Nucleo-32 board, refer to Table 1. For a detailed description of each board, refer to its user
manual on the product web page. Additional information is available from the datasheet and reference manual of
the target STM32.
Table 1. List of available products
Order code Board
reference
User
manual Target STM32 Differentiating features
NUCLEO-F031K6
MB1180 UM1956
STM32F031K6T6 • Arm® Mbed Enabled
• ST-LINK/V2-1
NUCLEO-F042K6 STM32F042K6T6 • Arm® Mbed Enabled
• ST-LINK/V2-1
NUCLEO-F301K8 STM32F301K8T6 • ST-LINK/V2-1
NUCLEO-F303K8 STM32F303K8T6 • Arm® Mbed Enabled
• ST-LINK/V2-1
NUCLEO-G031K8 MB1455 UM2591 STM32G031K8T6U • ST-LINK/V2-1
NUCLEO-G431KB MB1430 UM2397 STM32G431KBT6U • STLINK-V3E
24 MHz crystal oscillator
NUCLEO-L011K4
MB1180 UM1956
STM32L011K4T6 • Arm® Mbed Enabled
• ST-LINK/V2-1
NUCLEO-L031K6 STM32L031K6T6 • Arm® Mbed Enabled
• ST-LINK/V2-1
NUCLEO-L412KB STM32L412KBU6U • ST-LINK/V2-1
NUCLEO-L432KC STM32L432KCU6U • Arm® Mbed Enabled
• ST-LINK/V2-1
1.1 Product marking
Evaluation tools marked as “ES” or “E” are not yet qualified and therefore not ready to be used as reference
design or in production. Any consequences deriving from such usage will not be at ST charge. In no event, ST will
be liable for any customer usage of these engineering sample tools as reference design or in production.
“E” or “ES” marking examples of location:
On the targeted STM32 that is soldered on the board (for illustration of STM32 marking, refer to the STM32
datasheet “Package information” paragraph at the www.st.com website).
Next to the evaluation tool ordering part number that is stuck or silk-screen printed on the board.
Some boards feature a specific STM32 device version, which allows the operation of any bundled commercial
stack/library available. This STM32 device shows a "U" marking option at the end of the standard part number
and is not available for sales.
In order to use the same commercial stack in his application, a developer may need to purchase a part number
specific to this stack/library. The price of those part numbers includes the stack/library royalties.
1.2 Codification
The meaning of the codification is explained in Table 2.
NUCLEOXXXXKX
Ordering information
DB2638 - Rev 8 page 2/6
Table 2. Codification explanation
NUCLEO-XXYYKT Description Example: NUCLEO-G431KB
XX MCU series in STM32 Arm Cortex MCUs STM32G4 Series
YY MCU product line in the series STM32G431
K STM32 package pin count 32 pins
T
STM32 Flash memory size:
4 for 16 Kbytes
6 for 32 Kbytes
8 for 64 Kbytes
B for 128 Kbytes
C for 256 Kbytes
128 Kbytes
The order code is mentioned on a sticker placed on the top side of the board.
NUCLEOXXXXKX
Codification
DB2638 - Rev 8 page 3/6
2Development environment
2.1 System requirements
• Windows® OS (7, 8 and 10), Linux® 64-bit, or macOS®
USB Type-A to Micro-B cable
Note: macOS® is a trademark of Apple Inc. registered in the U.S. and other countries.
2.2 Development toolchains
• Keil® MDK-ARM(1)
• IAR EWARM(1)
GCC-based IDEs
• Arm® Mbed™(2) online(3) (see mbed.org)
Note: 1. On Windows® only.
2. Arm and Mbed are registered trademarks or trademarks of Arm Limited (or its subsidiaries) in the US and
or elsewhere.
3. Refer to the www.mbed.com website and to the “Ordering information” section to determine which order
codes are supported.
2.3 Demonstration software
The demonstration software, included in the STM32Cube MCU Package corresponding to the on-board
microcontroller, is preloaded in the STM32 Flash memory for easy demonstration of the device peripherals in
standalone mode. The latest versions of the demonstration source code and associated documentation can be
downloaded from www.st.com.
NUCLEOXXXXKX
Development environment
DB2638 - Rev 8 page 4/6
Revision history
Table 3. Document revision history
Date Version Changes
08-Sep-2015 1 Initial release.
15-Jan-2016 2 Added Table 1: Device summary and updated Table 2: Ordering information.
09-Jun-2016 3 Updated Section : Description and Section : System requirements to add
NUCLEO-L432KC.
07-Jul-2017 4 Updated Features.
23-Aug-2018 5
Extended document scope to NUCLEO-L412KB.
Updated Table 1: Device summary, System requirements, Development
toolchains, and Ordering information. Added Demonstration software.
13-Nov-2018 6 Extended document scope to NUCLEO-F301K8: updated Features, Table 1:
Device summary, and Table 2: Ordering information.
10-May-2019 7
Revised the entire document to accommodate multiple feature combinations:
Reorganized Features
Updated Description
Updated Ordering information
Added Development environment
Updated Table 1. List of available products and Table 2. Codification
explanation
Extended document scope to the NUCLEO-G431KB board.
5-Jun-2019 8
Extended document scope to the NUCLEO-G031K8 board.
Global product description: updated Features, Ordering information, and
System requirements.
NUCLEOXXXXKX
DB2638 - Rev 8 page 5/6
IMPORTANT NOTICE – PLEASE READ CAREFULLY
STMicroelectronics NV and its subsidiaries (“ST”) reserve the right to make changes, corrections, enhancements, modifications, and improvements to ST
products and/or to this document at any time without notice. Purchasers should obtain the latest relevant information on ST products before placing orders. ST
products are sold pursuant to ST’s terms and conditions of sale in place at the time of order acknowledgement.
Purchasers are solely responsible for the choice, selection, and use of ST products and ST assumes no liability for application assistance or the design of
Purchasers’ products.
No license, express or implied, to any intellectual property right is granted by ST herein.
Resale of ST products with provisions different from the information set forth herein shall void any warranty granted by ST for such product.
ST and the ST logo are trademarks of ST. For additional information about ST trademarks, please refer to www.st.com/trademarks. All other product or service
names are the property of their respective owners.
Information in this document supersedes and replaces information previously supplied in any prior versions of this document.
© 2019 STMicroelectronics – All rights reserved
NUCLEOXXXXKX
DB2638 - Rev 8 page 6/6

Products related to this Datasheet

NUCLEO-32 STM32F031K6 DEV EVAL
NUCLEO-32 STM32F042K6 DEV EVAL
NUCLEO-32 STM32F303K8 DEV EVAL
NUCLEO-32 STM32L031K6 EVAL BRD
NUCLEO-32 STM32L011K4 EVAL BRD
NUCLEO-32 STM32L432KC EVAL BRD
> /html>