EX-Z Series Instruction Manual Datasheet by Panasonic Industrial Automation Sales

View All Related Products | Download PDF Datasheet
E I Q? [F’fi : «33 \ I (E I <fl> (FR) J L? I , ,. g ‘ ,,}‘ \, / % * r T «r / \ Panasonic Industrial Devices SUNX Co., Ltd. , , \ / \ |:|
INSTRUCTION MANUAL
Ultra-minute Photoelectric Sensor
EX-Z Series
MJECK-EXZ No.0048-07V
Thank you very much for purchasing Panasonic prod-
ucts. Read this Instruction Manual carefully and thor-
oughly for the correct and optimum use of this product.
Kindly keep this manual in a convenient place for quick
reference.
Please refer “our web site (http://panasonic.net/id/
pidsx/global)”.
Access method is “Download” → “Manual”→ “Model No.”.
If you could not visit our web site, contact our sales
office near your sight.
WARNING
Never use this product as a sensing device for per-
sonnel protection.
In case of using sensing devices for personnel pro-
tection, use products which meet laws and standards,
such as OSHA, ANSI or IEC etc., for personnel pro-
tection applicable in each region or country.
1
INTENDED PRODUCTS FOR CE MARKING
This product complies with the following standards /
regulations.
<EU Directive>
EMC Directive
Contact for CE
Panasonic Marketing Europe GmbH Panasonic Testing Center
Winsbergring 15, 22525 Hamburg,Germany
2PART DESCRIPTION
Name Function
1
Stability indi-
cator (Green)
(Note)
Lights up under the sta-
ble light condition or the
stable dark condition.
2
Operation indi-
cator (Orange)
(Note)
Lights up when the
sensing output is
ON.
2 1
Side
sensing
2 1
Front
sensing
Note: Not incorporated on the emitter.
3MOUNTING
The tightening torque should be 0.2N∙m or less.
The M2 screws, nuts, spring washers and flat wash-
ers are provided with this product.
<Side sensing> <Front sensing>
(Unit: mm)
Sensing
direction
Sensing
direction
8.5 8.5
M2 screw (length 10)
Thickness of mounting plate:
2 or less
Thickness of mounting plate:
2 or less
M2 screw (length 6)
Nuts
Spring washer
Flat washer
4WIRING DIAGRAMS
NPN output type
(Brown) +V
(Black) Output
(Note)
(Blue) 0V
Load
+
12 to 24V DC
±10%
-
PNP output type
(Brown) +V
(Black) Output
(Note)
(Blue) 0V
Load
+
12 to 24V DC
±10%
-
Note: The emitter does not incorporate the output (black).
5CAUTIONS
This product has been developed / produced for in-
dustrial use only.
The thin cable 0.1mm2 is used for this product. Note
that if the cable is forcibly pulled, there is a possibility
of this product being damaged, or the cable being
disconnected.
Extension up to total 50m (each emitter and receiver),
or less, is possible with 0.3mm2, or more of conductor
area cable.
Make sure to carry out wiring in the power supply
OFF condition.
Take care that wrong wiring will damage the sensor.
Verify that the supply voltage variation is within the rating.
If power is supplied from a commercial switching reg-
ulator, ensure that the frame ground (F.G.) terminal of
the power supply is connected to an actual ground.
In case noise generating equipment (switching regu-
lator, inverter motor, etc.) is used in the vicinity of this
product, connect the frame ground (F.G.) terminal of
the equipment to an actual ground.
Do not run the wires together with high-voltage lines
or power lines or put them in the same raceway. This
can cause malfunction due to induction.
Take care that the sensor is not directly exposed to
fluorescent lamp from a rapid-starter lamp, a high
frequency lighting device or sunlight etc., as it may
affect the sensing performance.
Do not use during the initial transient time (50ms) af-
ter the power supply is switched ON.
This sensor is suitable for indoor use only.
Do not use this sensor in places having excessive
vapor, dust, etc., or where it may come in contact with
corrosive gas, etc.
Take care that the sensor does not come in contact
with oil, grease, organic solvents such as thinner,
etc., strong acid, or alkaline.
This sensor cannot be used in an environment con-
taining inflammable or explosive gases.
Never disassemble or modify the sensor.
Since the cable end is not waterproof, do not use the
sensor in the application where water may seep in
from the cable end.
6RoHS DIRECTIVE
This equipment complies with RoHS (EC and Chi-
nese directive).
Chinese RoHS indicates inclusion despite regulation
value. (Refer to Chinese part.)
http://panasonic.net/id/pidsx/global
Overseas Sales Division (Head Office)
2431-1 Ushiyama-cho, Kasugai-shi, Aichi, 486-0901, Japan
Phone: +81-568-33-7861 FAX: +81-568-33-8591
For sales network, please visit our website.
© Panasonic Industrial Devices SUNX Co., Ltd. 2015
PRINTED IN JAPAN

Products related to this Datasheet

SENSOR THROUGH-BEAM 50MM PNP
SENSOR THROUGH-BEAM 500MM PNP
SENSOR THROUGH-BEAM 200MM PNP
SENSOR THROUGH-BEAM 50MM NPN
SENSOR THROUGH-BEAM 200MM PNP
SENSOR THROUGH-BEAM 200MM NPN
SENSOR THROUGH-BEAM 50MM NPN
SENSOR THROUGH-BEAM 500MM PNP
SENSOR THROUGH-BEAM 500MM NPN
SENSOR THROUGH-BEAM 500MM PNP
SENSOR THROUGH-BEAM 200MM PNP
SENSOR THROUGH-BEAM 50MM PNP
SENSOR THROUGH-BEAM 200MM PNP
SENSOR THROUGH-BEAM 50MM PNP
SENSOR THROUGH-BEAM 50MM PNP
SENSOR THROUGH-BEAM 50MM NPN
MOUNTING BRACKET FOR FRONT EXZ S
SENSOR THROUGH-BEAM 500MM NPN
MOUNTING BRACKET FOR SIDE EXZ SE
SPACER FOR FRONT EXZ SERIES
SENSOR THROUGH-BEAM 50MM NPN
SENSOR THROUGH-BEAM 200MM PNP
SENSOR THROUGH-BEAM 50MM NPN
SENSOR THROUGH-BEAM 200MM NPN
SENSOR THROUGH-BEAM 500MM NPN
SENSOR THROUGH-BEAM 200MM NPN
SENSOR THROUGH-BEAM 200MM NPN
SENSOR THROUGH-BEAM 50MM PNP
SENSOR THROUGH-BEAM 200MM NPN
SENSOR THROUGH-BEAM 50MM NPN