1438~ Datasheet by Adafruit Industries LLC

View All Related Products | Download PDF Datasheet
ARDUINO / SHIELDS
Adafruit Motor/Stepper/Servo Shield for
Arduino v2 Kit - v2.3
PRODUCT ID: 1438
-DESCRIPTION
The original Adafruit Motorshield kit is one of our most beloved kits, which is why
we decided to make something even better. We have upgraded the shield kit to
make the bestest, easiest way to drive DC and Stepper motors. This shield will
make quick work of your next robotics project! We kept the ability to drive up to 4
DC motors or 2 stepper motors, but added many improvements:
Instead of a L293D darlington driver, we now have the TB6612 MOSFET driver: with
1.2A per channel and 3A peak current capability. It also has much lower voltage
drops across the motor so you get more torque out of your batteries, and there are
built-in flyback diodes as well.
Instead of using a latch and the Arduino's PWM pins, we have a fully-dedicated
PWM driver chip onboard. This chip handles all the motor and speed controls over
I2C. Only two pins (SDA & SCL) are required to drive the multiple motors, and since
it's I2C you can also connect any other I2C devices or shields to the same pins. This
also makes it drop-in compatible with any Arduino, such as the Uno, Due,
Leonardo and Mega R3.
Completely stackable design: 5 address-select pins means up to 32 stackable
shields: that's 64 steppers or 128 DC motors! What on earth could you do with that
many steppers? I have no idea but if you come up with something send us a photo
because that would be a pretty glorious project.
Lots of other little improvements such as a polarity protection FET on the power
pins and a bit of prototyping area. And the shield is assembled and tested here at
Adafruit so all you have to do is solder on straight or stacking headers and the
terminal blocks.
Lets check out these specs again:
http://www.adafruit.com/products/1438 7/16/2015
2 connections for 5V 'hobby' servos connected to the Arduino's high-
resolution dedicated timer - no jitter!
4 H-Bridges: TB6612 chipset provides 1.2A per bridge (3A peak) with thermal
shutdown protection, internal kickback protection diodes. Can run motors on
4.5VDC to 13.5VDC.
Up to 4 bi-directional DC motors with individual 8-bit speed selection (so,
about 0.5% resolution)
Up to 2 stepper motors (unipolar or bipolar) with single coil, double coil,
interleaved or micro-stepping.
Motors automatically disabled on power-up
Big terminal block connectors to easily hook up wires (18-26AWG) and power
Arduino reset button brought up top
Polarity protected 2-pin terminal block and jumper to connect external power,
for separate logic/motor supplies
Tested compatible with Arduino UNO, Leonardo, ADK/Mega R3, Due,
Diecimila & Duemilanove. Works with Mega/ADK R2 and earlier with 2 wire
jumpers.
Download the easy-to-use Arduino software library, check out the examples
and you're ready to go!
Comes with an assembled & tested shield, terminal block, plain header, jumper.
Some soldering is required to assemble the headers on. Stacking headers not
included, but we sell them in the shop so if you want to stack shields, please pick
them up at the same time. Arduino and motors are not included but we have lots of
motors in the shop and all our hobby servos, DC motors, and stepper motors work
great.
We have a great tutorial in the Adafruit Learning System with a lot of
documentation and example code, so please check it out
7
/
16
/
201
5
htt
p
://www.adafruit.com/
p
roducts/1438

Products related to this Datasheet

KIT MOTORSHIELD ARDUIN V2 KIT2.3