Confidential and Proprietary
TM
Erratum A-007207: TBI LINK
STATUS SGMII STAYS UP
PB #16225
May 2014
Affected Devices: 8156 8313 8315 8378 8533
8544 8535 8536 8569 8572 P1010 P1020 P1022
P1023 P2020

TM
Confidential and Proprietary 2
Erratum – A-007207

TM
Confidential and Proprietary 3
Erratum – A-007207
TBI link status may stay “up” after SGMII electrical idle detected
Devices: 8156 8313 8315 8378 8533 8544 8535 8536 8569 8572 P1010 P1020 P1022 P1023
P2020
Description:
The TBI Status Register (SR) contains a link status bit (TBI SR [Link Status]) that represents the current
state of the SGMII link. If Auto-Negotiation (AN) is disabled, the TBI link status bit should become a b’1
indicating the link is up after recognizing IDLE sequences, and stay at b’1 as long as valid data is received &
the TBI is not reset. TBI link status bit should become a b’0 indicating the link is down after several invalid
characters are received or the TBI is reset. If AN is enabled, the TBI link status bit does not become set to
b’1 until auto-negotiation is complete (TBI CR [AN DONE]=1), but the same conditions as AN disabled then
apply for the TBI link status bit to get cleared to b’0.
An electrical idle (common mode) condition on the SGMII link results in the reception of invalid data, and
should cause the TBI link status bit to get cleared. If the transition from active to common mode takes
enough time that the Rx is able to recognize at least 4 more K28.5 characters (for IDLE sequences, 70-80
UI), the portion of the design intended to detect the link down condition may shut off before the link down
condition is actually reflected in the TBI.
This premature shutdown may cause the TBI link status to remain set to a b’1 indicating the link is up. This
'stuck at 1' condition would persist until valid K28.5 characters are received again.

TM
Confidential and Proprietary 4
Erratum – A-007207
TBI link status may stay “up” after SGMII electrical idle detected (cont. 2 of 4)
Impact:
If the system never enters SGMII electrical idle, or if the transition
from active to common mode takes less than 40 UI (~32 ns), then
there is no impact and the false link up scenario does not occur.
If the system can generate an SGMII electrical idle condition as
described above, then the TBI status may stay stuck at 1 while the
link is down and does not transition to 0 until valid K28.5
characters are received again.

TM
Confidential and Proprietary 5
Erratum – A-007207
TBI link status may stay “up” after SGMII electrical idle detected (cont. 3 of 4)
Workaround:
For affected systems, there is no access to electrical idle detection circuitry
in SGMII mode and there is no bit replacement for TBI SR[Link Status] to
monitor.
When the TBI link status is set, the SW can periodically poll
the state of the Ethernet Controller by reading RBYT. If the controller is
expected to receive data packets, RBYT should increment. If RBYT has not
incremented over a period of time it could indicate the link is down. However,
there are various reason why RBYT may not increment (controller configuration
errors, SerDes PLL issues, or MIB Counter RCDE incremented). Examination of
system conditions may be necessary to determine why RBYT has not
incremented.
The link is down if TBI SR[Link Status]=0.

TM
Confidential and Proprietary 6
Erratum – A-007207
TBI link status may stay “up” after SGMII electrical idle detected (cont. 4 of 4)
Disposition:
No plans to fix.

TM
Products related to this Datasheet
IC MPU Q OR IQ 1.2GHZ 689TEBGA
IC MPU Q OR IQ 1.0GHZ 425TEBGA
IC MPU Q OR IQ 1.0GHZ 425TEBGA
IC MPU Q OR IQ 800MHZ 425TEBGA
IC MPU Q OR IQ 1.0GHZ 425TEBGA
IC MPU MPC83XX 333MHZ 516BGA
IC MPU Q OR IQ 1.2GHZ 689TEBGA
IC MPU Q OR IQ 1.067GHZ 689TBGA
IC MPU MPC83XX 667MHZ 689TEBGA
IC MPU MPC83XX 667MHZ 689TEBGA
IC MPU MPC83XX 667MHZ 689TEBGA
IC MPU MPC83XX 667MHZ 689TEBGA
IC MPU Q OR IQ 1.0GHZ 425TEBGA
IC MPU MPC83XX 333MHZ 516BGA
IC MPU MPC83XX 400MHZ 620BGA
IC MPU Q OR IQ 1.2GHZ 689TEBGA
IC MPU Q OR IQ 1.0GHZ 425TEBGA
IC MPU Q OR IQ 1.0GHZ 425TEBGA
IC MPU Q OR IQ 1.0GHZ 425TEBGA
IC MPU Q OR IQ 1.0GHZ 425TEBGA
IC MPU Q OR IQ 800MHZ 425TEBGA
IC MPU Q OR IQ 800MHZ 425TEBGA
IC MPU Q OR IQ 800MHZ 425TEBGA
IC MPU Q OR IQ 800MHZ 425TEBGA
IC MPU Q OR IQ 800MHZ 425TEBGA
IC MPU Q OR IQ 800MHZ 425TEBGA
IC MPU MPC83XX 400MHZ 620BGA
IC MPU Q OR IQ 1.055GHZ 689TBGA
IC MPU Q OR IQ 800MHZ 689TEBGA
IC MPU Q OR IQ 667MHZ 561TEBGA1