ADIS16IMU1/PCBZ Wiki-Guide Datasheet by Analog Devices Inc.
View All Related Products | Download PDF Datasheet
One Technology Way · P.O. Box 9106 · Norwood, MA 02062-9106 · Tel: 781.329.4700 · Fax: 781.461.3113 · www.analog.com
Rev 25 Jun 2013 19:50 | Page 1
ADIS16IMU1/PCBZ Breakout Board
Wiki-Guide
OVERVIEW
The ADIS1613x, ADIS1636x, ADIS16375, ADIS16407 and ADIS1648x IMU products all use a 24-pin,
dual-row, 1mm connector for their electrical interface. This mating connector for their interface
supports surface-mount solder attachment but does not support direct attachment with ribbon cables.
For those who are would like to connect to these IMU/gyroscope products to an existing processor
board, using a ribbon cable, the ADIS16IMU1/PCBZ provides a simple connector translation for this
purpose.
Here is a picture of the contents that come with the ADIS16IMU1/PCBZ.
IMU/GYROSCOPE MOUNTING HOLES
The ADIS16IMU1/PCBZ provides several sets of mounting holes that line up with mounting holes and
tabs on the following products: ADIS1613x, ADIS1636x, ADIS16375, ADIS1640x and ADIS1648x
products. Please see the following picture for device mounting hole locations.

Rev 25 Jun 2013 19:50 | Page 2
ADIS16133, ADIS16135, ADIS1636 Mounting
Use the M2x0.4x16mm machine screws (provided in pink bag) for mounting these products to the
ADIS16IMU1/PCBZ and set their torque for 20 inch-ounces. The yellow-highlights in the top-view
picture illustrate the location of the mounting holes for these products.

Rev 25 Jun 2013 19:50 | Page 3
ADIS16360, ADIS16362, ADIS16364, ADIS16365, ADIS16367,
ADIS16400, ADIS16405, ADIS16407 Mounting
Use the M2x0.4x4mm machine screws (provided in pink bag) for mounting these products to the
ADIS16IMU1/PCBZ and set their torque for 20 inch-ounces. The pink-highlights in the top-view picture
illustrate the location of the mounting holes for these products. For high-vibration environments,
consider using more than 2 screws, per AN-1045
ADIS16375, ADIS16480, ADIS16485, ADIS16488 Mounting
Use the M2x0.4x16mm machine screws (provided in pink bag) for mounting these products to the
ADIS16IMU1/PCBZ and set their torque for 20 inch-ounces. The blue-highlights in the top-view picture
illustrate the location of the mounting holes for these products. Here is an example of the
ADIS16IMU1/PCBZ, with an ADIS16485AMLZ mounted to it.
Make sure that the connector pins are in alignment with J2 on the ADIS16IMU1/PCBZ, before pressing
it into place.
Here is a close-up view, which shows the correct connector alignment.

Rev 25 Jun 2013 19:50 | Page 4
This picture provides an example of the an incorrect connector alignment. Note that this view is
on the EVAL-ADISZ board, not the ADIS16IMU1/PCBZ.
INTERFACE CONNECTOR
J1 is the electrical connector that provides direct access to power, ground and critical digital I/O pins
on the devices. It is a 16-pin, dual-row, 2-mm pitch connector that support 1mm ribbon cable systems.
Pin Assignments
Here is the pin assignments for J1, which is the connector that will interface with an embedded
processor board.

Rev 25 Jun 2013 19:50 | Page 6
© Analog Devices, Inc. All rights reserved. Trademarks and
registered trademarks are the property of their respective owners. www.analog.com
Products related to this Datasheet
BREAKOUT IMU INTERFACE BOARD