DA-70146 Installation Guide Datasheet by Assmann WSW Components

View All Related Products | Download PDF Datasheet
Found New Hardware Wizard Welcome to the Found New H ardware Wizard Windows will Search loi current and updated :oltware by looking on your computer, on the hardware installation CD. or on the Windows Update Web site [wth your permission] Head our privacy policy Can Wlndow: connect to Wlndows Update to Search lor sottware? 0 Yes, this iime only O Yes, now and every trmel connect a device 6- N o, not this time Click Next to cartinue
http://www.digitus.info/
Welcome to the Windows XP Installation Guide
Installing Drivers
To install drivers for an device under Windows XP and XP SP1, follow the instructions below:
· If a device of the same type has been installed on your machine before and the drivers that are about to be installed are
different from those installed already, the original drivers need to be uninstalled.
· If you are running Windows XP or Windows XP SP 1, temporarily disconnect your PC from the Internet. This can be
done by either removing the network cable from your PC or by disabling your network card by going to the "Control
Panel\Network and Dial-Up Connections", right-clicking on the appropriate connection and selecting "Disable" from the
menu. The connection can be re-enabled after the installation is complete. This is not necessary under Windows XP
SP 2 if configured to ask before connecting to Windows Update. Windows XP SP 2 can have the settings for Windows
Update changed through "Control Panel\System" then select the "Hardware" tab and click "Windows Update".
· Connect the device to a spare USB port on your PC. This will launch the Windows Found New Hardware Wizard. If there
is no available Internet connection or Windows XP SP 2 is configured to ask before connecting to Windows Update, the
screen below is shown. Select "No, not this time" from the options available and then click "Next" to proceed with the
installation. If there is an available Internet connection, Windows XP will silently connect to the Windows Update website
and install any suitable driver it finds for the device in preference to the driver manually selected.
· Select "Install from a list or specific location (Advanced)" as shown below and then click "Next".
Found New Hardware Wiz r1 This wizard helps you install software for USB <-> Seral Eable t’ -) tr your hardware came with an installation to a; a. floppy dilk. inlall a now. Whal do you want the wizard to do? C) Install the software automatically [Recommended] (o‘- Install from a list or specilic location [Advanced] Click Next to ccntrnue Found New Hardw e W Please choose your Search and installation options. \ § (9 Seach in. the best driver in these location: Use the check boxes below to Iirrit or emand the delault search, which inchdes local path: and removable media The best driver found wl be 'mtalled. I D Search removable media [lbDDyv CD-REIM...] lZI Include this location in the search revert—mes 7.] O Donl search. I will choose the driver to install Choose this option to setect the device driver lrom a list. Windows does not guarantee that the driver you chooxe wil be me best match lor your hardware,
http://www.digitus.info/
· Select "Search for the best driver in these locations" and enter the file path in the combo-box or browse to it by clicking
the browse button. Once the file path has been entered in the box, click next to proceed.
· If Windows XP is configured to warn when unsigned (non-WHQL certified) drivers are about to be installed, the following
screen will be displayed. Click on "Continue Anyway" to continue with the installation. If Windows XP is configured to
ignore file signature warnings, no message will appear.
‘ The sailwae you an 'nslaling in: this havdwave: USB HUI Speed Sevial Convene! has not passed Windows Logo testing to veliy its ounpatbflily with Windows XP- Emmi Cor-liming you: inflallalion at this sollvme may impail or dexlabilize lhe collect opelalion 0! you! sysleln eilhel inmadialely on in [he fulure. Micnnoll suongl’ recommend: lhal you slop this intlaildion now and contact lhe haldwale vendot in! wllwale lhal ha: pauzd Window: Logo tailing. Found New Ha 11w 9 W 11 Please wa‘t while the wizard installs the soflwale... e USB Serial Convener itdiunin.exe Tu E:\WINDDWS\syslem32
http://www.digitus.info/
· The following screen will be displayed as Windows XP copies the required driver files.
· Windows should then display a message indicating that the installation was successful. Click "Finish" to complete the
installation. This has installed the serial converter. The COM port emulation driver must be installed after this has
completed.
Found New Haldwale leald Completing the Found New Hardware Wizard The Wizald has finished installing Ihe soliwale fol: e USB Serial Converter Click Finish to c'use the wizaid ect "View > Devices b T e". The dewce auears as an additional COM -on With the label "USB Seri 55 Device Managel EileActionMe-«tleb «#Iééfl or i Compute A e 4’ Dlsk drivzs o g Display adapters e ~43 DVDJcD-zoM drives ¢ @ FluDDy diskcontrollers l e gin: ATArATAPl controllers e & + 1 4 69 IEEE 1394 ads hast controllers ‘ )3 Infrared devlces ‘2 Keyboards ‘3 Mice and other pointing devices I, Modems g Momtors I Netwovkadaptevs E Pcmcm adapters Ports (coM & LPT) USB 5 Ial Part (COMS 3 fl oce a 0 Sound, video and game controllers e System cevlces e Lhrversa Serial Bus controllers v
http://www.digitus.info/
· After clicking "Finish", the Found New Hardware Wizard will continue by installing the COM port emulation driver. The
procedure is the same as that above for installing the serial converter driver.
· Open the Device Manager (located in "Control Panel\System" then select the "Hardware" tab and click "Device Manger")
and select "View > Devices by Type". The device appears as an additional COM port with the label "USB Serial Port".
52 0.7343 s:- 1.31MB fll Wildnws xp Serving Packz 2'.
http://www.digitus.info/
Uninstalling Drivers
· Disconnect any devices that are attached to the PC.
· Open the Add/Remove Programs utility located in "Control Panel\Add/Remove Programs".
Select "FTDI USB Serial Converter Drivers" from the list of installed programs.
· Click the "Change/Remove" button. This will run the uninstaller program. Click "Continue" to run
the uninstaller or "Cancel" to exit.
http://www.digitus.info/
· When the uninstaller has finished removing the device from the system, the caption on the
"Cancel" button will change to "Finish". Click "Finish" to complete the process.
Tris wuald names In! new \imn tar. USE HS Said Convene! A data diva! is a uoflmns ”wall lhd makes a We dsvwe walk
http://www.digitus.info/
USB High Speed Serial Converter
User’s Guide
Overview
 The USB to Serial Converter provides a simple and easy way to afford a bridge/connectivity
between the Universal Serial Bus (USB) and Serial Port interface.
 With the advantages of USB port such as plug and play & hot swap, users have the capability to
utilize the peripheral with serial port interface in an easy-to-use environment. It is designed for
ideal connections to Cellular Phone, Digital Camera, Modems or ISDN terminal adapters.
 The USB to Serial Converter and software driver is able to make the USB interface to be
transparent to the peripherals without firmware changes, it's possible for serial port peripherals to
easily interface with USB with minimum modification.
Product Features
 USB Specification Rev. 2.0 compliant
 Support the RS232 Serial interface
 Support automatic handshake mode
 USB full speed communication and bus powered
 Support windows 98se/me/2000/xp, imac os 8.6 and above, linux
 Support remote wake-up and power management
System Requirements
 IBM PC 486DX4-100 MHz CPU or higher or compatible system
 Available USB port
 CD-ROM drive
Driver Installation
Follow the steps below to install Window 98se driver of USB-Serial Converter:
1. Power on your computer and make sure that the USB port is enabled and working properly.
2. Plug in the USB-Serial Converter into the USB port and run the Add New Hardware Wizard to assist
you in setting up the new device. Click Next to continue.
r? Sam-m mm. but dwallm ym devu: gamma--. __ _ _ __- , __ J r‘ Disvbyaktdalxmmminamfiic Inm,anymmnwn—muymmn < em="" natl=""> End Wndm wl seamlm mama: m I: drive! Mam: nnwll hand diva,u\d m n no If! [alumni-lama»! lawn tick Nadia «an lhe “an I— Em» dsk am I‘ :n-RUM am I‘ Mum-1n Wndomupdma l7 Stanly-hm HE Saba the luldal [ha coola'm diva Hannah" (.INF lb] 101 lhi: devise. ’ -_7 Plugam Hes E; Recs/dad _‘| schematic E J Wmnt m _‘| WW a -_‘1 Zdbench E [E ] g g) u2u323_um7lF] G] Punlevs (ii EontmlF'ane‘ Ll Em nuaLl In Nslwmkmn _c-=a
http://www.digitus.info/
2
3. Insert the USB-Serial Converter software driver into the CD-ROM drive and click Next to continue and
click to search driver from the CD-ROM drive
Wmdows M match rm haw flnvals m m aw “an“; an you mm am, and m any ml the In‘hwmg se‘ecled mum Elck Ne)! In an the Seavch I— E‘ww dik mve: r gDrRuM awe r Emma“ Wmdows Updahe [7 sunny 3 jocalmn D \UNSBEA . Add New Hardware w am Wmdows time! we neamh rm m dame USB Hub Sue-3d Seus‘ Convener me m nw veady lo msIal Ike has! dnvev 191 um dawns muck Back As sdacl a «ram mm, m cick Nax| m cnmm: Lmalmn nl duvet : D \LlNEBE-A\FTDIBIJS INF < eack="" 5am:="" add="" new="" hardware="" ma="" e="" usn="" hmsam="" sew="" eanvevlm="" wmdawx="" has="" 1mm="" mmuma="" the="" gunmen»;="" my="" new="" havdwave="" dzvu="" mm:="">
http://www.digitus.info/
3
4. Windows will detect the driver and shows the USB HS Serial Converter. Click Next to continue
installation.
5. Click Next to continue and let Windows copy the needed files to your hard disk.
6. When Windows finished installing the software,click Finish.
7. See the Device Manager to check the USB HS Serial Converter.
3:6 Flow» disk cmvolm [99 Had dtk «nudists m- Nammk adamant a J PutsllIlM I LPT] ; Enmmmicanm Pan [mm] 3 len'wiun: Pan [cum] ,3 EPSEIN Primal Pall [LPT1] \ (H a“ 5mm, mden and gain: namnllam 5: 5mm devim E) Univand Saial But convaleu amen. I'm meflle um ; :mmuricam Pan [mm] . J Centaur-balm": PonthZ] J EPSUN Him Pull [m1] , ,1 USE SerialPullDOMll 111% Smnd. video md can: cnrlrdlas (a El swam davicat Universal Serial Em cmmlan Gena-n USB Hub NEE PCI to USB Emmdd Han Bmhdla NED usa Dam Had lemlel NEE um: um Had Emlmlal P'nilp: Emma usa Davie: Standard Univemwu m usa Hod Eomdlu Sludard UniverdeU In USB Hm! cnmdla
http://www.digitus.info/
4
Changing the COM Port Number
1. From "Device Manager", select "View devices by type", then "Ports (COM & LPT)".
2. Select the USB serial port and click Properties.
3. Select the "Port Settings" tab, then click "Advanced". Choose the required COM port
132mm ameManaga | Havawepmw parmml r: V‘sNdevmeshyvae r Mewdewceshygnnneclmn E g Dwmm z a F‘nvwd‘sk cannaHevs E 4: Ham dsk cammHevx mm mm mm Dew-:2: Q mm mm MW II Nelwuk adamm y m [mm x. mm y Emmumcaham PW (cum! 5 Emmumcaham PW [:qu g EPSEIN PunlevallLPVU ”MW ‘4‘ a a 5m w a ma game-:amafim a - 5:13AM“ dzv‘czx E mm Ssua‘Eux cunhanu We. mm W mam: new PnflSemngx IBM | EM WWW-1 fl ' gem his a v EariLV [H mm; m flaw mm [mm Advancad Esme Dara-m2
http://www.digitus.info/
5
number from the list and click OK.
Notes
If a modem is attached to the USB serial port when the port number is changed, it will continue to work
under the new port number.
If a modem had been attached to the USB serial port but was not attached when the port number was
changed, it will not work when re-attached under the new port number. In this case, the modem must be
removed from the system and re-installed.
In general, if there are devices in the system which have been attached previously to the USB serial port,
they may not work after the port number has been changed. If this is true, remove the device from the
system and re-install it.
Advanced Pm|Se| as F UxaFlFflhuflalxhaqunflfififlmpallh\:LlART] _ ‘ ox 55km laws! sen-w: ta emu cwnsclm 9mm Sahd fish! :3ng: lm lane. whm 53“" Emma.“ Lawn] —J— Hmm] m lrammuflmev Lawn] —J Hams) DOMPoleunhev. |—_IEDW . Ftcomms vxd F|dlbus cat % Fldlumn .n. 41—] 1'1 mu] salecled FIDI Unlnslallel Ve n ynul usn device is cnnmscled. please unplug il nun... PIES! Ennfmu: la uninslnll the drive“, In Emcal to quit. Continue Emcal
http://www.digitus.info/
6
Uninstalling the Driver Program
If you want to remove the USB-Serial Converter driver program, you can uninstall it by following the steps
below:
1. Unplug the USB-Serial Converter from your PC.
2. Run the”Ftdiunin.exeprogram from the software CD-ROM, then Click continue to remove the USB-
Serial Converter driver program.
3. Click Finish, then reboot the PC.
FTnIlIm
http://www.digitus.info/
7
Welcome to the Found New Hardware Wizald This wizavd help: you mfldl a device din/e! lo. a hardware device Tu cnntinue. click Next, < bani:="" next="" )="" cancel="">
http://www.digitus.info/
Welcome to the Windows 2000 Installation Guide
Installing Drivers
· If a device of the same type has been installed on your machine before and the drivers that are
about to be installed are different from those installed already, the original drivers need to be
uninstalled.
· Connect the device to a spare USB port on your PC. This will launch the Windows Found New
Hardware Wizard. Click "Next" to proceed with the installation.
· Select "Search for a suitable driver for my device (recommended)" as shown below and then
click "Next".
rd a Found New Hardware lnslali Haldrrrrare Device Drivel: \ A dew» driver rs a :oiiware program that mables a hardware device in work with é an operating system. I This wizard will complete he intellation i0! Ihis device: g USB <-> Serial table A device driver is a soitware progam that makes a hardware device work. Windows needs diver iiles for your new device. To locate driver fies and cumulete the 'mlaiialbn click Next. What do you want the wizard lo do? (0‘ Search for a suilafle dtiver for my clerics [recommended] (‘ Display a list oi theknown drivers iorthis device so that i can choose a medic dliver < back="" next=""> Cancel rd Found New Hardware Locale Dliver Files Where do you want Winoows in Search ior drrver irles‘l 1% Search '01 driver Ties 10! [he Following hardware device: g USB <-> Serial cable The wilrd searches for Nitable drivers in it: driver daldzaseon your corrrwter and in av oi the Mowing optional search location: that you speed». To start the search, click Next. ll you are searching on a Happy disk or CDHDM drive 'meri lie lloooy disk or CD before clicking Next. Optional search location: '— Floppy nick drive: r ISO-HUM drives P' Specify a location [— Microsoit Wndow: Update < back="" next=""> Cancel
http://www.digitus.info/
· Check the box next to "Specify a location" and uncheck all others as shown below. · Clicking
"Next" displays a dialog box for you to enter to the location of the drivers.
found New Hardware Wizard Inset! the manufauum's Walden risk we the fiive mm md then click OK OK Copy manufadura‘: fie: [mm JI—;l am, | LuLulc hlc 9' x Loakiru avtporiveys vI 0- E! d? I' - E FTDIEUSJNF FTDIPORTJNF History 6-3:] FTSERMOUJNF My tempura. E Filanuns: IFTDIBUSJNF _] Open M y N e) . Files nf typa: Setup Information [‘ inil v I Cancel I
http://www.digitus.info/
· Click "Browse" to display an open file dialog box.
· click "Open", then click "OK". The PC autoselects the correct INF file, in this case
FTDIBUS.INF. Once Windows has found the required driver .INF file, click "Next" to proceed.
Found New Hardware rd Driver File: Search Resulls \ The wrzaid has linished searching loi driver liles loi your hardware device. Q I The wizard round a diver for the following avice: g USB <-> Serial cabie Windows found a diver lor this device. To 'vrstall the driver Mndows loud, click Next g c:\vr:p driversuldibusji < back="" next=""> Cancel ulaiion driver must be installed after this has completed. Found New Hardware Completing the Found New Hardware Wizard \ USB Serial Converter Windows has finished installing the sollwaie luv this device. To close this wrzard, click Finish
http://www.digitus.info/
· Windows should then display a message indicating that the installation was successful. Click
"Finish" to complete the installation. This has installed the serial converter. The COM port
emulation driver must be installed after this has completed.
DX ‘lm WIJ‘-* Elana .7 Compute a Dlsk arms Dlsplay adapters Dvo/cu—xoul drives a Floppy dsk cmmlevs a Flnppy dsk duves ‘é [DE Ammnm cantmllevs Q Keybnams « Mice and other poirtlng devlces Mnnltovs E] I Nelwovkadapters lntellR) monuo VE Network Common > - Reallek RTL61391310X Fam‘y Fast Ethunat NIC E 3 Plans (com &LPT) ,3 Cnmnu'licatinns Part (com) System cevices Unl'vevsa Sevlal Bus cartrolevs
http://www.digitus.info/
· After clicking "Finish", the Found New Hardware Wizard will continue by installing the COM
port emulation driver. The procedure is the same as that above for installing the serial
converter driver, except the PC will autoselect the FTDIPORT.INF file.
· Open the Device Manager (located in "Control Panel\System" then select the "Hardware" tab
and click "Device Manger…") and select "View > Devices by Type". The device appears as an
additional COM port with the label "USB Serial Port".
Uninstalling VCP Drivers
To uninstall drivers for devices, follow the instructions below:
· Disconnect any devices that are attached to the PC.
· Open the Add/Remove Programs utility located in "Control Panel\Add/Remove Programs".
Select "FTDI USB Serial Converter Drivers" from the list of installed programs.
£5; Add i Remove Prourams - Afll‘ Currently instdled programs: Sort by: Name v @ Adobe mrnbak » Reader 6.fl,2 Madam Size 5,6948 ‘ Programs E Adobe Aaobat 5‘0 SIZe 76mm 3 Adobe Ninosphere Player for Acrobat and Adobe Reader I é } a Adobe Download Manager 1.2 (Remove Only) Add New 5 Adobe Phatnshnp Album 2.0 Starter Edition Size 15.5w": ngmms @ Adobe Reader 6.0.1 Size 4mm , 1‘ Bovland Delphi 5 Size 127MB ‘ 3} EC Suirwere mr Scrzen Cnplur: z.) Add/Re e V! , I r Windows .A: FT [USE SEna ,onverter DerErS Components "*5 ' ”W, m I Help & Manual 3.40 A; fss iind g HTML Heb Workshop Size saw no .5 fl IAR Embedded Workbench Krckstart fut MSNII v2.2“; Size 1.53MB fl lnstantCDfDVD i5] Intexn) Extreme Graphics Driver Size 245m FTD Unlnstaller V3 "you USB device humid. plum unplug i m" Pru:Con|iuelowiutalflledim.quoqliL Lin-l
http://www.digitus.info/
· Click the "Change/Remove" button. This will run the FTDI uninstaller program. Click "Continue"
to run the uninstaller or "Cancel" to exit.
· When the uninstaller has finished removing the device from the system, the caption on the
"Cancel" button will change to "Finish". Click "Finish" to complete the process.
lTI-Illulnxlulln '1": I'I
http://www.digitus.info/

Products related to this Datasheet

ADAPTER USB 2.0 TO SERIAL M/DB-9