LS Series Datasheet

TDK-Lambda Americas Inc.

View All Related Products | Download PDF Datasheet

Datasheet

Page 1 of 6 24 November 2017 PA582-04-01-F (b)
LS25
-
150 Installation Manual
General Safety Instructions: ENGLISH
READ SAFETY INSTRUCTIONS
Servicing:
These products are not customer serviceable TDK-Lambda and their authorised agents only are permitted to carry out repairs.
Critical Components:
These products are not authorised for use as critical components in nuclear control systems, life support systems or equipment for use in
hazardous environments without the express written approval of the Managing Director of TDK-Lambda EMEA.
Product Usage:
These products are designed for use within a host equipment which restricts access to authorised competent personnel.
This product is a component power supply and complies with the EMC directive. The EMC performance of a component power supply will be
affected by the final installation, compliance to the stated EMC standards and conformance to the EMC Directive must be confirmed after
installation by the final equipment manufacturer.
For guidance with respect to test conditions please visit our website at https://emea.tdk-lambda.com/EMC_guidance or contact your local TDK-
Lambda sales office.
Environmental:
These products are IPX0, and therefore chemicals/solvents, cleaning agents and other liquids must not be used.
Environment:
This power supply is a switch mode power supply for use in applications within a Pollution Degree 2, overvoltage category II environment. Material
Group IIIb PCB’s are used within it.
Output Loading:
The output power taken from the power supply must not exceed the rating stated on the power supply label, except as stated in the product
limitations in this handbook.
Input Parameters:
This product must be operated within the input parameters stated in the product limitations in this handbook.
End of Life Disposal:
The unit contains components that require special disposal. Make sure that the unit is properly disposed of at the end of its service life and in
accordance with local regulations.
RISK OF ELECTRIC SHOCK
High Voltage Warning:
Dangerous voltages are present within the power supply.The professional installer must protect service personnel from inadvertent contact with
these dangerous voltages in the end equipment.
WARNING: When installed in a Class 1 end equipment, this product must be reliably earthed and professionally installed.
The (+) or (-) output(s) can be earthed or left floating.
The unit cover(s)/chassis (where applicable) must not be made user accessible.
The mains input connector is not acceptable for use as field wiring terminals.
For encased products, do not use mounting screws, which penetrate the unit more than; See drawings.
Internal fuses protect the unit and must not be replaced by the user. In case of internal defect, the unit must be returned to TDK-Lambda or one of
their authorised agents.
A suitable mechanical, electrical and fire enclosure must be provided by the end use equipment for mechanical, electric shock and fire hazard
protection.
Energy Hazards:
The main output of this product is capable of providing hazardous energy (240VA). Final equipment manufacturers must provide protection to
service personnel against inadvertent contact with the output terminals.
The unit cover/chassis, where applicable, is designed to protect skilled personnel from hazards. They must not be used as part of the external
covers of any equipment where they may be accessible to operators, since under full load conditions, part or parts of the unit chassis may reach
temperatures in excess of those considered safe for operator access.
Page 2 of 6 24 November 2017 PA582-04-01-F (b)
LS25
-
150 Installation Manual
Allgemeine Sicherheitsvorschriften: DEUTSCH
LESEN SIE DIE SICHERHEITSVORSCHRIFTEN
Wartung:
Diese Produkte können nicht durch den Kunden gewartet werden. Nur TDK-Lambda und deren zugelassene Vertriebshändler sind zur
Durchführung von Reparaturen berechtigt.
Kritische Komponenten:
Diese Produkte sind nicht für die Verwendung als kritische Komponenten in nuklearen Kontrollsystemen, Lebenserhaltungssystemen oder
Geräten in gefährlichen Umgebungen geeignet, sofern dies nicht ausdrücklich und in Schriftform durch den Geschäftsführer von TDK-Lambda
EMEA genehmigt wurde.
Produktverwendung:
Diese Produkte sind zur Verwendung innerhalb von Anlagen gedacht, die einen auf das Fachpersonal beschnkten Zugang haben.
Dieses Produkt ist ein Komponenten-Netzteil und entspricht der EMV-Richtlinie. Das EMV-Verhalten eines Einbaunetzteiles wird von der
Einbausituation im Endgerät maßgeblich beeinflusst. Die Übereinstimmung mit den angegebenen EMV-Normen und die Erfüllung der EMV-
Richtlinie muss nach dem Einbau vom Endgerätehersteller nachgewiesen werden. Für Anwendungshinweise besuchen Sie bitte unsere Website
auf https://emea.tdk-lambda.com/EMC_guidance oder kontaktieren Sie Ihr lokales TDK-Lambda Vertriebsbüro.
Umwelt:
Diese Produkte sind IPX0, aus diesem Grund dürfen keine Chemikalien/Lösungsmittel, Reinigungsmittel und andere Flüssigkeiten verwendet
werden.
Umgebung:
Dieses Netzteil ist ein Schaltnetzteil zur Verwendung in einer Umgebung mit einem Verschmutzungsgrad 2, Überspannungskategorie II. Es
werden PCBs Materialgruppe IIIb verwendet.
Ausgangsstrom:
Der Ausgangsstrom des Netzteiles darf die Leistung, die auf dem Label des Netzteiles vermerkt ist, nur dann überschreiten, wenn dies in diesem
Handbuch beschrieben und spezifiziert ist.
Eingangsparameter:
Dieses Produkt muss innerhalb der Eingangsparameter, die in der Produktspezifikation sowie in diesen Handbuch angegeben sind, betrieben
werden.
Entsorgung am Ende der Betriebszeit:
Das Gerät enthält Komponenten die unter Sondermüll fallen. Das Gerät muss am Ende der Betriebszeit ordnungsgemäß und in Übereinstimmung
mit den regionalen Bestimmungen entsorgt werden.
GEFAHR DURCH ELEKTRISCHEN SCHLAG
Hochspannungswarnung:
Innerhalb des Netzteiles gibt es gefährliche Spannungen.Der Elektroinstallateur muss das Wartungspersonal vor versehentlichem Kontakt mit
den gefährlichen Spannungen im Endgerät schützen.
WARNUNG! Falls Sie unser Netzgerät in eine Anwendung mit Schutzklasse 1 eingebaut haben, stellen Sie sicher, dass es fachgerecht installiert
und zuverlässig geerdet ist.
Die (+) oder (-) Ausgänge können geerdet werden oder potenzialfrei bleiben.
Die Abdeckung des Gerätes/das Gehäuse darf für den Benutzer nicht zugänglich sein.
Der Eingangsklemme ist nicht für die Verwendung als Verdrahtungsanschluss im Feld geeignet.
r Produkte mit Gehäuse, verwenden Sie keine Schrauben, die in das Gerät mehr eindringen als; siehe Zeichnung
Eine interne Sicherung schützt das Gerät und darf durch den Benutzer nicht ausgetauscht werden. Im Fall von einem Defekt muss das Gerät an
TDK-Lambda oder einen der autorisierten Vertriebshändler zurückgeschickt werden.
Ein geeignetes mechanisches, elektrisches und brandgeschütztes Gehäuse muss als Schutz vor der Gefahr von mechanischen Risiken,
Stromschlägen und Brandschutz in dem Endgerät vorgesehen werden.
Gefahren durch elektrische Energie:
Von bestimmten Netzteilen kann, je nach Einstellung der Ausgangsspannung, eine gefährliche elektrische Energie ausgehen (240VA). Die
Endgerätehersteller müssen einen Schutz für Servicepersonal vor unbeabsichtigtem Kontakt mit den Ausgangsanschlüssen dieser Netzteile
vorsehen. Kann aufgrund der Einstellung gefährliche elektrische Energie auftreten, dürfen die Anschlüsse für den Benutzer nicht zugänglich sein.
Die Geräteabdeckung/das Gehäuse wurde so entwickelt, dass das Fachpersonal vor Gefahren geschützt wird. Sie dürfen nicht als Teil der
externen Abdeckung der Endapplikation verwendet werden, die für den Betreiber zugänglich sind. Das Netzteilgehäuse oder Teile davon, können
unter voller Belastung erhöhte Temperaturen erreichen, die für den Betreiber als nicht sicher betrachtet werden.
Page 3 of 6 24 November 2017 PA582-04-01-F (b)
LS25
-
150 Installation Manual
Consignes générales de sécurité: FRANÇAIS
LIRE LES CONSIGNES DE SECURITE
Entretien:
Ces produits ne peuvent pas être réparés par l’utilisateur. Seuls, TDK-Lambda et ses agents agréés sont autorisés à effectuer des réparations.
Composants critiques:
Ces produits ne doivent pas être utilisés en tant que composants critiques dans des systèmes de commande nucléaire, dans des systèmes de
sauvetage ou dans des équipements utilisés dans des environnements dangereux, sans l'autorisation écrite expresse du directeur général de
TDK-Lambda EMEA.
Utilisation du produit:
Ces produits sont cous pour être utilisés dans un équipement hôte dont l'acs n'est autorisé qu'aux personnes compétentes.
Ce produit est un composant d'alimentation électrique et est conforme à la directive EMC.
La performance CEM d'une alimentation considérée comme un composant d'un équipement sera affectée par l'équipement final, la conformité
aux normes CEM énoncée et la conformité à la directive CEM doivent être confirmées après installation de l'alimentation par le fabricant de
l'équipement final.
Pour obtenir des conseils concernant nos conditions d'essai, veuillez consulter notre site Web à l'adresse https://emea.tdk-
lambda.com/EMC_guidance ou contacter votre bureau de vente local TDK-Lambda.
Environnement:
Ces produits sont IPX0, et donc on ne doit pas utiliser des produits chimiques/solvants, des produits de nettoyage et d'autres liquides.
Environnement fonctionnel :
Cette alimentation fonctionne en mode commutation pour utilisation dans des applications fonctionnant dans un environnement avec Degré de
Pollution 2 et catégorie de surtension II. Elle utilise des cartes des circuits imprimés (PCB) de Groupe IIIb.
Intensité soutirée:
L'intensité soutirée de l'alimentation ne doit pas dépasser l'intensité nominale marquée sur la plaque signalétique, sauf indications contraires dans
les limitations du produit crit dans ce manuel.
Paramètres d'entrée:
Ce produit doit être utilisé à l'intérieur des paramètres d'entrée indiqués dans les limitations du produit dans ce manuel.
Elimination en fin de vie:
L'alimentation contient des composants nécessitant des dispositions spéciales pour leur élimination. Vérifiez que cette alimentation est mise au
rebut correctement en fin de vie utile et conformément aux réglementations locales en vigueur.
RISQUE DE CHOC ELECTRIQUE
Attention-Danger haute tension:
Des tensions dangereuses sont présentes dans l'alimentation. L'installateur doit protéger le personnel d'entretien contre un contact involontaire
avec ces tensions dangereuses dans l'équipement final.
AVERTISSEMENT: Si ce produit est installé dans un équipement final de classe I, il doit être mis à la terre de manière fiable et installé par un
professionnel averti.
Les sorties (+) ou (-) peuvent être raccordées à la terre ou laissées flotttantes.
Le couvercle/châssis de l'alimentation ne doit pas être accessible à l'utilisateur.Le connecteur d'entrée d'alimentation principale ne doit pas être
utilisé comme borne de raccordement.
N'utilisez pas de vis pénétrant dans le module sur une profondeur supérieure à :Voir dessins.
Un fusible interne protège le module et ne doit pas être remplacé par l'utilisateur. En cas de défaut interne, le module doit être renvoyé à TDK-
Lambda ou l'un de ses agents agréés.
Une enceinte appropriée doit être prévue par l'utilisateur final pour assurer la protection contre les chocs mécaniques, les chocs électriques et
l'incendie.
Energies dangereuses:
Certains modules peuvent générer une énergie dangereuse (240VA) selon le réglage de tension de sortie. Le fabricant de l'équipement final doit
assurer la protection des techniciens d'entretien contre un contact involontaire avec les bornes de sortie de ces modules. Si une telle tension
dangereuse risque de se produire, les bornes ou les connexions du module ne doivent pas être accessibles par l'utilisateur.
Le couvercle et le châssis du module sont conçus pour protéger des personnels expérimentés. Ils ne doivent pas être utilisés comme couvercles
extérieurs d'un équipement, accessible aux opérateurs car en condition de puissance maximum, des parties du châssis peuvent atteindre des
températures considérées comme dangereuses pour l'opérateur.
Page 4 of 6 24 November 2017 PA582-04-01-F (b)
LS25
-
150 Installation Manual
Norme generali di sicurezza: ITALIANO
SI PREGA DI LEGGERE LE NORME DI SICUREZZA
Manutenzione:
Il cliente non può eseguire alcuna manutenzione su questi prodotti. L'esecuzione delle eventuali riparazioni è consentita solo a TDK-Lambda e ai
suoi agenti autorizzati.
Componenti critici:
Non si autorizza l'uso di questi prodotti come componenti critici all'interno di sistemi di controllo nucleari, sistemi necessari alla sopravvivenza o
apparecchiature destinate all'impiego in ambienti pericolosi, senza l'esplicita approvazione scritta dell'Amministratore Delegato di TDK-Lambda
EMEA.
Uso dei prodotti:
Questi prodotti sono progettati per l'uso all'interno di un'apparecchiatura ospite che limiti l'accesso al solo personale competente e autorizzato.
Questo prodotto è un alimentatore componenti ed è conforme alla direttiva EMC.
Le prestazioni EMC di un alimentatore utilizzato come componente di un'apparecchiatura saranno influenzate dal montaggio finale, la conformità
alle norme EMC indicate e la conformità alla direttiva EMC dovranno essere confermata dopo l'installazione dell'alimentatore da parte del
produttore dell'apparecchiatura finale.
Per indicazioni riguardanti le condizioni di test si prega di visitare il nostro sito web all'indirizzo https://emea.tdk-lambda.com/EMC_guidance o
contattare l'ufficio vendite TDK-Lambda locale.
Condizioni ambientali:
Questi prodotti sono classificati come IPX0, dunque non devono essere utilizzati sostanze chimiche/solventi, prodotti per la pulizia o liquidi di altra
natura.
Ambiente:
Questo prodotto è un alimentatore a commutazione, destinato all'uso in applicazioni rientranti in ambienti con le seguenti caratteristiche: Livello
inquinamento 2, Categoria sovratensione II. Questo prodotto contiene schede di circuiti stampati in materiali di Gruppo IIIb.
Carico in uscita:
La potenza in uscita ottenuta dall'alimentatore non deve superare la potenza nominale indicata sulla targhetta dell'alimentatore, fatto salvo dove
indicato nei limiti per i prodotto specificati in questo manuale.
Parametri di alimentazione:
Questo prodotto deve essere utilizzato entro i parametri di alimentazione indicati nei limiti per il prodotto, specificati in questo manuale.
Smaltimento:
L'unità contiene componenti che richiedono procedure speciali di smaltimento. Accertarsi che l'unità venga smaltita in modo corretto al termine
della vita utile e nel rispetto delle normative locali.
RISCHIO DI SCOSSA ELETTRICA
Avvertimento di alta tensione:
All'interno dell'alimentatore sono presenti tensioni pericolose. Gli installatori professionali devono proteggere il personale di manutenzione dal
rischio di contatto accidentale con queste tensioni pericolose all'interno dell'apparecchiatura finale.
ATTENZIONE: Se installato in un’attrezzatura di classe I, questo prodotto deve essere collegato a terra in modo affidabile ed installato in modo
professionale.
Le uscite (+) o (-) possono essere messa a terra o lasciate isolate.
I coperchi/il telaio dell'unità non devono essere accessibili da parte dell'utente.
Il connettore dell'alimentazione principale non può essere utilizzato come terminale di collegamento di campo.
Non utilizzare viti che penetrano nell'unità per più di : Vedi disegni
Un fusibile interno protegge l'unità e non deve essere sostituito dall'utente. Nell'eventualità di un difetto interno, restituire l'unità a TDK-Lambda o
a uno dei suoi agenti autorizzati.
L'apparecchiatura finale deve includere una recinzione meccanica, elettrica e antincendio per proteggere dai pericoli di natura meccanica, dalle
scosse elettriche e dai pericoli di incendio.
Pericoli energetici:
Alcuni moduli sono in grado di erogare energia pericolosa (240VA) a seconda della tensione in uscita impostata. I produttori delle apparecchiature
finali sono tenuti a proteggere il personale di manutenzione dal rischio di contatto accidentale con questi terminali dei moduli di uscita. Se
impostati su livelli che non escludono l'erogazione di energia pericolosa, questi terminali o collegamenti non devono risultare accessibili da parte
dell'utente.
Il coperchio/telaio dell'unità è realizzato per proteggere il personale esperto dai pericoli. Non deve essere usato come parte degli involucri esterni
di qualsiasi apparecchiatura, se risulta accessibile da parte degli addetti, poiché è possibile che in condizioni di pieno carico una o più parti del
telaio dell'unità giunga/giungano a temperature superiori ai limiti considerati sicuri per l'accesso da parte degli addetti.
Page 5 of 6 24 November 2017 PA582-04-01-F (b)
LS25
-
150 Installation Manual
Instrucciones generales de seguridad: ESPAÑOL
LEA LAS INSTRUCCIONES DE SEGURIDAD
Servicio:
Estos productos no pueden ser reparados por los clientes. TDK-Lambda y sus agentes autorizados son los únicos que pueden llevar a cabo las
reparaciones.
Componentes fundamentales:
Estos productos no pueden ser utilizados como componentes fundamentales en sistemas de control nuclear, sistemas de soporte vital o equipos
a utilizar en entornos peligrosos sin el consentimiento expreso por escrito del Director General de TDK-Lambda EMEA.
Uso de los productos:
Estos productos han sido diseñados para ser utilizados en un equipo central que restrinja el acceso al personal cualificado autorizado.
Este producto es una fuente de alimentación de componentes y cumple con la directiva EMC.
El rendimiento de CEM del suministro eléctrico de un componente se verá afectado por la instalación final; el fabricante del equipo final debe
confirmar el cumplimiento de las normas CEM establecidas y la conformidad con la Directiva CEM después de la instalación.
Si desea orientación sobre las condiciones de prueba, visite nuestro sitio web en https://emea.tdk-lambda.com/EMC_guidance o póngase en
contacto con la oficina de ventas local de TDK-Lambda
Medioambiental:
Estos productos son IPX0 y, por tanto, no pueden utilizarse sustancias químicas/disolventes, agentes de limpieza ni otros líquidos.
Medio ambiente:
Esta fuente de alimentación es una fuente de alimentación de modo conmutado a utilizar en aplicaciones dentro de un entorno con un Grado de
contaminación 2 y una Categoa de sobretensión II. En él se utilizan policloruros de bifenilo del Grupo de materiales IIIb.
Carga de salida:
La potencia de salida tomada de la fuente de alimentación no puede sobrepasar el valor nominal indicado en la etiqueta de la fuente de
alimentación, excepto en los casos indicados en las limitaciones del producto en este manual.
Parámetros de entrada:
Este producto debe ser utilizado dentro de los parámetros de entrada indicados en las limitaciones del producto en este manual.
Desecho de la unidad:
La unidad contiene componentes que deben ser desechados de una manera especial. Asegúrese de desechar correctamente la unidad al final
de su vida útil y conforme a las normas locales vigentes.
PELIGRO DE DESCARGAS ELÉCTRICAS
Advertencia de alta tensión:
En esta fuente de alimentación hay tensiones peligrosas. El instalador profesional debe proteger al personal de servicio contra cualquier
contacto accidental con estas tensiones peligrosas en el equipo final.
ADVERTENCIA: La instalación de este producto en un equipo de clase I la deben llevar a cabo profesionales y el producto debe estar conectado
a tierra.
La salida o salidas (+) o (-) pueden conectarse a tierra o se las puede dejar flotando.
Debe impedirse el acceso de los usuarios a la cubierta o cubiertas y al chasis de la unidad.
El conector de entrada de la red no es apto para ser utilizado a modo de bornes de cableado de campo.
No utilice tornillos de montaje susceptibles de penetrar en la unidad más de: Ver dibujos.
Un fusible interno protege la unidad y este no debe ser nunca reemplazado por el usuario. En caso de existir algún defecto interno, la unidad
debe ser enviada a TDK-Lambda o a uno de sus agentes autorizados.
El equipo de uso final debe constituir un recinto de protección mecánica, eléctrica y contra incendios de protección mecánica, contra descargas
eléctricas y contra el peligro de incendios.
Peligros de energía:
Algunos módulos pueden generar energía peligrosa (240VA) dependiendo de la configuración de la tensión de salida. Los fabricantes de equipos
finales deben proteger al personal de servicio contra un contacto accidental con estos bornes de salida de los módulos. Si se configura de modo
que pueda generarse energía peligrosa, hay que evitar que el usuario pueda acceder a los bornes o conexiones del módulo.
La cubierta/chasis de la unidad ha sido diseñada para que proteja a las personas cualificadas de los peligros. No deben ser utilizadas como parte
de las cubiertas externas de cualquier equipo al que pueden acceder los operarios, ya que bajo unas condiciones de carga completa, la pieza o
piezas del chasis de la unidad pueden alcanzar temperaturas superiores a las consideradas seguras para el acceso de los operarios.
Page 6 of 6 24 November 2017 PA582-04-01-F (b)
LS25
-
150 Installation Manual
Instruções gerais de segurança: PORTUGUÊS
LEIA AS INSTRUÇÕES DE SEGURANÇA
Manutenção:
Estes produtos não são podem ser submetidos a manutenção por parte do cliente. Apenas a TDK-Lambda e os seus agentes autorizados têm
permissão para realizar reparações.
Componentes essenciais:
Não é autorizada a utilização destes produtos como componentes essenciais de sistemas de controlo nuclear, sistemas de suporte de vida ou
equipamento para utilização em ambientes perigosos sem a expressa autorização por escrito do Director-Geral da TDK-Lambda EMEA.
Utilização do produto:
Estes produtos foram concebidos para utilização dentro de um equipamento de alojamento que apenas permita o acesso a pessoal qualificado
autorizado.
Este produto é uma fonte de alimentação componente e está em conformidade com a directiva EMC.
O desempenho EMC da fonte de alimentação de um componente será afetado pela instalação final. Após a instalação, o fabricante do
equipamento final tem de confirmar a conformidade com as normas EMC indicadas e a conformidade com a Diretiva EMC.
Para obter orientação relativamente às condições de teste, visite o nosso website, em https://emea.tdk-lambda.com/EMC_guidance, ou contacte
o seu escritório de vendas local da TDK-Lambda.
Ambiental:
Estes produtos são IPX0 e, como tal, o se devem utilizar químicos/solventes, agentes de limpeza e outros líquidos.
Ambiente:
Esta fonte de alimentação é uma fonte de alimentação do modo de comutação para utilização em aplicações com um Nível de Poluição 2 e
ambientes da categoria de sobretensão II. São utilizadas placas de circuitos impressos do grupo de materiais IIIb.
Carga de saída:
A potência de saída extraída da fonte de alimentação não deve exceder a classificação assinalada na etiqueta da fonte de alimentação, excepto
quando indicado nas limitações do produto neste guia.
Parâmetros de entrada:
Este produto deve ser utilizado dentro dos parâmetros de entrada indicados nas limitações do produto neste guia.
Eliminação no fim de vida:
A unidade contém componentes que necessitam de procedimentos especiais de eliminação. Certifique-se de que a unidade é devidamente
eliminada no fim da sua vida útil e que tal é feito em conformidade com os regulamentos locais.
RISCO DE CHOQUE ELÉCTRICO
Aviso de alta tensão:
Estão presentes tensões perigosas dentro da fonte de alimentação. O profissional que realizar a instalação deve proteger o pessoal de
assistência contra contactos inadvertidos com estas tensões perigosas do equipamento final.
AVISO: Quando instalado num equipamento de Classe I, este produto deve ser ligado à terra de forma fiável e instalado por um profissional.
As saídas (+) e (-) podem ser ligadas à terra ou deixadas soltas.
O chassis/cobertura(s) da unidade não deve estar acessível ao utilizador.
O conector de entrada de alimentação não deve ser utilizado como terminal de cablagens no local.
Não utilize parafusos de montagem, uma vez que estes penetrarão na unidade em mais do que: Veja os desenhos
Existe um fusível interno que protege a unidade e que não deve ser substituído pelo utilizador. Em caso de defeito interno, a unidade deve ser
devolvida à TDK-Lambda ou a um dos seus agentes autorizados.
O equipamento de utilização final deve fornecer um bastidor com protecção mecânica, eléctrica e contra incêndios adequada.
Perigos de energia:
Alguns módulos tem a capacidade de fornecer energia perigosa (240VA), de acordo com a configuração da tensão de saída. O equipamento final
do fabricante deve garantir que o pessoal de assistência está protegido contra contactos inadvertidos com estes terminais de saída do módulo.
Se essa energia perigosa for produzida, as ligações e os terminais do módulo não devem ser acessíveis pelos utilizadores.
O chassis/cobertura da unidade está concebido de forma a proteger o pessoal especializado de perigos. Não devem ser utilizados como parte
das coberturas externas de qualquer equipamento em que possam estar acessíveis aos operadores, uma vez que em condições de carga
máxima, algumas peças do chassis da unidade podem atingir temperaturas superiores às consideradas seguras para o acesso do operador.
TDK-Lambda Germany GmbH
Karl-Bold-Str. 40
D-77855 Achern, Germany
Tel: +49 (0) 7841 6660
Fax: +49 (0) 7841 5000
www.emea.tdk-lambda.com
TDK-Lambda
LS 25-150 Series
INSTRUCTION MANUAL
BEFORE USING THE POWER SUPPLY UNIT
Pay attention to all warnings and cautions before using the unit. Incorrect usage could lead to an electrical
shock, damage to the unit or a fire hazard.
WARNING and CAUTION
Do not modify.
Do not touch the internal components, they may have high voltage or high temperature. You may get
electrical shock or burned.
When the unit is operating, keep your hands and face away from it as you may be injured by flying debris in
the event of a fault.
This power supply is designed for use within an end product. Stick the WARNING label for users on the
system equipment and notify in the system instruction manual.
Never operate the unit under over current or short-circuit conditions for more than 30 seconds or outside its
specified Input Voltage Range, which could result in damage. There is no possibility of fire or burning.
Confirm connections to input/output terminals are correct as indicated in the instruction manual.
This power supply has a possibility for hazardous voltage to appear at output terminal depending on the type
of failure. The outputs of these products must be earthed in the end equipment to maintain SELV.
If the outputs are not earthed, they must be considered hazardous and must not be made user accessible.
Note: CE MARKING
CE marking, when applied to the LS series products, indicates compliance with the Low Voltage Directive
(2014/35/EU) in that it complies with EN60950-1.
DWG NO. : PA582-04-01-F
APPD CHK DWG
1
TDK-Lambda
LS 25-150 Series
INSTRUCTION MANUAL
1. Terminal Explanation
LS25, LS35, LS50, LS75
(1) L : Input terminal Live line (Fuse in line)
(2) N : Input terminal Neutral line
(3) FG : Functional Ground
(4) - V : - Output terminal
(5) +V : + Output terminal
(6) Output voltage adjustable trimmer
(7) Output monitoring indicator (Green LED : ON)
LS100, LS150
(1) L : Input terminal Live line(Fuse in line)
(2) N : Input terminal Neutral line
(3) FG : Functional Ground
(4) -V : - Output terminal
( 25A max./ terminal)
(5) +V : + Output terminal
( 25A max./ terminal)
(6) Output voltage adjustable trimmer
(7) Output monitoring indicator (Green LED : ON)
2. Terminal connecting method
Input must be off when making connection.
Connect FG terminal to ground terminal of the equipment.
The output load line and input line shall be separated and twisted to improve noise immunity.
LS25, LS35, LS50, LS75 LS100, LS150
Maximum output current of each output terminal is 25A except for LS25 (15A).
If more than 25A, use 2 terminals.
L N V ADJ
-V -V +V +V H
LOAD
-
+
L N V ADJ-V +V H
LOAD
-
+
5
4
3
2
1
L N V ADJ-V +V H
L N V ADJ
-V -V +V +V H
1
2
3
4
5
6
7
2
TDK-Lambda
LS 25-150 Series
INSTRUCTION MANUAL
3. Explanation of Functions and Precautions
3-1. Input Voltage Range
Input voltage range is single phase 88 ~ 264VAC (47 ~ 63Hz) or 125 ~ 373VDC for LS25 ~ LS100.
For LS150, selectable switch 115/230VAC will decide the input voltage range as mentioned in the table below.
Input voltage which is out of specification, may damage the unit. For cases where conformance to various
safety specs(UL,CSA,EN) are required, input voltage range will be 100~240VAC (50/60Hz ).
Note : LS series able to withstand Input Surge of 300VAC for 5 seconds.
LS150 – Selectable voltage range
Selected Range Applicable Input Voltage Range in VAC Applicable Input Voltage Range in VDC
115 88 ~ 132 NA
230 176 ~ 264 248 ~ 373
3-2. Output Voltage Range
V.ADJ trimmer is for output voltage adjustment within the range of specifications. Turning the trimmer clockwise will
increase the output voltage. Note over voltage protection ( OVP ) function may trigger if the output voltage is increased
excessively.
3-3. Inrush Current
Power Thermistor is built in to protect the circuit from high Inrush Current. Please select suitable input switch and fuse
rating in case of re-input the power at high temperature.
3-4. Over Voltage Protection (OVP)
The OVP function will shutdown the output except for LS25. The input need to be removed for a few minutes, and then
re-input for recovery of the output. OVP setting is fixed and cannot be adjusted externally.
Note : For LS25, OVP function will cause the output into ”hiccup” mode and damage the unit.
3-5. Over Current Protection (OCP)
OCP function operates when the output current exceeds OCP specifications. The output will automatically recover when
the overload condition is removed. Do not operate overload or dead short conditions for more than 30 seconds, which
could result in damage. There is no possibility of fire or burning.
3-6. Output Ripple & Noise
Ripple & noise are measured at 20MHz by using a 300mm twisted pair of load wires terminated with a 0.1uF film capac-
itor & 47uF electrolytic capacitor. When load lines are longer, ripple becomes larger. The output ripple cannot be meas-
ured accurately if the probe ground lead of oscilloscope is too long. At low temperature, large ripple & noise may also be
observed due to large ESR of the internal Electrolytic Capacitors especially at -25degC. Output voltage rise may not be
smooth during initial turn on at low temperature.
3-7. Series Operation
For series operation, either method ( A ) or ( B ) is possible.
3
TDK-Lambda
LS 25-150 Series
INSTRUCTION MANUAL
Method ( A ) Method ( B )
Output
Terminal
Output
Terminal
Load
Power
Supply
Power
Supply
Load
Load
Output
Terminal
Output
Terminal
Note : In case of Method ( A ), please connect diodes to prevent the reverse voltage.
3-8. Parallel Operation
(A) Operation to increase the Output Current is not possible.
(B) Operation as a Backup Power Supply is possible as follows.
1. Set the power supply output voltage higher by the amount of forward voltage drop ( VF) of the diode.
2. Please adjust the output voltage of each power supply to be the same.
3. Please use within the specifications for output voltage and output current.
(A) (B)
Load
Output
Terminal
Output
Terminal
Power
Supply
Output
Terminal
Output
Terminal
Load
Power
Supply
4. Isolation / Withstand Voltage
4-1. Isolation Test
Isolation resistance between output and FG (chassis) shall be more than 100Mat 500VDC. For safety, voltage setting
4
TDK-Lambda
LS 25-150 Series
INSTRUCTION MANUAL
of DC isolation tester must be done before the test. Ensure that the unit is fully discharged after the test.
(a) Output ~ FG (chassis) : 500VDC, 100Mor more
AC(L)
AC(N)
FG
+ V
+V
- V
- V
Isolation
Tester
4-2. Withstand Voltage
This series is designed to withstand 3.0kVAC between input and output, 1.5kVAC between input and FG (chassis) and
500VAC between output and FG (chassis) each for 1 minute. When testing withstand voltage, set current limit of with-
stand voltage test equipment at 20mA ( Output-FG (chassis) : 100mA ). The applied voltage must be gradually increased
from zero to testing value and then gradually decreased for shut down. When timer is used, the power supply may be
damaged by high impulse voltage at timer switch on and off. Connect input and output as follows :
(a) Input ~ FG (chassis) : solid line (c) Output ~ FG (chassis) : 500VAC, 1min (100mA)
1.5kVAC, 1min (20mA)
(b) Input ~ Output : dotted line
3kVAC, 1min ( 20mA )
AC(L)
AC(N)
FG
+V
+V
-V
-V
Withstand
Voltage
Tester
AC(L)
AC(N)
FG
+V
+V
-V
-V
Withstand
Voltage
Tester
5. Mounting Directions
5-1. Output Derating according to the Mounting Directions
Recommended standard mounting is Method ( A ). Method ( B ), ( C ) and ( D ) are also possible. Refer to the Output
Derating below. Please do not use installation Method ( E ), where the PCB will be on the topside and heat will be
5
TDK-Lambda
LS 25-150 Series
INSTRUCTION MANUAL
trapped inside the unit.
In the following derating curve, the maximum output current is denoted as 100%.
`
(A) Output Derating versus Ambient Temperature (Convection Cooling)
LS25-3.3
Output Derating Vs Ambient Temperature
0
20
40
60
80
100
120
-25 0 25 50 75 100
Ambient Temperature (oC)
LS25-5, -12, -15, -24, -36 & -48
Load (%)
Mounting
A&D
Mounting
B&C
50
40 65 70
6
TDK-Lambda
LS 25-150 Series
INSTRUCTION MANUAL
Output Derating Vs Ambient Temperature
0
20
40
60
80
100
120
-25 0 25 50 75 100
Ambient Temperature (oC)
LS35-3.3, -5, -12, -15, -24, -36 & -48
Output Derating Vs Ambient Temperature
0
20
40
60
80
100
120
-25 0 25 50 75 100
Ambient Temperature (oC)
LS50-3.3, -5, -12, -15, -24, -36 & -48
Mounting
A&D
Mounting
B&C
Load (%)
50
40 65 70
Mounting
A,B & D
Mounting
C
Load (%)
65 70
45
50
7
TDK-Lambda
LS 25-150 Series
INSTRUCTION MANUAL
LS75-3.3, -5
LS75-12, -15, -24, -36 & -48
Output Derating Vs Ambient Temperature
0
2
0
4
0
6
0
8
0
100
120
-
25
2
5
5
0
7
5
100
Ambient Temperature (°C)
Load (%)
Mounting
Mounting
A, B & D
C
70
706045
Output Derating Vs Ambient Temperature
0
2
0
4
0
6
0
8
0
100
120
-
25
0 2
5
5
0
7
5
100
Ambient Temperature (°C)
Load (%)
Mounting
Mounting
A, B & D
C
40 60 70
50
70
8
TDK-Lambda
LS 25-150 Series
INSTRUCTION MANUAL
LS100-3.3, -5
LS100-12, -15, -24, -36 & -48
Output Derating Vs Ambient Temperature
0
2
0
4
0
6
0
8
0
100
120
-
25
2
5
5
0
7
5
100
Ambient Temperature (°C)
Load (%)
Mounting
Mounting
A & B
C & D
50
70
4540
Output Derating Vs Ambient Temperature
2
0
4
0
6
0
8
0
100
120
-
25
0 2
5
5
0
7
5
100
Ambient Temperature (°C)
Load (%)
Mounting
Mounting
C
A, B & D
7060
70
9
TDK-Lambda
LS 25-150 Series
INSTRUCTION MANUAL
LS150-3.3, -5
LS150-12, -15, -24, -36 & -48
Output Derating Vs Ambient Temperature
0
2
0
4
0
6
0
8
0
100
120
-
25
0 2
5
5
0
7
5
100
Ambient Temperature (°C)
Load (%)
Mounting
Mounting
A
B, C & D
50
7030 40
Output Derating Vs Ambient Temperature
2
0
4
0
6
0
8
0
100
120
-
25
0 2
5
5
0
7
5
100
Ambient Temperature (°C)
Load (%)
Mounting
Mounting
A & B
C & D
50
70
45
10
TDK-Lambda
LS 25-150 Series
INSTRUCTION MANUAL
(B) Output Derating versus Input Voltage (Convection Cooling)
LS100-3.3, -5, -12, -15, -24, -36 & -48
NOTE : LS25, LS35, LS50, LS75 & LS150 series do not require Input Voltage Derating.
5-2 Mounting Method
1) This is convection cooling type power supply. In consideration of the heat radiation and safety, please keep a dis-
Output Derating Vs Ambient Temperature
0
2
0
4
0
6
0
8
0
100
120
-
25
2
5
5
0
7
5
100
Ambient Temperature (°C)
Load (%)
Mounting
Mounting
A
B, C & D
70
70
40
Output Derating Vs Input Voltage
0
20
40
60
80
10
0
12
0
88 23
0
Vin (VAC)
LOAD (%)
115 264
11
TDK-Lambda
LS 25-150 Series
INSTRUCTION MANUAL
tance of more than 15mm between the power supply and the peripheral parts. When lining up multiple units, please
make sure to place them 15mm or more apart from each other.
2) Maximum allowable penetration of mounting screws into the power-supply is 5mm except LS25 (4mm).
3) Recommended torque for mounting screws of LS25 ~ LS150 (M3 screw) : 0.49 Nm (5.0 kgfcm).
6. Wiring Method
The input and output load wires shall be separated and twisted to improve noise immunity.
Both wires must be as thick and short as possible to make lower impedance.
Noise can be reduced by connecting a film capacitor with 0.1uF capacitance across the load terminals.
For safety and EMI considerations, connect the FG terminal of LS series to mounting set ground terminal.
The recommended wire type :
MODEL Recommended
Wire
Recommended torque
Recommended crimp-type terminal
D
(MAX)
t
(MAX)
Mounting
Pieces
(MAX)
LS25 AWG16-22 M3.0 Screws
0.49 Nm (5.0 kgfcm) 6.0mm 0.8mm 2 pieces
LS35 ~ LS150 AWG14-22
M3.5 Screws
1.0 Nm (9.8 kgfcm) ~
1.4 Nm (13.7 kgfcm)
6.8mm 0.8mm 2 pieces
Note 1 : When using separate loads, it is recommended to use 2 pieces of 0.8mm thick crimp-type terminal.
Note 2 : For recommended wire diameter, refer to wire maker recommended allowable current and voltage
drop. For higher output current model like 3.3V & 5V, bigger diameter wire is recommended.
7. External Fuse Rating
Refer to the following fuse rating when selecting the external input fuse. Surge current flows when input turns on.
12
TDK-Lambda
LS 25-150 Series
INSTRUCTION MANUAL
Fuse rating is specified by Inrush Current value at input turn on. Do not select the fuse according to input current (rms)
values under the actual load condition.
LS25 : F1.6A , 250V
LS35, LS50 : T2A , 250V
LS75 : T2.5A , 250V
LS100 : F4A , 250V
LS150 : F5A , 250V
8. Before concluding that the unit is at fault, make the following checks.
Check if the rated input voltage is connected.
Check if the wiring of input and output is correct.
Check if the wire size is correct.
Check if the output voltage trimmer (V.ADJ) is properly adjusted.
Check if the output current and output wattage does not exceed the specification.
Ensure that a large capacitor is not connected across the output terminals. Please use within maximum capacitance
shown below.
Maximum external capacitance
MODEL 3.3V 5V 12V 15V 24V 36V 48V
LS25 10,000uF 5,000uF 2,000uF 1,000uF 500uF
LS35~LS50 10,000uF 5,000uF 2,000uF 500uF
LS75~LS150 10,000uF 5,000uF 1,000uF
NOTE : It is normal to hear audible noise from power-supply under Dynamic Load operation or if the input voltage
waveform is not sinusoidal.
9. Warranty Condition
This product is under warranty for 3 years (based on 8 hours/day operation) from the date of shipment. During the
warranty period, TDK-Lambda will, at it’s option, either repair or replace products prove to be defective.
Warranty applies but not limited to the following.
(1) Average operating temperature (ambient temperature of the power supply unit) is under 40oC.
(2) Average load factor is 80% or less.
(3) Installation method : Standard installation.
Following cases are not covered by warranty.
(1) Improper usage and mis-handling like dropping or applying shock to the unit and defects from operation
exceeding specification of the product.
(2) Defects resulting from natural disaster (fire, flood).
(3) Unauthorized modification or repair.

Products

AC/DC CONVERTER 5V 25W
Cantidad disponible967
Precio por unidad18.02
AC/DC CONVERTER 3.3V 25W
Cantidad disponible441
Precio por unidad18.02
AC/DC CONVERTER 12V 25W
Cantidad disponible1736
Precio por unidad18.67
AC/DC CONVERTER 24V 25W
Cantidad disponible683
Precio por unidad18.67
AC/DC CONVERTER 15V 25W
Cantidad disponible230
Precio por unidad18.67
AC/DC CONVERTER 24V 35W
Cantidad disponible1283
Precio por unidad19.39
AC/DC CONVERTER 12V 35W
Cantidad disponible844
Precio por unidad20.56
AC/DC CONVERTER 24V 50W
Cantidad disponible1085
Precio por unidad21.64
AC/DC CONVERTER 12V 50W
Cantidad disponible462
Precio por unidad22.94
AC/DC CONVERTER 24V 75W
Cantidad disponible1302
Precio por unidad26.65
AC/DC CONVERTER 48V 75W
Cantidad disponible828
Precio por unidad26.65
AC/DC CONVERTER 12V 75W
Cantidad disponible731
Precio por unidad26.65
AC/DC CONVERTER 15V 75W
Cantidad disponible158
Precio por unidad26.65
AC/DC CONVERTER 12V 100W
Cantidad disponible1285
Precio por unidad34.29
AC/DC CONVERTER 24V 100W
Cantidad disponible229
Precio por unidad34.29
AC/DC CONVERTER 36V 100W
Cantidad disponible148
Precio por unidad34.29
AC/DC CONVERTER 24V 150W
Cantidad disponible1039
Precio por unidad39.96
AC/DC CONVERTER 12V 150W
Cantidad disponible183
Precio por unidad39.96
AC/DC CONVERTER 15V 150W
Cantidad disponible178
Precio por unidad39.96
AC/DC CONVERTER 15V 35W
Cantidad disponible295
Precio por unidad19.39