Relays

0 Results
Suggestions

  • Make sure that all words or part numbers are entered correctly
  • Try different keywords
  • Try more general keywords
Additional Questions?

  • Can't find what you're looking for? Ask the TechForum
If new to Digi-Key

Digi-Key offers the world's largest selection of electronic components in stock and available for immediate shipment. From prototype to production, we are here to fuel innovation all over the world. We are proud to be highly recognized as the leader for:

  • Availability of Products
  • On time Delivery
  • Overall Performance
  • Engineer-Friendly Website

For more information visit Help & Support
Featured Manufacturers
Image of TE Connectivity color logo
Image of Panasonic color logo
Image of Omron Logo
Image of Sensata Technologies logo
Image of Omron Automation Logo
Image of TE Connectivity color logo

About Relays


Relays and contactors are devices used to switch or interrupt the flow of electrical current in one or more circuits, using a control signal which is galvanically isolated from the circuit(s) being controlled, with various sub-groups demarcated along lines of device construction or intended application. Traditionally and still-commonly based on the use of an electromagnet to open or close a set of mechanical switch contacts, newer devices using solid-state technologies are also widely available, with both types having characteristics to recommend them under different application conditions.

Image of Relay, SPDT schematic symbol Image of Relay, DPST schematic symbol Image of Relay, DPDT schematic symbol Image of Relay, SPST schematic symbol