MONSTER M4SK Datasheet by Adafruit Industries LLC

adafruit learning system
Adafruit MONSTER M4SK
Created by Phillip Burgess
Last updated on 2021-07-23 01:06:39 PM EDT
2
4
9
9
13
14
14
15
16
17
18
25
25
27
28
29
31
32
34
36
38
39
40
40
41
42
43
44
45
47
47
48
49
51
52
53
53
54
55
55
55
56
57
57
Guide Contents
Guide Contents
Overview
Update the UF2 Bootloader
Updating Your Bootloader
Quickstart
Flash Filesystem
Creating the SPI Flash Filesystem
I’m not seeing the MASKM4BOOT drive!
Initializing the filesystem is a one-time operation. You should not need to repeat this process, unless the flash drive contents somehow
get corrupted.
M4 EYES Firmware
Ready-Made Graphics
Customization Basics
Troubleshooting JSON
Preparing Graphics
Image Storage
Eyelids
Configurable Settings
Sizes and Shapes
Colors and Textures
Distinct Left/Right Eyes
Eyelids
Light Sensor
Voice Changer
Usage
Example Config.eye File
Tips for using the Monoprice 5-Watt Guitar Amplifier
Building Eyes from Source Code
Arduino IDE Setup
https://adafruit.github.io/arduino-board-index/package_adafruit_index.json
Using with Arduino IDE
Install SAMD Support
Install Adafruit SAMD
Install Drivers (Windows 7 & 8 Only)
Blink
Successful Upload
Compilation Issues
Manually bootloading
Ubuntu & Linux Issue Fix
Source, Libraries and Settings
Source Code
Libraries
Project Settings
Troubleshooting
Board Unresponsive; Flashing Red LED
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 2 of 76
57
57
58
58
58
59
59
61
63
64
64
65
67
67
68
69
70
70
71
71
72
73
73
73
74
Ol’ Blue Eyes
Crossed Eyes
Technicolor Snow
Erase the Filesystem
Diagnostics
Lens Holders
Lens Holders
3D Printed Options
Voice Changer
Pinouts
Displays and Display Connectors
Microcontrollers and Flash
Power Switch and Ports
Audio
Capacitive Touch Pad and Buttons
Sensors
I2C Connector
Digital/Analog Connectors
Reset Button
LED
SECTION TITLE HERE
Downloads
Files:
Schematic
Fab Print
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 3 of 76
Peep dis! Have you always wanted to have anoiher pair of eyes on me back of your head? Or ouifii costume with big beautiful orbs? The MONSTER M4SK b twice as good. with two gorgeous 240x240 pixel IPS TFT displays, driven by a 120MHz Cortex M4 processor that can pump out those pixels super fasi.
Overview
Peep dis! Have you always wanted to have another pair of eyes on the back of your head? Or outfit your
costume with big beautiful orbs? The MONSTER M4SK is like the Hallowing (https://adafru.it/CmY) but
twice
as good, with two gorgeous 240x240 pixel IPS TFT displays, driven by a 120MHZ Cortex M4
processor that can pump out those pixels super fast. You'll get the same quality display as our Raspberry
Pi Eyes kit but without needing to tote around a full Linux computer (https://adafru.it/FAY)
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 4 of 76
This unique design as a human (“63mm] but is designed so that the nose section c
This unique design has the eyes at the same pupil-distance as a human (~63mm) but is designed so that
the nose section can be broken apart with pliers/cutters and then wired together with a 9-pin JST SH cable
up to 100mm long (https://adafru.it/FAZ) so the eyes can be re-positioned or freely attached.
We wanted to make audio-effects easier so in addition to a class D audio amp, there's also a stereo
headphone jack that is connected to the two DACs on the chip. Use it when you want an externally sound
amplifier box for big effects. For small portable effects, the built-in amp can drive 8 ohm speakers up to 1
Watt.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 5 of 76
each side are JST-PH plu ces. The 3- on the SAMD51. so you 0 devices e |2C pen and you can lional Mar
On each side are JST-PH plugs for connecting external devices. The 3-pin JSTs connect to analog/timer
pins on the SAMD51, so you can use them for sensors or GPIO devices. The 4-pin JST connector connects
to the I2C port and you can fit Grove connectors in it for additional hardware support. For the PDM mic
port, you can use this cable (https://adafru.it/FA-) to wire to a PDM mic (https://adafru.it/FB0).
There's also plenty of sensors built in - light sensor, 3 tactile buttons, and a capacitive touch pad on the
nose.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 6 of 76
Speak Th oonuooluooluoo And as you can expect, we've got some great new eyeball code, which does 2 eyes with user-configura e graphics. Right now our code support is only for Arduino - Circuiththon isn't quite fast enough to do th 3D animation techniques we use to draw the eyeballs.
Speaking of that nose, the silkscreen is by the skillful Miss Monster, check out those
fangs! (https://adafru.it/FB1)
This is by far the cutest, creepiest and most incredible development board we've made so far!
Gaze upon
these features:
ATSAMD51G19 Cortex M4 microcontroller running at 120MHz with 512KB Flash, 192KB RAM
8 MB QSPI flash for storing graphics and sound effects
Two 240x240 IPS TFT displays each on their own SPI bus
Beautiful silkscreen with a boop-able nose that is a capacitive touch pad
Lipoly battery charge circuit for portable use
Stereo headphone jack out, for sound effects via an amplifier
Mono speaker driver for smaller 8 ohm 1W speakers
One 4 pin STEMMA JST connector for I2C connection (also Grove compatible)
Two 3 pin STEMMA JST connectors with digital/analog/PWM for servos, sensors, etc
One 4 pin JST SH port for connecting an optional PDM microphone
Backlight controls
Three tactile buttons
Light sensor
On/Off Switch and reset button
And as you can expect, we've got some great new eyeball code, which does 2 eyes with user-configurable
graphics. Right now our code support is only for Arduino - CircuitPython isn't quite fast enough to do the
3D animation techniques we use to draw the eyeballs. The eyes look
even better
if you pair them with
these 40mm glass or plastic lenses. (You'll need two of course) (https://adafru.it/FB2)
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 7 of 76
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 8 of 76
cunnenmrz unsxmm IDFQUFIIXT
Update the UF2 Bootloader
Your SAMD51 M4 board bootloader may need to be updated to fix an intermittent bug that can erase parts
of internal flash.
Updating Your Bootloader
To see if you need to update your bootloader, get the UF2 boot drive to appear as a mounted drive on
your computer, in a file browser window. If you're running MakeCode, click the reset button once. If you're
running CircuitPython or an Arduino program, double-click the reset button.
When you see the ...BOOT drive (FEATHERBOOT, METROM4BOOT, ITSYM4BOOT, PORTALBOOT, etc.) ,
click the drive in the file browser window and then double-click the INFO_UF2.TXT file to see what's
inside.
The example screenshots below are for a PyGamer. What you see for your board will be largely the same
except for the board name and the BOOT drive name.
The bootloader version is listed in INFO_UF2.TXT. In this example, the version is v3.6.0.
Update the Bootloader on your SAMD51 M4 board to prevent a somewhat rare problem of parts
of internal flash being overwritten on power-up.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 9 of 76
F2 59.9mm“; v3.6.0 SFHHRO Model: PyGamer Board—ID: SAMDSlJlBA—PyGaner—M4
If the bootloader version you see is older than
v3.9.0
, you need to update. For instance, the bootloader
above needs to be upgraded.
Download the latest version of the bootloader updater from the circuitpython.org Downloads page for your
board.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 10 of 76
ht‘lps://adafru.it/Em8
https://adafru.it/Em8
The bootloader updater will be named update-bootloader-
name_of_your_board
-v3.9.0.uf2 or some
later version. Drag that file from your Downloads folder onto the BOOT drive:
https://adafru.it/Em8
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 11 of 76
E Down‘oads <> Favwr‘ms \ @ AirDrop E Reoents A Application: updata~ bcdfloa..39.0m2 mm 0 icloud Drive a Desktop 3 Documents Lon-1mm Q PVGAMEREOOT = Tag: I Orange F2 “91mg; v3.9.0 smwnu Model: PyGamer Boa rd-ID: SAHD51J 19A-PyGaIIe r414
After you drag the updater onto the boot drive, the red LED on the board will flicker and then blink slowly
about five times. A few seconds later, the BOOT will appear in the Finder. After that, you can click on the
BOOT drive and double-click INFO_UF2.TXT again to confirm you've updated the bootloader.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 12 of 76
Quickstart
The MONSTER M4SK board should arrive ready-to-scare. Connect a battery or USB cable, move the
power switch to the “on” position, and after a few seconds you should get blinking eyes.
The next few pages cover…
How to reformat the flash storage. Most readers can skip this , unless you got one of the very earliest
MONSTER M4SK boards, or if it just needs a complete wipe.
How to install or update the eye firmware for the latest features and bug fixes.
Loading different eye designs.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 13 of 76
hrtps://adafru.it/FPn
Flash Filesystem
If plugging your MONSTER M4SK board into a computer over USB and it does
not
appear as a small flash
drive named CIRCUITPY, it’s usually one of three reasons:
Verify that you’re using a USB “charge and sync” cable,
not
a charge only cable.
The first batch of MONSTER M4SK boards did not have the flash filesystem initialized…we’ll cover
that below.
Something happened…maybe static, maybe a bug in the software…and corrupted the flash drive
contents.
If you do see the CIRCUITPY flash drive, everything’s good and you can skip ahead to the next page.
Creating the SPI Flash Filesystem
If the CIRCUITPY drive does not appear, this just involves temporarily installing a version of CircuitPython.
The eye code isn’t written in CircuitPython, we’ll just use it here to get the flash initialized!
Download that .UF2 file here:
https://adafru.it/FPn
Connect MONSTER M4SK to your computer with a USB
cable, set the power switch to the ON position and
double-tap the reset button to enter bootloader mode.
After a moment, a drive called MASKM4BOOT should appear.
https://adafru.it/FPn
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 14 of 76
v Devices and drives (4) I _:"‘“" ”a“ (‘3') mm mi». (0:) v QSIGBVMMDBITB J r; bum-p (2) Elm (6:) v m as in: M an as v 614 Mal-a: «7.74 w v Nemwork locations (1)
I’m not seeing the MASKM4BOOT drive!
Things to check:
Confirm the power switch is in the ON position.
Double-tap the reset button again. The red LED on the back should do a slow “breathing” cycle. If
not, try again.
Make sure you’re using a good USB “charge and sync” cable,
NOT
a “charge only” cable.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 15 of 76
v Devices and dnves (4) Laal DisH Wu DM (Ix) gz‘asnauuzfls ~ big badmp (a) CIRC|Il1PV(E) § 93‘ 689mg D1931 GE § 795mm: afisé MB
Drag the CircuitPython .UF2 file to this drive and wait a
few seconds.
After CircuitPython installs, and with the MONSTER M4SK board connected over USB, it should appear on
your computer as an 8 MB flash drive called CIRCUITPY.
Initializing the filesystem is a one-time operation. You should
not
need to repeat this
process, unless the flash drive contents somehow get corrupted.
In rare situations the flash memory might need a complete erasing, before even setting up the
flash filesystem. The Troubleshooting page of this guide includes a utility for this. Once erased,
you can then start again with the filesystem setup as described above.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 16 of 76
https://adafru.it/TPe https://adafru.it/TPA .‘g bdzlup m m o {m A. wxwmr m Nelwn x Ham m ‘ not the
M4 EYES Firmware
To update firmware on your MONSTER M4SK board with the latest eye animation software, start by
downloading this .UF2 file:
https://adafru.it/TPe
For a HALLOWING M4 board, use this .UF2 instead:
https://adafru.it/TPA
The firmware update sequence is:
1. Connect a USB cable and put the power switch in
the “on” position
2. Double-tap the reset button
3. Wait for the MASKM4BOOT drive to appear!
4. Drag the M4SKEYES.UF2 file to the MASKM4BOOT
drive and wait for it to copy over
5. The board will automatically reboot
After installing the firmware (and a brief pause while the
software initializes) you should get some animated
eyeballs.
If you don't see any eyes, make sure you dragged the
M4SKEYES.UF2 file to the M4SKBOOT bootloader drive
not the CIRCUITPY drive
If you get simple flat-colored eyes like shown here…that
just means no graphics files are installed yet. We cover
that on the next page. But at least we know the code’s
installed!
If you get textured eyes that blink…code and graphics are
all in good shape! The next page shows how to install
different looks…and later we get into total customization.
https://adafru.it/TPe
https://adafru.it/TPA
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 17 of 76
ht‘lps://adafru.it/FAH I config.eye V - hazel I config.eye 2 iris.bmp g |ower.bmp = sclera.bmp g upper.bmp " T _ > C‘RCU‘TPV(F:) > v b Siavth C‘F’CU‘TPV'iF P — I 19:“an had llb “Mitzi-(mu- Jmha mumm config.eye
Ready-Made Graphics
To install different “looks,” download and unzip this collection of eyeball graphics:
https://adafru.it/FAH
Inside the “eyes” folder are several sub-folders, one for each of our ready-made eye designs. “hazel” is
our standard human eye from prior projects…then we’re adding more as Halloween approaches.
Each folder contains a set of .bmp images for that eye, plus a file called “config.eye.” Copy one of these
folders to the CIRCUITPY drive —
not
the individual files, but the
whole folder.
Then copy or move the file
called config.eye out of the folder and into the drive’s root directory.
Copy these files to the CIRCUITPY drive.
Remember that config.eye goes in the root directory, along with the hazel (or other eye name) folder.
https://adafru.it/FAH
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 18 of 76
Press the board’s reset button…
There will be a delay of several seconds as the eye code initializes. Then…animation!
If you get a flat-colored white eyeball with blue irises and no eyelids, something’s wrong! Verify that you’ve
copied over a whole folder of graphics (not the individual files) and moved or copied that folder’s
config.eye to the root directory.
Aside from the stock hazel eyes, some of the alternate designs include:
big_blue is a pair of large and friendly blue-gray eyes.
The sclera doesn’t have all the veins of the hazel eyes,
making this less creepy.
fish_eyes is the same unblinking eyes used in our Fish
Head MONSTER M4SK project (https://adafru.it/FQj).
hypno_eyes have that cartoon mesmerizing look. “You
are in my power!”
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 19 of 76
reflection looks like a pair of shiny spheres. No eyelids or
pupils, just spheres looking extremely reflective.
*ting!*
snake_green is perfect for dragons and other reptilian
characters.
Rar!
This shows off the slit pupil option…also
useful for cats and the like.
spikes is adapted from the guide CustomEyesation: DIY
Monster M4SK Graphics (https://adafru.it/FFU) and
demonstrates a bit how the distortion of texture mapping
works.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 20 of 76
toonstripe is a different “mesmerizing eyes” look…candy
colors, no eyelids.
doom-red and doom-spiral were designed for the
MONSTER M4SK Toon Hat (https://adafru.it/FQk) guide
but might have other uses or tricks to learn from.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 21 of 76
The demon eyes have swirling fire … a bit of an “Eye of
Sauron” resemblance.
anime does its best approximation of The Quaking Moist
Anime Eyes Effect™.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 22 of 76
fizzgig resembles the fuzzy
Dark Crystal
character. These
react to ambient light and were designed with the lenses
in mind.
SECRET FEATURE: You can select among four different eye configurations on startup. Hold down one of
the three buttons on top when powering on (or pressing reset) to load files config1.eye (inner button),
config2.eye (middle button) or config3.eye (outer button) instead of the default config.eye. All go in the
root directory for now (but graphics & such can go in folders).
If one of the ready-made designs does what you need…fantastic, you’re all done! If you want to make
changes, or create your own custom eyes, read on…
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 23 of 76
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 24 of 76
If c on your compute n Troubleshooting 0 O O a“ NO NAME >> Eye graphics small buz
Customization Basics
If our ready-made eye designs don’t meet your needs, you can personalize quite a bit by editing a text file
and providing some graphics.
On startup, our eyeball code loads a file called config.eye from the device’s root directory. This is a plain-
text file that any simple editor can handle…
Notepad, TextEdit, vim
and so forth.
If customizing your eyes, maintain a backup of the board’s contents on your computer. There is a
small but
nonzero
chance of a glitch that could require a full reinstall. See the Troubleshooting (https://adafru.it/TPc)
page for help.
The
syntax
of this file is a format called
JSON.
There’s good and bad news…
The good: JSON has a standardized syntax and we can leverage existing code to read it…we’re not
starting from scratch with a new file format.
The bad: JSON files are really meant to be read and written by machines, as a way to preserve program
state…
not
edited by humans. It’s
phenomenally
picky about getting syntax
just right
and does not fall back
gracefully.
The saving grace: if you’re just changing colors and textures, you might not need to edit this file at all!
Quite often you can just substitute different graphics files with the same names.
Troubleshooting JSON
If even a
single character
is out of place in config.eye, the
whole thing
will fail to load and there’s no
helpful indication of where the problem lies.
If this happens, the eyes will run in a default state: blue eyes with no eyelids, and everything is “flat
colors, no textures. This isn’t helpful in
isolating
the problem but at least tells you there
is
a problem.
You wont be able to double-click this file, so open it from WITHIN your text editor
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 25 of 76
gggh a; this one a; h'gon org
One way to troubleshoot this is to start with a known valid eye configuration, then change one setting at a
time and restart the code. If the eyes revert to the default state, the last change contains the syntax error.
Quite often it’s just a missing double quote or extra comma.
Another option is to use a JSON validator such as this one at hjson.org (https://adafru.it/FzV). Copy-and-
paste your eyeball configuration into the left pane…if there’s a problem, this will be reported on the right.
Here’s an simple config.eye file to start with:
{
"pupilColor" : [ 0, 0, 0 ],
"backColor" : [ 140, 40, 20 ],
"irisTexture" : "graphics/iris.bmp",
"scleraTexture" : "graphics/sclera.bmp",
"upperEyelid" : "graphics/upper.bmp",
"lowerEyelid" : "graphics/lower.bmp"
}
Some things to notice:
The whole thing is contained within
curly braces
{ and }
Each item has a name (always in quotes), a colon separator ( : ) and a value. Values might be
numbers, strings (in quotes) or arrays (in square brackets) depending on what’s being configured.
This is a
list
and each line ends with a comma
except
for the last item in the list. Watch out for
missing or surplus commas!
JSON is case-sensitive. "Foo", "foo" and "FOO" are all different things.
Using extra spaces to line up columns really isn’t necessary, just something I do to assist with
legibility. Some folks just find it annoying.
Comments (starting with // ) are
not
standard JSON syntax, but the library we use allows them and I
find them very helpful.
Each option will be explained in detail on the “Configurable Settings” page. But first let’s talk about
graphics
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 26 of 76
wwiw ‘ , = Iris "lt'ext‘lfi‘ré'i/Igp H M
Preparing Graphics
So we’re singing from the same page, let’s lay out some eye terminology…
The technical term for the “white” of the eye is the
sclera.
The
iris
is the muscle that contracts to adjust the size of
the
pupil
in response to light.
The
upper
and
lower eyelids
are involved in blinking.
This program’s eye graphics are stored flat and unrolled, like a map projection. The horizontal (X) axis
works like the longitude, or angle around the eye, while the vertical (Y) axis is the latitude. The images are
wrapped around the pupil in a clockwise direction.
There are two images (or
texture maps
) associated with the eyes…one for the iris, another for the sclera.
The iris is what we think of as the “color” of the eye and is most often what you’ll want to edit. Sometimes
you just need to edit the hue & saturation in a program like Photoshop, or you can make something totally
custom if you’re after a particular look.
The sclera is the “white” of the eye…which really isn’t that white at all. There’s veins and blotches and
gross stuff!
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 27 of 76
Tiny 5x2 pixel texture —~ 1) Huge 512x128 pixel Iexture .I-I-III Same result!
Image Storage
The texture maps are stored as 24-bit BMP images…nobody’s favorite, but easy for microcontrollers to
handle. (This is also sometimes called “Windows Bitmap” format, though plenty of non-Windows software
can read and write these images…and
not
to be confused with “X BitMap” or “Portable Bitmap Format,”
different animals.)
Textures are loaded from drive into RAM, downsampled to 16-bit color (what the displays natively use) and
then written to the chip’s internal flash memory (different from the flash filesystem). Although the code
places no strict limit on image dimensions, RAM and flash are both finite resources , and this limits to how
large these textures can be…both individually and in total.
No
single
image can exceed available RAM, or about 160 kilobytes. The total of
all images
must fit within
flash, or about 360 kilobytes. These figures might change a bit in the future, so try to leave yourself some
overhead.
Use the following formula to determine the space needed for an image:
width in pixels × height in pixels × 2 bytes
For example, a 500 × 150 pixel texture would consume 500 × 150 × 2 = 150,000 bytes. This fits in RAM just
fine, and takes up a bit less than half of the flash space.
You
don’t
have to texture-map both the iris and sclera if you don’t want to…on the
Configurable Settings
page we explain how to use solid colors for either or both. Also shown there…it’s possible to assign
independent textures to the left and right eyes. When both eyes are sharing the same texture, the code will
place only one instance in flash, saving space.
To make the re-use of textures less obvious, the “seam” where a texture map wraps around is normally at
the 12 o’clock position for the right eye and 6 o’clock for the left eye. The
Configurable Settings
page
shows how to change this.
Eye textures can be any size (RAM permitting), on either
axis…even down to a single pixel. When wrapping small
images around the whole eye, nearest-neighbor sampling
(no interpolation) is used. This can be exploited to create
stylized blocky or grid designs…no need to waste space
on a big image when just a few pixels will do.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 28 of 76
Phatoshop users: the eye code maps textures differently than Phatoshop’s "Polar Coordinates" filter. Ours wra co p
Too-large images may exceed available space, while too-small images may exhibit visible jaggies (unless
you’re aiming for that effect as described above). The ideal size can be calculated based on the
circumference of the iris or the whole eye
The iris and overall eye size are configurable (shown on following page)…but for example, let’s assume
you’ve got an iris with a 60 pixel radius (120 pixel diameter) and the eyeball has a 125 pixel radius (250
pixel diameter)…both of these are the defaults.
Multiply the iris and/or eye diameters by Pi (3.14) to get the ideal width in pixels for the iris and sclera
images.
For example: iris with 120 pixel diameter. 120 px × 3.14 = 377 pixels wide. You can use that, or round up or
down a smidge to a round number if you like (e.g. 360 or 380 pixels).
Sclera image width for 250 pixel diameter eye: 250 × 3.14 = 785 pixels wide…but again, OK to round up or
down a little…use 800 pixels wide if you like, unless really pressed for space.
The ideal image
heights
are a bit different. First, although the code can
load
any size image, it won’t
actually
benefit
above 128 pixels on the vertical axis, it’s just wasted space. For the iris, use its radius (60
pixels in the case described above) or even a little less, since the pupil is always open a bit. For the
sclera…try 200 minus the iris radius, keeping in mind the 128 pixel recommended maximum (e.g. with a 60
pixel iris, 140 is our target, then cap it at 128). But…with an 800 pixel wide sclera as described above…800
× 128 × 2 = 204 kilobytes…quite a bit over the 160K RAM limit! Whittle down one or both axes, whatever
you think can best handle less resolution, until you find a size that fits. Once in motion, and at a reasonable
viewing distance, minor “jaggies” aren’t that noticeable.
Photoshop users: the eye code maps textures differently than Photoshops Polar Coordinates filter. Ours
wraps
clockwise,
with the
top
of the image becoming the outer circumference, while Photoshop wraps
counterclockwise,
with the
bottom
becoming the outer circumference. If using Photoshop to create or
preview textures, simply rotate the rectangular image 180°
before
applying a rectangular-to-polar filter, or
after
a polar-to-rectangular filter.
Eyelids
The eyelids have stricter requirements. There are always two files (one each for the upper and lower
eyelids) both 240 × 240 pixels exactly, both 1-bit BMP images
(NOT 24-bit like the texture maps!)
.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 29 of 76
v Upper Eyelid Lower Eyelid
The white area — which should span the entire 240 pixel widthrepresents the extent of vertical motion,
the “open-most” and “closed-most” range. The eyes won’t hold the open-most position all the time when
idle…the upper eyelid “tracks” the moving pupil, because that’s how eyes work.
A good set of eyelid images will overlap by a few pixels, so the eye makes a good solid blink.
This particular set of eyelids is slightly asymmetrical to approximate the eye’s
caruncle*
— that triangular
bit by the tear duct. The shape is mirrored between the two eyes. But it is super 100% okay to make
symmetrical eyelids if you prefer…a simple “football shape”…that usually looks better on a single-eye
board like the HalloWing M4. For some of the eye designs we’ll offer both.
* Which itself is a vestigial remnant of the
nictitating membrane,
the “third eyelid” that reptiles have.
How
cool is that!?
The eyelid images as shown above are for the right eye. That is… the
monster’s
right eye, meaning the eye
on the left when looking at the M4SK.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 30 of 76
Configurable Settings
Let’s look at the configuration for our stock “hazel” human eye. It doesn’t reference every configurable
setting, but shows the general format of these files
{
"eyeRadius" : 125,
"eyelidIndex" : "0x00", // From table: learn.adafruit.com/assets/61921
"pupilColor" : [ 0, 0, 0 ],
"backColor" : [ 140, 40, 20 ],
"irisTexture" : "hazel/iris.bmp",
"scleraTexture" : "hazel/sclera.bmp",
"upperEyelid" : "hazel/upper.bmp",
"lowerEyelid" : "hazel/lower.bmp",
"left" : {
},
"right" : {
}
}
This is a plain text file that any simple editor should be able to handle…Notepad or TextEdit or whatever
comes bundled on your computer.
It’s worth reiterating these points from the “Customization Basics” page:
The whole thing is contained within
curly braces
{ and }
Each item has a name (always in quotes), a colon separator ( : ) and a value. Values might be
numbers, strings (in quotes) or arrays (in square brackets) depending on what’s being configured.
This is a
list
and each line ends with a comma
except
for the last item in the list. Watch out for
missing or surplus commas!
JSON is case-sensitive. "Foo", "foo" and "FOO" are all different things.
Using extra spaces to line up columns really isn’t necessary, just something I do to assist with
legibility. Some folks just find it annoying.
Comments (starting with // ) are
not
standard JSON syntax, but the library we use allows them and I
find them very helpful.
The “Customization Basics” page also has some JSON troubleshooting tips. If you encounter trouble,
review that page!
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 31 of 76
Remember that JSON is case-sensitive. This must be spelled . Different capna/izatr'on will cause i
Sizes and Shapes
Two settings define the basic geometry of the eye…
eyeRadius establishes the size of the overall eyeball, in pixels. This is a
radius
— center to edge — so the
overall eye size is
twice this
across. For example eyeRadius:125 configures the eye to be 250 pixels wide.
This is the default if left unspecified.
The screens are only 240 pixels wide. Reason the eye is made a little bigger is because the code uses
tricks to
fake
a rotating sphere…and that faking is more apparent as the pupil approaches an edge. So we
push the edge out a few extra pixels, then
cover it up with eyelids.
If designing an eye with no eyelids, you might want eyeRadius:120 instead, which provides a nice perfect
circle on the screen.
Remember that JSON is case-sensitive. This must be spelled
eyeRadius
. Different capitalization will cause
it to be ignored!
irisRadius establishes the size of the iris…again a
radius,
in pixels.
irisRadius:60 will make the iris 120 pixels across, or half the width of the screen. If you plan to use lenses
over the displays, consider scaling down this number a bit to compensate.
Some creatures…cats and so forth…have
very large irises
and almost
no visible sclera
. In that case you can
set irisRadius much larger, up to (but not exceeding) eyeRadius .
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 32 of 76
Nate that using f Screen Size: 2401»: 120px Jé» snmeundndms
A third setting, slitPupilRadius , lets you make cat or dragon type eyes with a vertical slit pupil (only a
vertical slit
is available, no goat pupils, sorry). If set to 0 (the default), a normal round pupil is used. Larger
numbers (up to irisRadius ) make a taller/thinner pupil. This number sets the height. You’ll probably want an
in-between value…maybe irisRadius:80 (160 pixels round) and slitPupilRadius:60 (120 pixels tall) to start.
Note that using
slitPupilRadius
makes the program a bit slower to initialize …you’ll just see blank screens
for several seconds while it works. This is normal and just an unfortunate math thing.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 33 of 76
Colors and Textures
The texture map images for iris and sclera are specified with irisTexture and scleraTexture :
"irisTexture" : "hazel/iris.bmp",
"scleraTexture" : "hazel/sclera.bmp",
If you prefer a solid color to an image, omit those lines and instead use irisColor and/or scleraColor , with
color specified as three values [red, green,blue] in brackets:
"scleraColor" : [ 255, 255, 255 ],
Colors can either be three integers in the range 0 to 255 (like most folks are used to) or three floating-
point values from 0.0 to 1.0 (same idea, just different scale).
Solid colors save a TON of space compared to texture maps, if your design can get away with it.
A few more items have configurable colors:
"pupilColor" : [ 0, 0, 0 ],
"backColor" : [ 140, 40, 20 ],
pupilColor is self-explanatory…like if you want glowing red or white pupils or something.
backColor covers the outermost/backmost part of the eye where the sclera texture map (or color) doesn’t
reach. With a little planning, this and your sclera texture map can be designed to blend together…
otherwise you’ll see a conspicuous crescent of backColor when the eye is looking off to a side.
The eyelid (and background) color is also configurable, but it’s not a normal RGB color . Instead,
use eyelidIndex and an 8-bit value:
"eyelidIndex" : "0x00",
Notice the hexadecimal value must be quoted. The value corresponds to one of the colors in this palette:
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 34 of 76
DMA N0 OURCE-INCHEMEN'I' COLORS
eyelidIndex doesn’t use a normal RGB value because the code is using an optimization trick here, which
limits the available colors in this one area. The default eyelidIndex if unspecified is “0x00” — black.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 35 of 76
/ Texture Map Angle @@@ 0.0 0.25 0.75 or -0.75 or0 -0.5 or -0.25 Right eye default Left eye default
Distinct Left/Right Eyes
Colors/textures can be independent on the left and right eyes. Notice in the config file there’s these two
empty sections:
"left" : {
},
"right" : {
}
Between each item’s curly braces, independent irisTexture , scleraTexture , irisColor , scleraColor ,
pupilColor and backColor can be specified, which will override anything set outside of these.
It was mentioned earlier that the left eye’s textures are rotated 180° so it’s less obvious that the images are
being re-used. If you need to override this, so both eyes have aligned textures, the irisAngle and
scleraAngle settings can be used (either globally or in the left /right sections).
irisAngle and scleraAngle are a rotation offset in the clockwise direction, using either normalized floating
point where 0.0=seam at top, 0.25=seam at right, 0.5=bottom, 0.75=left, and 1.0=back to top. You can also
use integer units from 0 to 1024 (0=top, 256=right and so forth). Negative values are accepted for both the
floating-point and integer modes, in which case the angle will be counter-clockwise.
irisSpin and scleraSpin can be used to make the texture maps revolve around the pupil, which might be
handy for certain fun effects (spiral hypno-eyes, cyborg stuff, etc.). These are specified in RPM, with
positive values being clockwise. So for example, setting irisSpin to -60 will make the iris rotate counter-
clockwise once per second. These can be specified globally or on a left/right basis.
There’s also irisMirror and scleraMirror settings (specify as true or false, or 1 or 0 — default setting is false),
which flip the way the texture is wrapped (clockwise default vs counterclockwise override). If mirroring on
just one eye, you might want to set the corresponding irisAngle or scleraAngle value to 0 depending on
what you’re after.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 36 of 76
Texture Mirroring false true default
Screen orientation is specified with the rotate keyword, with a value from 0 to 3 (default is 3). This can be
helpful if you’ve split your MONSTER M4SK in two. Sometimes the mask-halves will fit into a project better
if they’re each turned 90 degrees, and this setting compensates so the eyes are right-side-up again. You
can put separate rotate values in the left and right sections…try 0 and 2 (or 2 and 0, depending which
way the eyes are turned).
None of this left /right stuff applies on the HalloWing M4, which only has one eye. Having these
sections
won’t
cause the config load to fail, it just ignores anything eye-specific.
The following are
NOT
left/right configurable: eyeRadius , irisRadius and slitPupilRadius (these affect how
certain tables are calculated and there isn’t enough RAM to have independent left and right tables).
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 37 of 76
tra
Eyelids
The eyelid graphics format is explained on the “Preparing Graphics” page. These are 1-bit BMPs, 240
pixels square. Use the upperEyelid and lowerEyelid settings to specify the filenames of these images.
Eyelids are one of those global (not configurable per-eye) things. The design of the eyelid graphics might
be symmetrical or asymmetrical…some eye designs might provide two sets of eyelid images, one for a
single-eye device (like HalloWing M4) and another for the Monster M4SK, where the left and right eyelid
shapes are mirrored.
If you want no eyelids at all, just leave out any upperEyelid or lowerEyelid filenames. You’ll then have a
circular unblinking eye…looks good for skulls!
With eyelids enabled, normally the upper lid “tracks” the movement of the pupil (when the eye looks down,
the eyelid follows with it). This is something that eyes do in real life…but some folks think it looks sleepy, or
just want a particular caffeinated look. Use the tracking keyword with a value of false to disable the eyelid
tracking and maintain wide-open eyes.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 38 of 76
Light Sensor
The pupils normally do some dilation movement on their own…but you can have them respond to light if
you like! Use the lightSensor keyword along with a pin number where the light sensor is connected. If it’s
on a Seesaw interface chip (e.g. on MONSTER M4SK), add 100 to the pin number. For example, on
MONSTER M4SK the built-in light sensor is:
"lightSensor" : 102
And for HalloWing M4, use:
"lightSensor" : 21
(Add a trailing comma if this appears mid-file.)
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 39 of 76
O MONSTER MASK board (https://adafru.il/FLO] I PDM microghone :l/adafrth/FNR] and JST SH cable (hupsWadafrth/FNS) a You can test hones...but for portable or costume use, you'll want a be amplified sp male/male 3.5mm audio cable (https://adafru.il/ch). 50 box speake be -worn sgeaker from Monogrice See the link below
Voice Changer
This used to be a separate program…it now works together with the eyes! This requires the following:
MONSTER M4SK board (https://adafru.it/FLO)
PDM microphone (https://adafru.it/FNR) and JST SH cable (https://adafru.it/FNS)
You can test with headphonesbut for portable or costume use, youll want a battery-operated
amplified speaker and a male/male 3.5mm audio cable (https://adafru.it/yNc). Some Bluetooth boom
box speakers include an aux input jack, or I’ve used this belt-worn speaker from
Monoprice (https://adafru.it/FNT) with some success (see notes below).
Usage
The PDM microphone connects using a tiny 4-pin cable to the “PDM MIC” port on MONSTER M4SK — it’s
near the reset button. You can optionally fashion a
pop filter
over the mic using a little fabric or foam, it’ll
probably sound better.
Connect an audio cable from MONSTER M4SK headphone jack to the aux input on the powered speaker.
The voice changer is off by default! It saps a fair bit of compute cycles (anywhere from about 25 to 50
percent…with a corresponding drop in eye animation frame rates) so you’ll have to turn this on only if you
really want it. To do so, you'll add a line to the config.eye JSON file on the root level of your MONSTER
M4SK. Use:
"voice" : true
to enable the voice changer. See the link below (https://adafru.it/FSh) for an example config file that's
been set up with voice changer parameters.
Add a trailing comma if it’s not the last line.
There are three buttons along the top edge of the monster’s left eye. Tapping the inner button (the one
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 40 of 76
closest to the nose) raises the pitch by 5%. Tapping the outer button (near the corner) lowers the pitch by
5%. Tapping the middle button resets the pitch to its default.
The default pitch is set with the pitch keyword. This is a floating-point value, where 1.0 is normal (voice is
passed straight through, no change), 2.0 will double the frequency (raising the voice by one octave), 0.5
will halve the frequency (lowering by one octave).
pitch can be from 0.4 to 4.0…but the actual usable range where you can still understand things is a bit
narrower, perhaps 0.6 to 2.0…you’ll want to experiment a bit to find a setting that achieves the desired
effect with your own voice.
Microphone gain (sensitivity) is set with the gain keyword. If installed in a mask and you need to adjust the
microphone to compensate for its placement relative to your mouth, use this with a floating-point value
where 1.0 is “normal” sensitivity, 0.5 is quieter by half, 2.0 is double the loudness and so forth. There are
limits to what can be done here, you may want to experiment a bit with this setting and the volume of an
external amplified speaker.
Don’t shout! Speak in a normal to soft voice , let the speaker take care of amplification. This helps the
“weird” voice be heard over your own.
Similarlyspeak at your normal voice pitch and let the voice changer do its thing. You don’t need to make
a funny voice.
Need a Dalek voice effect? With the voice changer enabled as described above, also add "waveform" :
"sine" to enable this effect, which applies a 30 Hz sine wave modulation to the pitch-adjusted voice —
same as used for the original
Dr Who
Daleks. You can try other waveforms ( "square" , "sine" , "tri" and
"saw" are all supported) and other modulation frequencies ( "modulate" : 100 for a 100 Hz modulation wave)
…but, to be perfectly honest…this all turned out a bit disappointing, the feature is only left in there because
the 30 Hz Dalek modulation was spot-on. With some experimentation with different pitch and modulation
settings you might also get a passable “Chicken, fight like a robot!” voice from
Berzerk,
if anyone even
remembers that one.
Example Config.eye File
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 41 of 76
{
// Doom-spiral eyes with voice changer
"voice" : true, //Turns on voice changer
"waveform" : "sine" , //Modulates voice with sine wave
"modulate" : 55 , //Modulation wave freq. in Hz
"eyeRadius" : 125,
"eyelidIndex" : "0x00", // From table: learn.adafruit.com/assets/61921
"irisRadius" : 125, // Iris = whole eye!
"pupilMin" : 0, // Pupil is always 0 size
"pupilMax" : 0,
"pupilColor" : [ 255, 255, 169 ], // Shouldn't show, but just in case
"scleraColor" : [ 255, 0, 0 ],
"backColor" : [ 255, 0, 0 ],
"irisTexture" : "doom-spiral/spiral.bmp",
// The doom-red and doom-spiral eyelid bitmaps don't fully close.
// This is to give the IMPRESSION of a blink without actually blinking,
// so human eye behind is hidden better when doing Pepper's ghost trick.
"upperEyelid" : "doom-spiral/upper.bmp",
"lowerEyelid" : "doom-spiral/lower.bmp",
"left" : {
"irisSpin" : 80 // Rotate iris @ 80 RPM
},
"right" : {
"irisMirror" : true, // Flip spiral image
"irisSpin" : 70 // Slightly different speed for weirdness
}
}
Tips for using the Monoprice 5-Watt Guitar Amplifier
I have a love/hate thing with this speaker. On the plus side: it’s pretty inexpensive, is rechargeable, and is
slim(ish) and clips to one’s belt or a lanyard, making it handy for costume use.
It’s really designed for guitar use and MP3 playback (from microSD card) and there’s some hoops
necessary to get it to pass through audio undistorted…
Connect MONSTER M4SK to the AUX phono jack (center of three),
not
the MIC input.
After powering on, wait a moment and then press the “ M” button to pass through audio.
You can see in the photo that I’ve labeled mine and highlighted the correct jack and button…I use it
infrequently and forget this ritual (also helps when others are borrowing it).
This is not an Adafruit product and we do not provide support. Please check with Monoprice if you
encounter trouble.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 42 of 76
Building Eyes from Source Code
The next couple of pages explain how to set up the Arduino software to work with the SAMD
microcontroller boards like the HalloWing M4 or MONSTER M4SK. If you’ve previously worked with
Adafruit SAMD boards with Arduino, that part’s already set up and you can skip ahead to the “Libraries
and Settings” page.
In summary: use the latest Arduino IDE, install the latest Adafruit SAMD boards package, install Windows
drivers if necessary, and install all the library dependencies for this project…
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 43 of 76
https://adafru.iUf1P @ Blink| Arduino 1.31 If [an sham Tools Hllp New cm. N 0pm... cm‘o 0pm Rxent Sketchbook Emupls cum cnuw I Save ChI~S Save As." 01leth ' Page Sflup cnl‘snmw pm cm 1) Pvdevenczs Ctyl~CommI Qun <3"va>
Arduino IDE Setup
The first thing you will need to do is to download the latest release of the Arduino IDE. You will need to be
using version 1.8 or higher for this guide
https://adafru.it/f1P
After you have downloaded and installed the latest version of Arduino IDE , you will need to start the
IDE and navigate to the Preferences menu. You can access it from the File menu in
Windows
or
Linux
, or
the Arduino menu on
OS X
.
A dialog will pop up just like the one shown below.
https://adafru.it/f1P
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 44 of 76
I I lemncu Sketchbonk lumlan Insets/Kodd/Documems/Avdulnn Blowse Edlmr language. Sysmn Delault : lmqulves mun eumumo) Edllor rem slu’ m (requlles resun olAraulno) shuw verbose auwm durlng compllaKlorl unload Compile! wamlrlgs None A Display Ilnn numbers ./ «My code .lm upland Use ummil mum J Check 6w uvdmcs on stanun -/ Update skelzh mu m new extznslnn on me ( pde 7) may ~/ me when verlfylng or upluamng meySeuingS semvmrm Ponmrm 3mm Sewev:(NTr>Sl PorHHTrPS)’ 34a; Usemame Password' Addltlnnal mam; MznagerURls | MW nlvle pmvs (ml ll» pawl (mull m ,lle ll 9 films/maulLibvary/Ardulnels/pmferences.m lam ollv w'len Aldullm l5 not lulmlnq) 0K Cincal To find the most thlrd 9am board URLs on the Arduino IDE wiki Y
We will be adding a URL to the new Additional Boards Manager URLs option. The list of URLs is comma
separated, and
you will only have to add each URL once.
New Adafruit boards and updates to existing
boards will automatically be picked up by the Board Manager each time it is opened. The URLs point to
index files that the Board Manager uses to build the list of available & installed boards.
To find the most up to date list of URLs you can add, you can visit the list of third party board URLs on the
Arduino IDE wiki (https://adafru.it/f7U). We will only need to add one URL to the IDE in this example, but
you can add multiple URLS by separating them with commas
. Copy and paste the link below into
the Additional Boards Manager URLs option in the Arduino IDE preferences.
https://adafruit.github.io/arduino-board-index/package_adafruit_index.json
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 45 of 76
mam-«m1 El Wk MWJM) mmmmdnq: Mun-darn. mum nus-m "nv Drawn...” Emmflfin Emmfimw Emma“: Emhmflflsmm Ekahhmm—mwmflfltvn} Emmm. mmmwm Mme Dvefevenres (an be Emma uhflmmummmm (edmr‘v MenArcmnn \s rutunnnfl) udes suppon for F 55, Gemma M0 a DI-USB - This a arcore gr ' ct
Here's a short description of each of the Adafruit supplied packages that will be available in the Board
Manager when you add the URL:
Adafruit AVR Boards - Includes support for Flora, Gemma, Feather 32u4, ItsyBitsy 32u4, Trinket, &
Trinket Pro.
Adafruit SAMD Boards - Includes support for Feather M0 and M4, Metro M0 and M4, ItsyBitsy M0 and
M4, Circuit Playground Express, Gemma M0 and Trinket M0
Arduino Leonardo & Micro MIDI-USB - This adds MIDI over USB support for the Flora, Feather 32u4,
Micro and Leonardo using the arcore project (https://adafru.it/eSI).
If you have multiple boards you want to support, say ESP8266 and Adafruit, have both URLs in the text
box separated by a comma (,)
Once done click OK to save the new preference settings. Next we will look at installing boards with the
Board Manager.
Now continue to the next step to actually install the board support package!
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 46 of 76
Am ram Armin sham Fix (Media; a Mom Suhl Mmihnl Bum "Alduinn/Gumim "no“ Pm Progrlmmu: "USBfivvylSP' Bum mum Bonds mugs Alduma mm mm; Ardmno van Mumu/Gflwino Hm Autumn Dumlllnwe m Died-lull
Using with Arduino IDE
The Feather/Metro/Gemma/QTPy/Trinket M0 and M4 use an ATSAMD21 or ATSAMD51 chip, and you can
pretty easily get it working with the Arduino IDE. Most libraries (including the popular ones like NeoPixels
and display) will work with the M0 and M4, especially devices & sensors that use I2C or SPI.
Now that you have added the appropriate URLs to the Arduino IDE preferences in the previous page, you
can open the Boards Manager by navigating to the Tools->Board menu.
Once the Board Manager opens, click on the category drop down menu on the top left hand side of the
window and select All. You will then be able to select and install the boards supplied by the URLs added to
the preferences.
Install SAMD Support
First up, install the latest Arduino SAMD Boards ( version 1.6.11 or later)
You can type Arduino SAMD in the top search bar, then when you see the entry, click Install
Remember you need SETUP the Arduino IDE to support our board packages - see the previous
page on how to add adafruit's URL to the preferences
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 47 of 76
“up. .Hvukwm,, uh sun—4, 011:, m WM?) 5, m.— mg." m: “mum and: “Ma in W mbgm m...» Due. mum mm min um... mum (ax-ans .— my I, m Ms mm: m ms unloge Mummy.“ 2., an». M2 mum WE v] atmwm, am at“ m u.‘ Mm mama“. “WWW um um“ n.4,... um m... a.“ u...“ um mm mm: mm, mm), M...“ mum. swan»: ms), Man... ”Emmy/.6“, mm, m"... warm-m mm, (mm. mm. 17mm 5...; mm. 17mm 15m. m m mum mum, m...“ mm, mm .m “mm, m m I." mum. onl‘ne MIR u. p.
Install Adafruit SAMD
Next you can install the Adafruit SAMD package to add the board file definitions
Make sure you have Type All selected to the left of the
Filter your search...
box
You can type Adafruit SAMD in the top search bar, then when you see the entry, click Install
Even though in theory you don't need to - I recommend rebooting the IDE
Quit and reopen the Arduino IDE to ensure that all of the boards are properly installed. You should now be
able to select and upload to the new boards listed in the Tools->Board menu.
Select the matching board, the current options are:
Feather M0 (for use with any Feather M0 other than the Express)
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 48 of 76
coo-cc... 00......000000 m an item m: My lithium-at am my.“ am a: Enwdnga a...“ Smll mm umsnitm Saul m... cumsnlm H “Hm Mm: amytumm // a,” mu, 1/ “mm, m, “Mum-mm swam um mammmn Pmlmmln 'usannylw' Bum mummy “a.“ my» so ,1 2:: Hum: mu (Mme: u mm x: // scum Amman u mmmm 1: .11 comma) Erbvnt mm a! a mm: 1 mm, . mmwn (327nm «mum m andKunuthDEnivds Adalmxkaxhuw “imam... w [W “-1..an m1 Em Adan-Kiwi bum-m We) Ann-mam» w MIMI-um m “awn/am, m Addnnfllky “mm-m m (swam
Feather M0 Express
Metro M0 Express
Circuit Playground Express
Gemma M0
Trinket M0
QT Py M0
ItsyBitsy M0
Hallowing M0
Crickit M0 (this is for direct programming of the Crickit, which is probably not what you want! For
advanced hacking only)
Metro M4 Express
Grand Central M4 Express
ItsyBitsy M4 Express
Feather M4 Express
Trellis M4 Express
PyPortal M4
PyPortal M4 Titano
PyBadge M4 Express
Metro M4 Airlift Lite
PyGamer M4 Express
MONSTER M4SK
Hallowing M4
MatrixPortal M4
BLM Badge
Install Drivers (Windows 7 & 8 Only)
When you plug in the board, you'll need to possibly install a driver
Click below to download our Driver Installer
https://adafru.it/EC0
https://adafru.it/EC0
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 49 of 76
rowing ammmsn: II Vouhlvldmfinnpufl Hum-1am Mid-i: Riv-yawn!) am W/ng-WJW Wmflywliztnmlflsfle’l fimnmmmfismmn- fig“ hm lite “mm! m Mifnflhid mflwwdmikmhdfilw is pmgram will allow van to inshll wmm drives for human: Adlfruit Indusuies pmduces. Please support U Adafluit by pumhasiru hardware from: mywmmimllmmfluildiledmbyufiu Mummemsopfimhcmumuookm mmmm-mmmn). Mummmmmmflkhm. admin mum (an! mm» In;
Download and run the installer
Run the installer! Since we bundle the SiLabs and FTDI drivers as well, you'll need to click through the
license
Select which drivers you want to install, the defaults will set you up with just about every Adafruit board!
Click Install to do the installin'
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 50 of 76
cancer NuHsnft Instau Sv/smm a up; : am o W!)- IMuim w vnxd :eumH // pm: yuux » mud Joann l // put wux
Blink
Now you can upload your first blink sketch!
Plug in the M0 or M4 board, and wait for it to be recognized by the OS (just takes a few seconds). It will
create a serial/COM port, you can now select it from the drop-down, it'll even be 'indicated' as
Trinket/Gemma/Metro/Feather/ItsyBitsy/Trellis!
Please note, the QT Py and Trellis M4 Express are two of our very few boards that does not have an
onboard pin 13 LED so you can follow this section to practice uploading but you wont see an LED blink!
Now load up the Blink example
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 51 of 76
\Dnne upluamnu use PM) .. coma
// the setup function runs once when you press reset or power the board
void setup() {
// initialize digital pin 13 as an output.
pinMode(13, OUTPUT);
}
// the loop function runs over and over again forever
void loop() {
digitalWrite(13, HIGH); // turn the LED on (HIGH is the voltage level)
delay(1000); // wait for a second
digitalWrite(13, LOW); // turn the LED off by making the voltage LOW
delay(1000); // wait for a second
}
And click upload! That's it, you will be able to see the LED blink rate change as you adapt the delay() calls.
Successful Upload
If you have a successful upload, you'll get a bunch of red text that tells you that the device was found and
it was programmed, verified & reset
After uploading, you may see a message saying "Disk Not Ejected Properly" about the ...BOOT drive. You
can ignore that message: it's an artifact of how the bootloader and uploading work.
If you are having issues, make sure you selected the matching Board in the menu that matches
the hardware you have in your hand.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 52 of 76
mm mow m m: [411 Shaun mummy; ’ ,/ n. qr ~ \chd "m // rm pnNCd ( ,/ m m ma ,mm mmmlfln mnm; a liyuflnil: Hdp Alla mm mm AKIMSkrkh Ex [an93 mm 5m: Mum. cwsmm P W“ Emmi “Mam-m Fun»:- m (Maw. usll yum » Purl - Swa‘ m, pmgmm “um",xsw . CW“ cowl Rumllnmlnadu comm (Wymranhu WIN-my: use mu 13, 1mm: r. m m u.) m mum m: um, , r. ”3,: x): 3 Juan) r. m m u.) m m mun) ue 'Iucaaé W
Compilation Issues
If you get an alert that looks like
Cannot run program "{runtime.tools.arm-none-eabi-gcc.path}\bin\arm-non-eabi-g++"
Make sure you have installed the Arduino SAMD boards package, you need
both
Arduino & Adafruit
SAMD board packages
Manually bootloading
If you ever get in a 'weird' spot with the bootloader, or you have uploaded code that crashes and doesn't
auto-reboot into the bootloader, click the RST button twice (like a double-click)to get back into the
bootloader.
The red LED will pulse and/or RGB LED will be green, so you know that its in bootloader mode.
Once it is in bootloader mode, you can select the newly created COM/Serial port and re-try uploading.
You may need to go back and reselect the 'normal' USB serial port next time you want to use the normal
upload.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 53 of 76
Follow the steps for installma Adafruit's udev rules on this Daqe.
Ubuntu & Linux Issue Fix
Follow the steps for installing Adafruit's udev rules on this page. (https://adafru.it/iOE)
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 54 of 76
oucoolcoolcoolcool the Adafruil Learning System Guides M4 Eyes ht‘lps://adafru.it/FAD
Source, Libraries and Settings
At this point you should be able to upload code (such as the “Blink” sketch) to the board, the basics are
confirmed working. If not, work though the prior two pages.
Source Code
Source code for this project is found in the Adafruit_Learning_System_Guides (https://adafru.it/Clx)
repository on Github, specifically in the M4_Eyes (https://adafru.it/FAD) subdirectory. Here’s a direct
download link:
https://adafru.it/FAD
Libraries
The following libraries are used by the eye code (or are referenced indirectly by libraries used). These can
be installed through the Arduino Library Manager (SketchInclude LibraryManage Libraries…)
Adafruit_Arcada
Adafruit_GFX
Adafruit_BusIO
Adafruit_ImageReader
Adafruit_LIS3DH
Adafruit_MSA301
Adafruit_NeoPixel
Adafruit_Seesaw
Adafruit_Sensor (
Adafruit Unified Sensor
in Library Manager)
Adafruit_SPIFlash
Adafruit_ST7789
Adafruit_TinyUSB
Adafruit_TouchScreen
Adafruit_ZeroDMA (
Adafruit Zero DMA
in Library Manager)
Adafruit_ZeroPDM (
Adafruit Zero PDM
in Library Manager)
Adafruit_ZeroTimer
ArduinoJson (
not
Arduino_JSON)
SdFat - Adafruit fork (
not
the standard SdFat fork)
Recent versions of the Arduino IDE install dependent automatically, so installing
Adafruit_Arcada
should
cover most if not all of this.
https://adafru.it/FAD
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 55 of 76
Additionally, depending on which of the “user” code tabs is active, you might need:
Adafruit_AMG88xx (used by user_watch.cpp)
Project Settings
ToolsCPU Speed180 MHz (overclock)
(200 MHz is a bit too much for some boards and may lock
up, but you can give it a try. We use 180 MHz for our prepackaged .UF2 files since it’s likely to work
on more boards in the wild.)
ToolsOptimizeFaster (-O3)
(do not use higher settings for this code, it may corrupt the flash
filesystem requiring a complete wipe)
ToolsUSB StackTinyUSB
(the code
will not compile
without this selected!)
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 56 of 76
Visit the CircuitPflhon download gage MONSTER M45 Download two updater UF2 Connect boa reset button HALLOM4B Drag the b0 rive. That d software w ‘s finished. Drag the drive. That drive will go away and is re seconds hould see some text on the board’s d Reload e drive, either one of the ready-made designs kup of your customized file as explained on this gage
Troubleshooting
Board Unresponsive; Flashing Red LED
There is an
extremely small but nonzero
chance of a glitch that wipes the board’s flash filesystem. No
eyes, just a flashing red LED. We’ve yet to track down the source of this bug. Fortunately it’s pretty rare,
and usually just when loading a new design.
If this happens with your board, you’ll need to completely wipe and reinstate the flash filesystem. Any files
on your board are lost … it’s strongly recommended to maintain a backup of any customized files.
To recover from this situation:
1. Visit the CircuitPython download page (https://adafru.it/Em8) and search for your board — either
MONSTER M4SK or HalloWing M4 (
not
M0).
2. Download
two
files there: a CircuitPython “UF2” installer (current stable release), and bootloader
updater UF2 (further down on the same page).
3. Connect board to computer with USB cable, set switch to “ onposition, and double-tap the board’s
reset button. After a few seconds, you should see a small flash drive called MASKM4BOOT or
HALLOM4BOOT.
4. Drag the bootloader UF2 file to the boot drive. That drive will go away for about 10 seconds while the
software works, and then reappear once its finished.
5. Drag the CircuitPython UF2 file to the boot drive. That drive will go away and is replaced in a few
seconds with one called CIRCUITPY. You should see some text on the boards display now.
6. Reload eye graphics files to the CIRCUITPY drive, either one of the ready-made
designs (https://adafru.it/FVx), or from a backup of your customized files.
7. Download and install the M4 EYES firmware as explained on this page (https://adafru.it/G8d). This is
another double-tap-drag-UF2 sequence, like we did above.
Everything on your board should be factory fresh now.
Ol’ Blue Eyes
If the eyes
used
to work but after editing have reverted to flat-colored blue irises, that’s almost always a
JSON syntax error…usually a missing or extra comma. The “Customization Basics” page has more tips for
ensuring proper syntax.
Crossed Eyes
Occasionally the eyes might go crossed and stay that way. The software thinks the “nose booper” is being
held and this is its attempt at being funny.
This false booping can happen when the battery is running low and its voltage starts to drop.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 57 of 76
ht‘lps://adafru.it/FU E ht‘lps://adafru.it/FU F
Occasionally though…it just gets a false reading, maybe due to gradual changes in temperature, humidity
or other unknown factors. Tap the reset button (or toggle power off and on) and this should clear up…the
booper calibrates it’s un-booped state on start-up.
Technicolor Snow
If you see one or more of your texture maps show up as multicolored snow/noise, it may be an indication
that you've run out of texture memory and will need to reduce the file size of some of your maps.
If the
entire screen
is snow, it usually means you’ve run out of RAM, and the most likely culprit there is the
eyeRadius setting. Larger eyes require geometrically more RAM. Dial it back until everything fits.
Erase the Filesystem
If your board has a filesystem problem that’s not fixed by the troubleshooting steps up top, you can try a
more thorough QSPI flash initialization. Download the UF2 file linked below, then plug in your M4SK and
double-click the reset button. You'll see a M4SKM4BOOT drive show up on your computer. Drag the
M4SK_QSPI_Eraser.UF2 onto that drive. After a few moments, the board's drive will disconnect. Double-
click reset to put the board back into bootloader mode. Then follow the CircuitPython, graphics and eye
firmware steps above.
https://adafru.it/FUE
Diagnostics
Want to see some stats on your M4SK? Double-click the board's reset button to get to bootloader mode,
then drag the M4SK_Diagnostics.UF2 onto the M4SKM4BOOT drive!
https://adafru.it/FUF
https://adafru.it/FUE
https://adafru.it/FUF
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 58 of 76
Here‘s for Ias plastic glass ht‘lps://adafru.il/FBS
Lens Holders
Lens Holders
Heres an Adobe Illustrator file for laser-cut 1/8" thick (3mm) acrylic that provides frames for two
plastic (https://adafru.it/FB4) or glass (https://adafru.it/CBn) lenses:
https://adafru.it/FB5
Each frame is held in place with three M3 x ~12-14mm screws. Slots are provided for a 3/4" (20mm) elastic
strap. This can be worn around a hat or the forehead of a mask. Not worn over your own eyes please …it
blocks your vision and might scratch your eyes!
https://adafru.it/FB5
The screws that come with the lens holder kit might be a little under 12mm, but they'll still fit -
gently press on the lens to squish the foam as you install each hex nut at a time and dont go
beyond finger-tightening.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 59 of 76
A last-minute change added foam tape to secure the
screens. The additional thickness meant that the “12mm-
ish” screws won’t always make a solid connection. Here’s
what to do…
Remove the plastic screen protector if you haven’t
already. Make sure the screen and back of the lens
are clean. Align the lens holder over this.
Insert a screw, then apply firm and even pressure
on the lens against the screen. With
pressure distributed across the whole screen like
this (using the lens), it won’t break.
It should be possible to push through just enough
threads for the nut to catch.
Repeat with other screws. Once they’re all caught,
move between the three screws giving each 1/4 to
1/2 turn at a time. The foam turns out to be quite
compressible and it should be possible to get the
tips of the screws flush with the face of the nuts.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 60 of 76
You can skip the lenses and just use the frames for the strap if that’s all you need. Regardless, don’t make
the strap
too
snugthe board
is
designed to be split in two, and we don’t want that happening
unintentionally.
There is an optional extra nose bridge piece. If you have split your MONSTER M4SK apart and want to use
it in its original shape again, this piece holds the frames at their original spacing. An optional 9-pin JST
cable must link the two boards, you’ll need some different length M3 screws, and you will not get the
boopable nose feature back.
3D Printed Options
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 61 of 76
We also have a nice 3D-printable MONSTER M4SK
case (https://adafru.it/FNy) — or use just the lens holder
rings if that’s the only part you need.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 62 of 76
Enabling Configurable Settings — oice Changer
Voice Changer
The voice changer is no longer a standalone program…it’s been merged in with the eye code and runs at
the same time now!
Enabling and customizing the voice changer are now documented on the Configurable Settings Voice
Changer (https://adafru.it/FSh) page.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 63 of 76
Pinouts
Displays and Display Connectors
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 64 of 76
On the front are two 240x240 IPS TFTs.
They are ST7789V chipset displays, with 240x240 pixels
and backlight control. Each has an individual unshared SPI
bus so we can DMA-blast pixels out as fast as possible.
The TFT displays are connected to the M4SK using
display connectors located on the back of the board. The
ribbon cables for the displays fit through a slot in the
center of each side of the M4SK.
Microcontrollers and Flash
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 65 of 76
The main processor chip is the ATSAMD51G19 Cortex M4
microcontroller running at 120MHz with 512KB Flash, and
192KB RAM.
Towards the center left on the right side, next to the
microcontroller, is 8 MB QSPI flash for storing graphics
and sound effects.
Towards the top center of the left side is the seesaw chip.
This chip handles the tactile buttons and the light sensor.
You can read the data from them using the I2C seesaw
library and the pins specified. This is what lets us have
only 9 wires to bridge the two halves of the PCB
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 66 of 76
Power Switch and Ports
There is one USB port on the board.
On the top of the right side is a USB Micro port, which is
used for powering and programming the board.
You can also power your MONSTER M4SK by plugging in
a 3.7/4.2V Lipoly battery into the JST 2-PH battery port
found in the center of the right side. You can then
recharge the battery over the Micro USB jack. When
charging, the CHG LED will light up.
It's normal for the yellow CHG LED to flicker when no
battery is in place, that's the charge circuitry trying to
detect whether a battery is there or not. If you are
powering only over USB, you can cover it with tape
In the upper right corner on the right side is the power
switch. You can power off the board when you're not
using it to conserve power.
Audio
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 67 of 76
There is a stereo headphone jack on the top of the right
side. This is connected to the two analog DAC pins on the
SAMD51 - A0 and A1
There is a mono speaker driver for smaller 8 ohm 1W
speakers. Add a speaker using the Molex
PicoBlade (https://adafru.it/C8p) speaker connector
located on the right side of the board towards the top. The
speaker is connected to the A0 analog DAC, and can be
enabled/disabled using the SPEAKER ENABLE pin (pin 20)
At the bottom on the right side is a 4 pin JST SH port for
connecting an optional PDM microphone. Note that the
PDM microphone is connected to two SERCOM pins, and
we use SPI2 to read PDM data (if you think about it, PDM
is just fixed-frequency SPI!) You
could
in theory turn this
into an I2C or UART port. The SAMD51G19 chip used on
this board does not support I2S, so we can't use I2S to
read the PDM data.
Capacitive Touch Pad and Buttons
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 68 of 76
Front and center, is a capacitive touch pad nose this is
connected to D2. It's not a
great
capacitive touch input,
because of the zener diode on D2's protection circuitry,
but it can detect presses with some startup-calibration.
Use as an input.
On the left side are three tactile buttons for user
interfacing. They are connected to the seesaw chip on
pins 9, 10, 11. You need to use the seesaw library to
enable the pull-ups on all three and read the buttons (they
will be connected to ground when pressed)
Sensors
There is an LIS3DH 3-axis accelerometer, on the right
side near the bottom towards the middle, connected to
the I2C pins for detection motion, tilt or taps.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 69 of 76
On the left side is a light sensor. It's connected to the
seesaw chip on pin 1. Read the analog value using the
seesaw library. Lower values like 50 mean its dark. Higher
values like 1000 means its bright. It's reverse mount so
you can read light levels from the front on the right side of
the M4SK.
I2C Connector
There is a 4-pin JST I2C connector in the center on the
left, that is STEMMA and Grove compatible. The I2C
connection is shared with the seesaw chip and the
accelerometer.
The I2C connector defaults to 5V. There is a jumper
located immediately to the right of the connector that you
can cut or solder to change it between 5V and 3V.
Digital/Analog Connectors
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 70 of 76
On the right and left sides, towards the bottom, are two
connectors labeled D2 and D3. These are 3-pin JST
digital or analog connectors for sensors or NeoPixels.
These pins can be analog inputs or digital I/O.
They have protection 1K resistors + 3.6V zener diodes so
you can drive an LED directly from the output. Connect to
them via board.D2 and board.D3 or Arduino 2 and 3.
For analog reading in Arduino use A2 for D2 and A3 for
D3.
Reset Button
The reset button is located on the bottom of the right
side.
Click it once to re-start your firmware. Click twice to enter
bootloader mode.
LED
On the top of the right side, next to the USB connector, is
a little red LED tied to pin D13. You can control it in your
code. It pulses when the board is in bootloader mode.
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 71 of 76
SECTION TITLE HERE
Located on the inside edge of each side is a 9-pin JST SH
connector. This connector works with a 9-pin cable and
allows you to break the board apart along the perforation,
and mount the two halves of the board separately from
each other!
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 72 of 76
Product gage with datasheel for ATSAMD51J19 EagleCAD files on GitHub (https://adafru.it/F 3D Models on GitHub (httsz/adafrqu/FNZ) Fritzin ob'ect in the Adafruit Frilzin librar nounm o o \o m. um um MINA v: lino x; mm: mm mm mm mm“ max m n \m 1/3 \
Downloads
Files:
Product page with datasheet for ATSAMD51J19 (https://adafru.it/Bf8)
EagleCAD files on GitHub (https://adafru.it/FTq)
3D Models on GitHub (https://adafru.it/FN2)
Fritzing object in the Adafruit Fritzing library (https://adafru.it/FTr)
Schematic
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 73 of 76
; “mm ficceleromeler Ti 33 «- . a 1&3”??? Jim. 2 “ & "Wh a“? m “" 2° *m;% 1. W nmsrzn msK rev a u/n/xsrxun” final: 24; , mm.“ [Muslims mm; >Aw~m \ Liqh‘ Sensor Dons 2% % nmsvzn msK rev a u/n/xsrxun” yam: 3/; , mm." [Muslims mm: mm: x
Fab Print
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 74 of 76
© Adafruit Industries https://learn.adafruit.com/adafruit-monster-m4sk-eyes Page 75 of 76
© Adafruit Industries Last Updated: 2021-07-23 01:06:39 PM EDT Page 76 of 76