VE_—:
wiik‘lH [LKKIRONIK
Cautions and Warnings:
The following conditions apply to all goods within the product series of Optoelectronic
Components of Würth Elektronik eiSos GmbH & Co. KG:
General:
• This optoelectronic component is designed and manufactured for use in general electronic equipment.
• Würth Elektronik must be asked for written approval (following the PPAP procedure) before incorporating the components into any
equipment in fields such as military, aerospace, aviation, nuclear control, submarine, transportation (automotive control, train control,
ship control), transportation signal, disaster prevention, medical, public information network, etc. where higher safety and reliability are
especially required and/or if there is the possibility of direct damage or human injury.
• Optoelectronic components that will be used in safety-critical or high-reliability applications, should be pre-evaluated by the customer.
• The optoelectronic component is designed and manufactured to be used within the datasheet specified values. If the usage and
operation conditions specified in the datasheet are not met, the component may be damaged or dissolved.
• Do not drop or impact the components, as the optoelectronic component body may flake apart.
• Würth Elektronik products are qualified according to international standards, which are listed in each product reliability report. Würth
Elektronik does not warrant any customer qualified product characteristics beyond Würth Elektroniks’ specifications, for its validity and
sustainability over time.
• The responsibility for the applicability of the customer specific products and use in a particular customer design is always within the
authority of the customer. All technical specifications for standard products also apply to customer specific products.
Product specific:
Soldering:
• The solder profile must comply with the Würth Elektronik technical soldering specification. All other profiles will void the warranty.
• All other soldering methods are at the customers’ own risk.
Cleaning and Washing:
• Washing agents used during the production to clean the customer application might damage or change the characteristics of the
optoelectronic component body, marking or plating. Washing agents may have a negative effect on the long-term functionality of the
product.
• Using a brush during the cleaning process may break the optoelectronic component body. Therefore, we do not recommend using a
brush during the PCB cleaning process.
Potting:
• If the product is potted in the customer application, the potting material may shrink or expand during and after hardening. Shrinking
could lead to an incomplete seal, allowing contaminants into the optoelectronic component body, pins or termination. Expansion could
damage the optoelectronic component body, pins or termination. We recommend a manual inspection after potting to avoid these
effects.
Storage Conditions:
• A storage of Würth Elektronik products for longer than 12 months is not recommended. Within other effects, the terminals may suffer
degradation, resulting in bad solderability. Therefore, all products shall be used within the period of 12 months based on the day of
shipment.
• Do not expose the optoelectronic component to direct sunlight.
• The storage conditions in the original packaging are defined according to DIN EN 61760-2.
• For a moisture sensitive component, the storage condition in the original packaging is defined according to IPC/JEDEC-J-STD-033. It is
also recommended to return the optoelectronic component to the original moisture proof bag and reseal the moisture proof bag again.
Handling:
• Violation of the technical product specifications such as exceeding the nominal rated current, will void the warranty.
• The product design may influence the automatic optical inspection.
• Certain optoelectronic component surfaces consist of soft material. Pressure on the top surface has to be handled carefully to prevent
negative influence to the function and reliability of the optoelectronic components.
• ESD prevention methods need to be applied for manual handling and processing by machinery.
• Resistors for protection are obligatory.
• Luminaires in operation may harm human vision or skin on a photo-biological level. Therefore direct light impact shall be avoided. All
products are additionally certified as risk groups 0 to 2 according to DIN EN 62471:2008.
• In addition to optoelectronic components testing, products incorporating these devices have to comply with the safety precautions given
in IEC 60825-1 and IEC 62471.
Technical specification:
• The typical and/or calculated values of technical parameters can only reflect statistical figures. The actual parameters of each single
product, may differ from the typical and/or calculated values or the typical characteristic line.
• On each reel, only one bin is sorted and taped. The bin is defined on intensity, chromaticity coordinate or wavelength and forward
voltage.
• In order to ensure highest availability, the reel binning of standard deliveries can vary. A single bin cannot be ordered. Please contact us
in advance, if you need a particular bin sorting before placing your order to clarify the lead time, MOQ and pricing.
These cautions and warnings comply with the state of the scientific and technical knowledge and are believed to be accurate and reliable.
However, no responsibility is assumed for inaccuracies or incompleteness.
Würth Elektronik eiSos GmbH & Co. KG
EMC & Inductive Solutions
Max-Eyth-Str. 1
74638 Waldenburg
Germany
Tel. +49 (0) 79 42 945 - 0
www.we-online.com
eiSos@we-online.com
CREATED CHECKED GENERAL TOLERANCE PROJECTION
METHOD
DaSc PLD DIN ISO 2768-1m
DESCRIPTION
WL-SBRW SMT Bi-color Reverse
mount Waterclear ORDER CODE
156125RV73000
SIZE REVISION STATUS DATE (YYYY-MM-DD) BUSINESS UNIT PAGE
1205 001.001 Valid 2018-10-24 eiPal 7/8
This electronic component has been designed and developed for usage in general electronic equipment only. This product is not authorized for use in equipment where a higher safety standard and reliability standard is especially required or where a failure of the product is reasonably expected to cause severe personal injury or death, unless the parties have executed an agreement specifically governing such use. Moreover Würth Elektronik eiSos GmbH
& Co KG products are neither designed nor intended for use in areas such as military, aerospace, aviation, nuclear control, submarine, transportation (automotive control, train control, ship control), transportation signal, disaster prevention, medical, public information network etc.. Würth Elektronik eiSos GmbH & Co KG must be informed about the intent of such usage before the design-in stage. In addition, sufficient reliability evaluation checks for safety
must be performed on every electronic component which is used in electrical circuits that require high safety and reliability functions or performance.