@um
Delta will not guarantee the performance of the products if the application condition falls
A written request should be submitted to Delta prior to approval if deviation from this
Please exercise caution when handling fans. Damage may be caused when pressure is applied
dropped to the
some special designs, there is no guarantee that the products will be free
from any such safety problems or failures as caused by the introduction of powder, droplets of
sentative of some unique examples and viewed as the
It is very important to establish the correct polarity before connecting the fan to the power
be caused to the fans if connection is
according to the storage temperature limits specified. Do not
store fans in a high humidity environment. We highly recommend performance testing is
ck Rotor Protection feature. If you impair the rotation of
the impeller for the fans that do not have this function, the performance of those fans will lead
It is important to consider safety when testing the fans. A suitable fan guard should be fitted to
rried out at relative (ambient) temperature and
F” capacitor to the fan externally when the application calls
Descriptions:
1.
Delta will not guarantee the performance of the products if the application condition falls
outside the parameters set forth in the specification.
2.
A written request should be submitted to Delta prior to approval if deviation from this
specification is required.
3.
Please exercise caution when handling fans. Damage may be caused when pressure is applied
to the impeller, if the fans are handled by the lead wires, or if the fans are hard-
production floor.
4. Except as pertains to s
ome special designs, there is no guarantee that the products will be free
from any such safety problems or failures as caused by the introduction of powder, droplets of
water or encroachment of insect into the hub.
5. The above-mentioned conditions are repre
sentative of some unique examples and viewed as the
first point of reference prior to all other information.
6.
It is very important to establish the correct polarity before connecting the fan to the power
source. Positive (+) and Negative (-). Damage may
be caused to the fans if connection is
with reverse polarity, as there is no foolproof method to protect against such error.
7. Delta fans are not suitable where any corrosive fluids are introduced to their environment.
8. Please ensure all fans are stored ac
cording to the storage temperature limits specified. Do not
store fans in a high humidity environment. We highly recommend performance testing is
conducted before shipping, if the fans have been stored over 6 months.
9. Not all fans are provided with the Lo
ck Rotor Protection feature. If you impair the rotation of
the impeller for the fans that do not have this function, the performance of those fans will lead
to failure.
10. Please be cautious when mounting the fan. Incorrect mounting of fans may cause exces
resonance, vibration and subsequent noise.
11.
It is important to consider safety when testing the fans. A suitable fan guard should be fitted to
the fan to guard against any potential for personal injury.
12. Except where specifically stated, all tests are ca
rried out at relative (ambient) temperature and
humidity conditions of 25oC, 65%. The test value is only for fan performance itself.
13. Be certain to connect an “over 4.7µ
F” capacitor to the fan externally when the application calls
for using multiple fans in parallel, to avoid any unstable power.