AFB0424SHB Spec Datasheet by Delta Electronics

DELTA ELECTRONICS. INC. 252, SHANG YEIG ROAD, KUEI SAN TEL 1 8867 0 373591968 TAOYUAN HSIEN 333, TAIWAN, R. 0. C. FAX : 886— D 3—3591991 SPECIFICATION FOR APPROVAL “HitMurattiiiihbbbbuiiiihbbbbfl Customer: 1. SCOPE: THIS SPECIFICATION DEFINES THE ELECTRICAL AND MECHANICAL CHARACTERISTICS OF THE DC BRUSHLESS AXIAL FLOW FAN. THE FAN MOTOR IS WITH TWO PEASES AND FOUR POLES. 2. CHARACTERS: ITEM DESCRIPTION I RATED VOLTAGE 24 we I I 14.0 — 27.6 vnc I 11000 MINI. (REE) I MAX. AIR FLOW I 0.420 (MIN. 0.375 ) MG/MIN. I I (AT ZERO STATIC PRESSURE) I 14.03 (MIN. 13.35 ) cm I I I ------------------------ --I I I 15.20 (MIN, 12.40 ) mud-120 I I I 0.601 (MIN. 0.488 ) inctho I I -- - - -- - - -I (continued) A00 page: 1
PART NO: 10 MEG OHM MIN AT 500 VDC . (BETWEEN FRAME AND (+) TERMINAL) W,WWWWWWWWRARWTWWWWWWW,,,,,,,,,,,,,,,,,,,,,,,, DIELECTRIC STRENGTH I 5 111A MAX. AT 500 VAC 60 Hz ONE MINUTE, (BETWEEN FRAME AND (+) TERMINAL) I OPEN TYPE I 70,000 HOURS CONTINUOUS OPERATION I AT 40 'C WITH 15 ~ 65 ZRH. LIFE EXPECTANCE ROTATION BLACK WIRE NEGATIVE(—) I RED WIRE POSITIVE(+) I CLOCKWISE VIEW 1 FROM L 1 UL] I .Mfiuflflufiflvgfigurfifiu#Agfipufig. 5 =2" a» r n o E 5:: NOTES: 1. ALL READINGS ARE MEASURED AFTER STABLY WARMING UP THROUGH 10 MINUTES. 2. THE VALUES WRITTEN IN PARENS , ( ), ARE LIMITED SPEC. 3. ACOUSTICAL NOISE IEASURING CONDITION: DC FAN MICROPHONE , <2: air="" flow="" firiiwiigl="" 1m="" noise="" is="" measured="" at="" rated="" voltage="" in="" free="" air="" in="" anechoic="" chamber="" with="" b="" 8:="" k="" sound="" level="" meter="" with="" microphone="" at="" a="" distance="" of="" one="" meter="" from="" the="" fan="" intake.="" a00="" page:="" 2="">
3—1. DIMENSIONS ------------------------------- SEE DIMENSIONS DRAWING 3—2. 7 PLASTIC UL: 94V—D 373. IMPELLER PLASTIC UL: 94H 3-4. BEARING SYSTEM TWO BALL BEARINGS 3—5. WEIGHT ------------------------------------------------- 25.0 GRAMS . ENVIRONMENTAL: 4—1. OPERATING TEMPERATURE - -- —10 T0 +70 DEGREE G 4—2. STORAGE TEMPERATURE ~77 —40 TO +75 DEGREE c 473, OPERATING HUMIDITY 7777777777777777777777777777777 5 T0 90 7. RH 4—4. STORAGE HUMIDITY ---------------------------------- 5 TO 95 7: RH . PROTECTION: 5-1. LOCKED ROTOR PROTECTION IMPEDANCE OF MOTOR WINDING PROTECTS MOTOR FROM FIRE IN 96 HOURS OF LOCKED ROTOR CONDITION AT THE RATED VOLTAGE. 572. POLARITY PROTECTION BE CAPABLE OF WITHSTANDINI} IF REVERSE CONNECTION FOR POSITIVE AND NEGATIVE LEADS. . RE OZONE DEPLETING SUBSTANCES: 6-1. NO CONTAINING PBBS, PBBOS, CFCS, PBHES, PBDPES AND HCFCS. . PRODUCTION LOCATION 7*1. PRODUCTS REL BE PRODUCED IN CHINA 0R THAILAND 0R TAIWAN, A00 page: 3
DELTA MODEL: AEB0424SHB 8. BASIC RELIABILITY REQUIREMENT: 8:1. THERMAL CYCLING 8-2. HUMIDITY EXPOSURE 8-3. VIBRATION 6-4. MECHANICAL SHOCK 8:5. LIFE LOW TEMPERATURE: *40'C HIGH TEMPERATURE: +80'C SOAK TIME: 30 MINUTES TRANSITION TIME < 5="" minutes="" duty="" cycles:="" 5="" temperature:="" +25'c="" ~="" +65°c="" humidity:="" 90-987.="" rh="" ®="" +65°c="" for="" 4="" hours/cycle="" power:="" non—operating="" test="" time:="" isb="" hours="" temperature:="" +25"c="" orientation:="" x,="" y,="" z="" power:="" nonioperating="" vibration="" level:="" overall="" grms="3.2" frequency‘hz)="" psn(c‘2/hz)="" 10="" 0.040="" 20="" 0.100="" 40="" 0.100="" 300="" 0.002="" 1000="" 0.002="" test="" time:="" 2="" hours="" on="" each="" orientation="" temperature:="" +20'c="" orientation:="" x,="" y,="" z="" power:="" nonioperating="" acceleration:="" 2|]="" g="" min.="" puise:="" 11="" ms="" half—sine="" wave="" number="" of="" shocks:="" 5="" shocks="" for="" each="" direction="" temperature:="" max="" ,="" operating="" temperature="" power:="" operating="" duration:="" 1000="" hours="" min.="" adi]="" page:="" 4="">
PART NO: AFB0424SHB T L E D B. P 3: Q CURVE: (mam-J MOW) 0.40 0.20 0.25 0.30 0.35 0.15 14 12 10 ——--- ROOM TEMPERATURE INPUT VOLTAGE WWW" OPERATION VOLTAGE TEMPERATURE - ‘ TEST CONDITION: HUMIDITY —-----------—— 65%RH A00 page: 5
9. DIMENSION DRAWING: LABEL: 15010.5 40 i0 5 (0.591100%) (15751-0020) 2‘5to.3 Z‘StOJ 52.0103 (aoeatomz) (aogaio‘om) (126010.012) I 32.0i073 (1‘250i0m2) 40 010 5 (1,575to.020) 10.0 0.394) 47¢3‘5t0J (47m0.138t0.012) smegma (13,386i01594) ‘ (\NCH) ADO page: 6
@um Delta will not guarantee the performance of the products if the application condition falls A written request should be submitted to Delta prior to approval if deviation from this Please exercise caution when handling fans. Damage may be caused when pressure is applied dropped to the some special designs, there is no guarantee that the products will be free from any such safety problems or failures as caused by the introduction of powder, droplets of sentative of some unique examples and viewed as the It is very important to establish the correct polarity before connecting the fan to the power be caused to the fans if connection is according to the storage temperature limits specified. Do not store fans in a high humidity environment. We highly recommend performance testing is ck Rotor Protection feature. If you impair the rotation of the impeller for the fans that do not have this function, the performance of those fans will lead It is important to consider safety when testing the fans. A suitable fan guard should be fitted to rried out at relative (ambient) temperature and F” capacitor to the fan externally when the application calls
Descriptions:
1.
Delta will not guarantee the performance of the products if the application condition falls
outside the parameters set forth in the specification.
2.
A written request should be submitted to Delta prior to approval if deviation from this
specification is required.
3.
Please exercise caution when handling fans. Damage may be caused when pressure is applied
to the impeller, if the fans are handled by the lead wires, or if the fans are hard-
production floor.
4. Except as pertains to s
ome special designs, there is no guarantee that the products will be free
from any such safety problems or failures as caused by the introduction of powder, droplets of
water or encroachment of insect into the hub.
5. The above-mentioned conditions are repre
sentative of some unique examples and viewed as the
first point of reference prior to all other information.
6.
It is very important to establish the correct polarity before connecting the fan to the power
source. Positive (+) and Negative (-). Damage may
be caused to the fans if connection is
with reverse polarity, as there is no foolproof method to protect against such error.
7. Delta fans are not suitable where any corrosive fluids are introduced to their environment.
8. Please ensure all fans are stored ac
cording to the storage temperature limits specified. Do not
store fans in a high humidity environment. We highly recommend performance testing is
conducted before shipping, if the fans have been stored over 6 months.
9. Not all fans are provided with the Lo
ck Rotor Protection feature. If you impair the rotation of
the impeller for the fans that do not have this function, the performance of those fans will lead
to failure.
10. Please be cautious when mounting the fan. Incorrect mounting of fans may cause exces
s
resonance, vibration and subsequent noise.
11.
It is important to consider safety when testing the fans. A suitable fan guard should be fitted to
the fan to guard against any potential for personal injury.
12. Except where specifically stated, all tests are ca
rried out at relative (ambient) temperature and
humidity conditions of 25oC, 65%. The test value is only for fan performance itself.
13. Be certain to connect an “over 4.7µ
F” capacitor to the fan externally when the application calls
for using multiple fans in parallel, to avoid any unstable power.