Flora RGB Smart NeoPixels Datasheet by Adafruit Industries LLC

-'.- adafruit learning system
Sewable NeoPixels
Created by Justin Cooper
Last updated on 2019-11-15 05:55:04 PM UTC
* adafrult learning system . o a i a I I i i I n I a
Overview
What's a wearable project without LEDs? These tiny smart pixels are our favorite thing. Designed specifically for
wearables, we found the brightest RGB LEDs available (an eye-blistering ~3800mcd) (http://adafru.it/619) and paired
them with a constant-current driver chip. The contacts are easily sewn with conductive thread. Use this guide to test
your first pixel and start on a blinding wearables project with Circuit Playground Express, FLORA or GEMMA!
Pictured above: LED Ampli-Tie (https://adafru.it/doN)
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 3 of 20
Prerequisite guides
Before you begin, familiarize yourself with the following tutorials:
Adafruit Circuit Playground Express (https://adafru.it/adafruit-cpx)
Getting Started with FLORA (https://adafru.it/dwi)
Introducing GEMMA (https://adafru.it/dgH)
NeoPixel Uberguide (https://adafru.it/dhw)
Conductive Thread (https://adafru.it/dn3)
Lots of Pixels?
Each pixel draws as much as 60mA (all three RGB LEDs on for full brightness white). In theory, FLORA can drive up to
500 pixels at 30 FPS (above which it will run out of RAM). Circuit Playground Express can drive more than that.
However, above about 20 pixels (and/or if the overall length of conductive thread exceeds ~6 feet/2 meters), the
nontrivial resistance of the thread adds up and can affect the power supply. For large quantities of pixels over 20 or if
you need to insulate your circuit, you should upgrade to silicone coated stranded core
wire (https://adafru.it/Cc0), which will provide better conductivity for the pixels - the current draw will add up fast!
This tutorial will cover the current v2 pixels as well as the older v1 pixels. The sewing part is the same for both
versions, but the library code is different because the controlling chipset has been upgraded in v2. Pixels
purchased after February 2013 are v2.
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 4 of 20
Pictured above: a FLORA prototype with v1 pixels
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 5 of 20
* adafruit learning system
Hook up alligator clips
Hook up three alligator clips to your Circuit Playground Express as shown: one to VOUT, one to A1, and one to GND. I
used a red wire for power and a black wire for ground for clarity, but it doesn't matter what color you use.
Hook up the other ends of your alligator clips to a single pixel. VOUT (red) connects to the + on the pixel, GND (black)
to the -, and A1 (yellow) to the pad marked with an arrow pointing towards the LED on the tiny board (not away from it).
Wiring on a FLORA is very similar. Just wire to D6 instead of A1. VBATT and VOUT are more or less the same, for our
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 6 of 20
purposes.
On GEMMA or Gemma M0, the wiring is very similar. Hook up VOUT (red in the picture above) to +, GND to - (black
above), and D1 to the inward facing arrow (yellow above).
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 7 of 20
* adafruit learning system
Code with MakeCode
MakeCode (https://adafru.it/Dyi) is Microsoft's drag-and-drop code editor, and it's about the easiest way to get your
pixels showing color.
Click the appropriate button below to go to the MakeCode strandtest project. Click the Download button on that page,
and a file called circuitplayground-strandtest.uf2 (for Circuit Playground Express) or maker-strandtest.uf2 (for Gemma
M0) will download to your computer.
Plug your Circuit Playground Express into your computer via a USB port and double-click the tiny "reset" button in the
center of the board. All the onboard lights will turn green, and a drive will appear on your computer called
CPLAYBOOT or GEMMABOOT. Drag the file you just downloaded onto this drive.
The pixel you have connected will light up in a succession of colors followed by a rainbow animation.
https://adafru.it/DIZ
https://adafru.it/DIZ
https://adafru.it/DI-
https://adafru.it/DI-
Note: MakeCode will NOT work on a FLORA or GEMMA v1 board. For those older boards you must use the Arduino
code method. However, Arduino will work on Circuit Playground Express or Gemma M0 as well as the older boards.
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 8 of 20
mm m mm m W .n “mm,” M- mam.“ anvgr‘ m We frmako :lnw' \uw “’ any 5:! ma {charm \Mu- m mu m m: up man Irv-um unp- my.» do 5KMP V :et anal (Mar :1: mm v to m. a; for Irma rm“. gm». mm a o mmnmuutrm »......W.. hm
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 9 of 20
* adafruit learning system HI: Edit m hols Help Venfy/Complle cum: Upload culw Upload Using Plogrammzl cwsnmu fl/ Dam: Expcrl compiled Binlry CuhAll~S ManageLibun s... demo Add .1111 lihmy... Alduma Ilblallas Show Sketch Foldu cm‘K Indudz Libmy AldulnnHttpClizm Add me... AldulnnScund r we ugh: n52 plxel at a curls, ch15 15 cu A“d‘°Z"° .. . My, , n. “M", Tyne All ram All amrmn "rowel um: —Pl-‘ by mm: m nrvmmmllnl- mum-mam. unnumwumllmuwmlm nnUI-mmflflmlnflmu Vevslonl 7 mull
Code with Arduino
Install the NeoPixel Arduino library
Open up the Arduino library manager:
Search for the Adafruit Neopixel library and install it
We also have a great tutorial on Arduino library installation at:
http://learn.adafruit.com/adafruit-all-about-arduino-libraries-install-use (https://adafru.it/aYM)
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 10 of 20
.0. x0 . x; «mm .u mm upmarmwma Mm mm. 3:33;; W x, W, — WW mmm WWW. Adilmhjnrillxel malmwmarkwu mtruusuzos Mm w m . mm msmwc , Milvu'njtssfils . minurysszmr-ry , Dvadlhéznsu » cams. . animal-Ht! . . . . . m MN _ um; umhm “use: Wm" mamcmwm Wan-NC Mihu'nfiurahxel MalnflLcPS mm mm: mm: r mumfiwlal Unload Usmg Programmer
Connect your FLORA and computer with a USB cable.
Now upload!
Install the NeoPixel library (https://adafru.it/aZU) and go to File --> Examples --> Adafruit_NeoPixel --> strandtest.
If you cannot find that file in the dropdown menu go back up and reinstall the library.
This will launch a window containing the sample sketch. Upload it to your FLORA or GEMMA with the Upload button.
Once successfully uploaded to your FLORA or GEMMA, the pixel will flash and fade different colors. Congrats, you've
tested your pixel!
We do test each pixel in the factory, but you should use this method to test that all three colors (red, green, blue)
work on each of your pixels before sewing them into your project!
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 11 of 20
800 slvanmesl§ #include #define PIN 1 // Parameter l : number of pixels 2 Arduino pin numbe // Parameter
For GEMMA, you'll need to change the pin number in the Arduino sketch before uploading. Change "6" to "1":
Then upload the sample code to GEMMA by pressing the reset button (the red LED should start pulsing) and clicking
the "upload" button in the Arduino software.
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 12 of 20
Sewing more pixels
The pixels are chainable - so you only need 1 pin/wire to control as many LEDs as you like. They're easy to sew, and
the chainable design means no crossed conductive threads (http://adafru.it/641). The output of one pixel connects
directly to the input of the next.
To begin sewing, stitch around the data pin of your microcontroller (A1 on Circuit Playground, D1 on GEMMA or Gemma
M0 and D6 on FLORA are ideal because they're right between power and ground), and stitch over to your first pixel.
Make sure that each arrow points away from the microcontroller in a line. Stitch around the input pad tightly, even
knotting the thread here to form an extra sturdy connection.
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 13 of 20
Stitch back to the thread origin and tie the two ends in a square knot. Use clear nail polish to seal this knot and pull
the ends tight until it dries. Do not clip the thread tails until later on.
All the positive pads (marked with a +) connect together to form one power bus. Likewise all the negative pads
(marked with a -) connect together to form one ground bus.
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 14 of 20
Here's what a three-pixel circuit looks like from the back. See the individual data connections in the center and the
continuous power and ground buses above and below?
Double check your knots are secure before clipping all your thread tails. Clean up your work space so there aren't any
stray bits of conductive thread hanging around.
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 15 of 20
Visually inspect your circuit to check for shorts or stray threads.
Plug your microcontroller into your computer with a USB cable. Change the number of pixels in the Arduino sketch or
MakeCode project to match the number of pixels in your projects, and make sure the pin number matches what you
sewed to. Upload the strandtest sample code as you did when testing a pixel earlier in this guide. Your pixels should
light up and animate different colors and patterns.
If they don't all come on or some later in the chain are flickering, your stitches might not be snug enough against the
pads of the circuit board. Double check your sewing and reinforce it where necessary (with the circuit off/unplugged).
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 16 of 20
The library for these pixels is very similar to our Adafruit_WS2801 (https://adafru.it/aRL) library for other types of RGB
pixels (https://adafru.it/aRL).
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 17 of 20
* adafruit learning system
Project Ideas
Light up Angler Fish Embroidery (https://adafru.it/qzd)
NeoPixel Coat Buttons (https://adafru.it/qze)
Sparkle Skirt with FLORA Motion Sensor (https://adafru.it/qzf)
Textile Potentiometer Hoodie (https://adafru.it/qzA)
NeoPixel Tiara (https://adafru.it/rza)
Close Encounters Hat (https://adafru.it/rzb)
Light-Activated Pixel Heart (https://adafru.it/rzc)
Space Face LED Galaxy Makeup (https://adafru.it/rzd)
Pac Man Pixel Suspenders (https://adafru.it/rze)
Chameleon Scarf with FLORA Color Sensor (https://adafru.it/dNd)
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 18 of 20
WSzaM fl adafrult \earning system
Downloads
Files
Fritzing object in Adafruit Fritzing library (https://adafru.it/aP3)
EagleCAD PCB files on GitHub (https://adafru.it/rzf)
WS2812 Datasheet (https://adafru.it/qta)
SK6812 Datasheet (https://adafru.it/Cc1)
NeoPixel Schematic
Fabrication Print
© Adafruit Industries https://learn.adafruit.com/flora-rgb-smart-pixels Page 19 of 20
© Adafruit Industries Last Updated: 2019-11-15 05:55:04 PM UTC Page 20 of 20