Micro SD Card Breakout Board Tutorial Datasheet by Adafruit Industries LLC

adafrull learning system ,_|r:‘na _..._ .s “ .— .. —. ‘ -,, 1C! (- w .-—.:= ‘K HI. _ :2 x
Micro SD Card Breakout Board Tutorial
Created by lady ada
Last updated on 2019-01-10 10:57:40 PM UTC
2
3
5
5
6
7
9
9
12
14
15
17
17
18
18
19
19
19
20
20
22
24
26
26
26
Guide Contents
Guide Contents
Introduction
Look out!
What to watch for!
Formatting notes
Arduino Wiring
Arduino Library
Arduino Library & First Test
Writing files
Reading from files
Recursively listing/reading files
Arduino Library Docs
Other useful functions
Examples
More examples!
CircuitPython
Adafruit CircuitPython Module Install
Usage
Initialize & Mount SD Card Filesystem
Reading & Writing Data
List Files
Logging Temperature
Download
Schematic
Fabrication Print
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 2 of 27
A DANEE 'CI‘O m'sz Adapter
Introduction
If you have a project with any audio, video, graphics, data logging, etc in it, you'll find that having a removable storage
option is essential. Most microcontrollers have extremely limited built-in storage. For example, even the Arduino Mega
chip (the Atmega2560) has a mere 4Kbytes of EEPROM storage. There's more flash (256K) but you can't write to it as
easily and you have to be careful if you want to store information in flash that you don't overwrite the program itself!
If you're doing any sort of data logging, graphics or audio, you'll need at least a megabyte of storage, and 64 M is
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 3 of 27
probab‘y the minimum, To get that kind of storage we‘re going to use me same type :hat's in every digital camera and
probably the minimum. To get that kind of storage we're going to use the same type that's in every digital camera and
mp3 player: flash cards! Often called SD or microSD cards, they can pack gigabytes into a space smaller than a coin.
They're also available in every electronics shop so you can easily get more and best of all, many computers have SD or
microSD card readers built in so you can move data back and forth between say your Arduino GPS data logger and
your computer graphing software:
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 4 of 27
Look out!
What to watch for!
There are a few things to watch for when interacting with SD cards:
One is that they are strictly 3.3V devices and the power draw when writing to the card can be fairly high, up to 100mA
(or more)! That means that you must have a fairly good 3.3V power supply for the card. Secondly you must also have
3.3V logic to interface to the pins. We've found that SD cards are fairly sensitive about the interface pins - the newest
cards are edge triggered and require very 'square' transitions - things like resistor dividers and long wires will have a
deleterious effect on the transition speed, so keep wires short, and avoid using resistor dividers for the 3.3V logic
lines. We suggest instead using level shifters, such as HEF4050, 74LVX245 or 74AHC125 chips.
For the level shifter we use the CD74HC4050 (https://adafru.it/Boj) which has a typical propagation delay of ~10ns
Secondly, there are two ways to interface with SD cards - SPI mode and SDIO mode. SDIO mode is faster, but is more
complex and as far as we can tell, requires signing non-disclosure documents. For that reason, you will likely never
encounter SDIO mode interface code. Instead, every SD card has a 'lower speed' SPI mode that is easy for any
microcontroller to use. SPI mode requires four pins (we'll discuss them in detail later) so it's not pin-heavy like some
parallel-interface components
SD cards come in two popular flavors - microSD and SD. The interface, code, structure, etc is all the same. The only
differences is the size. MicroSD are much much smaller in physical size.
Third, SD cards are 'raw' storage. They're just sectors in a flash chip, there's no structure that you
have
to use. That
means you could format an SD card to be a Linux filesystem, a FAT (DOS) filesystem or a Mac filesystem. You could
also not have any filesystem at all! However, 99% of computers, cameras, MP3 players, GPS loggers, etc require FAT16
or FAT32 for the filesystem. The tradeoff here is that for smaller microcontrollers (like the Arduino) the addition of the
complex file format handling can take a lot of flash storage and RAM.
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 5 of 27
Formatting notes
Even though you can/could use your SD card 'raw' - it's most convenient to format the card to a filesystem. For the
Arduino library we'll be discussing, and nearly every other SD library, the card must be formatted FAT16 or FAT32.
Some only allow one or the other. The Arduino SD library can use either.
If you bought an SD card, chances are it's already pre-formatted with a FAT filesystem. However you may have
problems with how the factory formats the card, or if it's an old card it needs to be reformatted. The Arduino SD library
we use supports both FAT16 and FAT32 filesystems. If you have a very small SD card, say 8-32 Megabytes you might
find it is formatted FAT12 which isn't supported. You'll have to reformat these card. Either way, it's always good idea to
format the card before using, even if it's new! Note that formatting will erase the card so save anything you want first.
Download the formatter from https://www.sdcard.org/downloads/formatter_3/ (https://adafru.it/c73)
Download it and run it on your computer, there's also a manual linked from that page for use.
We strongly recommend you use the official SD card formatter utility - written by the SD association it solves
many problems that come with bad formatting!
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 6 of 27
5U re d9 nlcro-SD Erea om board+ :4! A [II Q1
Arduino Wiring
Now that your card is ready to use, we can wire up the microSD breakout board! The breakout board we designed
takes care of a lot for you. There's an onboard ultra-low dropout regulator that will convert voltages from 3.3V-6v down
to ~3.3V (IC2). There's also a level shifter that will convert the interface logic from 3.3V-5V to 3.3V. That means you can
use this board to interact with a 3.3V or 5V microcontrollers.
In this tutorial we will be using an Arduino to demonstrate the wiring and interfacing. If you have another
microcontroller, you'll need to adapt the wiring and code to match!
Because SD cards require a lot of data transfer, they will give the best performance when connected up to the
hardware SPI pins on a microcontroller. The hardware SPI pins are much faster than 'bit-banging' the interface code
using another set of pins. For 'classic' Arduinos such as the Duemilanove/Diecimila/Uno those pins are digital 13 (SCK),
12 (MISO) and 11 (MOSI). You will also need a fourth pin for the 'chip/slave select' (SS) line. Traditionally this is pin 10
but you can actually use any pin you like. If you have a Mega, the pins are different! You'll want to use digital 50 (MISO),
51 (MOSI), 52 (SCK), and for the CS line, the most common pin is 53 (SS). Again, you can change the SS (pin 10 or 53)
later but for now, stick with those pins.
Connect the 5V pin to the 5V pin on the Arduino
Connect the GND pin to the GND pin on the Arduino
Connect CLK to pin 13 or 52
Connect DO to pin 12 or 50
Connect DI to pin 11 or 51
Connect CS to pin 10 or 53
There's one more pin CD - this is the Card Detect pin. It shorts to ground when a card is
not
inserted. (Note that some
card holders are the other way around). You should connect a pull up resistor (10K or so) and wire this to another pin if
you want to detect when a card is inserted. We won't be using it for now.
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 7 of 27
fl w mm m
That's it! Now you're ready to rock!
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 8 of 27
m sketchiapIMa \ Arduinn mm New calm Open‘ .. cm+o Shztthhuuk > E ‘ ampwes LEasvcs (\nss (ul+w zomal Save (nus 3.Ana\on Sav: As, ctvl+smrt+s 4-Cummumtatmn 5.Cuntml 5.5mm; UD‘oed to 1/0 Baud cul+u Page Setup cul+smrt+p 7,nusp\av Punt (rm? 3.5tvms Pvefetences ("Hams AvdulnolsP Qul Cbl+Q AldulnuTeitimla EEPROM Ethernet meata Matrix camm’o San/u Data‘oggav SP] Durwfll: steppev FIB WW: I‘smb; Readwne
Arduino Library
Arduino Library & First Test
Interfacing with an SD card is a bunch of work, but luckily for us, Adafruit customer fat16lib (William G) has written a
very nice Arduino library just for this purpose and it's now part of the Arduino IDE known as SD (pretty good name,
right?) You can see it in the Examples submenu
Next, select the CardInfo example sketch.
This sketch will not write any data to the card, just tell you if it managed to recognize it, and some information about it.
This can be very useful when trying to figure out whether an SD card is supported. Before trying out a new card,
please try out this sketch!
Go to the beginning of the sketch and make sure that the chipSelect line is correct, for this wiring we're using digital
pin 10 so change it to 10!
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 9 of 27
ea Canflnlo \ Arduinn mm QE‘ Fl: Edi 5mm Yods Heb Sdnle :onc: , ,I‘Y‘J“',l'VH1L>1V“|A/HH ,:r 4.,» \ H, “mm; m Mann: :‘ sl.)&,1‘ , . pm m ,r mmziun n1 amni. cons: an: chlpselecr. - 1n,- Snial.hsg)nl95[|0); Serial.p:1nc("\nIm:)al)z)ng 51) cans ,. Chi Ethexnét V Held, , . in cthpv kw x u: x m 1: m not - h m: laud!) , m m ms: anon: :Hiul', . new war 1‘: up >13 m a: m: ,4 luxury nmcnam mJA n01: mu pmflodeuo, UUTPUT): ,, any”. v1.17 m m m. ‘ “my , mum; llbtanes v >
OK, now insert the SD card into the breakout board and upload the sketch.
Open up the Serial Monitor and type in a character into the text box (& hit send) when prompted. You'll probably get
something like the following:
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 10 of 27
QC M53 ‘ Send Imcmnnng s» card...l¥1r1ng is Carrie: and a card x: pmm. « c m zyp : 5172 Volume cm. is nus mum 3m (was): 1575mm vum sue (Kb‘fies): messz Volume sxze (mes): use: 1711!: found an a; card (name, .451! and sxxe )2: bytes): awn-mu zuuo-Dl-Dl umoouw suuuuuo oLDLucs/ zuurorul 16:58:02 7er} 2011-04—01 l7:DD:15 spsmm 1x1 1980-00-00 00:00:00 1195571 cPsLucoqui xsso-uu-uu 0U:DD:UU 61621 DPSLDWLTXT xsaoiuoiou on:uo:no 2247 cpsnuwajxr lsioiflodm ou:uo:no szsosm magnum. 1x1 lSED-flD-DD 00:00:00 «7 cPsLucosti xsso-uu-uu 0U:DD:UU 55751 DPSLEIW7JXT xsaoiuoiou on:uo:no mu DPSLEIGOSJXT xsaoiuoiou ou:uo:no .LEISS spsnnmz 1x1 lSED-flD-DD on-mrnn 2597fl1 syswsost xsso-uu-uu 0U.UD.UU 3124: DPSLEIWEJXT xsaoiuoiou on:uo:no no v mama“ Nu‘neendng v Swflhaud v
It's mostly gibberish, but it's useful to see the Volume type is FAT16 part as well as the size of the card (about 2 GB
which is what it should be) etc.
If you have a bad card, which seems to happen more with ripoff version of good brands, you might see:
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 11 of 27
%- :ypi my aha-Eta: cu sun: nu: um: 1535 Card cypi: sm nmuuccuzu 11>: 0 cm x»: vadnc: ll/A Varslan: Ln Serial number: 231573372 flmtaccurxng date: S/ZDOE curdsxla: 15mm 4512 by“ [um-g; sushxusesue: 64 blocks erasesxnwleilnck: ctue pnn,bum,cypa,§naxl:,13nghh 1,u,n,u(u z,o,u,u,u 3,0,n,u,u «,o,n,n,u Vul.lnlc failed 5:: array axruxcadi: n exrurD-La: n v 960:: band v a cums: F‘EUX‘ ‘ Send Imuannng s» card...xnxcxelx:acxan tailed. Things cc check: . u .1 card 1: "mama: * I; you: mung cnxxecrfl . am you change an unpsueu pm M; 1-3th yuuz shxeld or manna Rw Home“ Nu‘neendng v wuhaud v
The card mostly responded, but the data is all bad. Note that the Product ID is "N/A" and there is no Manufacturer ID
or OEM ID. This card returned some SD errors. It's basically a bad scene, I only keep this card around to use as an
example of a bad card! If you get something like this (where there is a response but it's corrupted) you can try to
reformat it or if it still flakes out, should toss the card.
Finally, try taking out the SD card and running the sketch again, you'll get the following,
It couldn't even initialize the SD card. This can also happen if there's a soldering or wiring error or if the card is
really
damaged.
Writing files
The following sketch will do a basic demonstration of writing to a file. This is a common desire for datalogging and
such.
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 12 of 27
muialhinv 31> cut VxniKA-lilabion up“. Iucmw co “sax.“ dam.
When you run it you should see the following:
#include <SD.h>
File myFile;
void setup()
{
Serial.begin(9600);
Serial.print("Initializing SD card...");
// On the Ethernet Shield, CS is pin 4. It's set as an output by default.
// Note that even if it's not used as the CS pin, the hardware SS pin
// (10 on most Arduino boards, 53 on the Mega) must be left as an output
// or the SD library functions will not work.
pinMode(10, OUTPUT);
if (!SD.begin(10)) {
Serial.println("initialization failed!");
return;
}
Serial.println("initialization done.");
// open the file. note that only one file can be open at a time,
// so you have to close this one before opening another.
myFile = SD.open("test.txt", FILE_WRITE);
// if the file opened okay, write to it:
if (myFile) {
Serial.print("Writing to test.txt...");
myFile.println("testing 1, 2, 3.");
// close the file:
myFile.close();
Serial.println("done.");
} else {
// if the file didn't open, print an error:
Serial.println("error opening test.txt");
}
}
void loop()
{
// nothing happens after setup
}
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 13 of 27
You can then open up the file in your operating system by inserting the card. You'll see one line for each time the llsll l Not :Ieidlrwmatxwueh testing 1. 2. 3. A testing 1, 2, 2.
You can then open up the file in your operating system by inserting the card. You'll see one line for each time the
sketch ran. That is to say, it appends to the file, not overwriting it.
Some things to note:
You can have multiple files open at a time, and write to each one as you wish.
You can use print and println() just like Serial objects, to write strings, variables, etc
You must close() the file(s) when you're done to make sure all the data is written permanently!
You can open files in a directory. For example, if you want to open a file in the directory such as
/MyFiles/example.txt you can call SD.open("/myfiles/example.txt") and it will do the right thing.
Reading from files
Next up we will show how to read from a file, it's very similar to writing in that we SD.open() the file but this time we
don't pass in the argument FILE_WRITE this will keep you from accidentally writing to it. You can then call available()
(which will let you know if there is data left to be read) and read() from the file, which will return the next byte.
The SD card library does not support 'long filenames' such as we are used to. Instead, it uses the 8.3 format
for file names, so keep file names short! For example IMAGE.JPG is fine, and datalog.txt is fine but "My GPS
log file.text" is not! Also keep in mind that short file names do not have 'case' sensitivity, so datalog.txt is the
same file as DataLog.Txt is the same file as DATALOG.TXT
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 14 of 27
Some things to note:
You can have multiple files open at a time, and read from each one as you wish.
Read() only returns a byte at a time. It does not read a full line or a number!
You should close() the file(s) when you're done to reduce the amount of RAM used.
Recursively listing/reading files
#include <SD.h>
File myFile;
void setup()
{
Serial.begin(9600);
Serial.print("Initializing SD card...");
// On the Ethernet Shield, CS is pin 4. It's set as an output by default.
// Note that even if it's not used as the CS pin, the hardware SS pin
// (10 on most Arduino boards, 53 on the Mega) must be left as an output
// or the SD library functions will not work.
pinMode(10, OUTPUT);
if (!SD.begin(10)) {
Serial.println("initialization failed!");
return;
}
Serial.println("initialization done.");
// open the file for reading:
myFile = SD.open("test.txt");
if (myFile) {
Serial.println("test.txt:");
// read from the file until there's nothing else in it:
while (myFile.available()) {
Serial.write(myFile.read());
}
// close the file:
myFile.close();
} else {
// if the file didn't open, print an error:
Serial.println("error opening test.txt");
}
}
void loop()
{
// nothing happens after setup
}
The SD card library does not support 'long filenames' such as we are used to. Instead, it uses the 8.3 format
for file names, so keep file names short! For example IMAGE.JPG is fine, and datalog.txt is fine by "My GPS
log file.text" is not! Also keep in mind that short file names do not have 'case' sensitivity, so datalog.txt is the
same file as DataLog.Txt is the same file as DATALOG.TXT
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 15 of 27
The \ast example we have shows more advanced use, A common request is for example wanting to list every me on E coma H saw 1 Inxcunung :1) ma, ,munhmm am A nsmxr as nnummx 12160 mum 352225 Pnuwsvmz mssz cam mz 153512 mm/ 5|“.an use us]: ,, 52 mm” m momma 655 mu;- m m; mm” m 61111,? 52 61171,qu 52392 mm”: 557 awn m 1151 an 52 mm 3553 sauna m m shun-LI“: mu “mum m m 5:1"sz 1574 swam 775 mm» 52 mm...) 46 zmlx ,, 322 “9,1112 1311232 nwln.Env zmse am. Emma! km W
The last example we have shows more advanced use. A common request is for example wanting to list every file on
the SD card, or play ever music file or similar. In the latest version of the SD library, you can
recurse
through a
directory and call openNextFile() to get the next available file. These aren't in alphabetical order, they're in order of
creation so just watch out for that!
To see it, run the SDlistfiles example sketch
Here you can see that we have a subdirectory ANIM (we have animation files in it). The numbers after each file name
are the size in bytes of the file. This sketch is handy if you want to check what files are called on your card. The sketch
also demonstrates how to do directory handling.
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 16 of 27
Arduino Library Docs
Other useful functions
There's a few useful things you can do with SD objects we'll list a few here:
If you just want to check if a file exists, use SD.exists("filename.txt") which will return true or false.
You can delete a file by calling SD.remove("unwanted.txt") - be careful! This will really delete it, and there's no
'trash can' to pull it out of.
You can create a subdirectory by calling SD.mkdir("/mynewdir") handy when you want to stuff files in a location.
Nothing happens if it already exists but you can always call SD.exists() above first.
Also, there's a few useful things you can do with File objects:
You can seek() on a file. This will move the reading/writing pointer to a new location. For example seek(0) will
take you to the beginning of the file, which can be very handy!
Likewise you can call position() which will tell you where you are in the file.
If you want to know the size of a file, call size() to get the number of bytes in the file.
Directories/folders are special files, you can determine if a file is a directory by calling isDirectory()
Once you have a directory, you can start going through all the files in the directory by calling openNextFile()
You may end up with needing to know the name of a file, say if you called openNextFile() on a directory. In this
case, call name() which will return a pointer to the 8.3-formatted character array you can directly Serial.print() if
you want.
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 17 of 27
Examples
More examples!
If you want to use an SD card for datalogging, we suggest checking out our Datalogging shield (https://adafru.it/dpH)
and GPS logging shield (https://adafru.it/dpI) - there's example code specifically for those purposes.
If you want to use the SD card for loading images (such as for a color display) look at our 2.8" TFT
shield (https://adafru.it/dpJ) and 1.8" TFT breakout tutorials (https://adafru.it/ckK). Those have examples of how we read
BMP files off disk and parse them.
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 18 of 27
no. In: < .m.="" n~="" a-="" m="" i="" w="" us.="" ,.,._="" mmm="" ”wwi”,="" _="" i="" mumm-="" w.="" ,="" m="" m="" i="" ummhmml‘umwm="" ,="" i="" rum="" dml‘illuvm="" 8m="" lummu‘nn="" m="" "mu.="" .="" ”mm;="" "mm.”="" .="" a="" mums"="" .="" i="" n-irmn="" i="" th‘umfllw="" .="" a="" w.="" i="" mmmm-mlssmw="" i="" mmmw="" cwm="" mw.“="" .="" .,="" "mm-m="" ,="" i="" unvmm-s‘nnw="" ow":="" "www="" ,="" 0="" hum-="" db:="" .="" .im="" -="" i="" mmm‘m="" i="" “mum-1mm="" m="" a="" www="" 11:15:th="" '="" _="" .="" ..m....m="" -="" i="" -="" '="" 3221;“="" i="" mm-="" i="" ww="" i="" mm="" .="" :3flimm="" .="" w="" mm».="" d="" ._="" i="" m.="" .="" my="" a="" mu,="">
CircuitPython
Adafruit CircuitPython Module Install
To use a microSD card with your Adafruit CircuitPython board you'll need to install
the Adafruit_CircuitPython_SD (https://adafru.it/zwC) module on your board.
First make sure you are running the latest version of Adafruit CircuitPython (https://adafru.it/Amd) for your board.
Next you'll need to install the necessary libraries to use the hardware--carefully follow the steps to find and install these
libraries from Adafruit's CircuitPython library bundle (https://adafru.it/zdx). Our introduction guide has a great page on
how to install the library bundle (https://adafru.it/ABU) for both express and non-express boards. Be sure to use the
latest CircuitPython Bundle as it includes an updated version of the SD card module with a few necessary fixes!
Remember for non-express boards like the, you'll need to manually install the necessary libraries from the bundle:
adafruit_sdcard.mpy
adafruit_bus_device
If your board doesn't support USB mass storage, like the ESP8266, then use a tool like ampy to copy the file to the
board (https://adafru.it/s1f). You can use the latest version of ampy and its new directory copy
command (https://adafru.it/q2A) to easily move module directories to the board.
Before continuing make sure your board's lib folder or root filesystem has the adafruit_sdcard.mpy and
adafruit_bus_device modules copied over.
Usage
The following section will show how to initialize the SD card and read & write data to it from the board's Python prompt
/ REPL.
Next connect to the board's serial REPL (https://adafru.it/Awz)so you are at the CircuitPython >>> prompt.
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 19 of 27
Initialize & Mount SD Card Filesystem
Before you can use the microSD card you need to initialize its SPI connection and mount its filesystem. First import
the necessary modules to initialize the SPI and CS line physical connections:
Next create the SPI bus and a digital output for the microSD card's chip select line (be sure to select the right pin name
or number for your wiring):
Now import modules to access the SD card and filesystem:
At this point you're ready to create the microSD card object and the filesystem object:
Notice the adafruit_sdcard module has a SDCard class which contains all the logic for talking to the microSD card at a
low level. This class needs to be told the SPI bus and chip select digital IO pin in its initializer.
After a SDCard class is created it can be passed to the storage module's VfsFat class. This class has all the logic for
translating CircuitPython filesystem calls into low level microSD card access. Both the SDCard and VfsFat class
instances are required to mount the card as a new filesystem.
Finally you can mount the microSD card's filesystem into the CircuitPython filesystem. For example to make the path
/sd on the CircuitPython filesystem read and write from the card run this command:
The first parameter to the storage.mount command is the VfsFat class instance that was created above, and the
second parameter is the location within the CircuitPython filesystem that you'd like to 'place' the microSD card.
Remember the mount location as you'll need it to read and write files on the card!
Reading & Writing Data
Once the microSD card is mounted inside CircuitPython's filesystem you're ready to read and write data from it.
Reading and writing data is simple using Python's file operations like open (https://adafru.it/reL),
import board
import busio
import digitalio
spi = busio.SPI(board.SCK, MOSI=board.MOSI, MISO=board.MISO)
# Use board.SD_CS for Feather M0 Adalogger
cs = digitalio.DigitalInOut(board.SD_CS)
# Or use a GPIO pin like 15 for ESP8266 wiring:
#cs = digitalio.DigitalInOut(board.GPIO15)
import adafruit_sdcard
import storage
sdcard = adafruit_sdcard.SDCard(spi, cs)
vfs = storage.VfsFat(sdcard)
storage.mount(vfs, "/sd")
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 20 of 27
dose (hnps://adafru.itlryE), read (hupszl/adafrujuryE), and write (hnps://adafru.it/ryE). The beauty of Circuilethon and
close (https://adafru.it/ryE), read (https://adafru.it/ryE), and write (https://adafru.it/ryE). The beauty of CircuitPython and
MicroPython is that they try to be as similar to desktop Python as possible, including access to files.
For example to create a file and write a line of text to it you can run:
Notice the with statement is used to create a context manager that opens and automatically closes the file. This is
handy because with file access you Python you must close the file when you're done or else all the data you thought
was written might be lost!
The open function is used to open the file by telling it the path to it, and the mode (w for writing). Notice the path is
under /sd, /sd/test.txt. This means the file will be created on the microSD card that was mounted as that path.
Inside the context manager you can access the f variable to operate on the file while it's open. The write function is
called to write a line of text to the file. Notice that unlike a print statement you need to end the string passed to write
with explicit carriage returns and new lines.
You can also open a file and read a line from it with similar code:
If you wanted to read and print all of the lines from a file you could call readline in a loop. Once readline reaches the
end of the file it will return an empty string so you know when to stop:
There's even a readlines function that will read all of the lines in the file and return them in an array of lines. Be careful
though as this means the entire file must be loaded into memory, so if the file is very large you might run out of
memory. If you know your file is very small you can use it though:
Finally one other very common file scenario is opening a file to add new data at the end, or append data. This works
exactly the same as in Python and the open function can be told you'd like to append instead of erase and write new
data (what normally happens with the w option for open). For example to add a line to the file:
with open("/sd/test.txt", "w") as f:
f.write("Hello world!\r\n")
with open("/sd/test.txt", "r") as f:
print("Read line from file:")
print(f.readline())
with open("/sd/test.txt", "r") as f:
print("Printing lines in file:")
line = f.readline()
while line != '':
print(line)
line = f.readline()
with open("/sd/test.txt", "r") as f:
lines = f.readlines()
print("Printing lines in file:")
for line in lines:
print(line)
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 21 of 27
Notice the a option in the open function--this tells Python to add data at the end of the file instead of erasing it and
starting over at the top. Try reading the file with the code above to see the new line that was added!
That's all there is to manipulating files on microSD cards with CircuitPython!
Here are a few more complete examples of using a SD card from the Trinket M0 CircuitPython
guides (https://adafru.it/Bvi). These are great as a reference for more SD card usage.
List Files
Load this into main.py:
with open("/sd/test.txt", "a") as f:
f.write("This is another line!\r\n")
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 22 of 27
Once it's loaded up, open up the REPL (and restart it with ^D if necessary) to get a printout of all the files included. We
recursively print out all files and also the filesize. This is a good demo to start with because you can at least tell if your
files exist!
import os
import adafruit_sdcard
import board
import busio
import digitalio
import storage
# Use any pin that is not taken by SPI
SD_CS = board.D0
# Connect to the card and mount the filesystem.
spi = busio.SPI(board.SCK, board.MOSI, board.MISO)
cs = digitalio.DigitalInOut(SD_CS)
sdcard = adafruit_sdcard.SDCard(spi, cs)
vfs = storage.VfsFat(sdcard)
storage.mount(vfs, "/sd")
# Use the filesystem as normal! Our files are under /sd
# This helper function will print the contents of the SD
def print_directory(path, tabs=0):
for file in os.listdir(path):
stats = os.stat(path + "/" + file)
filesize = stats[6]
isdir = stats[0] & 0x4000
if filesize < 1000:
sizestr = str(filesize) + " by"
elif filesize < 1000000:
sizestr = "%0.1f KB" % (filesize / 1000)
else:
sizestr = "%0.1f MB" % (filesize / 1000000)
prettyprintname = ""
for _ in range(tabs):
prettyprintname += " "
prettyprintname += file
if isdir:
prettyprintname += "/"
print('{0:<40} Size: {1:>10}'.format(prettyprintname, sizestr))
# recursively print directory contents
if isdir:
print_directory(path + "/" + file, tabs + 1)
print("Files on filesystem:")
print("====================")
print_directory("/sd")
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 23 of 27
"mm... Has an filesystem- TeensyDeno.bin SEARflHrHTH 1w, bin System Volume Infernatian/ wusa:xings.dac IndexerVelumeGuid iesc,cxi~ kest. Dd binaries/ ZTTZCW'PYJHn 2772test,h1 n bmtloadJfl n 2772b1nk.h1n size, size Size Size: Size' Size, size: size, Size: size, size: Size: size: 23,4 75.5 13,0 0 12 76 154 12 a 239.5 29.5 z,z 18.9
Logging Temperature
But you probably want to do a little more, lets log the temperature from the chip to a file.
Here's the new script
import time
import adafruit_sdcard
import board
import busio
import digitalio
import microcontroller
import storage
# Use any pin that is not taken by SPI
SD_CS = board.D0
led = digitalio.DigitalInOut(board.D13)
led.direction = digitalio.Direction.OUTPUT
# Connect to the card and mount the filesystem.
spi = busio.SPI(board.SCK, board.MOSI, board.MISO)
cs = digitalio.DigitalInOut(SD_CS)
sdcard = adafruit_sdcard.SDCard(spi, cs)
vfs = storage.VfsFat(sdcard)
storage.mount(vfs, "/sd")
# Use the filesystem as normal! Our files are under /sd
print("Logging temperature to filesystem")
# append to the file!
while True:
# open file for append
with open("/sd/temperature.txt", "a") as f:
led.value = True # turn on LED to indicate we're writing to the file
t = microcontroller.cpu.temperature
print("Temperature = %0.1f" % t)
f.write("%0.1f\n" % t)
led.value = False # turn off LED to indicate we're done
# file is saved
time.sleep(1)
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 24 of 27
When saved, the Trinket will start saving the temperature once per second to the SD card under the n u L‘xv the Vi'.esy=leri t.) WWI: 0m rite, are under Md :4 )5 print( tugging temperature to fiiesysten“) :- e wire to the my. 11 ml. Yrun: a 4 we“ the «w fluent) J t. with open("/sd/temperature.tx:", "4”) r: a) i 'Ied.value . rm. : him on in» ”'3 mmmre we re .n'flng m rhn we Mu mcoerelead is on. simply save files over USB to run than or enter REPL to disable mu.” output: Legging temperature to ritesyscem remperature : 25.1 Temperature = 26‘2 remperamre : 25.9 remperature : 25.9
When saved, the Trinket will start saving the temperature once per second to the SD card under the
file temperature.txt
The key part of this demo is in these lines:
This is a slightly complex demo but it's for a good reason. We use with (a 'context') to open the file for appending, that
way the file is only opened for the very short time its written to. This is safer because then if the SD card is removed or
the board turned off, all the data will be safe(r).
We use the LED to let the person using this know that the temperature is being written, it turns on just before the write
and then off right after.
After the LED is turned off the with ends and the context closes, the file is safely stored.
print("Logging temperature to filesystem")
# append to the file!
while True:
# open file for append
with open("/sd/temperature.txt", "a") as f:
led.value = True # turn on LED to indicate we're writing to the file
t = microcontroller.cpu.temperature
print("Temperature = %0.1f" % t)
f.write("%0.1f\n" % t)
led.value = False # turn off LED to indicate we're done
# file is saved
time.sleep(1)
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 25 of 27
Mrnj‘FnrM um cm W so & MMC w or‘n' mm
Download
Transcend microSD card datasheet (https://adafru.it/cma)
EagleCAD PCB files on GitHub (https://adafru.it/rfT)
Fritzing object in the Adafruit Fritzing library (https://adafru.it/aP3)
Schematic
Click to embiggen
For the level shifter we use the CD74HC4050 (https://adafru.it/Boj) which has a typical propagation delay of ~10ns
Fabrication Print
Dims in inches
© Adafruit Industries https://learn.adafruit.com/adafruit-micro-sd-breakout-board-card-tutorial Page 26 of 27
. . . . . . A . . ,th ulrumw
© Adafruit Industries Last Updated: 2019-01-10 10:57:39 PM UTC Page 27 of 27