MAX 10 FPGA Eval Kit Guide Datasheet by Intel

101 Innovation Drive
San Jose, CA 95134
www.altera.com
UG-01158-1.2
User Guide
MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit
Feedback Subscribe
MAX 10 FPGAMAX 10 FPGAMAX 10 FPGA (10M08S,
144-EQFP) Evaluation Kit User Guide
© 2015 Altera Corporation. All rights reserved. ALTERA, ARRIA, CYCLONE, HARDCOPY, MAX, MEGACORE, NIOS, QUARTUS and STRATIX words and logos
are trademarks of Altera Corporation and registered in the U.S. Patent and Trademark Office and in other countries. All other words and logos identified as
trademarks or service marks are the property of their respective holders as described at www.altera.com/common/legal.html. Altera warrants performance of its
semiconductor products to current specifications in accordance with Altera's standard warranty, but reserves the right to make changes to any products and
services at any time without notice. Altera assumes no responsibility or liability arising out of the application or use of any information, product, or service
described herein except as expressly agreed to in writing by Altera. Altera customers are advised to obtain the latest version of device specifications before relying
on any published information and before placing orders for products or services.
September 2015 Altera Corporation MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit
User Guide
ISO
9001:2008
Registered
September 2015 Altera Corporation MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit
User Guide
Contents
Chapter 1. Overview
Board Component Blocks . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 1–1
Supported Items Not Included with the Kit . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 1–3
Chapter 2. Getting Started
Powering the Kit . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 2–1
Installing the USB-Blaster Driver . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 2–1
Handling the Kit . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 2–1
Factory Default Switch and Jumper Settings . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 2–2
Chapter 3. Board Components
Board Overview . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–1
Featured Device: MAX 10 FPGA . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–3
Configuration . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–3
FPGA Programming over External USB-Blaster . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 33
Configuring the FPGA Using the Quartus II Programmer . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–3
Selecting Internal Configuration Scheme . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–4
Generating a .pof File with ICB Settings . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–4
Programming Internal Flash Memory . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–6
Clock Circuitry . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–6
General-Purpose Clock . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–6
Arduino Connectors . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–7
General User Input/Output . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–8
User-Defined DIP Switch . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–8
User-Defined LEDs . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–9
Power Supply . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–9
Power Measurement . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–9
Power Distribution System . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–10
Temperature Sense . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 3–10
Additional Information
Document Revision History . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Info–1
How to Contact Altera . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Info–1
Typographic Conventions . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Info–1
Compliance and Conformity Statements . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Info–3
CE EMI Conformity Caution . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . Info–3
iv Contents
MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit September 2015 Altera Corporation
User Guide
September 2015 Altera Corporation MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit
User Guide
1. Overview
The MAX ®10 Evaluation Kit allows is an entry-level board for evaluating the MAX 10
FPGA technology and Enpirion® PowerSoC regulators. You can use this kit to do the
following:
Develop designs for the 10M08S, 144-EQFP FPGA
Measure FPGA power (VCC_CORE and VCC_IO)
Bridge between different I/O voltages
Read and write to the FPGA’s NOR flash memory
Use the FPGA’s analog-to-digital converter embedded block to measure incoming
analog signals
Interface to external functions or devices via Arduino UNO R3 connectors or
through-hole vias
Reuse the kit’s PCB board and schematic as a model for your design
Board Component Blocks
This evaluation kit features the following major component blocks. For a detailed
description of the board components, see “Board Components” on page 3–1.
Altera MAX 10 FPGA, 10M08SAE144C8G, (or ES variant)
8,000 logic elements (LE)
378 kilobits (Kb) M9K memory
32 – 172 (KB) user flash memory
One analog-to-digital (ADC) converter, 1 million samples per second (MSPS),
12-bit
FPGA configuration circuitry
JTAG header for external USB-Blaster™, USB-Blaster II, or Ethernet Blaster
download cable
Flash storage for two configuration images (factory and user)
Dual-image self-configuration via Programmer Object File (.pof)
Temporary engineering debug of FPGA design via SRAM Object File (.sof)
On-Board clocking circuitry
50 MHz oscillator connected to FPGA global clock input
General user I/O
8 analog input I/O, 14 Arduino I/O, 40 general purpose I/O
5 red user-defined LEDs
One green LED to show power from USB cable
1–2 Chapter 1: Overview
Board Component Blocks
MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit September 2015 Altera Corporation
User Guide
Push button and DIP switches
One reconfiguration push button (SW2)
One device-wide reset of all registers, push button (SW1)
User DIP switch (SW3)
Power
The board is powered by USB cable (from PC or wall jack)
One green power-on LED (D6)
Probe points for manual, multi-meter measurement of current to calculate
power consumption (TP2 - TP5) or to verify voltages on the selected internal
nodes (TP1, TP6 - TP9)
Figure 1–1. Example MAX 10 Evaluation Kit Block Diagram
Push Button
Push Button
10M08S
E144
Through-hole vias
* Potentiometer
Oscillator ~
JTAG
LEDs
To power source
Mini-USB
B
Enpirion
Supplies
Arduino UNO R3
connectors
DIP switch
Through-hole vias
* Customer must purchase and install.
Chapter 1: Overview 1–3
Supported Items Not Included with the Kit
September 2015 Altera Corporation MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit
User Guide
Supported Items Not Included with the Kit
The following items are not included in the kit but were designed to be used in
conjunction with this kit.
Table 1–1. Additional Components Not Included with the Kit
Board
Reference Description Manufacturer Manufacturing
Part Number
Manufacturer
Website
R94 Potentiometer Bourns 3362P-1-103TLF www.bourns.com
J8, J9 2x20 0.1-inch headers Sullins Connector
Solution PPPC202LFBN-RC www.sullinscorp.com
J2, J3, J4, J5
Optional daughter-
cards: Arduino UNO R3
revision shields.
Arduino —
www.adafruit.com
www.sainsmart.com
www.arduino.com
J1 USB-Blaster Download
Cable Altera PL-USB-BLASTER-RCN www.altera.com
J1 USB-Blaster II
Download Cable Altera PL-USB2-BLASTER Please call
1–4 Chapter 1: Overview
Supported Items Not Included with the Kit
MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit September 2015 Altera Corporation
User Guide
September 2015 Altera Corporation MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit
User Guide
2. Getting Started
Powering the Kit
You can apply power the MAX 10 FPGA Evaluation Kit by plugging in the USB cable
(J1) to your PC or wall jack. When powered correctly, a pre-programmed design
blinks LEDs D1 through D5 ON half a second then OFF half a second.
Installing the USB-Blaster Driver
You can configure the evaluation kit by programming on-chip flash memory using a
USB-Blaster™, USB-Blaster II, or Ethernet Blaster download cable. However, for the
host computer and board to communicate, you must install the appropriate
USB-Blaster, USB-Blaster II, or Ethernet Blaster driver on the host computer.
Installation instructions for the Blaster driver for your operating system are available
on the Altera website. On the Altera Programming Cable Driver Information page of
the Altera website, locate the table entry for your configuration and click the link to
access the instructions.
fYou can download the Blaster drivers from the Download Cables page.
Handling the Kit
When handling the board, it is important to observe the following static discharge
precaution:
cWithout proper anti-static handling, the board can be damaged. Therefore, use
anti-static handling precautions when touching the board.
The MAX 10 Evaluation Kit must be stored between –40º C and 100º C. The
recommended operating temperature is between 0º C and 85º C.
@© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© @© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© ©© Egg
2–2 Chapter 2: Getting Started
Factory Default Switch and Jumper Settings
MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit September 2015 Altera Corporation
User Guide
Factory Default Switch and Jumper Settings
Figure 2–1. Switch Locations and Default Settings (Board Top)
SW1
SW3
J6
1
2
3
1
2
3J7
SW2
ON
123456
MAX 10 FPGA
Table 2–1. Default SW3 DIP Switch Settings (Part 1 of 2)
Switch Function Default
Position
1 User-defined On
2 User-defined On
3 User-defined On
4 User-defined On
Chapter 2: Getting Started 2–3
Factory Default Switch and Jumper Settings
September 2015 Altera Corporation MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit
User Guide
5 User-defined On
6
BOOT_SEL: Use this switch to choose CFM0, CFM1, or
CFM2 image as the first image in a dual-image configuration.
If BOOT_SEL is set to low, the first boot image is CFM0
image, If set to high, the first boot image is the CFM1 or
CFM2 image. By default, the FPGA setting for this pin is tri-
stated.
On
Table 2–2. Default Jumper Settings
Jumper Function Setting
J6 Jumper for analog input channel #8. Default connection is to
GND. Pins 2 and 3
J7 Jumper for analog input channel #7. Default connection is to
potentiometer. Pins 2 and 3
Table 2–1. Default SW3 DIP Switch Settings (Part 2 of 2)
Switch Function Default
Position
2–4 Chapter 2: Getting Started
Factory Default Switch and Jumper Settings
MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit September 2015 Altera Corporation
User Guide
m m m m
September 2015 Altera Corporation MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit
User Guide
3. Board Components
This chapter introduces all the important components on the evaluation kit.
Figure 3–1 illustrates major component locations and Table 31 provides a brief
description of all features of the board.
Board Overview
This section provides an overview of the evaluation kit, including an annotated board
image and component descriptions.
Table 31 describes the components and lists their corresponding board references.
Figure 3–1. Overview of the MAX 10 FPGA Evaluation Kit Features
3–2 Chapter 3: Board Components
Board Overview
MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit September 2015 Altera Corporation
User Guide
Table 3–1. MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit Components
Board Reference Type Description
Featured Device
U2 FPGA
10M08SAE144C8G, (or ES variant) Plastic Enhanced Quad Flat Pack
(EQFP), 144 pins, 22 mm x 22 mm.
For package details, refer to the Altera Device Package Information
page.
Configuration, Status, and Setup Elements
J6 Jumper for analog input
channel #8
Default connection is to GND. Change jumper to pins 1 and 2 to switch
analog source to Arduino header.
J7 Jumper for analog input
channel #7
Default connection is to potentiometer (customer option to purchase
and install). Change jumper to pins 1 and 2 to switch analog source to
Arduino header.
SW3 User-defined DIP switch 6-position switch. SW3.1 through SW3.5 are user-defined. SW3.6 is
predefined for dual-image configuration.
D1, D2, D3, D4,
D5 LED, red These LEDs cycle off and on when the kit is powered on.
D6 Power LED, green Illuminates when USB power is present.
SW2 FPGA reconfiguration push-
button
Toggling this button causes the FPGA to reconfigure from on-die
Configuration Flash Memory (CFM).
Clock Circuitry
X1 50-MHz oscillator 50-MHz crystal oscillator for general purpose logic.
General User Input and Output
D1, D2, D3, D4,
D5 User-defined LEDs, red User-defined LEDs.
SW1 FPGA register push-button Toggling this button resets all registers in the FPGA.
R94 Potentiometer You must purchase and install this device to provide analog inputs
signals to the MAX 10 ADC IP block (analog input channel 8).
Connectors
J2, J3, J4, J5 Arduino UNO R3 connectors
You can purchase Arduino Uno R3 compatible Shields (i.e.
daughtercards) to connect to the Arduino headers installed on the
board.
J10 JTAG header Connects an Altera USB-Blaster, USB-Blaster II, or Ethernet Blaster to
program or configure the FPGA.
Prototype Area This through-hole area is not connected to the FPGA. You can use this
area to connect or solder additional components.
Power Supply
J1 USB connector Connects a USB cable to a power source.
Chapter 3: Board Components 3–3
Featured Device: MAX 10 FPGA
September 2015 Altera Corporation MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit
User Guide
Featured Device: MAX 10 FPGA
The evaluation kit features the MAX 10 FPGA 10M08SAE144C8G device (U2) in a
144-pin Plastic Enhanced Quad Flat Pack (EQFP) package.
fFor more detailed information about the MAX 10 FPGA device family, refer to the
MAX 10 FPGA Device Overview.
Configuration
The evaluation kit supports two configuration methods:
JTAG header (J10) for configuration by downloading a .sof file to the FPGA. Any
power cycling of the FPGA or reconfiguration will power up the FPGA to a blank
state.
JTAG header (J10) for programming of the on-die FPGA Configuration Flash
Memory (CFM) via a .pof file. Any power cycling of the FPGA or reconfiguration
will power up the FPGA in self-configuration mode, using the files stored in the
CFM.
FPGA Programming over External USB-Blaster
The JTAG header provides a method for configuring the FPGA (U2) using an external
USB-Blaster™, USB-Blaster II, or Ethernet Blaster download cable with the Quartus II
Programmer running on a PC. The external download cable connects to the board
through the JTAG header (J10).
Configuring the FPGA Using the Quartus II Programmer
You can use the Quartus II Programmer to configure the FPGA with a .sof. Before
configuring the FPGA, ensure that the Quartus II Programmer and the USB-Blaster
driver are installed on the host computer, the USB cable is connected to the evaluation
kit, power to the board is on, and no other applications that use the JTAG chain are
running.
1To successfully use the USB-Blaster cable, disconnect it before power cycling the
board. After you power cycled the board, then reconnect the USB-Blaster cable.
To configure the MAX 10 FPGA FPGA, perform the following steps:
1. Start the Quartus II Programmer.
2. Click Auto Detect to display the devices in the JTAG chain.
Table 3–2. MAX 10 FPGA Component Reference and Manufacturing Information
Board
Reference Description Manufacturer Manufacturing
Part Number
Manufacturer
Website
U2
10M08SAE144C8G, (or ES
variant) Plastic Enhanced Quad
Flat Pack (EQFP), 144 pins, 20
mm x 20mm
Altera Corporation 10M08SAE144C8GES www.altera.com/max10
3–4 Chapter 3: Board Components
Configuration
MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit September 2015 Altera Corporation
User Guide
3. Click Add File and select the path to the desired .sof.
4. Turn on the Program/Configure option for the added file.
5. Click Start to download the selected file to the FPGA. Configuration is complete
when the progress bar reaches 100%.
The Quartus II Convert Programming File (CPF) GUI can be used to generate a .pof
file that can use for internal configuration. You can directly program the MAX 10
device’s flash which included Configuration Flash Memory (CFM) and User Flash
Memory (UFM) by using a download cable with the Quartus II software programmer.
Selecting Internal Configuration Scheme
For all MAX 10 devices except 10M02 device, there are total of 5 different modes can
be selected when using Internal Configuration. The internal configuration scheme
needs to be selected before design compilation.
To select the configuration mode, follow these steps:
1. Open the Quartus II software and load a project using MAX 10 device family.
2. On the Assignments menu, click Settings. The Settings dialog box appears.
3. In the Category list, select Device. The Device page appears.
4. Click Device and Pin Options.
5. In the Device and Pin Options dialog box, click the Configuration tab.
6. In the Configuration Scheme list, select Internal Configuration.
7. In the Configuration Mode list, select 1 out of 5 configuration modes except
10M02 device, which has only 2 modes available.
8. Turn on Generate compressed bitstreams if needed.
9. Click OK.
Generating a .pof File with ICB Settings
To generate a .pof file from a .sof file for internal configuration, follow these steps:
1. On the File menu, click Convert Programming Files.
2. Under Output programming file, select Programmer Object File (.pof) in the
Programming file type list.
3. In the Mode list, select Internal Configuration.
Chapter 3: Board Components 3–5
Configuration
September 2015 Altera Corporation MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit
User Guide
4. To set the ICB settings, click Option/Boot Info button. An ICB setting dialog box
will appear.
Several ICB settings can be set through the ICB setting dialog box, including:
Power on Reset Scheme: Instant On, Fast POR Delay or Slow POR Delay.
Enable user IOs week pull up during configuration check box.
Enable the JTAG Security check box.
Verify Protect check box.
Enable watchdog for dual boot and watching value (initially grayed out, after
add 2 sof page with 2 design that compiled with Dual Compressed Internal
Images, the watchdog setting will then be enable).
User Flash Memory settings.
5. In the File name box, specify the file name for the programming file you want to
create.
6. To generate a Memory Map File (.map), turn on Create Memory Map File (Auto
generate output_file.map). In the .map file, not only will show the address of the
CFM and UFM, but also will contain the information of the ICB setting that user
set through the Option/Boot Info dialog box.
7. You can add an SRAM Object File (.sof) through Input files to convert list. The
maximum sof page is two.
8. After set all the desirable settings, click Generate to generate related programming
file.
unsung-1mm”; 1mm. pm... um um j anflmuhwmm Ill-IMP!“ ”' Device 2 n. m a... mu. ..,..., ii In... m.” mmhmmyflmw.“ xmum mun mun r . r nmm: mi 17 Devlte 3 In , X um WWI_W W amt-£5 “WIN m P W 9 am.“ um v ran-warn] .1 amp. 1mm 4"” LI I I hum mlmlws Imus nun-amass
3–6 Chapter 3: Board Components
Clock Circuitry
MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit September 2015 Altera Corporation
User Guide
Programming Internal Flash Memory
After generating the .pof file, Quartus II Programmer can be used to program the
internal flash memory through JTAG connection. The following shows an example of
the Quartus II Programmer.
There are 2 scenarios when using the Quartus II Programmer to program a .pof file
into MAX 10 devices:
1. For Device 2, the Programmer will just erase and configure CFM and UFM sector
in the internal flash memory, but the ICB setting will be preserved. However,
before starting the programming, the makes sure the ICB setting in the device and
the ICB setting in the .pof file are the same. If both ICB settings are different, the
Programmer still erases and programs the full internal memory including the ICB
setting, even though only CFM and UFM are selected in the Programmer.
2. For Device 3, the Programmer will erase and program full internal memory, which
includes the ICB setting, CFM, and UFM.
Before enabling real-time ISP for internal flash memory programming, you need to
ensure the MAX 10 FPGA is in user mode, otherwise the programming process will
fail.
Clock Circuitry
General-Purpose Clock
One general-purpose clock is provided to the FPGA global clock inputs for general
FPGA design. The clock source is from the following component:
A 50-MHz oscillator to the clock input
CLK0p
of bank 2.
Figure 3–2. Quartus II Programmer
Chapter 3: Board Components 3–7
Arduino Connectors
September 2015 Altera Corporation MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit
User Guide
Figure 3–3 shows the general purpose clock going in to the evaluation kit.
Arduino Connectors
Arduino connectors J3, J4, and J5 connect to the MAX 10 FPGA. Any analog inputs
signals sourced through the Arduino header J4 are first filtered by the evaluation
boards op-amp based circuit. This circuit scales the maximum allowable voltage per
the Arduino specification (5.0V) to the maximum allowable voltage per the MAX 10
FPGA ADC IP block (2.5V).
fYou can download an example design with pin locations and assignments completed
according to the following table from the Altera Design Store. In the MAX 10 FPGA
Evaluation Kit, under Design Examples, click MAX 10 Evaluation Kit Baseline
Pinout.
Figure 3–3. MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit General Purpose Clock
ICS8304
CLKBUF
MAX 10
FPGA
(U2)
50 MHz
Table 3–3. Arduino Connector Pin Assignments, Signal Names and Functions (Part 1 of 2)
Board
Reference Schematic Signal Name MAX 10 FPGA
Device Pin Number Description
J3.1
ANALOG_VREF
5 Arduino analog Vref input
J3.2
GND
Arduino GND input
J3.3
ARDUINO_IO13
70 Arduino digital I/O input to FPGA
J3.4
ARDUINO_IO12
69 Arduino digital I/O input to FPGA
J3.5
ARDUINO_IO11
66 Arduino digital I/O input to FPGA
J3.6
ARDUINO_IO10
65 Arduino digital I/O input to FPGA
J3.7
ARDUINO_IO9
64 Arduino digital I/O input to FPGA
J3.8
ARDUINO_IO8
62 Arduino digital I/O input to FPGA
J4.1
ARDUINO_A0
6
Arduino analog channel input through the op-amp
filter circuit to the FPGA ADC IP input channel
ADCIN1
J4.2
ARDUINO_A1
7
Arduino analog channel input through the op-amp
filter circuit to the FPGA ADC IP input channel
ADC1IN2
J4.3
ARDUINO_A2
8
Arduino analog channel input through the op-amp
filter circuit to the FPGA ADC IP input channel
ADC1IN3
J4.4
ARDUINO_A3
10
Arduino analog channel input through the op-amp
filter circuit to the FPGA ADC IP input channel
ADC1IN4
3–8 Chapter 3: Board Components
General User Input/Output
MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit September 2015 Altera Corporation
User Guide
General User Input/Output
This section describes the user I/O interface to the FPGA:
User-defined DIP switch
User-defined LEDs
User-Defined DIP Switch
Board reference SW3 is a 6-pin DIP switch. Switches 1 through 5 are user-defined, and
provide additional FPGA input control. When the switch is in the OPEN or OFF
position, a logic 1 is selected. When the switch is in the CLOSED or ON position, a
logic 0 is selected. There is no board-specific function for these switches.
J4.5
ARDUINO_A4
11
Arduino analog channel input through the op-amp
filter circuit to the FPGA ADC IP input channel
ADC1IN5
J4.6
ARDUINO_A5
12
Arduino analog channel input through the op-amp
filter circuit to the FPGA ADC IP input channel
ADC1IN6
J4.7
ARDUINO_A6
13
Arduino analog channel input through the op-amp
filter circuit to the FPGA ADC IP input channel
ADC1IN7
J4.8
ARDUINO_A7
14
Arduino analog channel input through the op-amp
filter circuit to the FPGA ADC IP input channel
ADC1IN8
J5.1
ARDUINO_IO7
86 Arduino digital I/O input to FPGA
J5.2
ARDUINO_IO6
84 Arduino digital I/O input to FPGA
J5.3
ARDUINO_IO5
81 Arduino digital I/O input to FPGA
J5.4
ARDUINO_IO4
79 Arduino digital I/O input to FPGA
J5.5
ARDUINO_IO3
77 Arduino digital I/O input to FPGA
J5.6
ARDUINO_IO2
76 Arduino digital I/O input to FPGA
J5.7
ARDUINO_IO1
75 Arduino digital I/O input to FPGA
J5.8
ARDUINO_IO0
74 Arduino digital I/O input to FPGA
Table 3–3. Arduino Connector Pin Assignments, Signal Names and Functions (Part 2 of 2)
Board
Reference Schematic Signal Name MAX 10 FPGA
Device Pin Number Description
Chapter 3: Board Components 3–9
Power Supply
September 2015 Altera Corporation MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit
User Guide
Table 34 lists the user-defined DIP switch schematic signal names and their
corresponding MAX 10 FPGA pin numbers.
User-Defined LEDs
The development board includes five user-defined LEDs. Board references D1
through D5 are user LEDs that allow status and debugging signals to be driven to the
LEDs from the designs loaded into the MAX 10 FPGA device. The LEDs illuminate
when a logic 0 is driven, and turns off when a logic 1 is driven. There is no
board-specific function for these LEDs.
Table 35 lists the user-defined LED schematic signal names and their corresponding
MAX 10 FPGA pin numbers.
Power Supply
The development board is powered up through a USB cable. The green LED
illuminates when the board is powered up.
Power Measurement
In order to measure the actual power of the FPGA, there are test pads on the board to
be used as probe points for multi-meter probes. The user can measure the current and
using the equation P = R x I2. (Power = Resistance x Current Squared), calculate the
power dissipation.
Table 3–4. User-Defined DIP Switch Schematic Signal Names and Functions
Board Reference
SW3 Schematic Signal Name I/O Standard MAX 10 FPGA Device Pin Number
1
Switch 1
3.3-V 120
2
Switch 2
3.3-V 124
3
Switch 3
3.3-V 127
4
Switch 4
3.3-V 130
5
Switch 5
3.3-V 131
Table 3–5. User-Defined LED Schematic Signal Names and Functions
Board Reference Schematic Signal Name I/O Standard MAX 10 FPGA Device Pin Number
D1
LED1
2.0-V 132
D2
LED2
2.0-V 134
D3
LED3
2.0-V 135
D4
LED4
2.0-V 140
D5
LED5
2.0-V 141
do
3–10 Chapter 3: Board Components
Power Supply
MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit September 2015 Altera Corporation
User Guide
Test pads TP2 and TP3 are used to measure the current consumed by the FPGA core.
Test pads TP4 and TP5 are used to measure the current consumed by all of the FPGA's
I/O banks. All the other test pads are used to verify the voltage levels of various
nodes on the board.
Power Distribution System
Figure 3–4 shows the power distribution system on the development board.
Temperature Sense
The ADCs provide the devices with built-in capability for on-die temperature
monitoring and external analog signal conversion.
Temperature sensing mode—monitors external temperature data input with a
sampling rate of up to 50 kilosamples per second. In dual ADC devices, only the first
ADC block contains the temperature sensing diode.
fFor more information on the ADC, refer to the MAX 10 FPGA Device Overview.
Table 3–6. Power Measurement Details
Test Pad #’s Measuring Description Expected Value
TP2 - TP3 FPGA core
current
Power calculation for FPGA Vcc-core power consumption.
Resistor R1 = 0.1 ohms. Current measured by user's multi-meter. ___ mWatts
TP4 - TP5 FPGA I/O
current
Power calculation for FPGA Vcc-io power consumption.
Resistor R4 = 0.1 ohms. Current measured by user's multi-meter. ___ mWatts
Test Pad #’s Measuring Description Expected Value
TP1 Board input
voltage Verify the USB input voltage 5.0-volts
TP6 Analog
voltage Verify the proper voltage required by the FPGA Vcca inputs 3.3-volts
TP7 Analog GND Verify the proper voltage required by the FPGA ADC IP block GND
inputs 0-volts
TP8 Digital GND Verify the proper voltage required by the FPGA digital GND inputs 0-volts
TP9 Digital GND Verify the proper voltage required by the FPGA digital GND inputs 0-volts
Figure 3–4. Power Distribution System
5V VCC_CORE
3.3V
VCC_IO
EP5388QI
September 2015 Altera Corporation MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit
User Guide
Additional Information
This chapter provides additional information about the document and Altera.
Document Revision History
The following table shows the revision history for this document.
How to Contact Altera
To locate the most up-to-date information about Altera products, refer to the
following table.
Typographic Conventions
The following table shows the typographic conventions this document uses.
Date Version Changes
September 2015 1.2
Corrected sense of switches in “User-Defined DIP Switch” on page 3–8.
Added link to Altera Design Store in “Arduino Connectors” on page 3–7
October 2014 1.1 Corrected FPGA pin number for SW3.2 from 121 to 124.
September 2014 1.0 Initial release.
Contact (1) Contact Method Address
Technical support Website www.altera.com/support
Technical training Website www.altera.com/training
Email custrain@altera.com
Product literature Website www.altera.com/literature
Nontechnical support (general) Email nacomp@altera.com
(software licensing) Email authorization@altera.com
Note to Table:
(1) You can also contact your local Altera sales office or sales representative.
Visual Cue Meaning
Bold Type with Initial Capital
Letters
Indicate command names, dialog box titles, dialog box options, and other GUI
labels. For example, Save As dialog box. For GUI elements, capitalization matches
the GUI.
bold type
Indicates directory names, project names, disk drive names, file names, file name
extensions, software utility names, and GUI labels. For example, \qdesigns
directory, D: drive, and chiptrip.gdf file.
Italic Type with Initial Capital Letters Indicate document titles. For example, Stratix IV Design Guidelines.
DI?
Info–2 Additional Information
Typographic Conventions
MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit September 2015 Altera Corporation
User Guide
italic type
Indicates variables. For example, n + 1.
Variable names are enclosed in angle brackets (< >). For example, <file name> and
<project name>.pof file.
Initial Capital Letters Indicate keyboard keys and menu names. For example, the Delete key and the
Options menu.
“Subheading Title” Quotation marks indicate references to sections in a document and titles of
Quartus II Help topics. For example, “Typographic Conventions.”
Courier type
Indicates signal, port, register, bit, block, and primitive names. For example,
data1
,
tdi
, and
input
. The suffix
n
denotes an active-low signal. For example,
resetn
.
Indicates command line commands and anything that must be typed exactly as it
appears. For example,
c:\qdesigns\tutorial\chiptrip.gdf
.
Also indicates sections of an actual file, such as a Report File, references to parts of
files (for example, the AHDL keyword
SUBDESIGN
), and logic function names (for
example,
TRI
).
r An angled arrow instructs you to press the Enter key.
1., 2., 3., and
a., b., c., and so on
Numbered steps indicate a list of items when the sequence of the items is important,
such as the steps listed in a procedure.
Bullets indicate a list of items when the sequence of the items is not important.
1The hand points to information that requires special attention.
h The question mark directs you to a software help system with related information.
f The feet direct you to another document or website with related information.
m The multimedia icon directs you to a related multimedia presentation.
cA caution calls attention to a condition or possible situation that can damage or
destroy the product or your work.
w A warning calls attention to a condition or possible situation that can cause you
injury.
The envelope links to the Email Subscription Management Center page of the Altera
website, where you can sign up to receive update notifications for Altera documents.
The feedback icon allows you to submit feedback to Altera about the document.
Methods for collecting feedback vary as appropriate for each document.
Visual Cue Meaning
C€
Additional Information Info–3
Compliance and Conformity Statements
September 2015 Altera Corporation MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit
User Guide
Compliance and Conformity Statements
CE EMI Conformity Caution
This evaluation kit is delivered conforming to relevant standards mandated by
Directive 2004/108/EC. Because of the nature of programmable logic devices, it is
possible for the user to modify the kit in such a way as to generate electromagnetic
interference (EMI) that exceeds the limits established for this equipment. Any EMI
caused as the result of modifications to the delivered material is the responsibility of
the user.
Info–4 Additional Information
Compliance and Conformity Statements
MAX 10 FPGA (10M08S, 144-EQFP) Evaluation Kit September 2015 Altera Corporation
User Guide