o Microsemi
5
3 – Installing Programmer Hardware
Installing USB Drivers for the FlashPro4/3x/3 and Low Cost
Programming Stick (LCPS) for IGLOO, ProASIC3 and Fusion
Device Programmers
To connect a single FlashPro4/3x/3/LCPS to your PC using a USB port:
1. After installing the software successfully, connect one end of the USB cable to the FlashPro4/3x/
3/LCPS device programmer and the other end to your PC USB port.
Depending on your operating system, the Found Hardware Wizard opens during the installation.
This occurs because FlashPro4/3x/3 and the LCPS require a software driver for the programmer.
If the Found Hardware Wizard does not open then your drivers were installed successfully.
2. The Found New Hardware Wizard may ask you to specify the driver location from the Files
Needed dialog box. If so, click the Browse button to navigate to your driver (if necessary). Once
the file location is in the Copy Files From text box, click OK.
If FlashPro was installed as part of the Libero IDE default installation, the drivers are located at C:/
Libero/Designer/Drivers/<DriverDirectory>, where <DriverDirectory> corresponds to the directory
assigned by your operating system. If you installed standalone FlashPro your drivers location
depends on your install directory and operating system.
3. If you are using the x86 version of Windows (XP, Vista, or Windows 7), the Hardware Installation
box may display a warning message regarding hardware testing. If you see the warning message
click Continue Anyway. Click Finish to complete the hardware installation process. If the Found
New Hardware Wizard starts again, repeat the steps to complete your hardware installation.
To connect multiple FlashPro4/3x/3/LCPSs using a powered USB hub:
1. Make sure your hub is a powered USB hub. Only powered USB hubs can be used.
2. Connect the USB hub to the PC. If the powered USB hub is not already connected, then follow
the instructions for the hub setup and connect the cable from the hub to the PC.
3. Connect programmer to powered USB hub.
4. Connect one end of the USB cable to the programmer's USB connector. Plug the other end of the
cable into a free port on the USB hub.
5. After you have successfully installed the driver, the amber LEDs activate and the power LED
marked ON remains illuminated, indicating a connection to a powered USB port. The ACTIVITY
LED turns off after 2 seconds.
6. Repeat steps 3-4 for each programmer you wish to add.
Note: USB is hot-swappable, which means you do not have to power down the PC when plugging/
unplugging the FlashPro4/3x/3LCPS programmer.
Do not unplug the programmer while the programmer is performing a programming
sequence.
FlashPro4/3x/3/LCPS Troubleshooting
If using FlashPro4, the minimum version of Libero IDE or FlashPro software required is v8.6 Service
Pack 1. You must have Libero IDE v8.6 SP1 or FlashPro v8.6 SP1 to use FlashPro4.
When installing/using a FlashPro4/3x/3/LCPS programmer for the first time, the Windows device wizard
may not always find the driver automatically. In this case you may have to use the Install Drivers wizard.
If FlashPro was installed as part of the Libero IDE default installation, the drivers are located at C:/Libero/
Designer/Drivers/<DriverDirectory>, where <DriverDirectory> corresponds to the directory assigned by