Code Download

ram.vhd

Features

Introduction

This details a single port RAM circuit, written in VHDL.  This memory component outputs data from the memory address specified and also writes input data to this address if a write enable is asserted.  It was designed using Quartus Prime, version 17.0.0.  Resource requirements depend on the implementation.  Figure 1 illustrates a typical example of the RAM integrated into a system.

Figure 1.  Example Implementation

Architecture

This RAM uses a write-before-read architecture.  During a write cycle, the RAM writes the data before reading it on the output port, so the data shown on the output port is the same as that being written, rather than the old data that is being overwritten.

Configuring the RAM

The RAM is configured by setting the GENERIC parameters in the ENTITY.  Table 1 describes the parameters.

Table 1.  Generic Descriptions

GenericData TypeDefaultDescription
d_widthinteger8The width of each data word
sizeinteger64

The number of data words the memory can store

Port Descriptions

Table 2 describes the RAM’s ports.

Table 2.  Port Descriptions

PortWidthModeData TypeInterfaceDescription
clk1instandard logicuser logicSystem clock
wr_ena1instandard logicuser logicWrite enable: synchronously writes data on data_in port to the memory location specified on addr port when ‘1’
addrM^inintegeruser logicAddress of memory location to access
data_inN*instandard logic vectoruser logicData to be written to memory location addr if wr_ena is asserted
data_outN*outstandard logic vectoruser logicData currently stored in memory location addr

Notes
* N is the specified width of a data word, set by the d_width generic in the entity
^ M is the required width for an integer equal to the memory size, set by the size generic in the entity

Conclusion

This programmable logic RAM is a simple, single port memory component that outputs data from the specified memory address and, if a write enable is asserted, writes input data to this address.  The number of memory locations and the data width are both configurable.

Contact

Comments, feedback, and questions can be sent to eewiki@digikey.com.