Page tree
Skip to end of metadata
Go to start of metadata

You are viewing an old version of this page. View the current version.

Compare with Current View Page History

« Previous Version 192 Next »

This is a page about TI's Cortex-A8 based; BeagleBoard.

Availability

Boards:
BeagleBoard xM at Digi-Key

Basic Requirements

ARM Cross Compiler: GCC

This is a pre-built (64bit) version of Linaro GCC that runs on generic linux, sorry (32bit) x86 users, it's time to upgrade...
Download/Extract:

~/
wget -c https://releases.linaro.org/components/toolchain/binaries/6.4-2017.11/arm-linux-gnueabihf/gcc-linaro-6.4.1-2017.11-x86_64_arm-linux-gnueabihf.tar.xz
tar xf gcc-linaro-6.4.1-2017.11-x86_64_arm-linux-gnueabihf.tar.xz
export CC=`pwd`/gcc-linaro-6.4.1-2017.11-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-

Test Cross Compiler:

~/
${CC}gcc --version
arm-linux-gnueabihf-gcc (Linaro GCC 6.4-2017.11) 6.4.1 20171012
Copyright (C) 2017 Free Software Foundation, Inc.
This is free software; see the source for copying conditions.  There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

Bootloader: U-Boot

Das U-Boot – the Universal Boot Loader: http://www.denx.de/wiki/U-Boot
eewiki.net patch archive: https://github.com/eewiki/u-boot-patches
Download:

~/
git clone https://github.com/u-boot/u-boot
cd u-boot/
git checkout v2018.01 -b tmp

Patches:

~/u-boot
wget -c https://rcn-ee.com/repos/git/u-boot-patches/v2018.01/0001-omap3_beagle-uEnv.txt-bootz-n-fixes.patch
 
patch -p1 < 0001-omap3_beagle-uEnv.txt-bootz-n-fixes.patch

Configure and Build:

~/u-boot
make ARCH=arm CROSS_COMPILE=${CC} distclean
make ARCH=arm CROSS_COMPILE=${CC} omap3_beagle_defconfig
make ARCH=arm CROSS_COMPILE=${CC}

Linux Kernel

This script will build the kernel, modules, device tree binaries and copy them to the deploy directory.
Download:

~/
git clone https://github.com/RobertCNelson/armv7-multiplatform
cd armv7-multiplatform/

For v4.9.x (Longterm 4.9.x):

~/armv7-multiplatform/
git checkout origin/v4.9.x -b tmp

For v4.9.x-rt (Longterm 4.9.x + Real-Time Linux):

~/armv7-multiplatform/
git checkout origin/v4.9.x-rt -b tmp

For v4.14.x (Longterm 4.14.x):

~/armv7-multiplatform/
git checkout origin/v4.14.x -b tmp

For v4.14.x-rt (Longterm 4.14.x + Real-Time Linux):

~/armv7-multiplatform/
git checkout origin/v4.14.x-rt -b tmp

For v4.15.x (Stable):

~/armv7-multiplatform/
git checkout origin/v4.15.x -b tmp

For v4.16.x (Prepatch):

~/armv7-multiplatform/
git checkout origin/v4.16.x -b tmp

Build:

~/armv7-multiplatform/
./build_kernel.sh

Root File System

Debian 9

User

Password

debian

temppwd

root

root

Download:

~/
wget -c https://rcn-ee.com/rootfs/eewiki/minfs/debian-9.3-minimal-armhf-2017-12-09.tar.xz

Verify:

~/
sha256sum debian-9.3-minimal-armhf-2017-12-09.tar.xz
5120fcfb8ff8af013737fae52dc0a7ecc2f52563a9aa8f5aa288aff0f3943d61  debian-9.3-minimal-armhf-2017-12-09.tar.xz

Extract:

~/
tar xf debian-9.3-minimal-armhf-2017-12-09.tar.xz

Ubuntu 16.04 LTS

User

Password

ubuntu

temppwd

Download:

~/
wget -c https://rcn-ee.com/rootfs/eewiki/minfs/ubuntu-16.04.3-minimal-armhf-2017-12-09.tar.xz

Verify:

~/
sha256sum ubuntu-16.04.3-minimal-armhf-2017-12-09.tar.xz
cacc1a8c56649808e3bc27ca58f94dbe817b9e86e660780009a3535709823cc1  ubuntu-16.04.3-minimal-armhf-2017-12-09.tar.xz

Extract:

~/
tar xf ubuntu-16.04.3-minimal-armhf-2017-12-09.tar.xz

Setup microSD card

For these instruction we are assuming, DISK=/dev/mmcblk0, lsblk is very useful for determining the device id.

export DISK=/dev/mmcblk0

Erase partition table/labels on microSD card:

sudo dd if=/dev/zero of=${DISK} bs=1M count=20

Create Partition Layout:
With util-linux v2.26, sfdisk was rewritten and is now based on libfdisk.

sudo sfdisk --version
sfdisk from util-linux 2.27.1
sfdisk >= 2.26.x
sudo sfdisk ${DISK} <<-__EOF__
1M,12M,0xE,*
13M,,,-
__EOF__
sfdisk <= 2.25.x
sudo sfdisk --unit M ${DISK} <<-__EOF__
1,12,0xE,*
13,,,-
__EOF__

Format Partition:

for: DISK=/dev/mmcblk0
sudo mkfs.vfat -F 16 -n BOOT ${DISK}p1
sudo mkfs.ext4 -L rootfs ${DISK}p2
 
for: DISK=/dev/sdX
sudo mkfs.vfat -F 16 -n BOOT ${DISK}1
sudo mkfs.ext4 -L rootfs ${DISK}2

Mount Partition:
On most systems these partitions may will be auto-mounted...

sudo mkdir -p /media/boot/
sudo mkdir -p /media/rootfs/
 
for: DISK=/dev/mmcblk0
sudo mount ${DISK}p1 /media/boot/
sudo mount ${DISK}p2 /media/rootfs/
 
for: DISK=/dev/sdX
sudo mount ${DISK}1 /media/boot/
sudo mount ${DISK}2 /media/rootfs/

Install Bootloader

Copy MLO/u-boot.img to the boot partition

~/
sudo cp -v ./u-boot/MLO /media/boot/
sudo cp -v ./u-boot/u-boot.img /media/boot/

Install Kernel and Root File System

To help new users, since the kernel version can change on a daily basis. The kernel building scripts listed on this page will now give you a hint of what kernel version was built.

-----------------------------
Script Complete
eewiki.net: [user@localhost:~$ export kernel_version=4.X.Y-Z]
-----------------------------

Copy and paste that "export kernel_version=4.X.Y-Z" exactly as shown in your own build/desktop environment and hit enter to create an environment variable to be used later.

export kernel_version=4.X.Y-Z

Copy Root File System

~/
sudo tar xfvp ./*-*-*-armhf-*/armhf-rootfs-*.tar -C /media/rootfs/
sync
sudo chown root:root /media/rootfs/
sudo chmod 755 /media/rootfs/

Set uname_r in /boot/uEnv.txt

~/
sudo sh -c "echo 'uname_r=${kernel_version}' >> /media/rootfs/boot/uEnv.txt"

Copy Kernel Image

Kernel Image:

~/
sudo cp -v ./armv7-multiplatform/deploy/${kernel_version}.zImage /media/rootfs/boot/vmlinuz-${kernel_version}

Copy Kernel Device Tree Binaries

~/
sudo mkdir -p /media/rootfs/boot/dtbs/${kernel_version}/
sudo tar xfv ./armv7-multiplatform/deploy/${kernel_version}-dtbs.tar.gz -C /media/rootfs/boot/dtbs/${kernel_version}/

Copy Kernel Modules

~/
sudo tar xfv ./armv7-multiplatform/deploy/${kernel_version}-modules.tar.gz -C /media/rootfs/

File Systems Table (/etc/fstab)

sudo sh -c "echo '/dev/mmcblk0p2  /  auto  errors=remount-ro  0  1' >> /media/rootfs/etc/fstab"
sudo sh -c "echo '/dev/mmcblk0p1  /boot/uboot  auto  defaults  0  2' >> /media/rootfs/etc/fstab"

Remove microSD/SD card

sync
sudo umount /media/boot
sudo umount /media/rootfs

Comments

Comments, feedback, and questions can be sent to: eewiki@digikey.com
Please use the Digi-Key's TechForum: TechForum

  • No labels