This is a page about TI's BeagleBoard and BeagleBoard xM.
ARM Cross Compiler: GCC
This is a pre-built (32bit) version of Linaro GCC that runs on generic linux, so 64bit users need to make sure they have installed the 32bit libraries for their distribution.
Download/Extract:
wget -c https://releases.linaro.org/13.12/components/toolchain/binaries/gcc-linaro-arm-linux-gnueabihf-4.8-2013.12_linux.tar.xz tar xJf gcc-linaro-arm-linux-gnueabihf-4.8-2013.12_linux.tar.xz export CC=`pwd`/gcc-linaro-arm-linux-gnueabihf-4.8-2013.12_linux/bin/arm-linux-gnueabihf-
Test:
If this test fails, verify that you have the 32bit libraries installed on your development system.
${CC}gcc --version arm-linux-gnueabihf-gcc (crosstool-NG linaro-1.13.1-4.8-2013.12 - Linaro GCC 2013.11) 4.8.3 20131202 (prerelease) Copyright (C) 2013 Free Software Foundation, Inc. This is free software; see the source for copying conditions. There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
Bootloader: U-Boot
Das U-Boot -- the Universal Boot Loader http://www.denx.de/wiki/U-Boot
Download:
git clone git://git.denx.de/u-boot.git cd u-boot/ git checkout v2014.01 -b tmp
Revert: ARM: omap3: Implement dpll5 (HSUSB clk) workaround for OMAP36xx/AM/DM37xx according to errata sprz318e. (unless your using v3.12.x/v3.13.x kernel branch)
git revert --no-edit a704a6d615179a25f556c99d31cbc4ee366ffb54
Patches:
wget -c https://raw.github.com/eewiki/u-boot-patches/master/v2014.01/0001-omap3_beagle-uEnv.txt-bootz-n-fixes.patch patch -p1 < 0001-omap3_beagle-uEnv.txt-bootz-n-fixes.patch
Configure and Build:
make ARCH=arm CROSS_COMPILE=${CC} distclean make ARCH=arm CROSS_COMPILE=${CC} omap3_beagle_config make ARCH=arm CROSS_COMPILE=${CC}
Linux Kernel
This script will build the kernel and modules and copy them to the deploy directory.
Old Board File tree
Download:
git clone git://github.com/RobertCNelson/stable-kernel.git cd stable-kernel/
For v3.9.x:
git checkout origin/v3.9.x -b tmp ./build_kernel.sh
Device Tree
Download:
git clone git://github.com/RobertCNelson/armv7-multiplatform.git cd armv7-multiplatform
Checkout v3.13.x branch and build:
git checkout origin/v3.13.x -b tmp ./build_kernel.sh
Root File System
Debian 7
This image contains, systemd: https://wiki.debian.org/systemd to enable, add to uEnv.txt:
optargs=quiet init=/lib/systemd/systemd
Download:
wget -c https://rcn-ee.net/deb/minfs/wheezy/debian-7.3-minimal-armhf-2013-12-18.tar.xz
Verify:
md5sum debian-7.3-minimal-armhf-2013-12-18.tar.xz a9b907cd03d46433782f851a20d74ee4 debian-7.3-minimal-armhf-2013-12-18.tar.xz
Extract:
tar xf debian-7.3-minimal-armhf-2013-12-18.tar.xz
Ubuntu 13.10
Download:
wget -c https://rcn-ee.net/deb/minfs/saucy/ubuntu-13.10-minimal-armhf-2013-12-18.tar.xz
Verify:
md5sum ubuntu-13.10-minimal-armhf-2013-12-18.tar.xz fa80534e0b1091afebbb6ce9ae65a0ff ubuntu-13.10-minimal-armhf-2013-12-18.tar.xz
Extract:
tar xf ubuntu-13.10-minimal-armhf-2013-12-18.tar.xz
Root File System (small flash)
A Root File System around 64Mb in size, for flash applications.
Debian 7 (small flash)
This image contains, systemd: https://wiki.debian.org/systemd to enable, add to uEnv.txt:
optargs=quiet init=/lib/systemd/systemd
Download:
wget -c https://rcn-ee.net/deb/barefs/wheezy/debian-7.3-bare-armhf-2013-12-18.tar.xz
Verify:
md5sum debian-7.3-bare-armhf-2013-12-18.tar.xz 1673993d8cbffe9dc95f157306e51657 debian-7.3-bare-armhf-2013-12-18.tar.xz
Extract:
tar xf debian-7.3-bare-armhf-2013-12-18.tar.xz
Setup microSD/SD card
For these instruction, we are assuming: DISK=/dev/mmcblk0, "lsblk" is very useful for determining the device id.
export DISK=/dev/mmcblk0
Erase microSD/SD card:
sudo dd if=/dev/zero of=${DISK} bs=1M count=16
Create Partition Layout:
sudo sfdisk --in-order --Linux --unit M ${DISK} <<-__EOF__ 1,48,0xE,* ,,,- __EOF__
Format Partitions:
for: DISK=/dev/mmcblk0 sudo mkfs.vfat -F 16 ${DISK}p1 -n boot sudo mkfs.ext4 ${DISK}p2 -L rootfs for: DISK=/dev/sdX sudo mkfs.vfat -F 16 ${DISK}1 -n boot sudo mkfs.ext4 ${DISK}2 -L rootfs
Mount Partitions:
On some systems, these partitions may be auto-mounted...
sudo mkdir -p /media/boot/ sudo mkdir -p /media/rootfs/ for: DISK=/dev/mmcblk0 sudo mount ${DISK}p1 /media/boot/ sudo mount ${DISK}p2 /media/rootfs/ for: DISK=/dev/sdX sudo mount ${DISK}1 /media/boot/ sudo mount ${DISK}2 /media/rootfs/
Install Bootloader
Copy MLO/u-boot.img to the boot partition
sudo cp -v ./u-boot/MLO /media/boot/ sudo cp -v ./u-boot/u-boot.img /media/boot/
uEnv.txt based bootscript
Create "uEnv.txt" boot script: (nano uEnv.txt)
#mmcroot=/dev/mmcblk0p2 ro #mmcrootfstype=ext4 rootwait fixrtc
Copy uEnv.txt to the boot partition:
sudo cp -v ./uEnv.txt /media/boot/
Install Kernel and Root File System
To help new users, since the kernel version can change on a daily basis. The kernel building scripts listed on this page will now give you a hint of what kernel version was built.
----------------------------- Script Complete eewiki.net: [user@localhost:~$ export kernel_version=3.X.Y-Z] -----------------------------
Copy and paste that "export kernel_version=3.X.Y-Z" exactly as shown in your own build/desktop environment and hit enter to create an environment variable to be used later.
export kernel_version=3.X.Y-Z
Copy Root File System
sudo tar xfvp ./*-*-*-armhf-*/armhf-rootfs-*.tar -C /media/rootfs/
Copy Kernel Files
Kernel Image:
sudo cp -v ./stable-kernel/deploy/${kernel_version}.zImage /media/boot/zImage (or if using the device tree v3.12.x branch) sudo cp -v ./armv7-multiplatform/deploy/${kernel_version}.zImage /media/boot/zImage
Kernel Device Tree Binaries (v3.12.x branch):
sudo mkdir -p /media/boot/dtbs/ sudo tar xfov ./armv7-multiplatform/deploy/${kernel_version}-dtbs.tar.gz -C /media/boot/dtbs/
Kernel Modules:
sudo tar xfv ./stable-kernel/deploy/${kernel_version}-modules.tar.gz -C /media/rootfs/ (or if using the device tree v3.12.x branch) sudo tar xfv ./armv7-multiplatform/deploy/${kernel_version}-modules.tar.gz -C /media/rootfs/
File Systems Table (/etc/fstab)
Edit: /etc/fstab
sudo nano /media/rootfs/etc/fstab
/dev/mmcblk0p2 / auto errors=remount-ro 0 1 /dev/mmcblk0p1 /boot/uboot auto defaults 0 2
Networking
Edit: /etc/network/interfaces
sudo nano /media/rootfs/etc/network/interfaces
Add:
auto lo iface lo inet loopback auto eth0 iface eth0 inet dhcp
Serial Login
Debian
Edit: /etc/inittab
sudo nano /media/rootfs/etc/inittab
Add this at the end of: /etc/inittab
T2:23:respawn:/sbin/getty -L ttyO2 115200 vt102
Ubuntu
Create new file: /etc/init/serial.conf
sudo nano /media/rootfs/etc/init/serial.conf
With this content:
start on stopped rc RUNLEVEL=[2345] stop on runlevel [!2345] respawn exec /sbin/getty 115200 ttyO2
Remove microSD/SD card:
sync sudo umount /media/boot sudo umount /media/rootfs
FAQ
No Ethernet:
- Check Power (aka use 5Volt DC Plug): The USB bus allows up to 100mA on initial connection and up to a max of 500mA can be requested by the end USB device. On the xM this is not enough to power the whole device and on the xM C there is an actual hardware switch to disable the smsc95xx usb hub/ethernet when powered by OTG (to prevent out of power crashes seen on the xM A/B with when users powered by OTG).
- Check Ethernet Cable/Plug: Is the Ethernet Cable actually plugged into the Beagle and Router?
- Check Modules: The smsc95xx kernel driver is usually built as an external module, double check that your kernel modules for this device are installed.
debian@devel:~$ find /lib/modules/`uname -r`/kernel/ | grep smsc95xx /lib/modules/3.2.26-x14/kernel/drivers/net/usb/smsc95xx.ko
debian@devel:~$ lsmod | grep smsc95xx smsc95xx 11302 0
- Reload smsc95xx kernel module (Checked all the above and the LAN LED's are still off)
sudo rmmod smsc95xx sudo modprobe smsc95xx sudo /etc/init.d/networking restart