This is a page about TI's BeagleBoard and BeagleBoard xM.
Availability:
BeagleBoard Cx at Digi-Key
BeagleBoard xM at Digi-Key
CircuitCo 7inch LCD at Digi-Key
Basic Requirements
- ARM Cross Compiler
- Bootloader
- Das U-Boot – the Universal Boot Loader http://www.denx.de/wiki/U-Boot
- Source – http://git.denx.de/?p=u-boot.git;a=summary
- Linux Kernel
- Linus's Mainline tree: http://git.kernel.org/?p=linux/kernel/git/torvalds/linux.git;a=summary
- Linux omap tree: http://git.kernel.org/?p=linux/kernel/git/tmlind/linux-omap.git
- ARM based rootfs
- Debian Squeeze: http://www.debian.org/
GCC Toolchain
wget https://launchpad.net/linaro-toolchain-binaries/trunk/2013.03/+download/gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux.tar.bz2 tar xjf gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux.tar.bz2 export CC=`pwd`/gcc-linaro-arm-linux-gnueabihf-4.7-2013.03-20130313_linux/bin/arm-linux-gnueabihf-
Bootloader
Das U-Boot – the Universal Boot Loader http://www.denx.de/wiki/U-Boot
U-Boot Download:
Download U-Boot via git:
git clone git://git.denx.de/u-boot.git cd u-boot/ git checkout v2013.04 -b tmp
U-Boot Patches:
wget https://raw.github.com/eewiki/u-boot-patches/master/v2013.04/0001-omap3_beagle-uEnv.txt-bootz-n-fixes.patch patch -p1 < 0001-omap3_beagle-uEnv.txt-bootz-n-fixes.patch
U-Boot Configure and Build:
make ARCH=arm CROSS_COMPILE=${CC} distclean make ARCH=arm CROSS_COMPILE=${CC} omap3_beagle_config make ARCH=arm CROSS_COMPILE=${CC}
Linux Kernel
Linux Build Script:
git clone git://github.com/RobertCNelson/stable-kernel.git cd stable-kernel/
For Mainline v3.9.x
git checkout origin/v3.9.x -b tmp
Run Build Script:
./build_kernel.sh
The kernel zImage and modules will be under the deploy directory.
Debian 7.0.0 (Wheezy) Root File System
Default User: debian
Password: temppwd
Root User: root
Root Password: root
wget -c http://rcn-ee.net/deb/minfs/wheezy/debian-7.0.0-minimal-armhf-2013-05-05.tar.xz
verify the image with:
md5sum debian-7.0.0-minimal-armhf-2013-05-05.tar.xz 7378ac1f20ca4857ac1994e22fd20277 debian-7.0.0-minimal-armhf-2013-05-05.tar.xz
Extract Image:
tar xJf debian-7.0.0-minimal-armhf-2013-05-05.tar.xz
Ubuntu 13.04 (Raring) Root File System
Default User: ubuntu
Password: temppwd
wget -c http://rcn-ee.net/deb/minfs/raring/ubuntu-13.04-minimal-armhf-2013-05-05.tar.xz
verify the image with:
md5sum debian-7.0.0-minimal-armhf-2013-05-05.tar.xz 952cf1f87c047653fb0f24818c8bfd26 ubuntu-13.04-minimal-armhf-2013-05-05.tar.xz
Extract Image:
tar xJf ubuntu-13.04-minimal-armhf-2013-05-05.tar.xz
Setup microSD/SD card
For these instruction, we are assuming: DISK=/dev/mmcblk0, "sudo fdisk -l" is useful for determining the device id..
export DISK=/dev/mmcblk0
Erase microSD/SD card:
sudo dd if=/dev/zero of=${DISK} bs=1024 count=1024 sudo parted --script ${DISK} mklabel msdos
Setup Boot Partition:
sudo fdisk ${DISK} << __EOF__ n p 1 +64M t e p w __EOF__
Set Boot Flag
sudo parted --script ${DISK} set 1 boot on
Format Boot Partition as vfat:
DISK=/dev/mmcblk0 sudo mkfs.vfat -F 16 ${DISK}p1 -n boot (or) DISK=/dev/sdX sudo mkfs.vfat -F 16 ${DISK}1 -n boot
Setup Root File System Partition:
sudo fdisk ${DISK} << __EOF__ n p 2 w __EOF__
Format rootfs as ext4:
DISK=/dev/mmcblk0 sudo mkfs.ext4 ${DISK}p2 -L rootfs (or) DISK=/dev/sdX sudo mkfs.ext4 ${DISK}2 -L rootfs
Mount Partitions:
Note: On most systems these partitions will be auto-mounted...
sudo mkdir -p /media/boot/ sudo mkdir -p /media/rootfs/ DISK=/dev/mmcblk0 sudo mount ${DISK}p1 /media/boot/ sudo mount ${DISK}p2 /media/rootfs/ (or) DISK=/dev/sdX sudo mount ${DISK}1 /media/boot/ sudo mount ${DISK}2 /media/rootfs/
Install Bootloaders:
Copy MLO/u-boot.img to the boot partition
sudo cp -v ./u-boot/MLO /media/boot/ sudo cp -v ./u-boot/u-boot.img /media/boot/
U-Boot user enviroment variables: uEnv.txt
Create U-Boot "uEnv.txt" boot script: (nano uEnv.txt)
#Camera: Uncomment to enable: #http://shop.leopardimaging.com/product.sc?productId=17 #camera=li5m03 #SPI: enable for userspace spi access on expansion header #buddy=spidev #LSR COM6L Adapter Board #http://eewiki.net/display/linuxonarm/LSR+COM6L+Adapter+Board #First production run has unprogramed eeprom: #buddy=lsr-com6l-adpt #LSR COM6L Adapter Board + TiWi5 #wl12xx_clk=wl12xx_26mhz #These are now set by default: uncomment/change if you need something else #defaultdisplay=dvi #dvimode=1280x720MR-16@60 #mmcroot=/dev/mmcblk0p2 ro #mmcrootfstype=ext4 rootwait fixrtc
Copy uEnv.txt to the boot partition:
sudo cp -v ./uEnv.txt /media/boot/
Install Kernel and Root File System:
To help new users, since the kernel version can change on a daily basis. The kernel building scripts in this git repo will now give you a hint of what kernel version was built.
----------------------------- Script Complete eewiki.net: [user@localhost:~$ export kernel_version=3.X.Y-Z] -----------------------------
Copy and Paste that "export kernel_version=3.X.Y-Z" exactly as shown in your own build/desktop environment:
export kernel_version=3.X.Y-Z
Copy Kernel zImage:
sudo cp -v ./stable-kernel/deploy/${kernel_version}.zImage /media/boot/zImage
Copy Kernel dtbs (Device Tree):
sudo mkdir -p /media/boot/dtbs/ sudo tar xofv ./stable-kernel/deploy/${kernel_version}-dtbs.tar.gz -C /media/boot/dtbs/
Copy Root File System:
sudo tar xfvp ./*-*-minimal-arm*-*/arm*-rootfs-*.tar -C /media/rootfs/
Copy Kernel modules:
sudo tar xfv ./stable-kernel/deploy/${kernel_version}-modules.tar.gz -C /media/rootfs/
Setup /etc/fstab:
sudo nano /media/rootfs/etc/fstab
Add:
/dev/mmcblk0p2 / auto errors=remount-ro 0 1 /dev/mmcblk0p1 /boot/uboot auto defaults 0 0
Enable Networking:
sudo nano /media/rootfs/etc/network/interfaces
Add:
auto lo iface lo inet loopback auto eth0 iface eth0 inet dhcp
Enable Serial Login:
Debian:
sudo nano /media/rootfs/etc/inittab
Add at end of file:
T2:23:respawn:/sbin/getty -L ttyO2 115200 vt102
Ubuntu:
sudo nano /media/rootfs/etc/init/serial.conf
Add:
start on stopped rc RUNLEVEL=[2345] stop on runlevel [!2345] respawn exec /sbin/getty 115200 ttyO2
Remove microSD/SD card:
sync sudo umount /media/boot sudo umount /media/rootfs
FAQ
No Ethernet:
- Check Power (aka use 5Volt DC Plug): The USB bus allows up to 100mA on initial connection and up to a max of 500mA can be requested by the end USB device. On the xM this is not enough to power the whole device and on the xM C there is an actual hardware switch to disable the smsc95xx usb hub/ethernet when powered by OTG (to prevent out of power crashes seen on the xM A/B with when users powered by OTG).
- Check Ethernet Cable/Plug: Is the Ethernet Cable actually plugged into the Beagle and Router?
- Check Modules: The smsc95xx kernel driver is usually built as an external module, double check that your kernel modules for this device are installed.
debian@devel:~$ find /lib/modules/`uname -r`/kernel/ | grep smsc95xx /lib/modules/3.2.26-x14/kernel/drivers/net/usb/smsc95xx.ko
debian@devel:~$ lsmod | grep smsc95xx smsc95xx 11302 0
- Reload smsc95xx kernel module (Checked all the above and the LAN LED's are still off)
sudo rmmod smsc95xx sudo modprobe smsc95xx sudo /etc/init.d/networking restart
Comments
Comments, feedback, and questions can be sent to eewiki@digikey.com.
[Comments Page]