Child pages
  • VGA Controller (VHDL)
Skip to end of metadata
Go to start of metadata

 

Code Downloads

VGA Controller

VGA Controller VHDL:  vga_controller.vhd

Supporting Example Material

Example hardware test image generator:  hw_image_generator.vhd

Archived complete Quartus II project using the DE2-115 development board:   vga_with_hw_test_image_v1_1.qar

Note:  If you are unfamiliar with Quartus II archives:  you can open the archive file just like a Quartus II project file.  When asked you if you want to restore it, say yes, and it places all contents of the original Quartus II project in the folder you specify.

Features

  • VHDL source code of a VGA interface controller
  • Generates the signal timing for a VGA interface
  • Configurable VGA mode (i.e. resolution and refresh rate)
  • Example implementation using a DE2-115 development board

Introduction

This details a VGA controller component that handles VGA signal timing, written in VHDL for use with CPLDs and FPGAs.  Figure 1 illustrates a typical example of the VGA controller integrated into a system.  As shown, the VGA controller requires a pixel clock at the frequency of the VGA mode being implemented.  It then derives all of the signal timing necessary to control the interface.  It outputs the current pixel coordinates to allow an image source to provide the appropriate pixel values to the video DAC, which in turn drives the VGA monitor’s analog inputs.  It also provides the sync signals for the VGA monitor.  This component was designed using Quartus II, version 12.1.  Resource requirements depend on the implementation.

Figure 1.  Example Implementation

Background

VGA is a standard interface for controlling analog monitors.  The computing side of the interface provides the monitor with horizontal and vertical sync signals, color magnitudes, and ground references.

The horizontal and vertical sync signals are 0V/5V digital waveforms that synchronize the signal timing with the monitor.  Being digital, they are provided directly by the FPGA (3.3V meets the minimum threshold for a logical high, so 3.3V can be used instead of 5V).

The color magnitudes are 0V-0.7V analog signals sent over the R, G, and B wires.  (Alternatively, the green wire can use 0.3V-1V signals that incorporate both the horizontal and vertical sync signals, eliminating the need for those lines.  This is called sync-on-green and is not addressed here.)  The three color magnitude wires are terminated with 75Ω resistors.  These lines are also terminated with 75Ω inside the monitor.  To create these analog signals, the FPGA outputs an 8-bit bus for each color to a video DAC, in this example an ADV7123 from Analog Devices.  This video DAC also requires a pixel clock to latch in these values.

The VGA interface also specifies four wires that can be used to communicate with a ROM in the monitor.  This ROM contains EDID (extended display identification data), which consists of the monitor’s parameters in a standard format.  Several communication standards exist to access this data, but in the simplest case, these lines can be left unconnected.

Connections

VGA connections use a 15 pin connector called a DB15.  Figure 2 shows the DB15 female receptacle.  Table 1 lists the pinout for the connector.

Figure 2.  VGA Female Connector (DB15 Receptacle)

Table 1.  VGA Connector Pinout and Signals

Pin

SignalDescriptionConnection
1

R

analog red, 0-0.7V

DAC output

2Ganalog green, 0-0.7V or 0.3-1V (if sync-on-green)DAC output
3Banalog blue, 0-0.7VDAC output
4EDID Interfacefunction varies depending on standard usedno connect
5GNDgeneralGND
6GNDfor RGND
7GNDfor GGND
8GND

for B

GND
9no pinor optional +5Vno connect
10GNDfor h_sync and v_syncGND
11EDID Interfacefunction varies depending on standard usedno connect
12EDID Interfacefunction varies depending on standard usedno connect
13h_synchorizontal sync, 0V/5V waveform

FPGA output

14v_syncvertical sync, 0V/5V waveformFPGA output
15EDID Interfacefunction varies depending on standard usedno connect

Signal Timing

There are a wide variety of standard VGA modes, each with a specific resolution and refresh rate.  Each mode has defined timing parameters.  The appendix lists the signal timing specifications for numerous VGA modes.  The VGA controller uses the GENERIC parameters declared in the ENTITY to set all of the timing specifications except for the pixel clock, which must be provided.

The provided example implementation of the VGA controller uses a 1920x1200 resolution with a 60Hz refresh rate, which is the maximum resolution of the monitor used.

Pixel Clock

This VGA controller requires the user to provide the pixel clock.  This can be brought into the FPGA on a dedicated clock pin or can be derived inside the FPGA using a PLL.  In the example project for the DE2-115 development board, the available 50MHz clock is input into one of the Cyclone IV FPGA's PLLs to produce a 193.16MHz pixel clock, as required by the 1920x1200 @60Hz VGA mode.

Theory of Operation

Figure 3 illustrates the timing signals produced by the VGA controller.  The controller contains two counters.  One counter increments on pixel clocks and controls the timing of the h_sync (horizontal sync) signal.  By setting it up such that the display time starts at counter value 0, the counter value equals the pixel’s column coordinate during the display time.  The horizontal display time is followed by a blanking time, which includes a horizontal front porch, the horizontal sync pulse itself, and the horizontal back porch, each of specified duration.  At the end of the row, the counter resets to start the next row.

The other counter increments as each row completes, therefore controlling the timing of the v_sync (vertical sync) signal.  Again, this is set up such that the display time starts at counter value 0, so the counter value equals the pixel’s row coordinate during the display time.  As before, the vertical display time is followed by a blanking time, with its corresponding front porch, sync pulse, and back porch.  Once the vertical blanking time completes, the counter resets to begin the next screen refresh.

A display enable is defined by the logical AND of the horizontal and vertical display times.

Using these counters, the VGA controller outputs the horizontal sync, vertical sync, display enable, and pixel coordinate signals.  The sync pulses are specified as positive or negative polarity for each VGA mode.  The GENERIC parameters h_pol (horizontal polarity) and v_pol (vertical polarity) set the polarity of the VGA controller’s h_sync and v_sync outputs, respectively.

Figure 3.  Signal Timing Diagram

Port Descriptions

Table 2 describes the VGA controller’s ports.

Table 2.  Port Descriptions

PortWidthModeData TypeInterfaceDescription
pixel_clk1instandard logicuser logicPixel clock at the frequency specified for the desired VGA mode.
reset_n1instandard logicuser logicAsynchronous active low reset.
h_sync1outstandard logicVGA monitorHorizontal sync signal.
v_sync1outstandard logicVGA monitorVertical sync signal.
disp_ena1outstandard logicuser logicDisplay enable; 1 = display time, 0 = blanking time.
row[31..0]32outintegeruser logicY pixel coordinate (i.e. row); 0 = top row, number of rows - 1 = bottom row.
column[31..0]32outintegeruser logicX pixel coordinate (i.e. column), 0 = leftmost column, number of columns - 1 = rightmost column.
n_blank1outstandard logicvideo DACDetermines if direct blanking is used.  This example permanently sets this bit to '1', so no direct blanking is used.
n_sync1outstandard logicvideo DACDetermines if sync-on-green is used.  This example permanently sets this bit to '0', so no sync-on-green is used.

Using the VGA Controller

To use the VGA Controller, simply set the GENERIC parameters in the ENTITY to values specified by the desired VGA mode.  The appendix lists the signal timing specifications for many VGA modes.  As explained above, the required pixel clock must also be provided.

In addition to the VGA Controller, the user must also provide an image source.  Images are generally provided via file in off-chip memory, but can also be provided by a file in on-chip memory or be generated by the FPGA hardware.  The example project here generates a hardware test image with the hw_image_generator.vhd file.  This VHDL takes the pixel coordinates and display enable signals from the VGA controller to output color values to the video DAC at the correct times.  The test image generated is a 600x478 pixel blue rectangle in the upper left corner of the screen, with the remainder of the screen yellow.  Figure 4 shows the resulting test image.

Figure 4.  Hardware Generated Test Image

Reset

The reset_n input port must have a logic high for the VGA controller component to operate.  A low logic level on this port asynchronously resets the component.  During reset, the component deasserts the horizontal and vertical counters, clears the pixel coordinates, and disables the display.  Once released from reset, the VGA controller resumes operation.

Conclusion

This VGA controller is a programmable logic component that accomplishes the signal timing necessary to interface with a VGA monitor.  It requires the user to provide only the pixel clock and, of course, the image source.  The VGA controller provides the horizontal and vertical sync signals, as well as the pixel coordinates and display enable needed to produce the image at the proper time.

Appendix:  VGA Timing Specifications

Table A1:  Timing Specifications for Various VGA Modes

Resolution (pixels)
Refresh Rate (Hz)Pixel Clock (MHz)Horizontal (pixel clocks)Vertical (rows)h_sync Polarityv_sync Polarity
DisplayFront PorchSync PulseBack PorchDisplayFront PorchSync PulseBack Porch
640x3507025.17564016964835037260pn
640x3508531.564032649635032360pn
640x4007025.17564016964840012235np
640x4008531.56403264964001341np
640x4806025.17564016964848010233nn
640x4807331.564024401284809229nn
640x4807531.564016641204801316nn
640x48085366405656804801325nn
640x48010043.1664040641044801325np
720x4008535.572036721084001342np
768x5766034.9676824801045761317np
768x5767242.9376832801125761321np
768x5767545.5176840801205761322np
768x5768551.8476840801205761325np
768x57610062.5776848801285761331np
800x600563680024721286001222pp
800x600604080040128886001423pp
800x6007549.580016801606001321pp
800x6007250800561206460037623pp
800x6008556.2580032641526001327pp
800x60010068.1880048881366001332np
1024x7684344.910248176567680841pp
1024x76860651024241361607683629nn
1024x76870751024241361447683629nn
1024x7687578.8102416961767681328pp
1024x7688594.5102448962087681336pp
1024x768100113.311024721121847681342np
1152x864751081152641282568641332pp
1152x86485119.651152721282008641339np
1152x864100143.471152801282088641347np
1152x8646081.621152641201848641327np
1280x10246010812804811224810241338pp
1280x10247513512801614424810241338pp
1280x102485157.512806416022410241344pp
1280x1024100190.9612809614424010241357np
1280x8006083.461280641362008001324np
1280x96060102.11280801362169601330np
1280x96072124.541280881362249601337np
1280x96075129.861280881362249601338np
1280x96085148.51280641602249601347pp
1280x960100178.991280961442409601353np
1368x7686085.861368721442167681323np
1400x105060122.6114008815224010501333np
1400x105072149.3414009615224810501340np
1400x105075155.8514009615224810501342np
1400x105085179.26140010415225610501349np
1400x1050100214.39140011215226410501358np
1440x90060106.471440801522329001328np
1600x12006016216006419230412001346pp
1600x120065175.516006419230412001346pp
1600x12007018916006419230412001346pp
1600x120075202.516006419230412001346pp
1600x120085229.516006419230412001346pp
1600x1200100280.64160012817630412001367np
1680x105060147.14168010418428810501333np
1792x134460204.8179212820032813441346np
1792x13447526117929621635213441369np
1856x139260218.318569622435213921343np
1856x1392752881856128224352139213104np
1920x120060193.16192012820833612001338np
1920x144060234192012820834414401356np
1920x144075297192014422435214401356n

p

Contact

Comments, feedback, and questions can be sent to eewiki@digikey.com.

 

  • No labels