We use cookies to provide our visitors with an optimal site experience. View our privacy notice and cookie notice to learn more about how we use cookies and how to manage your settings. By proceeding on our website you consent to the use of cookies.
Code Downloads
Accelerometer ADXL362 Pmod Controller (top-level file): pmod_accelerometer_adxl362.vhd
SPI Master (must also be included in the project): spi_master.vhd
Features
- VHDL source code of a streamlined interface to Digilent’s PmodACL2 (Pmod for Analog Devices ADXL362 Accelerometer)
- Continually outputs latest 3-axis acceleration data on 3 parallel buses
- Handles SPI communication to configure and retrieve data from the Accelerometer Pmod
- Configurable accelerometer data range
- Configurable accelerometer data rate
- Configurable system clock rate
Introduction
This details a VHDL component that handles interfacing to Digilent’s Accelerometer ADXL362 Pmod, shown in Figure 1. Figure 2 illustrates a typical example of this Accelerometer Pmod Controller integrated into a system. As shown, the Accelerometer Pmod Controller connects to the Pmod ports and executes transactions to configure the accelerometer and gather data. The data is continually updated and presented on 3 simple parallel buses (corresponding to the 3 axes), which can be connected to user logic or to output ports on the FPGA.
Figure 1. Digilent Accelerometer ADXL362 Pmod
Figure 2. Example Implementation
Theory of Operation
The Accelerometer Pmod Controller consists primarily of a state machine and an SPI Master component.
State Machine
The design uses the state machine depicted in Figure 3 to implement its operation. Upon start-up the component immediately enters the start state, where it initializes parameters used in other states. It then proceeds to the pause state. Here, it pauses for 200ns between SPI transactions. It then selects which of 3 transactions with the accelerometer to execute. The first 2 transactions are carried out by the configure state (setting the accelerometer’s data range and data rate, and then enabling measurements). At completion of each of these transactions, it returns to the pause state. Once both configuration transactions are finished, the pause state repetitively selects the 3rd transaction, proceeding to the read_data state to execute it. This state reads the accelerometer data for all 3 axes, then continues to the output_result state. The output_result state writes the data to the acceleration_x, acceleration_y, and acceleration_z output buses, then returns to the pause state. Resetting the component at any time returns it to the start state.
Figure 3. State Diagram
SPI Master
During the configure and read_data states, the state machine controls an SPI Master component to communicate with the accelerometer on the Pmod. Documentation for the SPI Master is available here.
This design implements the SPI master in the CPOL = ‘0’ and CPHA = ‘0’ mode. It sets the clk_div parameter based on the system clock frequency (specified with the clk_freq generic parameter, see below) to communicate with the accelerometer at the maximum SPI frequency specified in the ADXL362’s datasheet, i.e. 8 MHz.
This design also utilizes the Continuous Mode feature of the SPI Master to execute transactions of varying lengths. The transactions in the configure state are 24 bits long, whereas the transactions in the read_data state are comprised of 64 bits.
Configuring the Accelerometer Pmod Controller
The Accelerometer Pmod Controller is configured by setting the generic parameters in the entity.
System Clock Frequency
The generic parameter clk_freq must be set to the frequency of the system clock provided to the Accelerometer Pmod Controller on its clk port.
Data Rate
The generic parameter data_rate defines the frequency at which the ADXL362 accelerometer takes measurements. The parameter itself is the rate code that corresponds to the desired data rate, defined in Table 17 of the ADXL362’s datasheet. Bandwidth and power consumption increase with higher data rates. Table 1 describes the options and lists the rate codes. The default rate code is “011” which configures the accelerometer to a 100 Hz output data rate.
Table 1. Data Rate Options
Data Rate (Hz) | Bandwidth (Hz) | Rate Code |
---|---|---|
400 | 200 | 101…111 |
200 | 100 | 100 |
100 | 50 | 011 |
50 | 25 | 010 |
25 | 12.5 | 001 |
12.5 | 6.25 | 000 |
Data Range
The generic parameter data_range defines the range of acceleration values the accelerometer measures. The parameter itself consists of the bits used to configure the accelerometer’s data format register, defined in Table 17 of the ADXL362’s datasheet. Sensitivity scales with range. Table 2 describes the options and lists the parameter settings. The default setting is “00” which configures the accelerometer to a ±2g output data range.
Table 2. Data Range Options
Data Range | Sensitivity (mg/LSB) | Setting |
---|---|---|
±2g | 1 | 00 |
±4g | 2 | 01 |
±8g | 4 | 1X |
Port Descriptions
Table 3 describes the Accelerometer Pmod Controller’s ports.
Table 3. Port Descriptions
Port | Width | Mode | Data Type | Interface | Description |
---|---|---|---|---|---|
clk | 1 | in | standard logic | user logic | System clock |
reset_n | 1 | in | standard logic | user logic | Asynchronous active low reset |
miso | 1 | in | standard logic | Accelerometer Pmod | SPI master in, slave out data line |
sclk | 1 | buffer | standard logic | Accelerometer Pmod | SPI serial clock |
ss_n | 1 | buffer | standard logic vector | Accelerometer Pmod | SPI slave select signal |
mosi | 1 | out | standard logic | Accelerometer Pmod | SPI master out, slave in data line |
acceleration_x | 12 | out | standard logic vector | user logic | x-axis acceleration data |
acceleration_y | 12 | out | standard logic vector | user logic | y-axis acceleration data |
acceleration_z | 12 | out | standard logic vector | user logic | z-axis acceleration data |
Connections
This Pmod has a 12-pin connector. Table 4 provides the pinout for this connector. The Accelerometer Pmod Controller’s ports need to be assigned to the FPGA pins that are routed to this connector as listed.
Table 4. Accelerometer Pmod Pinout and Connections to Accelerometer Pmod Controller
Pmod Pin Number | Accelerometer Pmod Port | Accelerometer Pmod Controller Port |
---|---|---|
1 | chip select (CS) | ss_n(0) |
2 | master out, slave in (MOSI) | mosi |
3 | master in, slave out (MISO) | miso |
4 | serial clock (SCLK) | sclk |
5 | GND | - |
6 | VCC | - |
7 | interrupt 2 (INT2) | - |
8 | interrupt 1 (INT1) | - |
9 | no connect (NC) | - |
10 | no connect (NC) | - |
11 | GND | - |
12 | VCC | - |
Reset
The reset_n input port must have a logic high for the Accelerometer Pmod Controller component to operate. A low logic level on this port asynchronously resets the component. During reset, the component aborts the current transaction with the Pmod and clears the acceleration_x, acceleration_y, and acceleration_z data outputs. Once released from reset, the Acceleration Pmod Controller restarts its operation. It reconfigures the accelerometer and then resumes collecting and outputting acceleration data.
Conclusion
This Accelerometer Pmod Controller is a programmable logic component that interfaces to Digilent’s PmodACL2 (Accelerometer ADXL362 Pmod). It handles all communication with this Pmod to configure the Pmod accelerometer’s data range and data rate, activate measurements, and provide a continual stream of updated acceleration data on 3 parallel output buses, one for each axis.
Additional Information
Analog Devices ADXL362 datasheet: ADXL362.pdf
Related Topics
Serial Peripheral Interface (SPI) Master (VHDL)
Contact
Comments, feedback, and questions can be sent to eewiki@digikey.com.