Page tree

Versions Compared

Key

  • This line was added.
  • This line was removed.
  • Formatting was changed.
Comment: Migration of unmigrated content due to installation of a new plugin


This is a page about the NXP based i.MX6; Wandboard.

hide-comments
Table of Contents
indent20px
styledisc

Availability

Boards:
Wandboard SOLO at Digi-Key
Wandboard DUAL at Digi-Key
Wandboard QUAD at Digi-Key
Wandboard SOLO (WB-IMX6S) at Digi-Key
Wandboard DUAL (WB-IMX6U-BW) at Digi-Key
Wandboard QUAD (WB-IMX6Q-BW) at Digi-Key
Wandboard QUADPLUS (WB-IMX6QP-BW) at Digi-Key
Accessories:
Wandboard Antenna Kit at Digi-Key
Wandboard Enclosure at Digi-Key
5V 2A+ DC Power Supply (2.1mm ID x 5.5mm OD positive center plug) at Digi-Key

Vendor Documentation

Basic Requirements

ARM Cross Compiler: GCC

This is a pre-built (64bit) version of GCC that runs on generic linux, sorry (32bit) x86 users, it's time to upgrade...
Download/Extract:

Code Block
titleuser@localhost:~$
wget -c https://releases.linaro.org/components/toolchain/binaries/6.5-2018.12/arm-linux-gnueabihf/gcc-linaro-6.5.0-2018.12-x86_64_arm-linux-gnueabihf.tar.xz
tar xf gcc-linaro-6.5.0-2018.12-x86_64_arm-linux-gnueabihf.tar.xz
export CC=`pwd`/gcc-linaro-6.5.0-2018.12-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-

Test Cross Compiler:

Code Block
titleuser@localhost:~$
${CC}gcc --version
Code Block
titleTest Output:
arm-linux-gnueabihf-gcc (Linaro GCC 6.5-2018.12) 6.5.0
Copyright (C) 2017 Free Software Foundation, Inc.
This is free software; see the source for copying conditions.  There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

Bootloader: U-Boot

Das U-Boot – the Universal Boot Loader: http://www.denx.de/wiki/U-Boot
eewiki.net patch archive: https://github.com/eewiki/u-boot-patches
Download:

Code Block
titleuser@localhost:~$
git clone https://github.com/u-boot/u-boot
cd u-boot/
git checkout v2019.04 -b tmp

Patches:

Code Block
titleuser@localhost:~/u-boot$
wget -c https://github.com/eewiki/u-boot-patches/raw/master/v2019.04/0001-wandboard-uEnv.txt-bootz-n-fixes.patch
 
patch -p1 < 0001-wandboard-uEnv.txt-bootz-n-fixes.patch

Configure and Build:

Code Block
titleuser@localhost:~/u-boot$
make ARCH=arm CROSS_COMPILE=${CC} distclean
make ARCH=arm CROSS_COMPILE=${CC} wandboard_defconfig
make ARCH=arm CROSS_COMPILE=${CC}

Linux Kernel

This script will build the kernel, modules, device tree binaries and copy them to the deploy directory.
Download:

Code Block
titleuser@localhost:~$
git clone https://github.com/RobertCNelson/armv7-multiplatform
cd armv7-multiplatform/

For v4.14.x (Longterm 4.14.x):

Code Block
titleuser@localhost:~/armv7-multiplatform$
git checkout origin/v4.14.x -b tmp

For v4.14.x-rt (Longterm 4.14.x + Real-Time Linux):

Code Block
titleuser@localhost:~/armv7-multiplatform$
git checkout origin/v4.14.x-rt -b tmp

For v4.19.x (Longterm 4.19.x):

Code Block
titleuser@localhost:~/armv7-multiplatform$
git checkout origin/v4.19.x -b tmp

For v4.19.x-rt (Longterm 4.19.x + Real-Time Linux):

Code Block
titleuser@localhost:~/armv7-multiplatform$
git checkout origin/v4.19.x-rt -b tmp

For v5.0.x (Stable):

Code Block
titleuser@localhost:~/armv7-multiplatform$
git checkout origin/v5.0.x -b tmp

For v5.0.x-rt (Stable + Real-Time Linux):

Code Block
titleuser@localhost:~/armv7-multiplatform$
git checkout origin/v5.0.x-rt -b tmp

Build:

Code Block
titleuser@localhost:~/armv7-multiplatform$
./build_kernel.sh

Root File System

Debian 10

User

Password

debian

temppwd

root

root

Download:

Code Block
titleuser@localhost:~$
wget -c https://rcn-ee.com/rootfs/eewiki/minfs/debian-10.3-minimal-armhf-2020-02-10.tar.xz

Verify:

Code Block
titleuser@localhost:~$
sha256sum debian-10.3-minimal-armhf-2020-02-10.tar.xz
Code Block
titlesha256sum output:
a6645dfb49795bbe809dfc3c2b7dff53ad4daab24a654edd29bab29ae007cc40  debian-10.3-minimal-armhf-2020-02-10.tar.xz

Extract:

Code Block
titleuser@localhost:~$
tar xf debian-10.3-minimal-armhf-2020-02-10.tar.xz

Ubuntu 18.04 LTS

User

Password

ubuntu

temppwd

Download:

Code Block
titleuser@localhost:~$
wget -c https://rcn-ee.com/rootfs/eewiki/minfs/ubuntu-18.04.3-minimal-armhf-2020-02-10.tar.xz

Verify:

Code Block
titleuser@localhost:~$
sha256sum ubuntu-18.04.3-minimal-armhf-2020-02-10.tar.xz
Code Block
titlesha256sum output:
b28b356d75153bfb3beb5c96bf8eabe92025cf5e665e1a564b469bc70e5a363b  ubuntu-18.04.3-minimal-armhf-2020-02-10.tar.xz

Extract:

Code Block
titleuser@localhost:~$
tar xf ubuntu-18.04.3-minimal-armhf-2020-02-10.tar.xz

Setup microSD card

We need to access the External Drive to be utilized by the target device. Run lsblk to help figure out what linux device has been reserved for your External Drive.

Code Block
titleExample: for DISK=/dev/sdX
lsblk
NAME   MAJ:MIN RM   SIZE RO TYPE MOUNTPOINT
sda      8:0    0 465.8G  0 disk
├─sda1   8:1    0   512M  0 part /boot/efi
└─sda2   8:2    0 465.3G  0 part /                <- Development Machine Root Partition
sdb      8:16   1   962M  0 disk                  <- microSD/USB Storage Device
└─sdb1   8:17   1   961M  0 part                  <- microSD/USB Storage Partition
Code Block
titleThus you would use:
export DISK=/dev/sdb
Code Block
titleExample: for DISK=/dev/mmcblkX
lsblk
NAME      MAJ:MIN   RM   SIZE RO TYPE MOUNTPOINT
sda         8:0      0 465.8G  0 disk
├─sda1      8:1      0   512M  0 part /boot/efi
└─sda2      8:2      0 465.3G  0 part /                <- Development Machine Root Partition
mmcblk0     179:0    0   962M  0 disk                  <- microSD/USB Storage Device
└─mmcblk0p1 179:1    0   961M  0 part                  <- microSD/USB Storage Partition
Code Block
titleThus you would use:
export DISK=/dev/mmcblk0

Erase partition table/labels on microSD card:

Code Block
sudo dd if=/dev/zero of=${DISK} bs=1M count=10

Install Bootloader:

Code Block
titleuser@localhost:~$
sudo dd if=./u-boot/SPL of=${DISK} seek=1 bs=1k
sudo dd if=./u-boot/u-boot.img of=${DISK} seek=69 bs=1k

Create Partition Layout:
With util-linux v2.26, sfdisk was rewritten and is now based on libfdisk.

Code Block
titleCheck the version of sfdisk installed on your pc
sudo sfdisk --version
Code Block
titleExample Output
sfdisk from util-linux 2.27.1
Code Block
titlesfdisk >= 2.26.x
sudo sfdisk ${DISK} <<-__EOF__
1M,,L,*
__EOF__
Code Block
titlesfdisk <= 2.25.x
sudo sfdisk --unit M ${DISK} <<-__EOF__
1,,L,*
__EOF__

Format Partition:

Code Block
for: DISK=/dev/mmcblkX
sudo mkfs.ext4 -L rootfs ${DISK}p1
 
for: DISK=/dev/sdX
sudo mkfs.ext4 -L rootfs ${DISK}1

Mount Partition:
On most systems these partitions may be auto-mounted...

Code Block
sudo mkdir -p /media/rootfs/
 
for: DISK=/dev/mmcblkX
sudo mount ${DISK}p1 /media/rootfs/
 
for: DISK=/dev/sdX
sudo mount ${DISK}1 /media/rootfs/

Install Kernel and Root File System

To help new users, since the kernel version can change on a daily basis. The kernel building scripts listed on this page will now give you a hint of what kernel version was built.

Code Block
-----------------------------
Script Complete
eewiki.net: [user@localhost:~$ export kernel_version=5.X.Y-Z]
-----------------------------

Copy and paste that "export kernel_version=5.X.Y-Z" exactly as shown in your own build/desktop environment and hit enter to create an environment variable to be used later.

Code Block
export kernel_version=5.X.Y-Z

Copy Root File System

Code Block
titleuser@localhost:~$
sudo tar xfvp ./*-*-*-armhf-*/armhf-rootfs-*.tar -C /media/rootfs/
sync
sudo chown root:root /media/rootfs/
sudo chmod 755 /media/rootfs/

Set uname_r in /boot/uEnv.txt

Code Block
titleuser@localhost:~$
sudo sh -c "echo 'uname_r=${kernel_version}' >> /media/rootfs/boot/uEnv.txt"

Video

See other hints: https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/Documentation/fb/modedb.txt

Code Block
title~/
sudo sh -c "echo 'cmdline=video=HDMI-A-1:1024x768@60e' >> /media/rootfs/boot/uEnv.txt"

Copy Kernel Image

Kernel Image:

Code Block
titleuser@localhost:~$
sudo cp -v ./armv7-multiplatform/deploy/${kernel_version}.zImage /media/rootfs/boot/vmlinuz-${kernel_version}

Copy Kernel Device Tree Binaries

Code Block
titleuser@localhost:~$
sudo mkdir -p /media/rootfs/boot/dtbs/${kernel_version}/
sudo tar xfv ./armv7-multiplatform/deploy/${kernel_version}-dtbs.tar.gz -C /media/rootfs/boot/dtbs/${kernel_version}/

Copy Kernel Modules

Code Block
titleuser@localhost:~$
sudo tar xfv ./armv7-multiplatform/deploy/${kernel_version}-modules.tar.gz -C /media/rootfs/

File Systems Table (/etc/fstab)

Code Block
sudo sh -c "echo '/dev/mmcblk2p1  /  auto  errors=remount-ro  0  1' >> /media/rootfs/etc/fstab"

WiFi

Dual/Quad only (Solo has no WiFi module installed)
see: https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/drivers/net/wireless/brcm80211/brcmfmac/dhd_sdio.c?id=refs/tags/v3.11-rc3#n317

Code Block
title~/
wget -c https://git.kernel.org/cgit/linux/kernel/git/firmware/linux-firmware.git/plain/brcm/brcmfmac4329-sdio.bin
wget -c https://git.kernel.org/cgit/linux/kernel/git/firmware/linux-firmware.git/plain/brcm/brcmfmac4330-sdio.bin
 
wget -c https://rcn-ee.com/repos/git/meta-fsl-arm-extra/recipes-bsp/broadcom-nvram-config/files/wandboard/brcmfmac4329-sdio.txt
wget -c https://rcn-ee.com/repos/git/meta-fsl-arm-extra/recipes-bsp/broadcom-nvram-config/files/wandboard/brcmfmac4330-sdio.txt
 
sudo mkdir -p /media/rootfs/lib/firmware/brcm/
 
sudo cp -v ./brcmfmac43*-sdio.bin /media/rootfs/lib/firmware/brcm/
sudo cp -v ./brcmfmac43*-sdio.txt /media/rootfs/lib/firmware/brcm/

Status:

Code Block
debian@arm:~$ dmesg | grep brcm
[    4.798229] brcmfmac: F1 signature read @0x18000000=0x9934329
[    4.799328] brcmfmac: brcmf_sdio_chip_drivestrengthinit: No SDIO Drive strength init done for chip 4329 rev 3 pmurev 6
[    5.058286] brcmfmac: brcmf_c_preinit_dcmds: Firmware version = wl0: Sep  2 2011 14:48:19 version 4.220.48
[    5.082280] brcmfmac: brcmf_fil_cmd_data: Failed err=-23
[    5.087654] brcmfmac: brcmf_fws_init: failed to set bdcv2 tlv signaling
debian@arm:~$ /sbin/ifconfig -a
wlan0     Link encap:Ethernet  HWaddr 40:2c:f4:ae:17:91
          BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

Remove microSD/SD card

Code Block
sync
sudo umount /media/rootfs

2D/3D Video Acceleration via Etnaviv Project

Vivante GC320/GC880 (quad GC320/GC355/GC2000) 2D/3D Acceleration via Etnaviv
This sections assumes you have already installed your favorite xorg based window manager, such as lxde, lxqt, xfce, kde, gnome, etc... These are packages that need to be installed on top of your selected windows manager and an xorg.conf needed to correctly setup the video interface.
Verify your kernel has etnaviv support:

Code Block
titleSOLO/DUAL
debian@arm:~$ dmesg | grep etnaviv
[    4.047928] etnaviv gpu-subsystem: bound 134000.gpu (ops gpu_ops)
[    4.047955] etnaviv gpu-subsystem: bound 130000.gpu (ops gpu_ops)
[    4.047968] etnaviv-gpu 134000.gpu: model: GC320, revision: 5007
[    4.090180] etnaviv-gpu 130000.gpu: model: GC880, revision: 5106
Code Block
titleQUAD
debian@arm:~$ dmesg | grep etnaviv
[    4.025841] etnaviv gpu-subsystem: bound 134000.gpu (ops gpu_ops)
[    4.025868] etnaviv gpu-subsystem: bound 130000.gpu (ops gpu_ops)
[    4.025887] etnaviv gpu-subsystem: bound 2204000.gpu (ops gpu_ops)
[    4.025899] etnaviv-gpu 134000.gpu: model: GC320, revision: 5007
[    4.070139] etnaviv-gpu 130000.gpu: model: GC2000, revision: 5108
[    4.120479] etnaviv-gpu 2204000.gpu: model: GC355, revision: 1215
[    4.120492] etnaviv-gpu 2204000.gpu: Ignoring GPU with VG and FE2.0

edid parsing still seems hit and miss on the quad board, override default 1024x768 resolution via the video variable in uEnv.txt.
See other hints: https://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/tree/Documentation/fb/modedb.txt

Code Block
cmdline=video=HDMI-A-1:1024x768@60e

1080p

Code Block
cmdline=video=HDMI-A-1:1920x1080@60e
Code Block
sudo apt-get update
sudo apt-get install xserver-xorg-video-armada-etnaviv
Code Block
title/etc/X11/xorg.conf
Section "Monitor"
        Identifier      "Builtin Default Monitor"
EndSection
Section "Device"
        Identifier      "Builtin Default fbdev Device 0"
        Driver          "armada"
EndSection
Section "Screen"
        Identifier      "Builtin Default fbdev Screen 0"
        Device          "Builtin Default fbdev Device 0"
        Monitor         "Builtin Default Monitor"
EndSection
Section "ServerLayout"
        Identifier      "Builtin Default Layout"
        Screen          "Builtin Default fbdev Screen 0"
EndSection

Comments

Any questions or comments please go to our TechForum: TechForum