Page tree
Skip to end of metadata
Go to start of metadata

This is a page about the Freescale based i.MX7; PICO-PI-IMX7.

Availability

Boards:
1406-0013-ND at Digi-Key

Vendor Documentation

Basic Requirements

imx_usb_loader

imx_usb_loader – USB & UART loader for i.MX5/6/7/8 series:
Source: https://github.com/boundarydevices/imx_usb_loader
Download/build:

user@localhost:~$
git clone https://github.com/boundarydevices/imx_usb_loader
cd imx_usb_loader/
make

ARM Cross Compiler: GCC

This is a pre-built (64bit) version of GCC that runs on generic linux, sorry (32bit) x86 users, it's time to upgrade...
Download/Extract:

user@localhost:~$
wget -c https://releases.linaro.org/components/toolchain/binaries/6.5-2018.12/arm-linux-gnueabihf/gcc-linaro-6.5.0-2018.12-x86_64_arm-linux-gnueabihf.tar.xz
tar xf gcc-linaro-6.5.0-2018.12-x86_64_arm-linux-gnueabihf.tar.xz
export CC=`pwd`/gcc-linaro-6.5.0-2018.12-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf-

Test Cross Compiler:

user@localhost:~$
${CC}gcc --version
Test Output:
arm-linux-gnueabihf-gcc (Linaro GCC 6.5-2018.12) 6.5.0
Copyright (C) 2017 Free Software Foundation, Inc.
This is free software; see the source for copying conditions.  There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.

Bootloader: U-Boot

Das U-Boot – the Universal Boot Loader: http://www.denx.de/wiki/U-Boot
Download:

user@localhost:~$
git clone -b v2021.01 https://github.com/u-boot/u-boot --depth=1
cd u-boot/

Configure and Build:

user@localhost:~/u-boot$
make ARCH=arm CROSS_COMPILE=${CC} distclean
make ARCH=arm CROSS_COMPILE=${CC} pico-pi-imx7d_defconfig
make ARCH=arm CROSS_COMPILE=${CC}

Bootloader: imx_usb_loader

Place the board into USB boot mode, setting these Jumpers:

Power Board and Check lsusb:

user@localhost:~/u-boot$
lsusb | grep Freescale
Bus 00x Device 00y: ID 15a2:0076 Freescale Semiconductor, Inc

Load the SPL binary via USB:

user@localhost:~/u-boot$
sudo ~/imx_usb_loader/imx_usb SPL

Load the u-boot-dtb.img binary via USB:

user@localhost:~/u-boot$
sudo ~/imx_usb_loader/imx_usb u-boot-dtb.img

Using any key, break into U-Boot Console:

SERIAL_CONSOLE_U_BOOT
Loading Environment from MMC... OK
In:    serial
Out:   serial
Err:   serial
Net:   FEC0
Hit any key to stop autoboot:  0 
=> 

Use the default environment variables:

SERIAL_CONSOLE_U_BOOT
=> env default -f -a
=> setenv bootm_boot_mode nonsec
=> saveenv

Configure mmc 0 to boot from the data partition, and disable access to boot partitions:

SERIAL_CONSOLE_U_BOOT
=> mmc partconf 0 0 7 0

Run the DFU agent so we can flash the new images using dfu-util tool:

SERIAL_CONSOLE_U_BOOT
=> dfu 0 mmc 0

Load the SPL binary via dfu-util:

user@localhost:~/u-boot$
sudo dfu-util -D SPL -a spl

Load the SPL binary via dfu-util:

user@localhost:~/u-boot$
sudo dfu-util -R -D u-boot-dtb.img -a u-boot

Remove power and place the board into eMMC boot mode, setting these Jumpers:

Power Board and enable U-Boot USB Mass Storage mode:

SERIAL_CONSOLE_U_BOOT
Loading Environment from MMC... OK
In:    serial
Out:   serial
Err:   serial
Net:   FEC0
Hit any key to stop autoboot:  0 
=> ums 0 mmc 0

Verify Linux loaded the USB Mass Storage device, this will be the SD Card used thru out this wiki:

user@localhost:~/u-boot$
lsusb | grep Netchip
Bus 00x Device 00y: ID 0525:a4a5 Netchip Technology, Inc. Pocketbook Pro 903

Linux Kernel

This script will build the kernel, modules, device tree binaries and copy them to the deploy directory.
Download:

user@localhost:~$
git clone https://github.com/RobertCNelson/armv7-lpae-multiplatform
cd armv7-lpae-multiplatform/

For v5.10.x (Stable):

user@localhost:~/armv7-lpae-multiplatform$
git checkout origin/v5.10.x -b tmp

Build:

user@localhost:~/armv7-lpae-multiplatform$
./build_kernel.sh

Root File System

Debian 10

User

Password

debian

temppwd

root

root

Download:

user@localhost:~$
wget -c https://rcn-ee.com/rootfs/eewiki/minfs/debian-10.4-minimal-armhf-2020-05-10.tar.xz

Verify:

user@localhost:~$
sha256sum debian-10.4-minimal-armhf-2020-05-10.tar.xz
sha256sum output:
cd598e42850cbef87602bf15ee343abfbf0d8c6ba81028c741672b5f24263534  debian-10.4-minimal-armhf-2020-05-10.tar.xz

Extract:

user@localhost:~$
tar xf debian-10.4-minimal-armhf-2020-05-10.tar.xz

Ubuntu 20.04 LTS

User

Password

ubuntu

temppwd

Download:

user@localhost:~$
wget -c https://rcn-ee.com/rootfs/eewiki/minfs/ubuntu-20.04-minimal-armhf-2020-05-10.tar.xz

Verify:

user@localhost:~$
sha256sum ubuntu-20.04-minimal-armhf-2020-05-10.tar.xz
sha256sum output:
de0177ac9259fdbcc626ee239f4258b64070c0921dbc38c45fab6925a5becaa1  ubuntu-20.04-minimal-armhf-2020-05-10.tar.xz

Extract:

user@localhost:~$
tar xf ubuntu-20.04-minimal-armhf-2020-05-10.tar.xz

Setup microSD card

We need to access the External Drive to be utilized by the target device. Run lsblk to help figure out what linux device has been reserved for your External Drive.

Example: for DISK=/dev/sdX
lsblk
NAME   MAJ:MIN RM   SIZE RO TYPE MOUNTPOINT
sda      8:0    0 465.8G  0 disk
├─sda1   8:1    0   512M  0 part /boot/efi
└─sda2   8:2    0 465.3G  0 part /                <- Development Machine Root Partition
sdb      8:16   1   962M  0 disk                  <- microSD/USB Storage Device
└─sdb1   8:17   1   961M  0 part                  <- microSD/USB Storage Partition
Thus you would use:
export DISK=/dev/sdb
Example: for DISK=/dev/mmcblkX
lsblk
NAME      MAJ:MIN   RM   SIZE RO TYPE MOUNTPOINT
sda         8:0      0 465.8G  0 disk
├─sda1      8:1      0   512M  0 part /boot/efi
└─sda2      8:2      0 465.3G  0 part /                <- Development Machine Root Partition
mmcblk0     179:0    0   962M  0 disk                  <- microSD/USB Storage Device
└─mmcblk0p1 179:1    0   961M  0 part                  <- microSD/USB Storage Partition
Thus you would use:
export DISK=/dev/mmcblk0

Erase partition table/labels on microSD card:

sudo dd if=/dev/zero of=${DISK} bs=1M count=10

Install Bootloader:

user@localhost:~$
sudo dd if=./u-boot/SPL of=${DISK} seek=1 bs=1k
sudo dd if=./u-boot/u-boot-dtb.img of=${DISK} seek=69 bs=1k

Create Partition Layout:
With util-linux v2.26, sfdisk was rewritten and is now based on libfdisk.

Check the version of sfdisk installed on your pc
sudo sfdisk --version
Example Output
sfdisk from util-linux 2.27.1
sfdisk >= 2.26.x
sudo sfdisk ${DISK} <<-__EOF__
1M,,L,*
__EOF__
sfdisk <= 2.25.x
sudo sfdisk --unit M ${DISK} <<-__EOF__
1,,L,*
__EOF__

Format Partition:

for: DISK=/dev/mmcblkX
sudo mkfs.ext4 -L rootfs ${DISK}p1
 
for: DISK=/dev/sdX
sudo mkfs.ext4 -L rootfs ${DISK}1

Mount Partition:
On most systems these partitions may be auto-mounted...

sudo mkdir -p /media/rootfs/
 
for: DISK=/dev/mmcblkX
sudo mount ${DISK}p1 /media/rootfs/
 
for: DISK=/dev/sdX
sudo mount ${DISK}1 /media/rootfs/

Install Kernel and Root File System

To help new users, since the kernel version can change on a daily basis. The kernel building scripts listed on this page will now give you a hint of what kernel version was built.

-----------------------------
Script Complete
eewiki.net: [user@localhost:~$ export kernel_version=5.X.Y-Z]
-----------------------------

Copy and paste that "export kernel_version=5.X.Y-Z" exactly as shown in your own build/desktop environment and hit enter to create an environment variable to be used later.

export kernel_version=5.X.Y-Z

Copy Root File System

Debian; Root File System: user@localhost:~$
sudo tar xfvp ./debian-*-*-armhf-*/armhf-rootfs-*.tar -C /media/rootfs/
sync
sudo chown root:root /media/rootfs/
sudo chmod 755 /media/rootfs/
Ubuntu; Root File System: user@localhost:~$
sudo tar xfvp ./ubuntu-*-*-armhf-*/armhf-rootfs-*.tar -C /media/rootfs/
sync
sudo chown root:root /media/rootfs/
sudo chmod 755 /media/rootfs/

Setup extlinux.conf

user@localhost:~$
sudo mkdir -p /media/rootfs/boot/extlinux/
sudo sh -c "echo 'label Linux ${kernel_version}' > /media/rootfs/boot/extlinux/extlinux.conf"
sudo sh -c "echo '    kernel /boot/vmlinuz-${kernel_version}' >> /media/rootfs/boot/extlinux/extlinux.conf"
sudo sh -c "echo '    append root=/dev/mmcblk2p1 ro rootfstype=ext4 rootwait quiet' >> /media/rootfs/boot/extlinux/extlinux.conf"
sudo sh -c "echo '    fdtdir /boot/dtbs/${kernel_version}/' >> /media/rootfs/boot/extlinux/extlinux.conf"

Copy Kernel Image

Kernel Image:

user@localhost:~$
sudo cp -v ./armv7-lpae-multiplatform/deploy/${kernel_version}.zImage /media/rootfs/boot/vmlinuz-${kernel_version}

Copy Kernel Device Tree Binaries

user@localhost:~$
sudo mkdir -p /media/rootfs/boot/dtbs/${kernel_version}/
sudo tar xfv ./armv7-lpae-multiplatform/deploy/${kernel_version}-dtbs.tar.gz -C /media/rootfs/boot/dtbs/${kernel_version}/

Copy Kernel Modules

user@localhost:~$
sudo tar xfv ./armv7-lpae-multiplatform/deploy/${kernel_version}-modules.tar.gz -C /media/rootfs/

File Systems Table (/etc/fstab)

user@localhost:~/$
sudo sh -c "echo '/dev/mmcblk2p1  /  auto  errors=remount-ro  0  1' >> /media/rootfs/etc/fstab"

WiFi AP6335

user@localhost:~$
wget -c https://raw.githubusercontent.com/buildroot/buildroot/master/board/technexion/imx7dpico/rootfs_overlay/lib/firmware/brcm/brcmfmac4339-sdio.txt
sudo mkdir -p /media/rootfs/lib/firmware/brcm/
sudo cp -v ./brcmfmac4339-sdio.txt /media/rootfs/lib/firmware/brcm/

Status:

debian@arm:~$ dmesg | grep brcm
[   17.000227] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac4339-sdio for chip BCM4339/2
[   17.014290] usbcore: registered new interface driver brcmfmac
[   17.032649] brcmfmac mmc1:0001:1: Direct firmware load for brcm/brcmfmac4339-sdio.technexion,imx7d-pico-pi.txt failed with error -2
[   17.265035] brcmfmac: brcmf_fw_alloc_request: using brcm/brcmfmac4339-sdio for chip BCM4339/2
[   17.277324] brcmfmac: brcmf_c_process_clm_blob: no clm_blob available (err=-2), device may have limited channels available
[   17.290080] brcmfmac: brcmf_c_preinit_dcmds: Firmware: BCM4339/2 wl0: Feb 17 2016 18:29:33 version 6.37.32.RC23.34.42 (r608406)
 
debian@arm:~$ sudo ifconfig -a wlan0
wlan0: flags=-28669<UP,BROADCAST,MULTICAST,DYNAMIC>  mtu 1500
        ether 28:ed:e0:02:64:10  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 0  bytes 0 (0.0 B)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

Remove microSD/SD card

sync
sudo umount /media/rootfs

Stop U-Boot USB Mass Storage mode, with CTRL-C, and reset the board:

SERIAL_CONSOLE_U_BOOT
Loading Environment from MMC... OK
In:    serial
Out:   serial
Err:   serial
Net:   FEC0
Hit any key to stop autoboot:  0 
=> ums 0 mmc 0
UMS: LUN 0, dev0, hwpart 0, section 0x0, count 0x720000
Ctrl+C to exit ...
=> reset

Comments

Any questions or comments please go to our TechForum: TechForum


  • No labels