USD

Potentiometers, Variable Resistors

Devices that control the current that flows through a circuit.

Trimmer Potentiometers Trimmer Potentiometers A variable device that opposes the flow of current. The resistance of these devices is changed using a rotary portion of the device (usually needing a separate tool) that is attached to the center axis of the component.
View all Trimmer Potentiometers
Adjustable Power Resistor Adjustable Power Resistor A variable device that opposes the flow of current. The resistance of these devices is changed moving a central terminal between one end and the other of the component.
View all Adjustable Power Resistor
Thumbwheel Potentiometers Thumbwheel Potentiometers A variable device that opposes the flow of current. The resistance of these devices is changed using a rotary disk that is attached to the center axis of the component.
View all Thumbwheel Potentiometers
Slide Potentiometers Slide Potentiometers A variable device that opposes the flow of current. The resistance of these devices is changed using a stem that moves between one end and the other of the component.
View all Slide Potentiometers
Scale Dials Scale Dials A removable device with a face that is marked in predefined units to indicate the degree that a unit has been turned.
View all Scale Dials
Value Display Potentiometers Value Display Potentiometers A variable device that opposes the flow of current. The resistance of these devices is changed by pushing a button or rotating a wheel. The values that the device is being changed to is displayed on the front of the unit.
View all Value Display Potentiometers
Kits Kits A grouping of potentiometers of various styles, sizes, and values.
View all Kits
Accessories Accessories Supplementary items used with potentiometers.
View all Accessories
Rotary Potentiometers, Rheostats Rotary Potentiometers, Rheostats A variable device that opposes the flow of current. The resistance of these devices is changed using a revolving stem that is attached to the central axis.
View all Rotary Potentiometers, Rheostats