TechZone
Sensor solutions

Position Sensors

Position sensors measure linear or angular position in reference to a fixed point or arbitrary reference. They can be used to measure distance or displacement (change in position) or simply to detect the presence or absence of an object (proximity sensors).

The position information can then be processed with an external circuit to count events, monitor physical conditions, control processes, and many other applications. If the position or proximity information is combined with time measurements, then speed, velocity, and acceleration can be calculated for motion control.

Click here to view all Position Sensors available at Digi-Key


Position

  • Non-Contacting
  • Contacting
  • Dev Tools/Eval Boards
  • Product Training
Non-Contacting

Non-contacting position sensors measure the linear or angular position of an object without physical contact. The main advantage is high reliability and long functional life because of the absence of mechanical parts and lack of physical contact.

Photoelectric Sensor SD5600-001Photoelectric sensors use a light transmitter and photoelectric receiver to detect the presence or absence of an object. Photoelectric sensors can be divided into three basic sensing modes: opposed, retroreflective, and proximity.

View All available Photoelectric Sensors


Magnetic Sensor RI-02SMD-G2 Magnetic sensors use the Hall effect, anisotropic magnetoresistive effect, or a magnetically actuated reed switch to detect magnetic fields generated by a reference magnet to determine position, angle, or displacement.

View All available Magnetic Sensors


Capacitive Sensor E2K-C25ME1 Capacitive sensors detect changes in the capacitance between an object and a sensor. The amount of capacitance varies, depending on the size and distance of the object. Capacitive sensors can be used to detect metallic and non-metallic objects such as liquids and plastics.

View All available Capacitive Sensors


Inductive Sensor TL-W3MC1 Inductive sensors use a coil to generate a high frequency oscillating magnetic field to detect metallic objects. When a metal target enters the sensing field, eddy currents are induced in the target, which reduces the signal amplitude and triggers a change of state in the sensor output.

View All available Inductive Sensors


Ultrasonic Sensor 943-F4Y-2D-002-180E Ultrasonic sensors emit pulses of high frequency sound energy. A portion of this energy is reflected off a target and travels back to the sensor. The sensor measures the total time required for the pulse to return and calculates the distance from the sensor to the target.

View All available Ultrasonic Sensors

Contacting

Contacting position sensors measure linear or angular position through a mechanical connection.

Limit Switch ESE-18L11AA limit switch is a mechanical switch that is actuated by very little physical force through the use of a tipping-point mechanism. Limit switches are most commonly used in industrial environments to detect the movements of parts or control the movement of a mechanical part. They are very common due to their low cost and durability.

View All Limit Switches


Linear Sensor 02560993-000A linear variable differential transformer (LVDT) is a type of electrical transformer used for measuring linear displacement. LVDTs are commonly used for position feedback in servomechanisms as well as for automated measurement in machine tools and many other industrial and scientific applications.
View All LVDTs


Encoder EVE-JBBF2020BAn Encoder is an electromechanical device that converts the angular position of a shaft to a digital code. There are two main types: absolute and incremental. Absolute encoders produce a unique digital code for each distinct angle of the shaft. An incremental rotary encoder, also known as a quadrature encoder, generates a pulse for each incremental step. These pulses need to be counted by an external circuit to determine the displacement.

View All Encoders

Dev Tools/Eval Boards


Melexis                                                             
 Pricing & Availability

NVE
 Pricing & Availability

Silicon Labs
 Pricing & Availability

STMicroelectronics
 Pricing & Availability
Product Training

Position - Product Training Modules (PTMs)
Bourns
 Rotary Position Sensor - Model 3382

Freescale
 Proximity Sensors

Honeywell Microelectronics & Precision Sensors
 Magnetic Sensors

Honeywell Sensing and Control
 Magnetic Sensors
 RTY Series Hall-effect Rotary Position Sensors

Measurement Specialties/Schaevitz
 KMT32B Magneto Resistive Sensor

MEDER electronic Inc
 Reed Switch Technology 
 Reed Switch Magnet Interaction

NKK Switches
 Tilt Switches


Sensors Suppliers - Position