TechZone
Microcontroller Solutions
Programming, Debugging, and Emulating tools are all used during the development and testing phase of microcontroller code development. Some development tool manufacturers combine the functionality of these into one unit, while others make a clear distinction in products between them.

View all related microcontroller products available at Digi-Key


Programming Tools - Atmel

  • AVR
  • 32-bit AVR UC3
  • 8051
  • ATSAM
AVR

ISP Programmers/Debuggers/Emulators

Atmel ATAVRONEKIT

The AVR ONE! is a professional development tool for all Atmel 8 bit and 32 bit AVR devices with On-Chip Debug capability.  It is used for source level symbolic debugging, program trace and device programming.  AVR ONE! supports the complete development cycle and is the fastest debugging tool offered from Atmel.




Atmel - ATAVRONEKIT
Atmel - ATATMEL-ICE-BASIC
Atmel - ATAVRDRAGON
Epsilon - EPSILON5MK4(AVR-JTAG)
Equinox - FS2009USB(AVR-JTAG)
Equinox - FS2009USB(STD)
Equinox - PPM4-MK1(UN)
Phyton - CHIPPROG-ISP



Stand-Alone Programmers

Atmel MPQ-AVR

The MPQ-AVR provides both SPI and JTAG programming support (see ordering options), to accommodate the widest range of AVR devices and customer programming requirements.






RPM Systems - MPQ-AVR
Phyton - CHIPPROG-40
Phyton - CHIPPROG-48
Phyton - CHIPPROG-G41


32-bit AVR UC3

ISP Programmers/Debuggers/Emulators

Atmel ATAVRONEKIT

The AVR ONE! is a professional development tool for all Atmel 8-bit and 32-bit AVR devices with On-Chip Debug capability.  It is used for source level symbolic debugging, program trace and device programming.  AVR ONE! supports the complete development cycle and is the fastest debugging tool offered from Atmel.

 


Atmel - ATAVRONEKIT



Stand-Alone Programmers

Atmel MPQ-AVR32

The MPQ-AVR32 provides fast, reliable JTAG programming of both microcontroller Flash and User memories, as well as fuse-programmable chip options. No USB boot loader is required.







Atmel - MPQ-AVR32


8051

ISP Programmers/Debuggers/Emulators

Phyton CHIPPROG-ISP

Phyton's CHIPPROG-ISP is a low cost, universal ISP programmer designed for engineering and low-volume production. The programmer is compatible with many microcontrollers and Flash memory devices including variations of the ARM MCU as well as 8051, PIC, AVR, MSP430, Z8, 9S08, and 9S12 architectures.


Phyton - CHIPPROG-ISP



Software

Keil CA51 Compiler Kit

The CA51 Compiler Kit for the 8051 microcontroller family supports all 8051 derivatives including classic devices and IP cores from companies like Analog Devices, Atmel, Cypress Semiconductor, Dallas Semiconductor, Goal, Hynix, Infineon, Intel, NXP, OKI, Silicon Labs, SMSC, STMicroelectronics, Synopsis, TDK, Temic, Texas Instruments, and Winbond.



Keil - CA51
Keil - PK51



Stand-Alone Programmers

Xeltek SuperPro 5000

The SuperPro 5000 programmer has the largest device support in the industry with over 55,303 IC devices from 190 manufacturers. The 5000 programmer comes standard with a built in 144 universal pin drivers, and has many adapters available.

 

Xeltek - SUPERPRO 5000
Phyton - CHIPPROG-40
Phyton - CHIPPROG-48
Phyton - CHIPPROG-G41


ATSAM

ISP Programmers/Debuggers/Emulators

Atmel SAM-ICE

The SAM-ICE is a JTAG emulator/programmer designed specifically for Atmel® AT91 ARM® cores. It connects via USB to a PC running Microsoft Windows. SAM-ICE has a built-in 20-pin JTAG connector, which is compatible with the standard 20-pin connector defined by ARM®.





Atmel - AT91SAM-ICE
Equinox - EPSILON5(SAM7)
Equinox - AVR-JTAG Bundle
Equinox - AT91SAM7 JTAG Bundle
Equinox - FS2009 AVR-JTAG
Equinox - FS2009 Standard
Equinox - PPM4-MK1(UN)
Phyton - CHIPPROG-ISP
IAR - I-JET ARM
Segger - JLINK ARM
Segger - FLASHER ARM
Segger - JLINK ARM PRO
Segger - J-TRACE ARM
Keil - ULINKPRO



Software

Keil RealView

The RealView Microcontroller Development Kit (MDK) supports ARM7, ARM9, and Cortex-M3 technology based microcontrollers from Analog Devices, Atmel, Freescale, Luminary, NXP (founded by Philips), OKI, Samsung, Sharp, STMicroelectronics, and TI.




IAR - EWARMBL
Keil - MDK-ARM-BASIC
Keil - MDK-ARM



Stand-Alone Programmers

Xeltek SuperPro 5000

The SuperPro 5000 programmer has the largest device support in the industry with over 55,303 IC devices from 190 manufacturers. The 5000 programmer comes standard with a built in 144 universal pin drivers, and has many adapters available.

 

Xeltek - SUPERPRO 5000
Phyton - CHIPPROG-40
Phyton - CHIPPROG-48
Phyton - CHIPPROG-G41




Microcontroller Suppliers - Programming Tools - Atmel