Tricolor optical feedback is a proven color management solution, but its implementation can be complex. It doesn’t need to be.
Abstract
Combining red, green, and blue LEDs (light emitting diodes) to form a light source is an attractive proposition. Such a multi-color light source can generate a wide range of colors. The LEDs themselves are robust and highly efficient. LED light sources will improve many existing applications, such as LCD backlighting, and enable new ones, such as adaptive automotive interior lighting. There are, however, challenges to overcome before a high-quality multi-color LED light source can be produced. This paper describes an Application Specific Standard Product (ASSP) integrated circuit that addresses many of those challenges.

Figure 1: CIE 1931 Color Space. The triangle represents the color gamut formed by red, green, and blue LEDs. W—white, R—red, G—green and B—blue. The x, y coordinate defines the chromaticity of a light source. A third axis (not shown), Y, is needed to define the brightness of the light source.
Using RGB LEDs
The simplest multi-color LED light source consists of three sets of LEDs—red, green, and blue—with each set driven by a separate driver module. The resultant color of the light source is dependent on the ratio of light intensity between the red, green, and blue sets of LEDs. The light intensity of an LED can be controlled by varying its drive current, or by varying the duty cycle of the LED using pulsewidth modulation (PWM). The PWM method is popular because the relationship between duty factor and light intensity is more linear than that of current vs. intensity.
This simple, open loop method of constructing an LED light source has a critical flaw. Since an LED’s optical characteristic varies with operating conditions, the brightness and chromaticity of the combined RGB light output will vary. In addition, LEDs vary part-to-part, contributing to more variation in the RGB light output. Figures 2 and 3 below illustrate examples of LED variation.
One solution is to use optical feedback to produce a closed-loop system. A basic setup consists of a photo sensor to record the brightness of the LED light source and a method of modulating the light output with respect to the photo sensor readings. This permits the brightness of the LED light source to be consistent even if the individual LEDs vary. (i.e., the sum is constant, though the components vary).

Figure 2: Example of RGB LED spectral shift over temperature.

Figure 3: Example of LED relative intensity shift over temperature. Normalized at 25°C.
In Figure 4, an integrator (labeled 22) outputs a voltage that is dependent on the amount of light falling on a photodiode (11a). That voltage is compared against VSET. A counter (34) increments or decrements depending on the comparator decision. The counter value is used to drive a DAC (37), which determines the LED driving current.

Figure 4: Schematic showing a method of implementing optical feedback. This drawing was extracted from an Avago Technologies’ patent US 6,344,641. The concept of using color filters placed over the photo sensors was described in Avago Technologies’ patent US 6,448,550.
A more advanced optical feedback method uses a tricolor photo sensor, which typically consists of three independent photo sensors with a tricolor filter placed over them. Thus, the photo sensors are able to record color information, rather than just brightness. This allows the ratio of light intensity between red, green, and blue sets of LEDs to be controlled. This is a critical feature as it allows the brightness and chromaticity of the RGB light source to be controlled. It is in tricolor optical feedback where the ASSP plays an important role.

Figure 5: The tricolor optical feedback system. Each photo sensor has a color filter placed over it. The low-pass filters perform a “time-average” on the sensor output such that a DC voltage level is passed to the controller.
The tricolor optical feedback system
Essentially, a tricolor photo sensor creates a three-dimensional color specification system (henceforth known as the RGB sensor color space). This system allows specific colors to be specified in terms of the sensor’s output voltage. For example, a D65 white with a particular brightness can be specified as:
(Vred, Vgreen, Vblue) = (2.0, 2.2, 1.9) volts (see Figure 6)
Refer to Figure 5 and suppose that the D65 example above is used as the “TARGET COLOR.” The feedback system will periodically measure the red, green, and blue sensors (collectively known as the tricolor photo sensor) and compare the “MEASURED COLOR” against the “TARGET COLOR.” The goal of the feedback system is to adjust the difference (error) between the “MEASURED COLOR” and “TARGET COLOR” to zero.
Figure 6 illustrates the idea in a different way. All possible target color setpoints are specified as coordinates within the RGB sensor color space formed by the red, green, and blue sensors. As the LEDs change in characteristic, the measured color moves away from the target. The ASSP will detect this and adjust the LED PWM signals accordingly.

Figure 6: Trilinear coordinates representation of the RGB sensor color space. For clarity this trilinear representation only considers chromaticity and not brightness. In practice, the feedback system corrects for any deviation of the target color setpoint including brightness.
It is important to understand that as LEDs age, they degrade in light output intensity. Hence, over time, an RGB LED system’s maximum achievable brightness will decrease. In most applications, a gradual and graceful reduction in brightness is acceptable; what is not acceptable is a change in the chromaticity of the RGB light system. The ASSP has a feature that gracefully controls the diminishing brightness of the RGB light system such that the chromaticity is kept steady (within tolerance) even as the maximum achievable brightness decreases.
In applications where the system brightness must be maintained throughout the lifetime of the application, the user must ensure that the maximum selectable brightness is less than the maximum achievable brightness over the required lifetime, as shown in Figure 7.
As attractive as RGB light systems are, there are challenges that hinder widespread usage of this technology. There exists a need for a device that “hides” the complexity of tricolor optical feedback behind a simple user interface. The following sub-sections describe how the ASSP accomplishes this.

Figure 7: The ASSP keeps the chromaticity (defined here as 1931 x, y coordinates) of an RGB light source steady (within tolerance) even as the maximum achievable brightness decreases over time.
Zero external processing
The ASSP incorporates a set of algorithms that analyze color information from the tricolor photo sensor and compute the PWM drive signals to achieve the target color setpoint. The ASSP samples the photo sensor at about 100 times per second to ensure that the periodic adjustment to the PWM signals is not perceptible to the human eye. As mentioned previously, the ASSP also contains an algorithm that prevents LED degradation from changing the chromaticity of the RGB light output.
No other calculations are necessary to achieve and maintain a target color.
Color space standardization
This relates to device independence in selecting a target color setpoint.

Figure 8: The ASSP samples the tricolor photo sensor directly and translates the readings into the required LED PWM signals.
The RGB sensor color space varies with differences in photo sensor output, photo sensor location, LEDs, LED drivers, etc. Figure 9 illustrates the problem. Each system will have a slightly different RGB sensor color space. Hence, a D65 specification for system A will be different than that for system B.
Example:
System A (Vred, Vgreen, Vblue)D65 = (2.0, 2.2, 1.9) volts
System B (Vred, Vgreen, Vblue)D65 = (2.1, 2.4, 2.3) volts
The tricolor photo sensor in system A will produce the voltage levels above when D65 light output is achieved.
System B’s photo sensor will produce a different set of voltage levels even though it generates the same D65 light output as system A. In other words, the color specification system as defined by the RGB sensor color space is unique system-to-system.
The ASSP incorporates a calibration procedure to allow every system to use a standard color specification system. CIE 1931 xyY and CIE RGB are two such systems built into the ASSP. By having a standard color space input, the user can send the same target color to every system and expect that each system will produce the same color (within tolerance).


Figure 9: Variations in the RGB sensor color space are calibrated out using the ASSP. A transformation is performed to map the RGB sensor color space to a standard color system such as 1931 CIE xyY, to allow every system to pick a target color using a standard color system.
Design-in simplicity
Typically, the ASSP only requires only passive components for support and an external PROM to store calibration data. In most cases, memory space can be shared with other peripherals at a system level, since calibration data is only 31 bytes.
The ASSP has a standard two-wire 100 kHz I2C interface, and all major functions are mapped to an 8-bit address space. For example, to run the calibration calculator, simply write 0x01 to register CTRL2. Implementation details can be found in the device datasheet.
In the manufacturing stage, the system is calibrated using a standard CIE camera. The calibration data needs to be stored in an external non-volatile memory. The calibration process is not required after the system is deployed in an application. In application, the user first configures the device and then writes the previously stored calibration data into the calibration registers. This is a simple read-then-write process. After that, the system is ready to accept a target color.
Color selection is simple. In the examples, a D65 target color was specified in terms of sensor voltages. In actual application, the target color can be specified as coordinates in the CIE 1931 xyY system. Other color systems such as CIE uvY and CIE RGB can also be used. For example, to select illuminant E as the target color, a value of (x, y, Y) = (330, 330, 250) is sent to the appropriate registers in the ASSP.
- Illuminant E CIE x, y coordinates are 0.33, 0.33
- Scale that by 1000 to get 330, 330
- Choose a relative brightness level of Y = 250
- Write 250 into register address 237 and 236 to set brightness (Y value)
- Write 330 into register address 235 and 234 to set the x chromaticity coordinate
- Write 330 into register address 233 and 232 to set the y chromaticity coordinate
- Write 0x12 to register address 1 (CTRL1) to update the new target color

Figure 10: Typical configuration of a tricolor color management system. The internal reference and oscillator options are enabled. Only passive components support the device.

Figure 11: A sample of the ASSP register space. Each bit is mapped to a function.

Figure 12: Typical design-in flow.
Experimental results
Figure 13 shows the performance difference between an open-loop and a closed-loop RGB light system. The experiment was conducted using a 9000 K white target color and uses duv as the figure-of-merit.

where,
(u25, v25) = 1976 CIE u, v chromaticity coordinates at +25°C
(uT, vT) = 1976 CIE u, v chromaticity coordinates at temperature T
A good rule-of-thumb to judge performance is to use duv = 0.005 as the minimum change in chromaticity before the human eye can detect a change.

Figure 13: Measurement of chromaticity change over temperature.

Figure 14: Spectral shift over temperature. Chromaticity shift duv <0.005.
Figure 14 illustrates the severity of LED spectral shift as temperature increases. This data was collected from a closed-loop system with a 9000 K white target color. Although the spectral curves shifted significantly, duv was kept below 0.005 by the feedback system.
Conclusion
RGB LED lighting is an appealing lighting solution. However, the variability of LED characteristics causes the RGB light to deviate from the intended color. Tricolor optical feedback is a proven solution, but its implementation can be complex. Avago Technologies’ feedback controller simplifies the implementation of such a system.
Powered By 
Discover the benefits of becoming a My Digi-Key registered user.
• Enjoy faster, easier ordering with your information preloaded.
• View your order status, web order history
• Use our BOM Manager tool
• Import a text file into a RoHS query

Quick Links: