NXP Semiconductors Supplier Page

mbed LPC1768 Development Board


NXP's mbed LPC1768 development board available at Digi-Key


mbed LPC1768 Development BoardThe mbed NXP LPC1768 board allows for the creation of prototypes without having to work with low-level microcontroller details. Therefore, a designer can experiment and iterate faster than ever. Using a browser-based IDE, software can be composed and compiled, then downloaded quickly and easily to the board’s NXP Cortex-M3 microcontroller LPC1768 using a simple drag-and-drop function.

Engineers new to embedded applications can use the board to prototype real products incorporating microcontrollers, while experienced engineers can use it to be more productive in early stages of development. The mbed tools are designed so that new ideas can be tested quickly.


  • Overview
  • Features
  • Diagram
  • Buy Now

Overview

Elegant Simplicity
The mbed tool has been designed for the best trade-off between versatility and immediate connectivity. The LPC1768, housed in an LQFP package, is mounted on the mbed board, which uses a 40-pin DIP with a 0.1in pitch. The convenient form factor works seamlessly with broad-boards, strip-boards, and PCBs.

There is no software to install – everything, even the compiler, is online. The compiler and libraries are completely modular, so they’re easy to use, yet they’re powerful enough to take on complex, real-world applications.

Hassle-Free Startup
Getting started is as simple as using a USB Flash drive. The mbed NXP LPC1768 board can easily be connected to a Windows, Mac or Linux computer and it will appear as a USB drive. The link on the board can be used to connect to the mbed website, where individuals can sign up and begin designing. There are no drivers to install or setup programs to run.

Online Compiler
The mbed compiler lets a designer write programs in C++ and then compile and download them to run on the mbed NXP LPC1768 Microcontroller. There’s no need to run an install or setup program, since the compiler runs online. Supported browsers include Internet Explorer, Safari, or Chrome running on a Windows, Mac, or Linux PC. Engineers can log in from anywhere and simply pick up where they left off.

The compiler uses the ARM RealView compile engine, so it produces clean, efficient code that can be used free-of-charge, even in production. Existing ARM application code and middleware can be ported to the mbed Microcontroller, and the mbed tools can be used alongside other professional production-level tools.

Peripheral Libraries
The mbed library provides an API-driven approach to coding that eliminates much of the low-level work normally associated with MCU code development. One can develop code using meaningful peripheral abstractions and API calls that are intuitive and already tested. That allows designers to experiment without worrying about the implementation of the MCU core or its peripherals. Work can be faster and be more creative.

Rather than simply providing examples, mbed focuses on reusable library functionality, with clear interfaces and solid implementations. The core mbed library supports the main LPC1768 peripherals, and the libraries already contributed by the mbed design community include USB, TCP/IP, and HTTP support. It’s also possible to add third-party and open-source stacks.

The libraries comply with the ARM EABI and are built on the Cortex Microcontroller Software Interface Standard (CMSIS), making it possible to migrate to other tool-chains or implement custom code for peripheral interfaces.

LPC1768 Microcontroller
The NXP LPC1768 microcontroller is a cost-effective, low-power Cortex-M3 device that operates at up to 100MHz. It features best-in-class peripheral support, including Ethernet, USB 2.0 host/OTG/device, and CAN 2.0B. There are 512kB of Flash memory and 64kB of SRAM. The architecture uses a multi-layer AHB bus that allows high-bandwidth peripherals such as Ethernet and USB to run simultaneously, without impacting performance. The device is pin-compatible with NXP’s 100-pin LPC236x series of ARM7-based microcontrollers.


Features

ARM Cortex-M3 Core
  • 100MHz operation
  • Nested Vectored Interrupt Controller for fast deterministic interrupts
  • Wakeup Interrupt Controller allows automatic wake from any priority interrupt
  • Memory Protection Unit
  • Four reduced-power modes: sleep, deep sleep, power-down and deep power-down
Memories
  • 512kB Flash memory
  • 64kB SRAM
Serial Peripherals
  • 10/100 Ethernet MAC
  • USB 2.0 full-speed device/Host/ OTG controller with on-chip PHY
  • Four UARTs with fractional baud rate generation, RS-48, modem control, and IrDA
  • Two CAN 2.0B controllers
  • Three SSP/SPI controllers
  • Three I²C-bus interfaces with one supporting Fast Mode Plus (1-Mbit/s data rates)
  • I²S interface for digital audio
Analog Peripherals
  • 12-bit ADC with eight channels
  • 10-bit DAC
Other Peripherals
  • Ultra-low-power (< 1uA) RTC
  • General-purpose DMA controller with eight channels
  • Up to 70 GPIO
  • Motor control PWM and Quadrature Encoder Interface to support three-phase motors
  • Four 32-bit general-purpose timers/counters
Package
  • 100-pin LQFP (14mm x 14mm x 1.4mm)

Diagram

mbed LPC1768 Development Board diagram

Buy Now

Digi-Key P/N Manufacturer's P/N Description
568-4916-ND OM11043 DEVELOPMENT BOARD FOR LPC1768


Please visit Digi-Key's Microcontroller Solutions Technology Zone to learn more about NXP Semiconductor microcontroller products.
 

All parts by: Title Manufacturer Category Manufacturer Part No.   |   Electronic parts by: Component Title Manufacturer Category Manufacturer Part No.
Part categories by: Name Manufacturer   |   Manufacturers by: Name Number of Parts   |   Products by: Category Title   |   Grouped parts by: Title Model Number
Austria Parts  Canada Parts  France Parts  Germany Parts  Italy Parts  Japan Parts  Spain Parts  United Kingdom Parts United States Parts