Fluke Electronics Supplier Page   

The Fluke 8808A multimeter has a broad range of functions, measuring volts, ohms and amps with a basic V dc accuracy of 0.015 %. It includes features that go beyond a standard volts, ohms and amp meter.


Product Brochure
  Fluke Product

Measure Two Parameters At Once
The 8808A features a unique dual display that allows you to measure two different parameters of the same signal from one test connection. Looking at dual interrelated parameters like voltage and current simultaneously can reveal conditions that might go unnoticed otherwise, greatly simplifying test and troubleshooting.
Measure Sensitive Leakage Current
Typical multimeters use a shunt method to measure current, creating a measurement burden voltage that increases the error in low current measurements. This makes it difficult, if not impossible, to perform tasks such as determining the true leakage current on a battery-powered device while it is powered down, or measuring small currents in sensitive circuits. The Fluke 8808A is the only multimeter in its class  
to use a low-impedance operational amplifier and current-to-voltage conversion technique to eliminate the burden voltage and measure sensitive low currents. In this special mode, the 8808A can accurately measure small currents with a resolution of up to 100 nA.
Perform 4-Wire Measurements With Only Two Leads
Patented split terminal jacks for the 2x4-wire ohms function allow you to perform 4-wire measurements using only two leads instead of four. Today's surface mount components make it difficult to make connections. The task becomes even more difficult when you need to use a 4-wire technique for accurate low ohms measurements. The Fluke test lead accessory combines the four wires into two test lead pairs, making it easy for you to establish connections. You get excellent resolution and accuracy, plus the convenience and ease of using a single pair of leads.

Simplify Routine Tests
Six setup buttons on the 8808A front panel operate like a car radio's station presets. Simply set up the meter for a common measurement, then press shift followed by a setup button (S1 to S6) to save the setup. Now each time you perform that measurement, you simply press the appropriate setup key. It's that easy!

  The setup buttons eliminate the need to follow complex work instruction sheets. Operators no longer need to press multiple buttons to set up a measurement function and range, test limits, or enter other parameters to make a measurement.
Eliminate Production Mistakes
The Fluke 8808A 5.5 digit multimeter dependably performs the most common measurements required by today's applications. Whether you are performing functional tests or making critical measurements on test points, using the limit compare mode with pass/fail indicators eliminates production mistakes, especially those where results are "on the edge". The 8808A display has built-in enunciators that clearly show the operator whether a test passes or fails. The pass/fail indicators take the guesswork out of testing: the result is either within limits or it's out!