Skip navigation
TechXchange
Digi-Key TechXchange Communities > Projects and Designs > Discussions
9229 Views 6 Replies Latest reply: Mar 17, 2014 7:35 AM by davecuthbert RSS
Currently Being Moderated

Mar 13, 2014 12:49 PM

switching circuit

I need to make a circuit to latch and unlatch a latching relay part # 399-11030-5-nd   using only one wire from a mom. neg. output switch.

  • davecuthbert Journeyman 65 posts since
    Feb 18, 2014
    Currently Being Moderated
    Mar 15, 2014 6:31 AM (in response to jpitman93)
    Re: switching circuit

    30.JPG

    The switch needs to apply at least -9 volts to pin 12 with the return being pin 1. Driving the coil directly from a switch may or may not work well because switch bounce might toggle the relay more than once as it closes and opens. The required coil pulse width is >10 ms and the rise time is described as "fast."

     

    The circuit above will debounce the switch with an attack time of about 2 ms and a debounce time of about 50 ms. The capacitor can be a 33 uF electrolytic, tantalum, or ceramic with a voltage rating of 15 volts or more.

     

    Note that on page 3 of the datasheet the diagrams for the Single coil and the Dual coil are switched (they are in the wrong place).

     

    http://www.kemet.com/kemet/web/homepage/kechome.nsf/vapubfiles/KEM_R7002_EC2_EE2.pdf/$file/KEM_R7002_EC2_EE2.pdf

    • NITMOI Novice 10 posts since
      Mar 14, 2014
      Currently Being Moderated
      Mar 15, 2014 12:39 AM (in response to davecuthbert)
      Re: switching circuit

      Don't forget the diode across the coil to absorb switching transients.

      • davecuthbert Journeyman 65 posts since
        Feb 18, 2014
        Currently Being Moderated
        Mar 15, 2014 6:27 AM (in response to NITMOI)
        Re: switching circuit

        In this circuit the 33 uF capacitor performs the clamp function and a diode is not needed.

        • NITMOI Novice 10 posts since
          Mar 14, 2014
          Currently Being Moderated
          Mar 16, 2014 8:19 PM (in response to davecuthbert)
          Re: switching circuit

          Unless they fixed the pdf, the diagrams look right to me.  The double latch set coil is between pins 1 and 12 and the reset coil is between pins 5 and 7.  The single latch uses a single coil for both reset and set between pins 1 and 12 thus relying on polarity of the signal/pulse on the pins.  Your circuit will set it, reset is not shown.  On using the capacitor in place of a diode, the diode will impart opposite polarity to a polarized cap - will that matter since it's only briefly?

          • davecuthbert Journeyman 65 posts since
            Feb 18, 2014
            Currently Being Moderated
            Mar 17, 2014 7:35 AM (in response to NITMOI)
            Re: switching circuit

            You're right! The diagrams are correct, and to operate the single coil latch type a circuit with these characteristics is needed:

             

            • Pin 1 positive and Pin 12 negative to set
            • Pin 1 negative and Pin 12 positive to reset
            • Coil voltage rise time and fall time < 1ms
            • Coil on time >10 ms
            • Set by depressing the momentary switch
            • Reset by depressing the momentary switch
            • Momentary switch supplies -12 volts

             

            Do we want the relay to power-up in the last state it was in or should it have a power-up reset to a specific state?

             

            It will work like so:

            • power-up reset to put the relay into a known state or leave it in the state it was in
            • Momentary switch signal to
            • debouncing circuit to
            • flip flop to
            • one shot to
            • tri-state coil drivers to
            • coil

    More Like This

    • Retrieving data ...

    Bookmarked By (0)

    Legend

    • Correct Answers - 4 points
    • Helpful Answers - 3 points