Skip navigation
TechXchange
Digi-Key TechXchange Communities > Projects and Designs > Discussions
9982 Views 5 Replies Latest reply: Apr 11, 2012 5:25 PM by JMAR RSS
Currently Being Moderated

Apr 2, 2012 4:55 PM

LM741 looses gain when connected to another LM741

I'm probably in the wrong forum but am really stuck.  I have two identical LM741 circuits.  In the first circuit, I inject a 60HZ, 1Vpp signal into PIN 2.  Pin 3 has 6Vdc or 1/2 VCC.  The resistor to pin 2 is a 600 ohm.  The Gain is adjusted (pin 2 to pin 6 10k trimmer) to 4Vpp.

 

I need to input this signal into four other 741 circuits so I don't want to loose any of the signal.

 

When I attach the output of the first circuit to the input of a second IDENTICAL 741 circuit, the signal drops to 1Vpp.   How/why does the input become affected in any way?  I have to keep the input at 4Vpp to drive the other 741 circuits.

  • Rick designspecialist-power 36 posts since
    Mar 22, 2011
    Currently Being Moderated
    Apr 3, 2012 2:18 PM (in response to JMAR)
    LM741 looses gain when connected to another LM741

    First off, pictures are worth a thousand words;  http://www.digikey.com/schemeit is an a free online schematic drawing tool that could be useful if you don't have a regular CAD package handy.  There are some pieces missing from your description, such as how your signal source is connected, where the "resistor to pin 2" is coming from, and how you're taking the output measurements--a schematic could help clarify that.

     

    Assembly/layout errors are the most common problem I have with simple circuits like this: solder bridges, unintended connections, unintended non-connections, incorrect component values, etc.  Test/measurement errors are also common; forgetting to connect a ground lead, measuring the wrong point, improper loading of the signal source, and the like.  Try testing your second circuit by itself; if it doesn't work, it's likely got a issue.  If it does, then an interaction between the two is more likely.  Assuming nothing starts on fire if you do, power up the circuit, and work your way from input to output measuring the signal at each node, comparing it to what it should be according to your schematic.  Measure directly at the pins of the package whenever possible--I've found many a flawed joint this way.  At some point, you should notice that the signals start to diverge from their expected values; the place where it does so is a good place to start looking for the root of your problem.

  • TommyTech Novice 3 posts since
    Apr 11, 2012
    Currently Being Moderated
    Apr 11, 2012 1:36 PM (in response to JMAR)
    LM741 looses gain when connected to another LM741

    Are you using a single supply for the 741s? Sounds like the bias circuit may be adding a voltage divider to your circuit changing the gain calculation. Op amps also have problems with resistors with M in the value, you may have better results if you keep them in the kilo range. You may also find you can direct couple the output of the first stage into the second if the DC level is in range (offset X stage 2 gain =~ VCC/2). Try one of more of the free SPICE programs available on line to help with ballpark numbers. Remember you can get some very incorrect results with SPICE if you give it oddball numbers of incomplete data.

     

    Next step is to add AVC to the microphone preamp and maybe a VOX or noise gate to cut background noise.

More Like This

  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 3 points