Skip navigation
TechXchange
Digi-Key TechXchange Communities > Projects and Designs > Discussions
11089 Views 4 Replies Latest reply: Feb 28, 2012 11:25 AM by daveatwave RSS
Currently Being Moderated

Sep 7, 2011 10:05 AM

design and test

Does anyone know of a company that will program TXM 418 and RXM 418 for a specific function?

  • Mike Novice 8 posts since
    Mar 31, 2011
    Currently Being Moderated
    Sep 7, 2011 10:29 AM (in response to jimmy3)
    design and test

    Hello jimmy3,

    This transmitter and receiver have a fixed function and are not prgrammable. What function does your application require? This could be interfaced to a microcontroller or depening on whats needed, I could suggest a different device that may fit the application better.

        • daveatwave Novice 2 posts since
          Feb 28, 2012
          Currently Being Moderated
          Feb 28, 2012 11:25 AM (in response to jimmy3)
          design and test

          300 yards...that's 900ft....probably won't happen legally with those two parts...at least not reliably. Most people expect wireless devices to be reliable as a wired device. Let's put it in perspective...a wired device with unbroken wire is very reliable at close to 100%. A wireless device won't touch that. A bating average in baseball of 0.95 would be great. But for wireless...as the perception is "as good as wired".....even at 95% batting average many people find it INTOLERABLE if they don't have some ability to re-orient and re-transmit in case of failed transmission.

More Like This

  • Retrieving data ...

Bookmarked By (0)

Legend

  • Correct Answers - 4 points
  • Helpful Answers - 3 points