I'm trying to figure out how to take the design below and make it an actual object.
For the black casing, I was thinking of going with stacked lens filter cases - http://ecx.images-amazon.com/images/I/61OFaQ5AZaL._SL1024_.jpg (picture is slightly large) -
and thinning out each side so LEDs could shine through. For the white sheen, I have thought of using using a polished glass or plastic petri dish. The size would be
between 2.5-3 inches.
The current idea is to make one side that toggles between displaying the "M" and "N" then another side that constantly displays the "O". Using a gyroscope, the device
would change between the M and N whenever the device was turned. The overall size of each LED grid would be 9x8. Each LED would shine white. Lastly, I would like the
battery to be replaceable.
Aside from those few ideas, I'm not sure which LEDs, which accelerometer and gyroscope, which board, or really anything else I should use for the device. Feel free to
add any suggestions.
A few follow up questions to help to try and narrow down some parts ![]()
Are you planning on using a microcontroller? What communication are you planning on using for the accelerometer/gyro? Ex. SPI, I2C, analog etc.
What sensitivity do you need out of the accelerometer/gyro?
What brightness/current rating/voltage rating do you need on the LEDs? Surface mount, or through hole?
What power setup are you going to be using? LDO regulator, buck/boost, etc?
A microcontroller is definitely within question for controlling the device; the accelerometer will be used to wake the device, and the gyro will be used to measure
when the device has rotated a certain amount. The device is meant to be spun when held vertical, similar to the animation above. The sensitivity of the gyro would
need to accurate enough to recognize medium to fast movement from someone spinning it under normal circumstances (in their palm).
As per LEDs - if an LED matrix (9x8) were used, they would need to be fairly low power. As someone has recommended, edge lighting may be a possibility
while being much more energy efficient. The immediate issue that I would probably run into would be light bleeding through the darker sections. Assuming I went
with that design, I would probably opt to go with some sort of glossy plastic cylinder. The top and bottom would use a layer of dark/black acrylic with two sheets
behind the M and N side and one behind the O. I'm not quite sure if two extremely thin sheets would have bleeding issues. A possible fix would be narrowing the
lighting angle.
For power, I intend to use a battery; the battery would need to fit within a 2.5 x 2.5 x 1 space alongside the other components. For all other specifics, I'm not
entirely sure. I apologize for the nondescript hardware references; I'm without a clue which pieces I would be looking for.
Try taking a look at this board - It is an IMU (inertial measurement unit) board. It is not a self contained unit, but just the sensor board.
http://www.digikey.com/product-search/en?lang=en&site=us&KeyWords=xplained+imu
And perhaps this for the MCU board.
http://www.digikey.com/product-detail/en/ATAVRXPLAIN/ATAVRXPLAIN-ND/2217263
Hardware guide
Privacy Statement | Terms & Conditions | Careers | webmaster@digikey.com |
|
701 Brooks Avenue South, Thief River Falls, MN 56701 USA Phone: 1-800-344-4539 or 218-681-6674 or Fax: 218-681-3380 |
|||||||||

Quick Links: